![]() |
MCUXpresso SDK API Reference Manual
Rev 2.13.0
NXP Semiconductors
|
Macros | |
| #define | MAKE_VERSION(major, minor, bugfix) (((major) << 16) | ((minor) << 8) | (bugfix)) |
| Constructs the version number for drivers. More... | |
| #define | MAKE_STATUS(group, code) ((((group)*100) + (code))) |
| Constructs a status code value from a group and a code number. More... | |
| #define | FOUR_CHAR_CODE(a, b, c, d) (((uint32_t)(d) << 24u) | ((uint32_t)(c) << 16u) | ((uint32_t)(b) << 8u) | ((uint32_t)(a))) |
| Constructs the four character code for the Flash driver API key. More... | |
| #define | B1P4(b) (((uint32_t)(b)&0xFFU) << 24U) |
| bytes2word utility. More... | |
Alignment macros | |
| #define | ALIGN_DOWN(x, a) (((uint32_t)(x)) & ~((uint32_t)(a)-1u)) |
| Alignment(down) utility. More... | |
| #define | ALIGN_UP(x, a) ALIGN_DOWN((uint32_t)(x) + (uint32_t)(a)-1u, a) |
| Alignment(up) utility. More... | |
| #define MAKE_VERSION | ( | major, | |
| minor, | |||
| bugfix | |||
| ) | (((major) << 16) | ((minor) << 8) | (bugfix)) |
| #define MAKE_STATUS | ( | group, | |
| code | |||
| ) | ((((group)*100) + (code))) |
| #define FOUR_CHAR_CODE | ( | a, | |
| b, | |||
| c, | |||
| d | |||
| ) | (((uint32_t)(d) << 24u) | ((uint32_t)(c) << 16u) | ((uint32_t)(b) << 8u) | ((uint32_t)(a))) |
| #define ALIGN_DOWN | ( | x, | |
| a | |||
| ) | (((uint32_t)(x)) & ~((uint32_t)(a)-1u)) |
| #define ALIGN_UP | ( | x, | |
| a | |||
| ) | ALIGN_DOWN((uint32_t)(x) + (uint32_t)(a)-1u, a) |
| #define B1P4 | ( | b | ) | (((uint32_t)(b)&0xFFU) << 24U) |