The MCUXpresso SDK provides a peripheral driver for the Capacitive Touch (CAPT) module of MCUXpresso SDK devices.
The Capacitive Touch module measures the change in capacitance of an electrode plate when an earth-ground connected object (for example, the finger or stylus) is brought within close proximity. Simply stated, the module delivers a small charge to an X capacitor (a mutual capacitance touch sensor), then transfers that charge to a larger Y capacitor (the measurement capacitor), and counts the number of iterations necessary for the voltage across the Y capacitor to cross a predetermined threshold.
Typical use case
Normal Configuration
See the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/capt/capt_basic.
|
| enum | _capt_xpins {
kCAPT_X0Pin = 1U << 0U,
kCAPT_X1Pin = 1U << 1U,
kCAPT_X2Pin = 1U << 2U,
kCAPT_X3Pin = 1U << 3U,
kCAPT_X4Pin = 1U << 4U,
kCAPT_X5Pin = 1U << 5U,
kCAPT_X6Pin = 1U << 6U,
kCAPT_X7Pin = 1U << 7U,
kCAPT_X8Pin = 1U << 8U,
kCAPT_X9Pin = 1U << 9U,
kCAPT_X10Pin = 1U << 10U,
kCAPT_X11Pin = 1U << 11U,
kCAPT_X12Pin = 1U << 12U,
kCAPT_X13Pin = 1U << 13U,
kCAPT_X14Pin = 1U << 14U,
kCAPT_X15Pin = 1U << 15U
} |
| | The enumeration for X pins. More...
|
| |
| enum | _capt_interrupt_enable {
kCAPT_InterruptOfYesTouchEnable,
kCAPT_InterruptOfNoTouchEnable,
kCAPT_InterruptOfPollDoneEnable = CAPT_INTENSET_POLLDONE_MASK,
kCAPT_InterruptOfTimeOutEnable = CAPT_INTENSET_TIMEOUT_MASK,
kCAPT_InterruptOfOverRunEnable = CAPT_INTENSET_OVERUN_MASK
} |
| | The enumeration for enabling/disabling interrupts. More...
|
| |
| enum | _capt_interrupt_status_flags {
kCAPT_InterruptOfYesTouchStatusFlag = CAPT_INTSTAT_YESTOUCH_MASK,
kCAPT_InterruptOfNoTouchStatusFlag = CAPT_INTSTAT_NOTOUCH_MASK,
kCAPT_InterruptOfPollDoneStatusFlag = CAPT_INTSTAT_POLLDONE_MASK,
kCAPT_InterruptOfTimeOutStatusFlag = CAPT_INTSTAT_TIMEOUT_MASK,
kCAPT_InterruptOfOverRunStatusFlag = CAPT_INTSTAT_OVERUN_MASK
} |
| | The enumeration for interrupt status flags. More...
|
| |
| enum | _capt_status_flags {
kCAPT_BusyStatusFlag = CAPT_STATUS_BUSY_MASK,
kCAPT_XMAXStatusFlag = CAPT_STATUS_XMAX_MASK
} |
| | The enumeration for CAPT status flags. More...
|
| |
| enum | capt_trigger_mode_t {
kCAPT_YHPortTriggerMode = 0U,
kCAPT_ComparatorTriggerMode = 1U
} |
| | The enumeration for CAPT trigger mode. More...
|
| |
| enum | capt_inactive_xpins_mode_t {
kCAPT_InactiveXpinsHighZMode,
kCAPT_InactiveXpinsDrivenLowMode
} |
| | The enumeration for the inactive X pins mode. More...
|
| |
| enum | capt_measurement_delay_t {
kCAPT_MeasureDelayNoWait = 0U,
kCAPT_MeasureDelayWait3FCLKs = 1U,
kCAPT_MeasureDelayWait5FCLKs = 2U,
kCAPT_MeasureDelayWait9FCLKs = 3U
} |
| | The enumeration for the delay of measuring voltage state. More...
|
| |
| enum | capt_reset_delay_t {
kCAPT_ResetDelayNoWait = 0U,
kCAPT_ResetDelayWait3FCLKs = 1U,
kCAPT_ResetDelayWait5FCLKs = 2U,
kCAPT_ResetDelayWait9FCLKs = 3U
} |
| | The enumeration for the delay of reseting or draining Cap. More...
|
| |
| enum | capt_polling_mode_t {
kCAPT_PollInactiveMode,
kCAPT_PollNowMode = 1U,
kCAPT_PollContinuousMode
} |
| | The enumeration of CAPT polling mode. More...
|
| |
| enum | capt_dma_mode_t {
kCAPT_DMATriggerOnTouchMode = 1U,
kCAPT_DMATriggerOnBothMode = 2U,
kCAPT_DMATriggerOnAllMode = 3U
} |
| | The enumeration of CAPT DMA trigger mode. More...
|
| |
| bool capt_config_t::enableWaitMode |
Other-wise, measurements continue.
| bool capt_config_t::enableTouchLower |
Trigger at count > TCNT is a no-touch. enableTouchLower = false: Trigger at count > TCNT is a touch. Trigger at count < TCNT is a no-touch. Notice: TCNT will be set by "CAPT_DoCalibration" API.
| uint8_t capt_config_t::clockDivider |
The function clock is divided by clockDivider+1 to produce the divided FCLK for the module. The available range is 0-15.
| uint8_t capt_config_t::timeOutCount |
The time-out count value is calculated as 2^timeOutCount. The available range is 0-12.
| uint8_t capt_config_t::pollCount |
After each polling round completes, the module will wait 4096 x PollCount divided FCLKs before starting the next polling round. The available range is 0-255.
| uint16_t capt_config_t::enableXpins |
Please refer to '_capt_xpins'. For example, if want to enable X0, X2 and X3 pins, you can set "enableXpins = kCAPT_X0Pin | kCAPT_X2Pin | kCAPT_X3Pin".
Data Fields |
| bool | yesTimeOut |
| | 'true': if the measurement resulted in a time-out event, 'false': otherwise. More...
|
| |
| bool | yesTouch |
| | 'true': if the trigger is due to a touch even, 'false': if the trigger is due to a no-touch event. More...
|
| |
| uint8_t | XpinsIndex |
| | Contains the index of the X pin for the current measurement, or lowest X for a multiple-pin poll now measurement. More...
|
| |
| uint8_t | sequenceNumber |
| | Contains the 4-bit(0-7) sequence number, which increments at the end of each polling round. More...
|
| |
| uint16_t | count |
| | Contains the count value reached at trigger or time-out. More...
|
| |
| bool capt_touch_data_t::yesTimeOut |
| bool capt_touch_data_t::yesTouch |
| uint8_t capt_touch_data_t::XpinsIndex |
| uint8_t capt_touch_data_t::sequenceNumber |
| uint16_t capt_touch_data_t::count |
| Enumerator |
|---|
| kCAPT_X0Pin |
CAPT_X0 pin.
|
| kCAPT_X1Pin |
CAPT_X1 pin.
|
| kCAPT_X2Pin |
CAPT_X2 pin.
|
| kCAPT_X3Pin |
CAPT_X3 pin.
|
| kCAPT_X4Pin |
CAPT_X4 pin.
|
| kCAPT_X5Pin |
CAPT_X5 pin.
|
| kCAPT_X6Pin |
CAPT_X6 pin.
|
| kCAPT_X7Pin |
CAPT_X7 pin.
|
| kCAPT_X8Pin |
CAPT_X8 pin.
|
| kCAPT_X9Pin |
CAPT_X9 pin.
|
| kCAPT_X10Pin |
CAPT_X10 pin.
|
| kCAPT_X11Pin |
CAPT_X11 pin.
|
| kCAPT_X12Pin |
CAPT_X12 pin.
|
| kCAPT_X13Pin |
CAPT_X13 pin.
|
| kCAPT_X14Pin |
CAPT_X14 pin.
|
| kCAPT_X15Pin |
CAPT_X15 pin.
|
| Enumerator |
|---|
| kCAPT_InterruptOfYesTouchEnable |
Generate interrupt when a touch has been detected.
|
| kCAPT_InterruptOfNoTouchEnable |
Generate interrupt when a no-touch has been detected.
|
| kCAPT_InterruptOfPollDoneEnable |
Genarate interrupt at the end of a polling round, or when a POLLNOW completes.
|
| kCAPT_InterruptOfTimeOutEnable |
Generate interrupt when the count reaches the time-out count value before a trigger occurs.
|
| kCAPT_InterruptOfOverRunEnable |
Generate interrupt when the Touch Data register has been up-dated before software has read the previous data, and the touch has been detected.
|
| Enumerator |
|---|
| kCAPT_InterruptOfYesTouchStatusFlag |
YESTOUCH interrupt status flag.
|
| kCAPT_InterruptOfNoTouchStatusFlag |
NOTOUCH interrupt status flag.
|
| kCAPT_InterruptOfPollDoneStatusFlag |
POLLDONE interrupt status flag.
|
| kCAPT_InterruptOfTimeOutStatusFlag |
TIMEOUT interrupt status flag.
|
| kCAPT_InterruptOfOverRunStatusFlag |
OVERRUN interrupt status flag.
|
| Enumerator |
|---|
| kCAPT_BusyStatusFlag |
Set while a poll is currently in progress, otherwise cleared.
|
| kCAPT_XMAXStatusFlag |
The maximum number of X pins available for a given device is equal to XMAX+1.
|
| Enumerator |
|---|
| kCAPT_YHPortTriggerMode |
YH port pin trigger mode.
|
| kCAPT_ComparatorTriggerMode |
Analog comparator trigger mode.
|
| Enumerator |
|---|
| kCAPT_InactiveXpinsHighZMode |
Xpins enabled in the XPINSEL field are controlled to HIGH-Z mode when not active.
|
| kCAPT_InactiveXpinsDrivenLowMode |
Xpins enabled in the XPINSEL field are controlled to be driven low mode when not active.
|
| Enumerator |
|---|
| kCAPT_MeasureDelayNoWait |
Don’t wait.
|
| kCAPT_MeasureDelayWait3FCLKs |
Wait 3 divided FCLKs.
|
| kCAPT_MeasureDelayWait5FCLKs |
Wait 5 divided FCLKs.
|
| kCAPT_MeasureDelayWait9FCLKs |
Wait 9 divided FCLKs.
|
| Enumerator |
|---|
| kCAPT_ResetDelayNoWait |
Don’t wait.
|
| kCAPT_ResetDelayWait3FCLKs |
Wait 3 divided FCLKs.
|
| kCAPT_ResetDelayWait5FCLKs |
Wait 5 divided FCLKs.
|
| kCAPT_ResetDelayWait9FCLKs |
Wait 9 divided FCLKs.
|
| Enumerator |
|---|
| kCAPT_PollInactiveMode |
No measurements are taken, no polls are performed.
The module remains in the Reset/ Draining Cap.
|
| kCAPT_PollNowMode |
Immediately launches (ignoring Poll Delay) a one-time-only, simultaneous poll of all X pins that are enabled in the XPINSEL field of the Control register, then stops, returning to Reset/Draining Cap.
|
| kCAPT_PollContinuousMode |
Polling rounds are continuously performed, by walking through the enabled X pins.
|
| Enumerator |
|---|
| kCAPT_DMATriggerOnTouchMode |
Trigger on touch.
|
| kCAPT_DMATriggerOnBothMode |
Trigger on both touch and no-touch.
|
| kCAPT_DMATriggerOnAllMode |
Trigger on all touch, no-touch and time-out.
|
| void CAPT_Init |
( |
CAPT_Type * |
base, |
|
|
const capt_config_t * |
config |
|
) |
| |
- Parameters
-
| base | CAPT peripheral base address. |
| config | Pointer to "capt_config_t" structure. |
| void CAPT_Deinit |
( |
CAPT_Type * |
base | ) |
|
- Parameters
-
| base | CAPT peripheral base address. |
This function initializes the converter configuration structure with available settings. The default values are:
* config->enableWaitMode = false;
* config->enableTouchLower = true;
* config->clockDivider = 15U;
* config->timeOutCount = 12U;
* config->pollCount = 0U;
* config->enableXpins = 0U;
*
- Parameters
-
| config | Pointer to the configuration structure. |
| static void CAPT_SetThreshold |
( |
CAPT_Type * |
base, |
|
|
uint32_t |
count |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | CAPT peripheral base address. |
| count | The count threshold. |
- Parameters
-
| base | CAPT peripheral base address. |
| mode | The selection of polling mode. |
| static void CAPT_EnableInterrupts |
( |
CAPT_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | CAPT peripheral base address. |
| mask | The mask of enabling interrupt features. Please refer to "_capt_interrupt_enable". |
| static void CAPT_DisableInterrupts |
( |
CAPT_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | CAPT peripheral base address. |
| mask | The mask of disabling interrupt features. Please refer to "_capt_interrupt_enable". |
| static uint32_t CAPT_GetInterruptStatusFlags |
( |
CAPT_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | CAPT peripheral base address. |
- Returns
- The mask of interrupts' status flags. please refer to "_capt_interrupt_status_flags".
| static void CAPT_ClearInterruptStatusFlags |
( |
CAPT_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | CAPT peripheral base address. |
| mask | The mask of clearing the interrupts' status flags, please refer to "_capt_interrupt_status_flags". |
| static uint32_t CAPT_GetStatusFlags |
( |
CAPT_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | CAPT peripheral base address. |
- Returns
- The mask of CAPT status flags. Please refer to "_capt_status_flags" Or use CAPT_GET_XMAX_NUMBER(mask) to get XMAX number.
- Parameters
-
| base | CAPT peripheral base address. |
| data | The structure to store touch data. |
- Returns
- If return 'true', which means get valid data. if return 'false', which means get invalid data.
| void CAPT_PollNow |
( |
CAPT_Type * |
base, |
|
|
uint16_t |
enableXpins |
|
) |
| |
This function starts new data polling using polling-now method, CAPT stops when the polling is finished, application could check the status or monitor interrupt to know when the progress is finished.
Note that this is simultaneous poll of all X pins, all enabled X pins are activated concurrently, rather than walked one-at-a-time
- Parameters
-
| base | CAPT peripheral base address. |
| enableXpins | The X pins enabled in this polling. |