MCUXpresso SDK API Reference Manual  Rev 2.13.0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
IOCON: I/O pin configuration

Overview

The MCUXpresso SDK provides Peripheral driver for the I/O pin configuration (IOCON) module of MCUXpresso SDK devices.

Function groups

Pin mux set

The function IOCONPinMuxSet() set pinmux for single pin according to selected configuration.

Pin mux set

The function IOCON_SetPinMuxing() set pinmux for group of pins according to selected configuration.

Typical use case

Example use of IOCON API to selection of GPIO mode. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/iocon

Files

file  fsl_iocon.h
 

Data Structures

struct  iocon_group_t
 Array of IOCON pin definitions passed to IOCON_SetPinMuxing() must be in this format. More...
 

Functions

__STATIC_INLINE void IOCON_PinMuxSet (IOCON_Type *base, uint8_t ionumber, uint32_t modefunc)
 IOCON function and mode selection definitions. More...
 
__STATIC_INLINE void IOCON_SetPinMuxing (IOCON_Type *base, const iocon_group_t *pinArray, uint32_t arrayLength)
 Set all I/O Control pin muxing. More...
 

Driver version

#define LPC_IOCON_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))
 IOCON driver version 2.0.1. More...
 

Data Structure Documentation

struct iocon_group_t

Macro Definition Documentation

#define LPC_IOCON_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))

Function Documentation

__STATIC_INLINE void IOCON_PinMuxSet ( IOCON_Type *  base,
uint8_t  ionumber,
uint32_t  modefunc 
)
Note
See the User Manual for specific modes and functions supported by the various pins. Sets I/O Control pin mux
Parameters
base: The base of IOCON peripheral on the chip
ionumber: GPIO number to mux
modefunc: OR'ed values of type IOCON_*
Returns
Nothing
__STATIC_INLINE void IOCON_SetPinMuxing ( IOCON_Type *  base,
const iocon_group_t pinArray,
uint32_t  arrayLength 
)
Parameters
base: The base of IOCON peripheral on the chip
pinArray: Pointer to array of pin mux selections
arrayLength: Number of entries in pinArray
Returns
Nothing