![]() |
MCUXpresso SDK API Reference Manual
Rev 2.13.0
NXP Semiconductors
|
Files | |
| file | fsl_i2s.h |
Data Structures | |
| struct | i2s_config_t |
| I2S configuration structure. More... | |
| struct | i2s_transfer_t |
| Buffer to transfer from or receive audio data into. More... | |
| struct | i2s_handle_t |
| Members not to be accessed / modified outside of the driver. More... | |
Macros | |
| #define | I2S_NUM_BUFFERS (4U) |
| Number of buffers . More... | |
Typedefs | |
| typedef void(* | i2s_transfer_callback_t )(I2S_Type *base, i2s_handle_t *handle, status_t completionStatus, void *userData) |
| Callback function invoked from transactional API on completion of a single buffer transfer. More... | |
Enumerations | |
| enum | { kStatus_I2S_BufferComplete, kStatus_I2S_Done = MAKE_STATUS(kStatusGroup_I2S, 1), kStatus_I2S_Busy } |
| _i2s_status I2S status codes. More... | |
| enum | i2s_flags_t { kI2S_TxErrorFlag = I2S_FIFOINTENSET_TXERR_MASK, kI2S_TxLevelFlag = I2S_FIFOINTENSET_TXLVL_MASK, kI2S_RxErrorFlag = I2S_FIFOINTENSET_RXERR_MASK, kI2S_RxLevelFlag = I2S_FIFOINTENSET_RXLVL_MASK } |
| I2S flags. More... | |
| enum | i2s_master_slave_t { kI2S_MasterSlaveNormalSlave = 0x0, kI2S_MasterSlaveWsSyncMaster = 0x1, kI2S_MasterSlaveExtSckMaster = 0x2, kI2S_MasterSlaveNormalMaster = 0x3 } |
| Master / slave mode. More... | |
| enum | i2s_mode_t { kI2S_ModeI2sClassic = 0x0, kI2S_ModeDspWs50 = 0x1, kI2S_ModeDspWsShort = 0x2, kI2S_ModeDspWsLong = 0x3 } |
| I2S mode. More... | |
| enum | { kI2S_SecondaryChannel1 = 0U, kI2S_SecondaryChannel2 = 1U, kI2S_SecondaryChannel3 = 2U } |
| _i2s_secondary_channel I2S secondary channel. More... | |
Driver version | |
| #define | FSL_I2S_DRIVER_VERSION (MAKE_VERSION(2, 3, 2)) |
| I2S driver version 2.3.2. More... | |
Initialization and deinitialization | |
| void | I2S_TxInit (I2S_Type *base, const i2s_config_t *config) |
| Initializes the FLEXCOMM peripheral for I2S transmit functionality. More... | |
| void | I2S_RxInit (I2S_Type *base, const i2s_config_t *config) |
| Initializes the FLEXCOMM peripheral for I2S receive functionality. More... | |
| void | I2S_TxGetDefaultConfig (i2s_config_t *config) |
| Sets the I2S Tx configuration structure to default values. More... | |
| void | I2S_RxGetDefaultConfig (i2s_config_t *config) |
| Sets the I2S Rx configuration structure to default values. More... | |
| void | I2S_Deinit (I2S_Type *base) |
| De-initializes the I2S peripheral. More... | |
| void | I2S_SetBitClockRate (I2S_Type *base, uint32_t sourceClockHz, uint32_t sampleRate, uint32_t bitWidth, uint32_t channelNumbers) |
| Transmitter/Receiver bit clock rate configurations. More... | |
Non-blocking API | |
| void | I2S_TxTransferCreateHandle (I2S_Type *base, i2s_handle_t *handle, i2s_transfer_callback_t callback, void *userData) |
| Initializes handle for transfer of audio data. More... | |
| status_t | I2S_TxTransferNonBlocking (I2S_Type *base, i2s_handle_t *handle, i2s_transfer_t transfer) |
| Begins or queue sending of the given data. More... | |
| void | I2S_TxTransferAbort (I2S_Type *base, i2s_handle_t *handle) |
| Aborts sending of data. More... | |
| void | I2S_RxTransferCreateHandle (I2S_Type *base, i2s_handle_t *handle, i2s_transfer_callback_t callback, void *userData) |
| Initializes handle for reception of audio data. More... | |
| status_t | I2S_RxTransferNonBlocking (I2S_Type *base, i2s_handle_t *handle, i2s_transfer_t transfer) |
| Begins or queue reception of data into given buffer. More... | |
| void | I2S_RxTransferAbort (I2S_Type *base, i2s_handle_t *handle) |
| Aborts receiving of data. More... | |
| status_t | I2S_TransferGetCount (I2S_Type *base, i2s_handle_t *handle, size_t *count) |
| Returns number of bytes transferred so far. More... | |
| status_t | I2S_TransferGetErrorCount (I2S_Type *base, i2s_handle_t *handle, size_t *count) |
| Returns number of buffer underruns or overruns. More... | |
Enable / disable | |
| static void | I2S_Enable (I2S_Type *base) |
| Enables I2S operation. More... | |
| void | I2S_EnableSecondaryChannel (I2S_Type *base, uint32_t channel, bool oneChannel, uint32_t position) |
| Enables I2S secondary channel. More... | |
| static void | I2S_DisableSecondaryChannel (I2S_Type *base, uint32_t channel) |
| Disables I2S secondary channel. More... | |
| static void | I2S_Disable (I2S_Type *base) |
| Disables I2S operation. More... | |
Interrupts | |
| static void | I2S_EnableInterrupts (I2S_Type *base, uint32_t interruptMask) |
| Enables I2S FIFO interrupts. More... | |
| static void | I2S_DisableInterrupts (I2S_Type *base, uint32_t interruptMask) |
| Disables I2S FIFO interrupts. More... | |
| static uint32_t | I2S_GetEnabledInterrupts (I2S_Type *base) |
| Returns the set of currently enabled I2S FIFO interrupts. More... | |
| status_t | I2S_EmptyTxFifo (I2S_Type *base) |
| Flush the valid data in TX fifo. More... | |
| void | I2S_TxHandleIRQ (I2S_Type *base, i2s_handle_t *handle) |
| Invoked from interrupt handler when transmit FIFO level decreases. More... | |
| void | I2S_RxHandleIRQ (I2S_Type *base, i2s_handle_t *handle) |
| Invoked from interrupt handler when receive FIFO level decreases. More... | |
| struct i2s_config_t |
Data Fields | |
| i2s_master_slave_t | masterSlave |
| Master / slave configuration. | |
| i2s_mode_t | mode |
| I2S mode. | |
| bool | rightLow |
| Right channel data in low portion of FIFO. | |
| bool | leftJust |
| Left justify data in FIFO. | |
| bool | pdmData |
| Data source is the D-Mic subsystem. | |
| bool | sckPol |
| SCK polarity. | |
| bool | wsPol |
| WS polarity. | |
| uint16_t | divider |
| Flexcomm function clock divider (1 - 4096) | |
| bool | oneChannel |
| true mono, false stereo | |
| uint8_t | dataLength |
| Data length (4 - 32) | |
| uint16_t | frameLength |
| Frame width (4 - 512) | |
| uint16_t | position |
| Data position in the frame. | |
| uint8_t | watermark |
| FIFO trigger level. | |
| bool | txEmptyZero |
| Transmit zero when buffer becomes empty or last item. | |
| bool | pack48 |
| Packing format for 48-bit data (false - 24 bit values, true - alternating 32-bit and 16-bit values) | |
| struct i2s_transfer_t |
| struct _i2s_handle |
Transactional state of the intialized transfer or receive I2S operation.
Data Fields | |
| volatile uint32_t | state |
| State of transfer. | |
| i2s_transfer_callback_t | completionCallback |
| Callback function pointer. | |
| void * | userData |
| Application data passed to callback. | |
| bool | oneChannel |
| true mono, false stereo | |
| uint8_t | dataLength |
| Data length (4 - 32) | |
| bool | pack48 |
| Packing format for 48-bit data (false - 24 bit values, true - alternating 32-bit and 16-bit values) | |
| uint8_t | watermark |
| FIFO trigger level. | |
| bool | useFifo48H |
| When dataLength 17-24: true use FIFOWR48H, false use FIFOWR. | |
| volatile i2s_transfer_t | i2sQueue [I2S_NUM_BUFFERS] |
| Transfer queue storing transfer buffers. | |
| volatile uint8_t | queueUser |
| Queue index where user's next transfer will be stored. | |
| volatile uint8_t | queueDriver |
| Queue index of buffer actually used by the driver. | |
| volatile uint32_t | errorCount |
| Number of buffer underruns/overruns. | |
| volatile uint32_t | transferCount |
| Number of bytes transferred. | |
| #define FSL_I2S_DRIVER_VERSION (MAKE_VERSION(2, 3, 2)) |
| #define I2S_NUM_BUFFERS (4U) |
| typedef void(* i2s_transfer_callback_t)(I2S_Type *base, i2s_handle_t *handle, status_t completionStatus, void *userData) |
| base | I2S base pointer. |
| handle | pointer to I2S transaction. |
| completionStatus | status of the transaction. |
| userData | optional pointer to user arguments data. |
| anonymous enum |
| enum i2s_flags_t |
| enum i2s_master_slave_t |
| enum i2s_mode_t |
| anonymous enum |
| void I2S_TxInit | ( | I2S_Type * | base, |
| const i2s_config_t * | config | ||
| ) |
Ungates the FLEXCOMM clock and configures the module for I2S transmission using a configuration structure. The configuration structure can be custom filled or set with default values by I2S_TxGetDefaultConfig().
| base | I2S base pointer. |
| config | pointer to I2S configuration structure. |
| void I2S_RxInit | ( | I2S_Type * | base, |
| const i2s_config_t * | config | ||
| ) |
Ungates the FLEXCOMM clock and configures the module for I2S receive using a configuration structure. The configuration structure can be custom filled or set with default values by I2S_RxGetDefaultConfig().
| base | I2S base pointer. |
| config | pointer to I2S configuration structure. |
| void I2S_TxGetDefaultConfig | ( | i2s_config_t * | config | ) |
This API initializes the configuration structure for use in I2S_TxInit(). The initialized structure can remain unchanged in I2S_TxInit(), or it can be modified before calling I2S_TxInit(). Example:
Default values:
| config | pointer to I2S configuration structure. |
| void I2S_RxGetDefaultConfig | ( | i2s_config_t * | config | ) |
This API initializes the configuration structure for use in I2S_RxInit(). The initialized structure can remain unchanged in I2S_RxInit(), or it can be modified before calling I2S_RxInit(). Example:
Default values:
| config | pointer to I2S configuration structure. |
| void I2S_Deinit | ( | I2S_Type * | base | ) |
This API gates the FLEXCOMM clock. The I2S module can't operate unless I2S_TxInit or I2S_RxInit is called to enable the clock.
| base | I2S base pointer. |
| void I2S_SetBitClockRate | ( | I2S_Type * | base, |
| uint32_t | sourceClockHz, | ||
| uint32_t | sampleRate, | ||
| uint32_t | bitWidth, | ||
| uint32_t | channelNumbers | ||
| ) |
| base | SAI base pointer. |
| sourceClockHz | bit clock source frequency. |
| sampleRate | audio data sample rate. |
| bitWidth | audio data bitWidth. |
| channelNumbers | audio channel numbers. |
| void I2S_TxTransferCreateHandle | ( | I2S_Type * | base, |
| i2s_handle_t * | handle, | ||
| i2s_transfer_callback_t | callback, | ||
| void * | userData | ||
| ) |
| base | I2S base pointer. |
| handle | pointer to handle structure. |
| callback | function to be called back when transfer is done or fails. |
| userData | pointer to data passed to callback. |
| status_t I2S_TxTransferNonBlocking | ( | I2S_Type * | base, |
| i2s_handle_t * | handle, | ||
| i2s_transfer_t | transfer | ||
| ) |
| base | I2S base pointer. |
| handle | pointer to handle structure. |
| transfer | data buffer. |
| kStatus_Success | |
| kStatus_I2S_Busy | if all queue slots are occupied with unsent buffers. |
| void I2S_TxTransferAbort | ( | I2S_Type * | base, |
| i2s_handle_t * | handle | ||
| ) |
| base | I2S base pointer. |
| handle | pointer to handle structure. |
| void I2S_RxTransferCreateHandle | ( | I2S_Type * | base, |
| i2s_handle_t * | handle, | ||
| i2s_transfer_callback_t | callback, | ||
| void * | userData | ||
| ) |
| base | I2S base pointer. |
| handle | pointer to handle structure. |
| callback | function to be called back when transfer is done or fails. |
| userData | pointer to data passed to callback. |
| status_t I2S_RxTransferNonBlocking | ( | I2S_Type * | base, |
| i2s_handle_t * | handle, | ||
| i2s_transfer_t | transfer | ||
| ) |
| base | I2S base pointer. |
| handle | pointer to handle structure. |
| transfer | data buffer. |
| kStatus_Success | |
| kStatus_I2S_Busy | if all queue slots are occupied with buffers which are not full. |
| void I2S_RxTransferAbort | ( | I2S_Type * | base, |
| i2s_handle_t * | handle | ||
| ) |
| base | I2S base pointer. |
| handle | pointer to handle structure. |
| status_t I2S_TransferGetCount | ( | I2S_Type * | base, |
| i2s_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | I2S base pointer. | |
| handle | pointer to handle structure. | |
| [out] | count | number of bytes transferred so far by the non-blocking transaction. |
| kStatus_Success | |
| kStatus_NoTransferInProgress | there is no non-blocking transaction currently in progress. |
| status_t I2S_TransferGetErrorCount | ( | I2S_Type * | base, |
| i2s_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | I2S base pointer. | |
| handle | pointer to handle structure. | |
| [out] | count | number of transmit errors encountered so far by the non-blocking transaction. |
| kStatus_Success | |
| kStatus_NoTransferInProgress | there is no non-blocking transaction currently in progress. |
|
inlinestatic |
| base | I2S base pointer. |
| void I2S_EnableSecondaryChannel | ( | I2S_Type * | base, |
| uint32_t | channel, | ||
| bool | oneChannel, | ||
| uint32_t | position | ||
| ) |
| base | I2S base pointer. |
| channel | seondary channel channel number, reference _i2s_secondary_channel. |
| oneChannel | true is treated as single channel, functionality left channel for this pair. |
| position | define the location within the frame of the data, should not bigger than 0x1FFU. |
|
inlinestatic |
| base | I2S base pointer. |
| channel | seondary channel channel number, reference _i2s_secondary_channel. |
|
inlinestatic |
| base | I2S base pointer. |
|
inlinestatic |
| base | I2S base pointer. |
| interruptMask | bit mask of interrupts to enable. See i2s_flags_t for the set of constants that should be OR'd together to form the bit mask. |
|
inlinestatic |
| base | I2S base pointer. |
| interruptMask | bit mask of interrupts to enable. See i2s_flags_t for the set of constants that should be OR'd together to form the bit mask. |
|
inlinestatic |
| base | I2S base pointer. |
| status_t I2S_EmptyTxFifo | ( | I2S_Type * | base | ) |
| base | I2S base pointer. |
| void I2S_TxHandleIRQ | ( | I2S_Type * | base, |
| i2s_handle_t * | handle | ||
| ) |
| base | I2S base pointer. |
| handle | pointer to handle structure. |
| void I2S_RxHandleIRQ | ( | I2S_Type * | base, |
| i2s_handle_t * | handle | ||
| ) |
| base | I2S base pointer. |
| handle | pointer to handle structure. |