![]() |
MCUXpresso SDK API Reference Manual
Rev 2.13.0
NXP Semiconductors
|
Power driver provides APIs to control peripherals power and control the system power mode.
Files | |
| file | fsl_power.h |
Data Structures | |
| struct | power_bod_config_t |
| The configuration of power bod, including reset level, interrupt level, and so on. More... | |
Enumerations | |
| enum | power_bod_status_t { kBod_ResetStatusFlag = SYSCON_BODCTRL_BODRSTSTAT_MASK, kBod_InterruptStatusFlag = SYSCON_BODCTRL_BODINTSTAT_MASK } |
| The enumeration of BOD status flags. More... | |
| enum | power_bod_reset_level_t { kBod_ResetLevel0 = 0U, kBod_ResetLevel1, kBod_ResetLevel2, kBod_ResetLevel3 } |
| The enumeration of BOD reset level. More... | |
| enum | power_bod_interrupt_level_t { kBod_InterruptLevel0 = 0U, kBod_InterruptLevel1, kBod_InterruptLevel2, kBod_InterruptLevel3 } |
| The enumeration of BOD interrupt level. More... | |
Driver version | |
| #define | FSL_POWER_DRIVER_VERSION (MAKE_VERSION(2, 1, 0)) |
| power driver version 2.1.0. More... | |
Power Configuration | |
| static void | POWER_EnablePD (pd_bit_t en) |
| API to enable PDRUNCFG bit in the Syscon. More... | |
| static void | POWER_DisablePD (pd_bit_t en) |
| API to disable PDRUNCFG bit in the Syscon. More... | |
| static void | POWER_EnableDeepSleep (void) |
| API to enable deep sleep bit in the ARM Core. More... | |
| static void | POWER_DisableDeepSleep (void) |
| API to disable deep sleep bit in the ARM Core. More... | |
| void | POWER_OtpReload (void) |
| Power Library API to reload OTP. More... | |
| void | POWER_SetPLL (void) |
| Power Library API to power the PLLs. More... | |
| void | POWER_SetUsbPhy (void) |
| Power Library API to power the USB PHY. More... | |
| void | POWER_EnterPowerMode (power_mode_cfg_t mode, uint64_t exclude_from_pd) |
| Power Library API to enter different power modes. More... | |
| void | POWER_EnterSleep (void) |
| Power Library API to enter sleep mode. More... | |
| void | POWER_EnterDeepSleep (uint64_t exclude_from_pd) |
| Power Library API to enter deep sleep mode. More... | |
| void | POWER_EnterDeepPowerDown (uint64_t exclude_from_pd) |
| Power Library API to enter deep power down mode. More... | |
| void | POWER_SetVoltageForFreq (uint32_t freq) |
| Power Library API to choose normal regulation and set the voltage for the desired operating frequency. More... | |
| uint32_t | POWER_GetLibVersion (void) |
| Power Library API to return the library version. More... | |
| void | POWER_InitBod (const power_bod_config_t *bodConfig) |
| Initialize BOD, including enabling/disabling BOD interrupt, enabling/disabling BOD reset, setting BOD interrupt level, and reset level. More... | |
| void | POWER_GetDefaultBodConfig (power_bod_config_t *bodConfig) |
| Get default BOD configuration. More... | |
| static void | POWER_DeinitBod (void) |
| De-initialize BOD. | |
| static uint32_t | POWER_GetBodStatusFlags (void) |
| Get Bod status flags. More... | |
| static void | POWER_ClearBodStatusFlags (uint32_t mask) |
| Clear Bod status flags. More... | |
| struct power_bod_config_t |
Data Fields | |
| bool | enableReset |
| Enable/disable BOD reset function. More... | |
| power_bod_reset_level_t | resetLevel |
| BOD reset level, please refer to power_bod_reset_level_t. More... | |
| bool | enableInterrupt |
| Enable/disable BOD interrupt function. More... | |
| power_bod_interrupt_level_t | interruptLevel |
| BOD interrupt level, please refer to power_bod_interrupt_level_t. More... | |
| bool power_bod_config_t::enableReset |
| power_bod_reset_level_t power_bod_config_t::resetLevel |
| bool power_bod_config_t::enableInterrupt |
| power_bod_interrupt_level_t power_bod_config_t::interruptLevel |
| #define FSL_POWER_DRIVER_VERSION (MAKE_VERSION(2, 1, 0)) |
| enum power_bod_status_t |
|
inlinestatic |
Note that enabling the bit powers down the peripheral
| en | peripheral for which to enable the PDRUNCFG bit |
|
inlinestatic |
Note that disabling the bit powers up the peripheral
| en | peripheral for which to disable the PDRUNCFG bit |
|
inlinestatic |
|
inlinestatic |
| void POWER_OtpReload | ( | void | ) |
This API must be called if VD6 is power down and power back again since FROHF TRIM value is store in OTP. If not, when calling FROHF settng API in clock driver then the FROHF clock out put will be inaccurate.
| void POWER_SetPLL | ( | void | ) |
| void POWER_SetUsbPhy | ( | void | ) |
| void POWER_EnterPowerMode | ( | power_mode_cfg_t | mode, |
| uint64_t | exclude_from_pd | ||
| ) |
| mode | power mode |
| exclude_from_pd | Bit mask of the PDRUNCFG0(low 32bits) and PDRUNCFG1(high 32bits) that needs to be powered on during power mode selected. |
| void POWER_EnterSleep | ( | void | ) |
| void POWER_EnterDeepSleep | ( | uint64_t | exclude_from_pd | ) |
| exclude_from_pd | Bit mask of the PDRUNCFG0(low 32bits) and PDRUNCFG1(high 32bits) bits that needs to be powered on during deep sleep |
| void POWER_EnterDeepPowerDown | ( | uint64_t | exclude_from_pd | ) |
| exclude_from_pd | Bit mask of the PDRUNCFG0(low 32bits) and PDRUNCFG1(high 32bits) that needs to be powered on during deep power down mode, but this is has no effect as the voltages are cut off. |
| void POWER_SetVoltageForFreq | ( | uint32_t | freq | ) |
| freq | - The desired frequency at which the part would like to operate, note that the voltage and flash wait states should be set before changing frequency |
| uint32_t POWER_GetLibVersion | ( | void | ) |
| void POWER_InitBod | ( | const power_bod_config_t * | bodConfig | ) |
| bodConfig | Pointer the the structure power_bod_config_t. |
| void POWER_GetDefaultBodConfig | ( | power_bod_config_t * | bodConfig | ) |
| bodConfig | Pointer the the structure power_bod_config_t. |
|
inlinestatic |
|
inlinestatic |
| mask | The mask of status flags to clear, should be the OR'ed value of power_bod_status_t. |