MCUXpresso SDK API Reference Manual  Rev 2.13.0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
AES: AES encryption decryption driver

Overview

The MCUXpresso SDK provides a peripheral driver for the AES module in MCUXpresso SDK devices.

The driver provides blocking synchronous APIs. The AES operations are complete (and results are made availabe for further usage) when a function returns. When called, these functions do not return until an AES operation is complete. These functions use main CPU for simple polling loops to determine operation complete or error status, as well as plaintext or ciphertext data movements. The driver functions are not re-entrant. These functions provide typical interface to upper layer or application software.

AES Driver Initialization and Configuration

Clock to the AES module has to be enabled before using the driver API. The function AES_SetKey() has to be used to store encryption key into device registers prior to using other API.

Comments about API usage in RTOS

AES operations provided by this driver are not re-entrant. Because of this, the application software should ensure the AES module operation is not requested from different tasks or interrupt service routines while an operation is in progress.

AES Driver Examples

Encrypt plaintext and decrypt it back by AES engine Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/aes Encrypts AES using CTR block mode. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/aes Generation of GCM tag only Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/aes

Files

file  fsl_aes.h
 

Driver version

#define FSL_AES_DRIVER_VERSION   (MAKE_VERSION(2, 0, 3))
 Defines LPC AES driver version 2.0.3. More...
 

AES Functional Operation

status_t AES_SetKey (AES_Type *base, const uint8_t *key, size_t keySize)
 Sets AES key. More...
 
status_t AES_EncryptEcb (AES_Type *base, const uint8_t *plaintext, uint8_t *ciphertext, size_t size)
 Encrypts AES using the ECB block mode. More...
 
status_t AES_DecryptEcb (AES_Type *base, const uint8_t *ciphertext, uint8_t *plaintext, size_t size)
 Decrypts AES using the ECB block mode. More...
 
status_t AES_EncryptCbc (AES_Type *base, const uint8_t *plaintext, uint8_t *ciphertext, size_t size, const uint8_t iv[AES_IV_SIZE])
 Encrypts AES using CBC block mode. More...
 
status_t AES_DecryptCbc (AES_Type *base, const uint8_t *ciphertext, uint8_t *plaintext, size_t size, const uint8_t iv[AES_IV_SIZE])
 Decrypts AES using CBC block mode. More...
 
status_t AES_EncryptCfb (AES_Type *base, const uint8_t *plaintext, uint8_t *ciphertext, size_t size, const uint8_t iv[AES_IV_SIZE])
 Encrypts AES using CFB block mode. More...
 
status_t AES_DecryptCfb (AES_Type *base, const uint8_t *ciphertext, uint8_t *plaintext, size_t size, const uint8_t iv[AES_IV_SIZE])
 Decrypts AES using CFB block mode. More...
 
status_t AES_EncryptOfb (AES_Type *base, const uint8_t *plaintext, uint8_t *ciphertext, size_t size, const uint8_t iv[AES_IV_SIZE])
 Encrypts AES using OFB block mode. More...
 
status_t AES_DecryptOfb (AES_Type *base, const uint8_t *ciphertext, uint8_t *plaintext, size_t size, const uint8_t iv[AES_IV_SIZE])
 Decrypts AES using OFB block mode. More...
 
status_t AES_CryptCtr (AES_Type *base, const uint8_t *input, uint8_t *output, size_t size, uint8_t counter[AES_BLOCK_SIZE], uint8_t counterlast[AES_BLOCK_SIZE], size_t *szLeft)
 Encrypts or decrypts AES using CTR block mode. More...
 
status_t AES_EncryptTagGcm (AES_Type *base, const uint8_t *plaintext, uint8_t *ciphertext, size_t size, const uint8_t *iv, size_t ivSize, const uint8_t *aad, size_t aadSize, uint8_t *tag, size_t tagSize)
 Encrypts AES and tags using GCM block mode. More...
 
status_t AES_DecryptTagGcm (AES_Type *base, const uint8_t *ciphertext, uint8_t *plaintext, size_t size, const uint8_t *iv, size_t ivSize, const uint8_t *aad, size_t aadSize, const uint8_t *tag, size_t tagSize)
 Decrypts AES and authenticates using GCM block mode. More...
 
#define AES_BLOCK_SIZE   16
 AES block size in bytes.
 
#define AES_IV_SIZE   16
 AES Input Vector size in bytes.
 

Macro Definition Documentation

#define FSL_AES_DRIVER_VERSION   (MAKE_VERSION(2, 0, 3))

Change log:

  • Version 2.0.3
    • Edit aes_one_block() function to be interrupt safe.
  • Version 2.0.2
    • Fix MISRA-2012 issues
  • Version 2.0.1
    • GCM constant time tag comparison
  • Version 2.0.0
    • initial version

Function Documentation

status_t AES_SetKey ( AES_Type *  base,
const uint8_t *  key,
size_t  keySize 
)

Sets AES key.

Parameters
baseAES peripheral base address
keyInput key to use for encryption or decryption
keySizeSize of the input key, in bytes. Must be 16, 24, or 32.
Returns
Status from Set Key operation
status_t AES_EncryptEcb ( AES_Type *  base,
const uint8_t *  plaintext,
uint8_t *  ciphertext,
size_t  size 
)

Encrypts AES using the ECB block mode.

Parameters
baseAES peripheral base address
plaintextInput plain text to encrypt
[out]ciphertextOutput cipher text
sizeSize of input and output data in bytes. Must be multiple of 16 bytes.
Returns
Status from encrypt operation
status_t AES_DecryptEcb ( AES_Type *  base,
const uint8_t *  ciphertext,
uint8_t *  plaintext,
size_t  size 
)

Decrypts AES using the ECB block mode.

Parameters
baseAES peripheral base address
ciphertextInput ciphertext to decrypt
[out]plaintextOutput plain text
sizeSize of input and output data in bytes. Must be multiple of 16 bytes.
Returns
Status from decrypt operation
status_t AES_EncryptCbc ( AES_Type *  base,
const uint8_t *  plaintext,
uint8_t *  ciphertext,
size_t  size,
const uint8_t  iv[AES_IV_SIZE] 
)
Parameters
baseAES peripheral base address
plaintextInput plain text to encrypt
[out]ciphertextOutput cipher text
sizeSize of input and output data in bytes. Must be multiple of 16 bytes.
ivInput initial vector to combine with the first input block.
Returns
Status from encrypt operation
status_t AES_DecryptCbc ( AES_Type *  base,
const uint8_t *  ciphertext,
uint8_t *  plaintext,
size_t  size,
const uint8_t  iv[AES_IV_SIZE] 
)
Parameters
baseAES peripheral base address
ciphertextInput cipher text to decrypt
[out]plaintextOutput plain text
sizeSize of input and output data in bytes. Must be multiple of 16 bytes.
ivInput initial vector to combine with the first input block.
Returns
Status from decrypt operation
status_t AES_EncryptCfb ( AES_Type *  base,
const uint8_t *  plaintext,
uint8_t *  ciphertext,
size_t  size,
const uint8_t  iv[AES_IV_SIZE] 
)
Parameters
baseAES peripheral base address
plaintextInput plain text to encrypt
[out]ciphertextOutput cipher text
sizeSize of input and output data in bytes. Must be multiple of 16 bytes.
ivInput Initial vector to be used as the first input block.
Returns
Status from encrypt operation
status_t AES_DecryptCfb ( AES_Type *  base,
const uint8_t *  ciphertext,
uint8_t *  plaintext,
size_t  size,
const uint8_t  iv[AES_IV_SIZE] 
)
Parameters
baseAES peripheral base address
ciphertextInput cipher text to decrypt
[out]plaintextOutput plain text
sizeSize of input and output data in bytes. Must be multiple of 16 bytes.
ivInput Initial vector to be used as the first input block.
Returns
Status from decrypt operation
status_t AES_EncryptOfb ( AES_Type *  base,
const uint8_t *  plaintext,
uint8_t *  ciphertext,
size_t  size,
const uint8_t  iv[AES_IV_SIZE] 
)
Parameters
baseAES peripheral base address
plaintextInput plain text to encrypt
[out]ciphertextOutput cipher text
sizeSize of input and output data in bytes.
ivInput Initial vector to be used as the first input block.
Returns
Status from encrypt operation
status_t AES_DecryptOfb ( AES_Type *  base,
const uint8_t *  ciphertext,
uint8_t *  plaintext,
size_t  size,
const uint8_t  iv[AES_IV_SIZE] 
)
Parameters
baseAES peripheral base address
ciphertextInput cipher text to decrypt
[out]plaintextOutput plain text
sizeSize of input and output data in bytes.
ivInput Initial vector to be used as the first input block.
Returns
Status from decrypt operation
status_t AES_CryptCtr ( AES_Type *  base,
const uint8_t *  input,
uint8_t *  output,
size_t  size,
uint8_t  counter[AES_BLOCK_SIZE],
uint8_t  counterlast[AES_BLOCK_SIZE],
size_t *  szLeft 
)

Encrypts or decrypts AES using CTR block mode. AES CTR mode uses only forward AES cipher and same algorithm for encryption and decryption. The only difference between encryption and decryption is that, for encryption, the input argument is plain text and the output argument is cipher text. For decryption, the input argument is cipher text and the output argument is plain text.

Parameters
baseAES peripheral base address
inputInput data for CTR block mode
[out]outputOutput data for CTR block mode
sizeSize of input and output data in bytes
[in,out]counterInput counter (updates on return)
[out]counterlastOutput cipher of last counter, for chained CTR calls. NULL can be passed if chained calls are not used.
[out]szLeftOutput number of bytes in left unused in counterlast block. NULL can be passed if chained calls are not used.
Returns
Status from crypt operation
status_t AES_EncryptTagGcm ( AES_Type *  base,
const uint8_t *  plaintext,
uint8_t *  ciphertext,
size_t  size,
const uint8_t *  iv,
size_t  ivSize,
const uint8_t *  aad,
size_t  aadSize,
uint8_t *  tag,
size_t  tagSize 
)

Encrypts AES and optionally tags using GCM block mode. If plaintext is NULL, only the GHASH is calculated and output in the 'tag' field.

Parameters
baseAES peripheral base address
plaintextInput plain text to encrypt
[out]ciphertextOutput cipher text.
sizeSize of input and output data in bytes
ivInput initial vector
ivSizeSize of the IV
aadInput additional authentication data
aadSizeInput size in bytes of AAD
[out]tagOutput hash tag. Set to NULL to skip tag processing.
tagSizeInput size of the tag to generate, in bytes. Must be 4,8,12,13,14,15 or 16.
Returns
Status from encrypt operation
status_t AES_DecryptTagGcm ( AES_Type *  base,
const uint8_t *  ciphertext,
uint8_t *  plaintext,
size_t  size,
const uint8_t *  iv,
size_t  ivSize,
const uint8_t *  aad,
size_t  aadSize,
const uint8_t *  tag,
size_t  tagSize 
)

Decrypts AES and optionally authenticates using GCM block mode. If ciphertext is NULL, only the GHASH is calculated and compared with the received GHASH in 'tag' field.

Parameters
baseAES peripheral base address
ciphertextInput cipher text to decrypt
[out]plaintextOutput plain text.
sizeSize of input and output data in bytes
ivInput initial vector
ivSizeSize of the IV
aadInput additional authentication data
aadSizeInput size in bytes of AAD
tagInput hash tag to compare. Set to NULL to skip tag processing.
tagSizeInput size of the tag, in bytes. Must be 4, 8, 12, 13, 14, 15, or 16.
Returns
Status from decrypt operation