![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev 2.13.0
    
   NXP Semiconductors 
   | 
 
The wm8960 driver provides a codec control interface.
Data Structures | |
| struct | wm8960_audio_format_t | 
| wm8960 audio format  More... | |
| struct | wm8960_master_sysclk_config_t | 
| wm8960 master system clock configuration  More... | |
| struct | wm8960_config_t | 
| Initialize structure of WM8960.  More... | |
| struct | wm8960_handle_t | 
| wm8960 codec handler  More... | |
Macros | |
| #define | WM8960_I2C_HANDLER_SIZE CODEC_I2C_MASTER_HANDLER_SIZE | 
| wm8960 handle size  | |
| #define | WM8960_LINVOL 0x0U | 
| Define the register address of WM8960.  More... | |
| #define | WM8960_CACHEREGNUM 56U | 
| Cache register number.  | |
| #define | WM8960_CLOCK2_BCLK_DIV_MASK 0xFU | 
| WM8960 CLOCK2 bits.  | |
| #define | WM8960_IFACE1_FORMAT_MASK 0x03U | 
| WM8960_IFACE1 FORMAT bits.  | |
| #define | WM8960_IFACE1_WL_MASK 0x0CU | 
| WM8960_IFACE1 WL bits.  | |
| #define | WM8960_IFACE1_LRP_MASK 0x10U | 
| WM8960_IFACE1 LRP bit.  | |
| #define | WM8960_IFACE1_DLRSWAP_MASK 0x20U | 
| WM8960_IFACE1 DLRSWAP bit.  | |
| #define | WM8960_IFACE1_MS_MASK 0x40U | 
| WM8960_IFACE1 MS bit.  | |
| #define | WM8960_IFACE1_BCLKINV_MASK 0x80U | 
| WM8960_IFACE1 BCLKINV bit.  | |
| #define | WM8960_IFACE1_ALRSWAP_MASK 0x100U | 
| WM8960_IFACE1 ALRSWAP bit.  | |
| #define | WM8960_POWER1_VREF_MASK 0x40U | 
| WM8960_POWER1.  | |
| #define | WM8960_POWER2_DACL_MASK 0x100U | 
| WM8960_POWER2.  | |
| #define | WM8960_I2C_ADDR 0x1A | 
| WM8960 I2C address.  More... | |
| #define | WM8960_I2C_BAUDRATE (100000U) | 
| WM8960 I2C baudrate.  | |
| #define | WM8960_ADC_MAX_VOLUME_vALUE 0xFFU | 
| WM8960 maximum volume value.  | |
Functions | |
| status_t | WM8960_Init (wm8960_handle_t *handle, const wm8960_config_t *config) | 
| WM8960 initialize function.  More... | |
| status_t | WM8960_Deinit (wm8960_handle_t *handle) | 
| Deinit the WM8960 codec.  More... | |
| status_t | WM8960_SetDataRoute (wm8960_handle_t *handle, wm8960_route_t route) | 
| Set audio data route in WM8960.  More... | |
| status_t | WM8960_SetLeftInput (wm8960_handle_t *handle, wm8960_input_t input) | 
| Set left audio input source in WM8960.  More... | |
| status_t | WM8960_SetRightInput (wm8960_handle_t *handle, wm8960_input_t input) | 
| Set right audio input source in WM8960.  More... | |
| status_t | WM8960_SetProtocol (wm8960_handle_t *handle, wm8960_protocol_t protocol) | 
| Set the audio transfer protocol.  More... | |
| void | WM8960_SetMasterSlave (wm8960_handle_t *handle, bool master) | 
| Set WM8960 as master or slave.  More... | |
| status_t | WM8960_SetVolume (wm8960_handle_t *handle, wm8960_module_t module, uint32_t volume) | 
| Set the volume of different modules in WM8960.  More... | |
| uint32_t | WM8960_GetVolume (wm8960_handle_t *handle, wm8960_module_t module) | 
| Get the volume of different modules in WM8960.  More... | |
| status_t | WM8960_SetMute (wm8960_handle_t *handle, wm8960_module_t module, bool isEnabled) | 
| Mute modules in WM8960.  More... | |
| status_t | WM8960_SetModule (wm8960_handle_t *handle, wm8960_module_t module, bool isEnabled) | 
| Enable/disable expected devices.  More... | |
| status_t | WM8960_SetPlay (wm8960_handle_t *handle, uint32_t playSource) | 
| SET the WM8960 play source.  More... | |
| status_t | WM8960_ConfigDataFormat (wm8960_handle_t *handle, uint32_t sysclk, uint32_t sample_rate, uint32_t bits) | 
| Configure the data format of audio data.  More... | |
| status_t | WM8960_SetJackDetect (wm8960_handle_t *handle, bool isEnabled) | 
| Enable/disable jack detect feature.  More... | |
| status_t | WM8960_WriteReg (wm8960_handle_t *handle, uint8_t reg, uint16_t val) | 
| Write register to WM8960 using I2C.  More... | |
| status_t | WM8960_ReadReg (uint8_t reg, uint16_t *val) | 
| Read register from WM8960 using I2C.  More... | |
| status_t | WM8960_ModifyReg (wm8960_handle_t *handle, uint8_t reg, uint16_t mask, uint16_t val) | 
| Modify some bits in the register using I2C.  More... | |
Driver version | |
| #define | FSL_WM8960_DRIVER_VERSION (MAKE_VERSION(2, 2, 1)) | 
| CLOCK driver version 2.2.1.  | |
| struct wm8960_audio_format_t | 
Data Fields | |
| uint32_t | mclk_HZ | 
| master clock frequency  | |
| uint32_t | sampleRate | 
| sample rate  | |
| uint32_t | bitWidth | 
| bit width  | |
| struct wm8960_master_sysclk_config_t | 
Data Fields | |
| wm8960_sysclk_source_t | sysclkSource | 
| sysclk source  | |
| uint32_t | sysclkFreq | 
| PLL output frequency value.  | |
| struct wm8960_config_t | 
Data Fields | |
| wm8960_route_t | route | 
| Audio data route.  More... | |
| wm8960_protocol_t | bus | 
| Audio transfer protocol.  | |
| wm8960_audio_format_t | format | 
| Audio format.  | |
| bool | master_slave | 
| Master or slave.  More... | |
| wm8960_master_sysclk_config_t | masterClock | 
| master clock configurations  | |
| bool | enableSpeaker | 
| True means enable class D speaker as output, false means no.  | |
| wm8960_input_t | leftInputSource | 
| Left input source for WM8960.  | |
| wm8960_input_t | rightInputSource | 
| Right input source for wm8960.  | |
| wm8960_play_source_t | playSource | 
| play source  | |
| uint8_t | slaveAddress | 
| wm8960 device address  | |
| codec_i2c_config_t | i2cConfig | 
| i2c configuration  | |
| wm8960_route_t wm8960_config_t::route | 
| bool wm8960_config_t::master_slave | 
| struct wm8960_handle_t | 
Data Fields | |
| const wm8960_config_t * | config | 
| wm8904 config pointer  | |
| uint8_t | i2cHandle [WM8960_I2C_HANDLER_SIZE] | 
| i2c handle  | |
| #define WM8960_LINVOL 0x0U | 
| #define WM8960_I2C_ADDR 0x1A | 
| enum wm8960_module_t | 
| anonymous enum | 
| enum wm8960_play_source_t | 
| enum wm8960_route_t | 
Only provide some typical data route, not all route listed. Note: Users cannot combine any routes, once a new route is set, the previous one would be replaced.
| enum wm8960_protocol_t | 
| enum wm8960_input_t | 
| anonymous enum | 
| anonymous enum | 
| status_t WM8960_Init | ( | wm8960_handle_t * | handle, | 
| const wm8960_config_t * | config | ||
| ) | 
The second parameter is NULL to WM8960 in this version. If users want to change the settings, they have to use wm8960_write_reg() or wm8960_modify_reg() to set the register value of WM8960. Note: If the codec_config is NULL, it would initialize WM8960 using default settings. The default setting: codec_config->route = kWM8960_RoutePlaybackandRecord codec_config->bus = kWM8960_BusI2S codec_config->master = slave
| handle | WM8960 handle structure. | 
| config | WM8960 configuration structure. | 
| status_t WM8960_Deinit | ( | wm8960_handle_t * | handle | ) | 
This function close all modules in WM8960 to save power.
| handle | WM8960 handle structure pointer. | 
| status_t WM8960_SetDataRoute | ( | wm8960_handle_t * | handle, | 
| wm8960_route_t | route | ||
| ) | 
This function would set the data route according to route. The route cannot be combined, as all route would enable different modules. Note: If a new route is set, the previous route would not work.
| handle | WM8960 handle structure. | 
| route | Audio data route in WM8960. | 
| status_t WM8960_SetLeftInput | ( | wm8960_handle_t * | handle, | 
| wm8960_input_t | input | ||
| ) | 
| handle | WM8960 handle structure. | 
| input | Audio input source. | 
| status_t WM8960_SetRightInput | ( | wm8960_handle_t * | handle, | 
| wm8960_input_t | input | ||
| ) | 
| handle | WM8960 handle structure. | 
| input | Audio input source. | 
| status_t WM8960_SetProtocol | ( | wm8960_handle_t * | handle, | 
| wm8960_protocol_t | protocol | ||
| ) | 
WM8960 only supports I2S, left justified, right justified, PCM A, PCM B format.
| handle | WM8960 handle structure. | 
| protocol | Audio data transfer protocol. | 
| void WM8960_SetMasterSlave | ( | wm8960_handle_t * | handle, | 
| bool | master | ||
| ) | 
| handle | WM8960 handle structure. | 
| master | 1 represent master, 0 represent slave. | 
| status_t WM8960_SetVolume | ( | wm8960_handle_t * | handle, | 
| wm8960_module_t | module, | ||
| uint32_t | volume | ||
| ) | 
This function would set the volume of WM8960 modules. Uses need to appoint the module. The function assume that left channel and right channel has the same volume.
Module:kWM8960_ModuleADC, volume range value: 0 is mute, 1-255 is -97db to 30db Module:kWM8960_ModuleDAC, volume range value: 0 is mute, 1-255 is -127db to 0db Module:kWM8960_ModuleHP, volume range value: 0 - 2F is mute, 0x30 - 0x7F is -73db to 6db Module:kWM8960_ModuleLineIn, volume range value: 0 - 0x3F is -17.25db to 30db Module:kWM8960_ModuleSpeaker, volume range value: 0 - 2F is mute, 0x30 - 0x7F is -73db to 6db
| handle | WM8960 handle structure. | 
| module | Module to set volume, it can be ADC, DAC, Headphone and so on. | 
| volume | Volume value need to be set. | 
| uint32_t WM8960_GetVolume | ( | wm8960_handle_t * | handle, | 
| wm8960_module_t | module | ||
| ) | 
This function gets the volume of WM8960 modules. Uses need to appoint the module. The function assume that left channel and right channel has the same volume.
| handle | WM8960 handle structure. | 
| module | Module to set volume, it can be ADC, DAC, Headphone and so on. | 
| status_t WM8960_SetMute | ( | wm8960_handle_t * | handle, | 
| wm8960_module_t | module, | ||
| bool | isEnabled | ||
| ) | 
| handle | WM8960 handle structure. | 
| module | Modules need to be mute. | 
| isEnabled | Mute or unmute, 1 represent mute. | 
| status_t WM8960_SetModule | ( | wm8960_handle_t * | handle, | 
| wm8960_module_t | module, | ||
| bool | isEnabled | ||
| ) | 
| handle | WM8960 handle structure. | 
| module | Module expected to enable. | 
| isEnabled | Enable or disable moudles. | 
| status_t WM8960_SetPlay | ( | wm8960_handle_t * | handle, | 
| uint32_t | playSource | ||
| ) | 
| handle | WM8960 handle structure. | 
| playSource | play source , can be a value combine of kWM8960_ModuleHeadphoneSourcePGA, kWM8960_ModuleHeadphoneSourceDAC, kWM8960_ModulePlaySourceInput, kWM8960_ModulePlayMonoRight, kWM8960_ModulePlayMonoLeft. | 
| status_t WM8960_ConfigDataFormat | ( | wm8960_handle_t * | handle, | 
| uint32_t | sysclk, | ||
| uint32_t | sample_rate, | ||
| uint32_t | bits | ||
| ) | 
This function would configure the registers about the sample rate, bit depths.
| handle | WM8960 handle structure pointer. | 
| sysclk | system clock of the codec which can be generated by MCLK or PLL output. | 
| sample_rate | Sample rate of audio file running in WM8960. WM8960 now supports 8k, 11.025k, 12k, 16k, 22.05k, 24k, 32k, 44.1k, 48k and 96k sample rate. | 
| bits | Bit depth of audio file (WM8960 only supports 16bit, 20bit, 24bit and 32 bit in HW). | 
| status_t WM8960_SetJackDetect | ( | wm8960_handle_t * | handle, | 
| bool | isEnabled | ||
| ) | 
| handle | WM8960 handle structure. | 
| isEnabled | Enable or disable moudles. | 
| status_t WM8960_WriteReg | ( | wm8960_handle_t * | handle, | 
| uint8_t | reg, | ||
| uint16_t | val | ||
| ) | 
| handle | WM8960 handle structure. | 
| reg | The register address in WM8960. | 
| val | Value needs to write into the register. | 
| status_t WM8960_ReadReg | ( | uint8_t | reg, | 
| uint16_t * | val | ||
| ) | 
| reg | The register address in WM8960. | 
| val | Value written to. | 
| status_t WM8960_ModifyReg | ( | wm8960_handle_t * | handle, | 
| uint8_t | reg, | ||
| uint16_t | mask, | ||
| uint16_t | val | ||
| ) | 
| handle | WM8960 handle structure. | 
| reg | The register address in WM8960. | 
| mask | The mask code for the bits want to write. The bit you want to write should be 0. | 
| val | Value needs to write into the register. |