![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev 2.13.0
    
   NXP Semiconductors 
   | 
 
Macros | |
| #define | OSA_WAIT_FOREVER 0xFFFFFFFFU | 
| Constant to pass as timeout value in order to wait indefinitely.  More... | |
| #define | FSL_OSA_TIME_RANGE 0xFFFFFFFFU | 
| OSA's time range in millisecond, OSA time wraps if exceeds this value.  More... | |
| #define | OSA_DEFAULT_INT_HANDLER ((osa_int_handler_t)(&DefaultISR)) | 
| The default interrupt handler installed in vector table.  More... | |
Typedefs | |
| typedef TaskHandle_t | task_handler_t | 
| Type for a task handler, returned by the OSA_TaskCreate function.  More... | |
| typedef portSTACK_TYPE | task_stack_t | 
| Type for a task stack.  More... | |
| typedef void * | task_param_t | 
| Type for task parameter.  | |
| typedef EventBits_t | event_flags_t | 
| Type for an event flags object.  More... | |
Thread management | |
| #define | PRIORITY_OSA_TO_RTOS(osa_prio) (((UBaseType_t)configMAX_PRIORITIES - 1U) * (OSA_TASK_PRIORITY_MIN - osa_prio) / OSA_TASK_PRIORITY_MIN) | 
| To provide unified task piority for upper layer, OSA layer makes conversion.  | |
| #define | PRIORITY_RTOS_TO_OSA(rtos_prio) | 
Message queues | |
| #define | MSG_QUEUE_DECLARE(name, number, size) msg_queue_t *name = NULL | 
| This macro statically reserves the memory required for the queue.  More... | |
| #define OSA_WAIT_FOREVER 0xFFFFFFFFU | 
| #define FSL_OSA_TIME_RANGE 0xFFFFFFFFU | 
| #define OSA_DEFAULT_INT_HANDLER ((osa_int_handler_t)(&DefaultISR)) | 
| #define MSG_QUEUE_DECLARE | ( | name, | |
| number, | |||
| size | |||
| ) | msg_queue_t *name = NULL | 
| name | Identifier for the memory region. | 
| number | Number of elements in the queue. | 
| size | Size of every elements in words. | 
| typedef TaskHandle_t task_handler_t | 
| typedef portSTACK_TYPE task_stack_t | 
| typedef EventBits_t event_flags_t |