![]() |
MCUXpresso SDK API Reference Manual
Rev 2.13.1
NXP Semiconductors
|
Data Structures | |
| struct | flexio_camera_edma_handle_t |
| Camera eDMA handle. More... | |
Typedefs | |
| typedef void(* | flexio_camera_edma_transfer_callback_t )(FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle, status_t status, void *userData) |
| Camera transfer callback function. More... | |
Driver version | |
| #define | FSL_FLEXIO_CAMERA_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 3)) |
| FlexIO Camera EDMA driver version 2.1.3. More... | |
eDMA transactional | |
| status_t | FLEXIO_CAMERA_TransferCreateHandleEDMA (FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle, flexio_camera_edma_transfer_callback_t callback, void *userData, edma_handle_t *rxEdmaHandle) |
| Initializes the Camera handle, which is used in transactional functions. More... | |
| status_t | FLEXIO_CAMERA_TransferReceiveEDMA (FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle, flexio_camera_transfer_t *xfer) |
| Receives data using eDMA. More... | |
| void | FLEXIO_CAMERA_TransferAbortReceiveEDMA (FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle) |
| Aborts the receive data which used the eDMA. More... | |
| status_t | FLEXIO_CAMERA_TransferGetReceiveCountEDMA (FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle, size_t *count) |
| Gets the remaining bytes to be received. More... | |
| struct _flexio_camera_edma_handle |
Forward declaration of the handle typedef.
Data Fields | |
| flexio_camera_edma_transfer_callback_t | callback |
| Callback function. More... | |
| void * | userData |
| Camera callback function parameter. More... | |
| size_t | rxSize |
| Total bytes to be received. More... | |
| edma_handle_t * | rxEdmaHandle |
| The eDMA RX channel used. More... | |
| uint8_t | nbytes |
| eDMA minor byte transfer count initially configured. More... | |
| volatile uint8_t | rxState |
| RX transfer state. | |
| flexio_camera_edma_transfer_callback_t flexio_camera_edma_handle_t::callback |
| void* flexio_camera_edma_handle_t::userData |
| size_t flexio_camera_edma_handle_t::rxSize |
| edma_handle_t* flexio_camera_edma_handle_t::rxEdmaHandle |
| uint8_t flexio_camera_edma_handle_t::nbytes |
| #define FSL_FLEXIO_CAMERA_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 3)) |
| typedef void(* flexio_camera_edma_transfer_callback_t)(FLEXIO_CAMERA_Type *base, flexio_camera_edma_handle_t *handle, status_t status, void *userData) |
| status_t FLEXIO_CAMERA_TransferCreateHandleEDMA | ( | FLEXIO_CAMERA_Type * | base, |
| flexio_camera_edma_handle_t * | handle, | ||
| flexio_camera_edma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | rxEdmaHandle | ||
| ) |
| base | Pointer to the FLEXIO_CAMERA_Type. |
| handle | Pointer to flexio_camera_edma_handle_t structure. |
| callback | The callback function. |
| userData | The parameter of the callback function. |
| rxEdmaHandle | User requested DMA handle for RX DMA transfer. |
| kStatus_Success | Successfully create the handle. |
| kStatus_OutOfRange | The FlexIO Camera eDMA type/handle table out of range. |
| status_t FLEXIO_CAMERA_TransferReceiveEDMA | ( | FLEXIO_CAMERA_Type * | base, |
| flexio_camera_edma_handle_t * | handle, | ||
| flexio_camera_transfer_t * | xfer | ||
| ) |
This function receives data using eDMA. This is a non-blocking function, which returns right away. When all data is received, the receive callback function is called.
| base | Pointer to the FLEXIO_CAMERA_Type. |
| handle | Pointer to the flexio_camera_edma_handle_t structure. |
| xfer | Camera eDMA transfer structure, see flexio_camera_transfer_t. |
| kStatus_Success | if succeeded, others failed. |
| kStatus_CAMERA_RxBusy | Previous transfer on going. |
| void FLEXIO_CAMERA_TransferAbortReceiveEDMA | ( | FLEXIO_CAMERA_Type * | base, |
| flexio_camera_edma_handle_t * | handle | ||
| ) |
This function aborts the receive data which used the eDMA.
| base | Pointer to the FLEXIO_CAMERA_Type. |
| handle | Pointer to the flexio_camera_edma_handle_t structure. |
| status_t FLEXIO_CAMERA_TransferGetReceiveCountEDMA | ( | FLEXIO_CAMERA_Type * | base, |
| flexio_camera_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
This function gets the number of bytes still not received.
| base | Pointer to the FLEXIO_CAMERA_Type. |
| handle | Pointer to the flexio_camera_edma_handle_t structure. |
| count | Number of bytes sent so far by the non-blocking transaction. |
| kStatus_Success | Succeed get the transfer count. |
| kStatus_InvalidArgument | The count parameter is invalid. |