![]() |
MCUXpresso SDK API Reference Manual
Rev 2.13.1
NXP Semiconductors
|
This section describes the programming interface of the CAAM HASH driver.
Macros | |
| #define | CAAM_SHA_BLOCK_SIZE 128U |
| CAAM HASH Context size. More... | |
| #define | CAAM_HASH_BLOCK_SIZE CAAM_SHA_BLOCK_SIZE |
| CAAM hash block size. | |
| #define | CAAM_HASH_CTX_SIZE 58 |
| CAAM HASH Context size. More... | |
Typedefs | |
| typedef uint32_t | caam_hash_ctx_t [CAAM_HASH_CTX_SIZE] |
| Storage type used to save hash context. More... | |
Enumerations | |
| enum | caam_hash_algo_t { kCAAM_XcbcMac = 0, kCAAM_Cmac, kCAAM_Sha1, kCAAM_Sha224, kCAAM_Sha256, kCAAM_Sha384, kCAAM_Sha512 } |
| Supported cryptographic block cipher functions for HASH creation. More... | |
Functions | |
| status_t | CAAM_HASH_Init (CAAM_Type *base, caam_handle_t *handle, caam_hash_ctx_t *ctx, caam_hash_algo_t algo, const uint8_t *key, size_t keySize) |
| Initialize HASH context. More... | |
| status_t | CAAM_HASH_Update (caam_hash_ctx_t *ctx, const uint8_t *input, size_t inputSize) |
| Add data to current HASH. More... | |
| status_t | CAAM_HASH_Finish (caam_hash_ctx_t *ctx, uint8_t *output, size_t *outputSize) |
| Finalize hashing. More... | |
| status_t | CAAM_HASH (CAAM_Type *base, caam_handle_t *handle, caam_hash_algo_t algo, const uint8_t *input, size_t inputSize, const uint8_t *key, size_t keySize, uint8_t *output, size_t *outputSize) |
| Create HASH on given data. More... | |
| #define CAAM_SHA_BLOCK_SIZE 128U |
up to SHA-512 block size
| #define CAAM_HASH_CTX_SIZE 58 |
| typedef uint32_t caam_hash_ctx_t[CAAM_HASH_CTX_SIZE] |
| enum caam_hash_algo_t |
| status_t CAAM_HASH_Init | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| caam_hash_ctx_t * | ctx, | ||
| caam_hash_algo_t | algo, | ||
| const uint8_t * | key, | ||
| size_t | keySize | ||
| ) |
This function initializes the HASH. Key shall be supplied if the underlaying algoritm is AES XCBC-MAC or CMAC. Key shall be NULL if the underlaying algoritm is SHA.
For XCBC-MAC, the key length must be 16. For CMAC, the key length can be the AES key lengths supported by AES engine. For MDHA the key length argument is ignored.
This functions is used to initialize the context for both blocking and non-blocking CAAM_HASH API. For blocking CAAM HASH API, the HASH context contains all information required for context switch, such as running hash or MAC. For non-blocking CAAM HASH API, the HASH context is used to hold SGT. Therefore, the HASH context cannot be shared between blocking and non-blocking HASH API. With one HASH context, either use only blocking HASH API or only non-blocking HASH API.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. | |
| [out] | ctx | Output hash context |
| algo | Underlaying algorithm to use for hash computation. | |
| key | Input key (NULL if underlaying algorithm is SHA) | |
| keySize | Size of input key in bytes |
| status_t CAAM_HASH_Update | ( | caam_hash_ctx_t * | ctx, |
| const uint8_t * | input, | ||
| size_t | inputSize | ||
| ) |
Add data to current HASH. This can be called repeatedly with an arbitrary amount of data to be hashed. The functions blocks. If it returns kStatus_Success, the running hash or mac has been updated (CAAM has processed the input data), so the memory at input pointer can be released back to system. The context is updated with the running hash or mac and with all necessary information to support possible context switch.
| [in,out] | ctx | HASH context |
| input | Input data | |
| inputSize | Size of input data in bytes |
| status_t CAAM_HASH_Finish | ( | caam_hash_ctx_t * | ctx, |
| uint8_t * | output, | ||
| size_t * | outputSize | ||
| ) |
Outputs the final hash (computed by CAAM_HASH_Update()) and erases the context.
| [in,out] | ctx | Input hash context |
| [out] | output | Output hash data |
| [out] | outputSize | Output parameter storing the size of the output hash in bytes |
| status_t CAAM_HASH | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| caam_hash_algo_t | algo, | ||
| const uint8_t * | input, | ||
| size_t | inputSize, | ||
| const uint8_t * | key, | ||
| size_t | keySize, | ||
| uint8_t * | output, | ||
| size_t * | outputSize | ||
| ) |
Perform the full keyed XCBC-MAC/CMAC or SHA in one function call.
Key shall be supplied if the underlaying algoritm is AES XCBC-MAC or CMAC. Key shall be NULL if the underlaying algoritm is SHA.
For XCBC-MAC, the key length must be 16. For CMAC, the key length can be the AES key lengths supported by AES engine. For MDHA the key length argument is ignored.
The function is blocking.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. | |
| algo | Underlaying algorithm to use for hash computation. | |
| input | Input data | |
| inputSize | Size of input data in bytes | |
| key | Input key (NULL if underlaying algorithm is SHA) | |
| keySize | Size of input key in bytes | |
| [out] | output | Output hash data |
| [out] | outputSize | Output parameter storing the size of the output hash in bytes |