MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
DCDC: DCDC Converter

Overview

The MCUXpresso SDK provides a Peripheral driver for the DCDC Converter (DCDC) module of MCUXpresso SDK devices.

This section describes the programming interface of the DCDC Converter Peripheral driver.

The DCDC converter module is a switching mode DC-DC converter supporting Buck, Boost and Bypass mode. It could produce multiple switching outputs for SoC peripherals and external devices with high conversion efficiency. The converter can be operated in continuous or pulsed mode.

As a module to provide the power for hardware system, the DCDC would start working when the system is powered up before the software takes over SoC. Some important configuration like selecting BUCK/BOOST/BYPASS mode is done by board settings. Before software can access the DCDC's registers, DCDC are already working normally with default settings.

However, if the application needs to improve the DCDC's performance or change the default settings, DCDC driver would help. The DCDC's register can not be accessed by software before its initialization (open the clock gate). Then user can configure the hardware according to the application guide from RM.

Function groups

Initialization and deinitialization

This function group is to enable/disable the operations to DCDC module through the driver.

Status

Provides functions to get and clear the DCDC status.

Interrupts

Provides functions to enable/disable DCDC interrupts.

Misc control

Provides functions to set the DCDC's miscellaneous control.

Application guideline

Continuous mode

As guideline from RM, to have better efficiency and ripple. The following call is recommended:

dcdc_loop_control_config_t dcdcLoopCtrlConfigStruct;
DCDC_GetDefaultLoopControlConfig(&dcdcLoopCtrlConfigStruct);
dcdcLoopCtrlConfigStruct.enableDiffHysteresis = true; //DCDC_LOOPCTRL_EN_DF_HYST = 1
dcdcLoopCtrlConfigStruct.enableCommonHysteresis = true; //DCDC_LOOPCTRL_EN_CM_HYST = 1
dcdcLoopCtrlConfigStruct.enableInvertHysteresisSign = true; //DCDC_LOOPCTRL_HYST_SIGN = 1
DCDC_SetLoopControlConfig(DCDC, &dcdcLoopCtrlConfigStruct);

In boost mode, POSLIMIT_BOOST_IN is set to small value by default. To limit startup voltage, set it to 0x12 after startup, to provide high current to output, especially when battery voltage is low. The following call could be used.

Target voltage adjustment

To adjust target voltage of VDD1P8 and VDD1P5. The following code could be used:

DCDC_AdjustTargetVoltage(DCDC, vdd1p45Boost, vdd1p45Buck, vdd1p8); // Target voltage is unlocked.
// DCDC_STS_DC_OK bit will be de-asserted after target register changes.
// After output voltage settling to new target value, DCDC_STS_DC_OK will be asserted.
{
}

Pulsed mode

Before entering pulsed mode, the target voltage should be locked. Also, there are some recommended setting.

dcdc_low_power_config_t dcdcLpConfigStruct;
dcdc_loop_control_config_t dcdcLoopCtrlConfigStruct;
DCDC_GetDefaultLoopControlConfig(&dcdcLoopCtrlConfigStruct);
dcdcLoopCtrlConfigStruct.enableDiffHysteresis = true; //DCDC_LOOPCTRL_EN_DF_HYST = 1
dcdcLoopCtrlConfigStruct.enableCommonHysteresis = true; //DCDC_LOOPCTRL_EN_CM_HYST = 1
dcdcLoopCtrlConfigStruct.enableInvertHysteresisSign = true; //DCDC_LOOPCTRL_HYST_SIGN = 1
DCDC_SetLoopControlConfig(DCDC, &dcdcLoopCtrlConfigStruct);
DCDC_GetDefaultLowPowerConfig(&dcdcLpConfigStruct);
dcdcLpConfigStruct.enableDiffComparators = true;
DCDC_SetLowPowerConfig(DCDC, &dcdcLpConfigStruct)
// Enter low power mode.

Data Structures

struct  dcdc_low_power_config_t
 Configuration for the low power. More...
 
struct  dcdc_loop_control_config_t
 Configuration for the loop control. More...
 
struct  dcdc_min_power_config_t
 Configuration for min power setting. More...
 
struct  dcdc_pulsed_integrator_config_t
 Configuration for the integrator in pulsed mode. More...
 

Macros

#define FSL_DCDC_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))
 DCDC driver version. More...
 

Enumerations

enum  _dcdc_status_flags_t {
  kDCDC_LockedOKStatus = (1U << 0),
  kDCDC_PSwitchStatus = (1U << 1),
  kDCDC_PSwitchInterruptStatus = (1U << 2)
}
 Status flags. More...
 
enum  _dcdc_interrupt_enable_t { kDCDC_PSwitchEdgeDetectInterruptEnable = DCDC_REG6_PSWITCH_INT_MUTE_MASK }
 Interrupts. More...
 
enum  _dcdc_pswitch_detect_event_t {
  kDCDC_PSwitchFallingEdgeDetectEnable = DCDC_REG6_PSWITCH_INT_FALL_EN_MASK,
  kDCDC_PSwitchRisingEdgeDetectEnable = DCDC_REG6_PSWITCH_INT_RISE_EN_MASK
}
 Events for PSWITCH signal(pin). More...
 
enum  dcdc_work_mode_t {
  kDCDC_WorkInContinuousMode = 0U,
  kDCDC_WorkInPulsedMode = 1U
}
 DCDC work mode in SoC's low power condition. More...
 
enum  dcdc_hysteretic_threshold_offset_value_t {
  kDCDC_HystereticThresholdOffset0mV = 0U,
  kDCDC_HystereticThresholdOffset25mV = 1U,
  kDCDC_HystereticThresholdOffset50mV = 2U,
  kDCDC_HystereticThresholdOffset75mV = 3U
}
 Hysteretic upper/lower threshold value in low power mode. More...
 
enum  dcdc_vbat_divider_t {
  kDCDC_VBatVoltageDividerOff = 0U,
  kDCDC_VBatVoltageDivider1 = 1U,
  kDCDC_VBatVoltageDivider2 = 2U,
  kDCDC_VBatVoltageDivider4 = 3U
}
 VBAT voltage divider. More...
 
enum  dcdc_clock_source_t { kDCDC_ClockAutoSwitch = 0U }
 Oscillator clock option. More...
 

Initialization and deinitialization

void DCDC_Init (DCDC_Type *base)
 Enable the access to DCDC registers. More...
 
void DCDC_Deinit (DCDC_Type *base)
 Disable the access to DCDC registers. More...
 

Status

uint32_t DCDC_GetStatusFlags (DCDC_Type *base)
 Get status flags. More...
 
void DCDC_ClearStatusFlags (DCDC_Type *base, uint32_t mask)
 Clear status flags. More...
 

Interrupts

static void DCDC_EnableInterrupts (DCDC_Type *base, uint32_t mask)
 Enable interrupts. More...
 
static void DCDC_DisableInterrupts (DCDC_Type *base, uint32_t mask)
 Disable interrupts. More...
 
void DCDC_SetPSwitchInterruptConfig (DCDC_Type *base, uint32_t mask)
 Configure the PSWITCH interrupts. More...
 

Misc control.

void DCDC_GetDefaultLowPowerConfig (dcdc_low_power_config_t *config)
 Get the default setting for low power configuration. More...
 
void DCDC_SetLowPowerConfig (DCDC_Type *base, const dcdc_low_power_config_t *config)
 Configure the low power for DCDC. More...
 
void DCDC_GetDefaultLoopControlConfig (dcdc_loop_control_config_t *config)
 Get the default setting for loop control configuration. More...
 
void DCDC_SetLoopControlConfig (DCDC_Type *base, const dcdc_loop_control_config_t *config)
 Configure the loop control for DCDC. More...
 
static void DCDC_EnableXtalOKDetectionCircuit (DCDC_Type *base, bool enable)
 Enable the XTAL OK detection circuit. More...
 
static void DCDC_EnableOutputRangeComparator (DCDC_Type *base, bool enable)
 Enable the output range comparator. More...
 
static void DCDC_EnableReduceCurrent (DCDC_Type *base, bool enable)
 Enable to reduce the DCDC current. More...
 
void DCDC_SetClockSource (DCDC_Type *base, dcdc_clock_source_t clockSource)
 Set the clock source for DCDC. More...
 
static void DCDC_SetBatteryVoltageDivider (DCDC_Type *base, dcdc_vbat_divider_t divider)
 Set the battery voltage divider for ADC sample. More...
 
void DCDC_SetBatteryMonitorValue (DCDC_Type *base, uint32_t battValue)
 Set battery monitor value. More...
 
static void DCDC_DoSoftShutdown (DCDC_Type *base)
 Software shutdown the DCDC module to stop the power supply for chip. More...
 
static void DCDC_SetUpperLimitDutyCycleBoost (DCDC_Type *base, uint32_t value)
 Set upper limit duty cycle limit in DCDC converter in Boost mode. More...
 
static void DCDC_SetUpperLimitDutyCycleBuck (DCDC_Type *base, uint32_t value)
 Set upper limit duty cycle limit in DCDC converter in Buck mode. More...
 
static void DCDC_AdjustDutyCycleSwitchingTargetOutput (DCDC_Type *base, uint32_t value)
 Adjust value of duty cycle when switching between VDD1P45 and VDD1P8. More...
 
static void DCDC_LockTargetVoltage (DCDC_Type *base)
 Lock the setting of target voltage. More...
 
void DCDC_AdjustTargetVoltage (DCDC_Type *base, uint32_t vdd1p5xBoost, uint32_t vdd1p5xBuck, uint32_t vdd1p8)
 Adjust the target voltage of DCDC output. More...
 
void DCDC_GetDefaultMinPowerDefault (dcdc_min_power_config_t *config)
 Get the default configuration for min power. More...
 
void DCDC_SetMinPowerConfig (DCDC_Type *base, const dcdc_min_power_config_t *config)
 Configure for the min power. More...
 
void DCDC_GetDefaultPulsedIntegratorConfig (dcdc_pulsed_integrator_config_t *config)
 Get the default setting for integrator configuration in pulsed mode. More...
 
void DCDC_SetPulsedIntegratorConfig (DCDC_Type *base, const dcdc_pulsed_integrator_config_t *config)
 Configure the integrator in pulsed mode. More...
 

Data Structure Documentation

struct dcdc_low_power_config_t

Data Fields

dcdc_work_mode_t workModeInVLPRW
 Select the behavior of DCDC in device VLPR and VLPW low power modes. More...
 
dcdc_work_mode_t workModeInVLPS
 Select the behavior of DCDC in device VLPS low power modes. More...
 
bool enableHysteresisVoltageSense
 Enable hysteresis in low power voltage sense. More...
 
bool enableAdjustHystereticValueSense
 Adjust hysteretic value in low power voltage sense. More...
 
bool enableHystersisComparator
 Enable hysteresis in low power comparator. More...
 
bool enableAdjustHystereticValueComparator
 Adjust hysteretic value in low power comparator. More...
 
dcdc_hysteretic_threshold_offset_value_t hystereticUpperThresholdValue
 Configure the hysteretic upper threshold value in low power mode. More...
 
dcdc_hysteretic_threshold_offset_value_t hystereticLowerThresholdValue
 Configure the hysteretic lower threshold value in low power mode. More...
 
bool enableDiffComparators
 Enable low power differential comparators, to sense lower supply in pulsed mode. More...
 

Field Documentation

dcdc_work_mode_t dcdc_low_power_config_t::workModeInVLPRW
dcdc_work_mode_t dcdc_low_power_config_t::workModeInVLPS
bool dcdc_low_power_config_t::enableHysteresisVoltageSense
bool dcdc_low_power_config_t::enableAdjustHystereticValueSense
bool dcdc_low_power_config_t::enableHystersisComparator
bool dcdc_low_power_config_t::enableAdjustHystereticValueComparator
dcdc_hysteretic_threshold_offset_value_t dcdc_low_power_config_t::hystereticUpperThresholdValue
dcdc_hysteretic_threshold_offset_value_t dcdc_low_power_config_t::hystereticLowerThresholdValue
bool dcdc_low_power_config_t::enableDiffComparators
struct dcdc_loop_control_config_t

Data Fields

bool enableDiffHysteresis
 Enable hysteresis in switching converter differential mode analog comparators. More...
 
bool enableCommonHysteresis
 Enable hysteresis in switching converter common mode analog comparators. More...
 
bool enableDiffHysteresisThresh
 This field act the same rule as enableDiffHysteresis. More...
 
bool enableCommonHysteresisThresh
 This field act the same rule as enableCommonHysteresis. More...
 
bool enableInvertHysteresisSign
 Invert the sign of the hysteresis in DC-DC analog comparators. More...
 

Field Documentation

bool dcdc_loop_control_config_t::enableDiffHysteresis

This feature improves transient supply ripple and efficiency.

bool dcdc_loop_control_config_t::enableCommonHysteresis

This feature improves transient supply ripple and efficiency.

bool dcdc_loop_control_config_t::enableDiffHysteresisThresh

However, if this field is enabled along with the enableDiffHysteresis, the Hysteresis would be doubled.

bool dcdc_loop_control_config_t::enableCommonHysteresisThresh

However, if this field is enabled along with the enableCommonHysteresis, the Hysteresis would be doubled.

bool dcdc_loop_control_config_t::enableInvertHysteresisSign
struct dcdc_min_power_config_t

Data Fields

bool enableUseHalfFetForContinuous
 Use half switch FET for the continuous mode. More...
 
bool enableUseDoubleFetForContinuous
 Use double switch FET for the continuous mode. More...
 
bool enableUseHalfFreqForContinuous
 Set DCDC clock to half frequency for the continuous mode. More...
 
bool enableUseHalfFetForPulsed
 Use half switch FET for the Pulsed mode. More...
 
bool enableUseDoubleFetForPulsed
 Use double switch FET for the Pulsed mode. More...
 
bool enableUseHalfFreqForPulsed
 Set DCDC clock to half frequency for the Pulsed mode. More...
 

Field Documentation

bool dcdc_min_power_config_t::enableUseHalfFetForContinuous
bool dcdc_min_power_config_t::enableUseDoubleFetForContinuous
bool dcdc_min_power_config_t::enableUseHalfFreqForContinuous
bool dcdc_min_power_config_t::enableUseHalfFetForPulsed
bool dcdc_min_power_config_t::enableUseDoubleFetForPulsed
bool dcdc_min_power_config_t::enableUseHalfFreqForPulsed
struct dcdc_pulsed_integrator_config_t

Data Fields

bool enableUseUserIntegratorValue
 Enable to use the setting value in userIntegratorValue field. More...
 
uint32_t userIntegratorValue
 User defined integrator value. More...
 
bool enablePulseRunSpeedup
 Enable pulse run speedup. More...
 

Field Documentation

bool dcdc_pulsed_integrator_config_t::enableUseUserIntegratorValue

Otherwise, the predefined hardware setting would be applied internally.

uint32_t dcdc_pulsed_integrator_config_t::userIntegratorValue

The available value is 19-bit.

bool dcdc_pulsed_integrator_config_t::enablePulseRunSpeedup

Macro Definition Documentation

#define FSL_DCDC_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))

Version 2.0.1.

Enumeration Type Documentation

Enumerator
kDCDC_LockedOKStatus 

Status to indicate DCDC lock.

Read only bit.

kDCDC_PSwitchStatus 

Status to indicate PSWITCH signal.

Read only bit.

kDCDC_PSwitchInterruptStatus 

PSWITCH edge detection interrupt status.

Enumerator
kDCDC_PSwitchEdgeDetectInterruptEnable 

Enable the edge detect interrupt.

Enumerator
kDCDC_PSwitchFallingEdgeDetectEnable 

Enable falling edge detect.

kDCDC_PSwitchRisingEdgeDetectEnable 

Enable rising edge detect.

Enumerator
kDCDC_WorkInContinuousMode 

DCDC works in continuous mode when SOC is in low power mode.

kDCDC_WorkInPulsedMode 

DCDC works in pulsed mode when SOC is in low power mode.

Enumerator
kDCDC_HystereticThresholdOffset0mV 

Target voltage value +/- 0mV.

kDCDC_HystereticThresholdOffset25mV 

Target voltage value +/- 25mV.

kDCDC_HystereticThresholdOffset50mV 

Target voltage value +/- 50mV.

kDCDC_HystereticThresholdOffset75mV 

Target voltage value +/- 75mV.

Enumerator
kDCDC_VBatVoltageDividerOff 

The sensor signal is disabled.

kDCDC_VBatVoltageDivider1 

VBat.

kDCDC_VBatVoltageDivider2 

VBat/2.

kDCDC_VBatVoltageDivider4 

VBat/4.

Enumerator
kDCDC_ClockAutoSwitch 

Automatic clock switch from internal oscillator to external clock.

Function Documentation

void DCDC_Init ( DCDC_Type *  base)
Parameters
baseDCDC peripheral base address.
void DCDC_Deinit ( DCDC_Type *  base)
Parameters
baseDCDC peripheral base address.
uint32_t DCDC_GetStatusFlags ( DCDC_Type *  base)

base DCDC peripheral base address.

Returns
Masks of asserted status flags. See to "_dcdc_status_flags_t".
void DCDC_ClearStatusFlags ( DCDC_Type *  base,
uint32_t  mask 
)

base DCDC peripheral base address. mask Mask of status values that would be cleared. See to "_dcdc_status_flags_t".

static void DCDC_EnableInterrupts ( DCDC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseDCDC peripheral base address.
maskMask of interrupt events that would be enabled. See to "_dcdc_interrupt_enable_t".
static void DCDC_DisableInterrupts ( DCDC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseDCDC peripheral base address.
maskMask of interrupt events that would be disabled. See to "_dcdc_interrupt_enable_t".
void DCDC_SetPSwitchInterruptConfig ( DCDC_Type *  base,
uint32_t  mask 
)

There are PSWITCH interrupt events can be triggered by falling edge or rising edge. So user can set the interrupt events that would be triggered with this function. Un-asserted events would be disabled. The interrupt of PSwitch should be enabled as well if to sense the PSWTICH event. By default, no interrupt events would be enabled.

Parameters
baseDCDC peripheral base address.
maskMask of interrupt events for PSwtich. See to "_dcdc_pswitch_detect_event_t".
void DCDC_GetDefaultLowPowerConfig ( dcdc_low_power_config_t *  config)

The default configuration are set according to responding registers' setting when powered on. They are:

* config->workModeInVLPRW = kDCDC_WorkInPulsedMode;
* config->workModeInVLPS = kDCDC_WorkInPulsedMode;
* config->enableHysteresisVoltageSense = true;
* config->enableAdjustHystereticValueSense = false;
* config->enableHystersisComparator = true;
* config->enableAdjustHystereticValueComparator = false;
* config->hystereticUpperThresholdValue = kDCDC_HystereticThresholdOffset75mV;
* config->hystereticLowerThresholdValue = kDCDC_HystereticThresholdOffset0mV;
* config->enableDiffComparators = false;
*
Parameters
configPointer to configuration structure. See to "dcdc_low_power_config_t".
void DCDC_SetLowPowerConfig ( DCDC_Type *  base,
const dcdc_low_power_config_t *  config 
)
Parameters
baseDCDC peripheral base address.
configPointer to configuration structure. See to "dcdc_low_power_config_t".
void DCDC_GetDefaultLoopControlConfig ( dcdc_loop_control_config_t *  config)

The default configuration are set according to responding registers' setting when powered on. They are:

* config->enableDiffHysteresis = false;
* config->enableCommonHysteresis = false;
* config->enableDiffHysteresisThresh = false;
* config->enableCommonHysteresisThresh = false;
* config->enableInvertHysteresisSign = false;
*
Parameters
configPointer to configuration structure. See to "dcdc_loop_control_config_t".
void DCDC_SetLoopControlConfig ( DCDC_Type *  base,
const dcdc_loop_control_config_t *  config 
)
Parameters
baseDCDC peripheral base address.
configPointer to configuration structure. See to "dcdc_loop_control_config_t".
static void DCDC_EnableXtalOKDetectionCircuit ( DCDC_Type *  base,
bool  enable 
)
inlinestatic

The XTAL OK detection circuit is enabled by default.

Parameters
baseDCDC peripheral base address.
enableEnable the feature or not.
static void DCDC_EnableOutputRangeComparator ( DCDC_Type *  base,
bool  enable 
)
inlinestatic

The output range comparator is enabled by default.

Parameters
baseDCDC peripheral base address.
enableEnable the feature or not.
static void DCDC_EnableReduceCurrent ( DCDC_Type *  base,
bool  enable 
)
inlinestatic

To enable this feature will save approximately 20 µA in RUN mode. This feature is disabled by default.

Parameters
baseDCDC peripheral base address.
enableEnable the feature or not.
void DCDC_SetClockSource ( DCDC_Type *  base,
dcdc_clock_source_t  clockSource 
)

This function is to set the clock source for DCDC. By default, DCDC can switch the clock from internal oscillator to external clock automatically. Once the application chooses to use the external clock with function, the internal oscillator would be powered down. However, the internal oscillator could be powered down only when 32MHz crystal oscillator is available.

Parameters
baseDCDC peripheral base address.
clockSourceClock source for DCDC. See to "dcdc_clock_source_t".
static void DCDC_SetBatteryVoltageDivider ( DCDC_Type *  base,
dcdc_vbat_divider_t  divider 
)
inlinestatic

This function controls VBAT voltage divider. The divided VBAT output is input to an ADC channel which allows the battery voltage to be measured.

Parameters
baseDCDC peripheral base address.
dividerSetting divider selection. See to "dcdc_vbat_divider_t"
void DCDC_SetBatteryMonitorValue ( DCDC_Type *  base,
uint32_t  battValue 
)

This function is to set the battery monitor value. If the feature of monitoring battery voltage is enabled (with non-zero value set), user should set the battery voltage measured with an 8 mV LSB resolution from the ADC sample channel. It would improve efficiency and minimize ripple.

Parameters
baseDCDC peripheral base address.
battValueBattery voltage measured with an 8 mV LSB resolution with 10-bit ADC sample. Setting 0x0 would disable feature of monitoring battery voltage.
static void DCDC_DoSoftShutdown ( DCDC_Type *  base)
inlinestatic

This function is to shutdown the DCDC module and stop the power supply for chip. Shutdown is only allowed in Buck mode, Manual start and PSWITCH must be at logic zero.

Parameters
baseDCDC peripheral base address.
static void DCDC_SetUpperLimitDutyCycleBoost ( DCDC_Type *  base,
uint32_t  value 
)
inlinestatic
Parameters
baseDCDC peripheral base address.
valueSetting value for limit duty cycle. Available range is 0-127.
static void DCDC_SetUpperLimitDutyCycleBuck ( DCDC_Type *  base,
uint32_t  value 
)
inlinestatic
Parameters
baseDCDC peripheral base address.
valueSetting value for limit duty cycle. Available range is 0-127.
static void DCDC_AdjustDutyCycleSwitchingTargetOutput ( DCDC_Type *  base,
uint32_t  value 
)
inlinestatic

Adjust value of duty cycle when switching between VDD1P45 and VDD1P8. The unit is 1/32 or 3.125%.

Parameters
baseDCDC peripheral base address.
valueSetting adjust value. The available range is 0-15. The unit is 1/32 or 3.125&.
static void DCDC_LockTargetVoltage ( DCDC_Type *  base)
inlinestatic

This function is to lock the setting of target voltage. This function should be called before entering the low power modes to lock the target voltage.

Parameters
baseDCDC peripheral base address.
void DCDC_AdjustTargetVoltage ( DCDC_Type *  base,
uint32_t  vdd1p5xBoost,
uint32_t  vdd1p5xBuck,
uint32_t  vdd1p8 
)

This function is to adjust the target voltage of DCDC output. It would unlock the setting of target voltages, change them and finally wait until the output is stabled.

Parameters
baseDCDC peripheral base address.
vdd1p5xBoostTarget value of VDD1P5X in boost mode, 25 mV each step from 0x00 to 0x0F. 0x00 is for 1.275V.
vdd1p5xBuckTarget value of VDD1P5X in buck mode, 25 mV each step from 0x00 to 0x0F. 0x00 is for 1.275V.
vdd1p8Target value of VDD1P8, 25 mV each step in two ranges, from 0x00 to 0x11 and 0x20 to 0x3F and 50 mV each step in range from 0x12 to 0x1F. 0x00 is for 1.65V, 0x20 is for 2.8V.
void DCDC_GetDefaultMinPowerDefault ( dcdc_min_power_config_t *  config)

The default configuration are set according to responding registers' setting when powered on. They are:

* config->enableUseHalfFetForContinuous = false;
* config->enableUseDoubleFetForContinuous = false;
* config->enableUseHalfFreqForContinuous = false;
* config->enableUseHalfFetForPulsed = false;
* config->enableUseDoubleFetForPulsed = false;
* config->enableUseHalfFreqForPulsed = false;
*
Parameters
configPointer to configuration structure. See to "dcdc_min_power_config_t".
void DCDC_SetMinPowerConfig ( DCDC_Type *  base,
const dcdc_min_power_config_t *  config 
)
Parameters
baseDCDC peripheral base address.
configPointer to configuration structure. See to "dcdc_min_power_config_t".
void DCDC_GetDefaultPulsedIntegratorConfig ( dcdc_pulsed_integrator_config_t *  config)

The default configuration are set according to responding registers' setting when powered on. They are:

* config->enableUseUserIntegratorValue = false;
* config->userIntegratorValue = 0U;
* config->enablePulseRunSpeedup = false;
*
Parameters
configPointer to configuration structure. See to "dcdc_pulsed_integrator_config_t".
void DCDC_SetPulsedIntegratorConfig ( DCDC_Type *  base,
const dcdc_pulsed_integrator_config_t *  config 
)
Parameters
baseDCDC peripheral base address. Pointer to configuration structure. See to "dcdc_pulsed_integrator_config_t".