![]() |
MCUXpresso SDK API Reference Manual
Rev 2.14.0
NXP Semiconductors
|
Data Structures | |
struct | flexio_i2s_edma_handle_t |
FlexIO I2S DMA transfer handle, users should not touch the content of the handle. More... | |
Typedefs | |
typedef void(* | flexio_i2s_edma_callback_t )(FLEXIO_I2S_Type *base, flexio_i2s_edma_handle_t *handle, status_t status, void *userData) |
FlexIO I2S eDMA transfer callback function for finish and error. | |
Driver version | |
#define | FSL_FLEXIO_I2S_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 7)) |
FlexIO I2S EDMA driver version 2.1.7. More... | |
eDMA Transactional | |
void | FLEXIO_I2S_TransferTxCreateHandleEDMA (FLEXIO_I2S_Type *base, flexio_i2s_edma_handle_t *handle, flexio_i2s_edma_callback_t callback, void *userData, edma_handle_t *dmaHandle) |
Initializes the FlexIO I2S eDMA handle. More... | |
void | FLEXIO_I2S_TransferRxCreateHandleEDMA (FLEXIO_I2S_Type *base, flexio_i2s_edma_handle_t *handle, flexio_i2s_edma_callback_t callback, void *userData, edma_handle_t *dmaHandle) |
Initializes the FlexIO I2S Rx eDMA handle. More... | |
void | FLEXIO_I2S_TransferSetFormatEDMA (FLEXIO_I2S_Type *base, flexio_i2s_edma_handle_t *handle, flexio_i2s_format_t *format, uint32_t srcClock_Hz) |
Configures the FlexIO I2S Tx audio format. More... | |
status_t | FLEXIO_I2S_TransferSendEDMA (FLEXIO_I2S_Type *base, flexio_i2s_edma_handle_t *handle, flexio_i2s_transfer_t *xfer) |
Performs a non-blocking FlexIO I2S transfer using DMA. More... | |
status_t | FLEXIO_I2S_TransferReceiveEDMA (FLEXIO_I2S_Type *base, flexio_i2s_edma_handle_t *handle, flexio_i2s_transfer_t *xfer) |
Performs a non-blocking FlexIO I2S receive using eDMA. More... | |
void | FLEXIO_I2S_TransferAbortSendEDMA (FLEXIO_I2S_Type *base, flexio_i2s_edma_handle_t *handle) |
Aborts a FlexIO I2S transfer using eDMA. More... | |
void | FLEXIO_I2S_TransferAbortReceiveEDMA (FLEXIO_I2S_Type *base, flexio_i2s_edma_handle_t *handle) |
Aborts a FlexIO I2S receive using eDMA. More... | |
status_t | FLEXIO_I2S_TransferGetSendCountEDMA (FLEXIO_I2S_Type *base, flexio_i2s_edma_handle_t *handle, size_t *count) |
Gets the remaining bytes to be sent. More... | |
status_t | FLEXIO_I2S_TransferGetReceiveCountEDMA (FLEXIO_I2S_Type *base, flexio_i2s_edma_handle_t *handle, size_t *count) |
Get the remaining bytes to be received. More... | |
struct _flexio_i2s_edma_handle |
Data Fields | |
edma_handle_t * | dmaHandle |
DMA handler for FlexIO I2S send. | |
uint8_t | bytesPerFrame |
Bytes in a frame. | |
uint8_t | nbytes |
eDMA minor byte transfer count initially configured. More... | |
uint32_t | state |
Internal state for FlexIO I2S eDMA transfer. | |
flexio_i2s_edma_callback_t | callback |
Callback for users while transfer finish or error occurred. | |
void * | userData |
User callback parameter. | |
edma_tcd_t | tcd [FLEXIO_I2S_XFER_QUEUE_SIZE+1U] |
TCD pool for eDMA transfer. More... | |
flexio_i2s_transfer_t | queue [FLEXIO_I2S_XFER_QUEUE_SIZE] |
Transfer queue storing queued transfer. More... | |
size_t | transferSize [FLEXIO_I2S_XFER_QUEUE_SIZE] |
Data bytes need to transfer. | |
volatile uint8_t | queueUser |
Index for user to queue transfer. More... | |
volatile uint8_t | queueDriver |
Index for driver to get the transfer data and size. | |
uint8_t flexio_i2s_edma_handle_t::nbytes |
edma_tcd_t flexio_i2s_edma_handle_t::tcd[FLEXIO_I2S_XFER_QUEUE_SIZE+1U] |
flexio_i2s_transfer_t flexio_i2s_edma_handle_t::queue[FLEXIO_I2S_XFER_QUEUE_SIZE] |
volatile uint8_t flexio_i2s_edma_handle_t::queueUser |
#define FSL_FLEXIO_I2S_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 7)) |
void FLEXIO_I2S_TransferTxCreateHandleEDMA | ( | FLEXIO_I2S_Type * | base, |
flexio_i2s_edma_handle_t * | handle, | ||
flexio_i2s_edma_callback_t | callback, | ||
void * | userData, | ||
edma_handle_t * | dmaHandle | ||
) |
This function initializes the FlexIO I2S master DMA handle which can be used for other FlexIO I2S master transactional APIs. Usually, for a specified FlexIO I2S instance, call this API once to get the initialized handle.
base | FlexIO I2S peripheral base address. |
handle | FlexIO I2S eDMA handle pointer. |
callback | FlexIO I2S eDMA callback function called while finished a block. |
userData | User parameter for callback. |
dmaHandle | eDMA handle for FlexIO I2S. This handle is a static value allocated by users. |
void FLEXIO_I2S_TransferRxCreateHandleEDMA | ( | FLEXIO_I2S_Type * | base, |
flexio_i2s_edma_handle_t * | handle, | ||
flexio_i2s_edma_callback_t | callback, | ||
void * | userData, | ||
edma_handle_t * | dmaHandle | ||
) |
This function initializes the FlexIO I2S slave DMA handle which can be used for other FlexIO I2S master transactional APIs. Usually, for a specified FlexIO I2S instance, call this API once to get the initialized handle.
base | FlexIO I2S peripheral base address. |
handle | FlexIO I2S eDMA handle pointer. |
callback | FlexIO I2S eDMA callback function called while finished a block. |
userData | User parameter for callback. |
dmaHandle | eDMA handle for FlexIO I2S. This handle is a static value allocated by users. |
void FLEXIO_I2S_TransferSetFormatEDMA | ( | FLEXIO_I2S_Type * | base, |
flexio_i2s_edma_handle_t * | handle, | ||
flexio_i2s_format_t * | format, | ||
uint32_t | srcClock_Hz | ||
) |
Audio format can be changed in run-time of FlexIO I2S. This function configures the sample rate and audio data format to be transferred. This function also sets the eDMA parameter according to format.
base | FlexIO I2S peripheral base address. |
handle | FlexIO I2S eDMA handle pointer |
format | Pointer to FlexIO I2S audio data format structure. |
srcClock_Hz | FlexIO I2S clock source frequency in Hz, it should be 0 while in slave mode. |
status_t FLEXIO_I2S_TransferSendEDMA | ( | FLEXIO_I2S_Type * | base, |
flexio_i2s_edma_handle_t * | handle, | ||
flexio_i2s_transfer_t * | xfer | ||
) |
base | FlexIO I2S peripheral base address. |
handle | FlexIO I2S DMA handle pointer. |
xfer | Pointer to DMA transfer structure. |
kStatus_Success | Start a FlexIO I2S eDMA send successfully. |
kStatus_InvalidArgument | The input arguments is invalid. |
kStatus_TxBusy | FlexIO I2S is busy sending data. |
status_t FLEXIO_I2S_TransferReceiveEDMA | ( | FLEXIO_I2S_Type * | base, |
flexio_i2s_edma_handle_t * | handle, | ||
flexio_i2s_transfer_t * | xfer | ||
) |
base | FlexIO I2S peripheral base address. |
handle | FlexIO I2S DMA handle pointer. |
xfer | Pointer to DMA transfer structure. |
kStatus_Success | Start a FlexIO I2S eDMA receive successfully. |
kStatus_InvalidArgument | The input arguments is invalid. |
kStatus_RxBusy | FlexIO I2S is busy receiving data. |
void FLEXIO_I2S_TransferAbortSendEDMA | ( | FLEXIO_I2S_Type * | base, |
flexio_i2s_edma_handle_t * | handle | ||
) |
base | FlexIO I2S peripheral base address. |
handle | FlexIO I2S DMA handle pointer. |
void FLEXIO_I2S_TransferAbortReceiveEDMA | ( | FLEXIO_I2S_Type * | base, |
flexio_i2s_edma_handle_t * | handle | ||
) |
base | FlexIO I2S peripheral base address. |
handle | FlexIO I2S DMA handle pointer. |
status_t FLEXIO_I2S_TransferGetSendCountEDMA | ( | FLEXIO_I2S_Type * | base, |
flexio_i2s_edma_handle_t * | handle, | ||
size_t * | count | ||
) |
base | FlexIO I2S peripheral base address. |
handle | FlexIO I2S DMA handle pointer. |
count | Bytes sent. |
kStatus_Success | Succeed get the transfer count. |
kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress. |
status_t FLEXIO_I2S_TransferGetReceiveCountEDMA | ( | FLEXIO_I2S_Type * | base, |
flexio_i2s_edma_handle_t * | handle, | ||
size_t * | count | ||
) |
base | FlexIO I2S peripheral base address. |
handle | FlexIO I2S DMA handle pointer. |
count | Bytes received. |
kStatus_Success | Succeed get the transfer count. |
kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress. |