MCUXpresso SDK API Reference Manual  Rev 2.14.0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

Data Structures

struct  uart_sdma_handle_t
 UART sDMA handle. More...
 

Typedefs

typedef void(* uart_sdma_transfer_callback_t )(UART_Type *base, uart_sdma_handle_t *handle, status_t status, void *userData)
 UART transfer callback function. More...
 

Driver version

#define FSL_UART_SDMA_DRIVER_VERSION   (MAKE_VERSION(2, 3, 0))
 UART SDMA driver version. More...
 

sDMA transactional

void UART_TransferCreateHandleSDMA (UART_Type *base, uart_sdma_handle_t *handle, uart_sdma_transfer_callback_t callback, void *userData, sdma_handle_t *txSdmaHandle, sdma_handle_t *rxSdmaHandle, uint32_t eventSourceTx, uint32_t eventSourceRx)
 Initializes the UART handle which is used in transactional functions. More...
 
status_t UART_SendSDMA (UART_Type *base, uart_sdma_handle_t *handle, uart_transfer_t *xfer)
 Sends data using sDMA. More...
 
status_t UART_ReceiveSDMA (UART_Type *base, uart_sdma_handle_t *handle, uart_transfer_t *xfer)
 Receives data using sDMA. More...
 
void UART_TransferAbortSendSDMA (UART_Type *base, uart_sdma_handle_t *handle)
 Aborts the sent data using sDMA. More...
 
void UART_TransferAbortReceiveSDMA (UART_Type *base, uart_sdma_handle_t *handle)
 Aborts the receive data using sDMA. More...
 
void UART_TransferSdmaHandleIRQ (UART_Type *base, void *uartSdmaHandle)
 UART IRQ handle function. More...
 

Data Structure Documentation

struct _uart_sdma_handle

Data Fields

uart_sdma_transfer_callback_t callback
 Callback function. More...
 
void * userData
 UART callback function parameter. More...
 
size_t rxDataSizeAll
 Size of the data to receive. More...
 
size_t txDataSizeAll
 Size of the data to send out. More...
 
sdma_handle_t * txSdmaHandle
 The sDMA TX channel used. More...
 
sdma_handle_t * rxSdmaHandle
 The sDMA RX channel used. More...
 
volatile uint8_t txState
 TX transfer state. More...
 
volatile uint8_t rxState
 RX transfer state.
 

Field Documentation

uart_sdma_transfer_callback_t uart_sdma_handle_t::callback
void* uart_sdma_handle_t::userData
size_t uart_sdma_handle_t::rxDataSizeAll
size_t uart_sdma_handle_t::txDataSizeAll
sdma_handle_t* uart_sdma_handle_t::txSdmaHandle
sdma_handle_t* uart_sdma_handle_t::rxSdmaHandle
volatile uint8_t uart_sdma_handle_t::txState

Macro Definition Documentation

#define FSL_UART_SDMA_DRIVER_VERSION   (MAKE_VERSION(2, 3, 0))

Typedef Documentation

typedef void(* uart_sdma_transfer_callback_t)(UART_Type *base, uart_sdma_handle_t *handle, status_t status, void *userData)

Function Documentation

void UART_TransferCreateHandleSDMA ( UART_Type *  base,
uart_sdma_handle_t *  handle,
uart_sdma_transfer_callback_t  callback,
void *  userData,
sdma_handle_t *  txSdmaHandle,
sdma_handle_t *  rxSdmaHandle,
uint32_t  eventSourceTx,
uint32_t  eventSourceRx 
)
Parameters
baseUART peripheral base address.
handlePointer to the uart_sdma_handle_t structure.
callbackUART callback, NULL means no callback.
userDataUser callback function data.
rxSdmaHandleUser-requested DMA handle for RX DMA transfer.
txSdmaHandleUser-requested DMA handle for TX DMA transfer.
eventSourceTxEventsource for TX DMA transfer.
eventSourceRxEventsource for RX DMA transfer.
status_t UART_SendSDMA ( UART_Type *  base,
uart_sdma_handle_t *  handle,
uart_transfer_t *  xfer 
)

This function sends data using sDMA. This is a non-blocking function, which returns right away. When all data is sent, the send callback function is called.

Parameters
baseUART peripheral base address.
handleUART handle pointer.
xferUART sDMA transfer structure. See uart_transfer_t.
Return values
kStatus_Successif succeeded; otherwise failed.
kStatus_UART_TxBusyPrevious transfer ongoing.
kStatus_InvalidArgumentInvalid argument.
status_t UART_ReceiveSDMA ( UART_Type *  base,
uart_sdma_handle_t *  handle,
uart_transfer_t *  xfer 
)

This function receives data using sDMA. This is a non-blocking function, which returns right away. When all data is received, the receive callback function is called.

Parameters
baseUART peripheral base address.
handlePointer to the uart_sdma_handle_t structure.
xferUART sDMA transfer structure. See uart_transfer_t.
Return values
kStatus_Successif succeeded; otherwise failed.
kStatus_UART_RxBusyPrevious transfer ongoing.
kStatus_InvalidArgumentInvalid argument.
void UART_TransferAbortSendSDMA ( UART_Type *  base,
uart_sdma_handle_t *  handle 
)

This function aborts sent data using sDMA.

Parameters
baseUART peripheral base address.
handlePointer to the uart_sdma_handle_t structure.
void UART_TransferAbortReceiveSDMA ( UART_Type *  base,
uart_sdma_handle_t *  handle 
)

This function aborts receive data using sDMA.

Parameters
baseUART peripheral base address.
handlePointer to the uart_sdma_handle_t structure.
void UART_TransferSdmaHandleIRQ ( UART_Type *  base,
void *  uartSdmaHandle 
)

This function handles the UART transmit complete IRQ request and invoke user callback.

Parameters
baseUART peripheral base address.
uartSdmaHandleUART handle pointer.