MCUXpresso SDK API Reference Manual  Rev 2.14.0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
GPC: General Power Controller Driver

Overview

The MCUXpresso SDK provides a peripheral driver for the General Power Controller (GPC) module of MCUXpresso SDK devices.

API functions are provided to configure the system about working in dedicated power mode. There are mainly about enabling the power for memory, enabling the wakeup sources for STOP modes, and power up/down operations for various peripherals.

Macros

#define GPC_PCG_TIME_SLOT_TOTAL_NUMBER   GPC_SLT_CFG_PU_COUNT
 Total number of the timeslot.
 

Enumerations

enum  _gpc_lpm_mode {
  kGPC_RunMode = 0U,
  kGPC_WaitMode = 1U,
  kGPC_StopMode = 2U
}
 GPC LPM mode definition. More...
 
enum  _gpc_pgc_ack_sel {
  kGPC_DummyPGCPowerUpAck = GPC_PGC_ACK_SEL_DUMMY_PGC_PUP_ACK_MASK,
  kGPC_VirtualPGCPowerUpAck = GPC_PGC_ACK_SEL_VIRTUAL_PGC_PUP_ACK_MASK,
  kGPC_DummyPGCPowerDownAck = GPC_PGC_ACK_SEL_DUMMY_PGC_PDN_ACK_MASK,
  kGPC_VirtualPGCPowerDownAck = GPC_PGC_ACK_SEL_VIRTUAL_PGC_PDN_ACK_MASK,
  kGPC_NocPGCPowerUpAck = GPC_PGC_ACK_SEL_NOC_PGC_PUP_ACK,
  kGPC_NocPGCPowerDownAck = GPC_PGC_ACK_SEL_NOC_PGC_PDN_ACK
}
 PGC ack signal selection. More...
 
enum  _gpc_standby_count {
  kGPC_StandbyCounter4CkilClk = 0U,
  kGPC_StandbyCounter8CkilClk = 1U,
  kGPC_StandbyCounter16CkilClk = 2U,
  kGPC_StandbyCounter32CkilClk = 3U,
  kGPC_StandbyCounter64CkilClk = 4U,
  kGPC_StandbyCounter128CkilClk = 5U,
  kGPC_StandbyCounter256CkilClk = 6U,
  kGPC_StandbyCounter512CkilClk = 7U
}
 Standby counter which GPC will wait between PMIC_STBY_REQ negation and assertion of PMIC_READY. More...
 

Functions

static void GPC_AllowIRQs (GPC_Type *base)
 Allow all the IRQ/Events within the charge of GPC. More...
 
static void GPC_DisallowIRQs (GPC_Type *base)
 Disallow all the IRQ/Events within the charge of GPC. More...
 
static uint32_t GPC_GetLpmMode (GPC_Type *base)
 Get current LPM mode. More...
 
void GPC_EnableIRQ (GPC_Type *base, uint32_t irqId)
 Enable the IRQ. More...
 
void GPC_DisableIRQ (GPC_Type *base, uint32_t irqId)
 Disable the IRQ. More...
 
bool GPC_GetIRQStatusFlag (GPC_Type *base, uint32_t irqId)
 Get the IRQ/Event flag. More...
 
static void GPC_DsmTriggerMask (GPC_Type *base, bool enable)
 Mask the DSM trigger. More...
 
static void GPC_WFIMask (GPC_Type *base, bool enable)
 Mask the WFI. More...
 
static void GPC_SelectPGCAckSignal (GPC_Type *base, uint32_t mask)
 Select the PGC ACK signal. More...
 
static void GPC_PowerDownRequestMask (GPC_Type *base, bool enable)
 Power down request to virtual PGC mask or not. More...
 
static void GPC_PGCMapping (GPC_Type *base, uint32_t mask)
 PGC CPU Mapping. More...
 
static void GPC_TimeSlotConfigureForPUS (GPC_Type *base, uint8_t slotIndex, uint32_t value)
 Time slot configure. More...
 
void GPC_EnterWaitMode (GPC_Type *base, gpc_lpm_config_t *config)
 Enter WAIT mode. More...
 
void GPC_EnterStopMode (GPC_Type *base, gpc_lpm_config_t *config)
 Enter STOP mode. More...
 
void GPC_Init (GPC_Type *base, uint32_t powerUpSlot, uint32_t powerDownSlot)
 GPC init function. More...
 

Driver version

#define FSL_GPC_DRIVER_VERSION   (MAKE_VERSION(2, 2, 0))
 GPC driver version 2.2.0. More...
 

Macro Definition Documentation

#define FSL_GPC_DRIVER_VERSION   (MAKE_VERSION(2, 2, 0))

Enumeration Type Documentation

Enumerator
kGPC_RunMode 

run mode

kGPC_WaitMode 

wait mode

kGPC_StopMode 

stop mode

Enumerator
kGPC_DummyPGCPowerUpAck 

dummy power up ack signal

kGPC_VirtualPGCPowerUpAck 

virtual pgc power up ack signal

kGPC_DummyPGCPowerDownAck 

dummy power down ack signal

kGPC_VirtualPGCPowerDownAck 

virtual pgc power down ack signal

kGPC_NocPGCPowerUpAck 

NOC power up ack signal.

kGPC_NocPGCPowerDownAck 

NOC power.

Enumerator
kGPC_StandbyCounter4CkilClk 

4 ckil clocks

kGPC_StandbyCounter8CkilClk 

8 ckil clocks

kGPC_StandbyCounter16CkilClk 

16 ckil clocks

kGPC_StandbyCounter32CkilClk 

32 ckil clocks

kGPC_StandbyCounter64CkilClk 

64 ckil clocks

kGPC_StandbyCounter128CkilClk 

128 ckil clocks

kGPC_StandbyCounter256CkilClk 

256 ckil clocks

kGPC_StandbyCounter512CkilClk 

512 ckil clocks

Function Documentation

static void GPC_AllowIRQs ( GPC_Type *  base)
inlinestatic
Parameters
baseGPC peripheral base address.
static void GPC_DisallowIRQs ( GPC_Type *  base)
inlinestatic
Parameters
baseGPC peripheral base address.
static uint32_t GPC_GetLpmMode ( GPC_Type *  base)
inlinestatic
Parameters
baseGPC peripheral base address.
Return values
lpmmode, reference _gpc_lpm_mode
void GPC_EnableIRQ ( GPC_Type *  base,
uint32_t  irqId 
)
Parameters
baseGPC peripheral base address.
irqIdID number of IRQ to be enabled, available range is 0-127,reference SOC headerfile IRQn_Type.
void GPC_DisableIRQ ( GPC_Type *  base,
uint32_t  irqId 
)
Parameters
baseGPC peripheral base address.
irqIdID number of IRQ to be disabled, available range is 0-127,reference SOC headerfile IRQn_Type.
bool GPC_GetIRQStatusFlag ( GPC_Type *  base,
uint32_t  irqId 
)
Parameters
baseGPC peripheral base address.
irqIdID number of IRQ to be enabled, available range is 0-127,reference SOC headerfile IRQn_Type.
Returns
Indicated IRQ/Event is asserted or not.
static void GPC_DsmTriggerMask ( GPC_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseGPC peripheral base address.
enabletrue to enable mask, false to disable mask.
static void GPC_WFIMask ( GPC_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseGPC peripheral base address.
enabletrue to enable mask, false to disable mask.
static void GPC_SelectPGCAckSignal ( GPC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseGPC peripheral base address.
maskreference _gpc_pgc_ack_sel.
static void GPC_PowerDownRequestMask ( GPC_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseGPC peripheral base address.
enabletrue to mask, false to not mask.
static void GPC_PGCMapping ( GPC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseGPC peripheral base address.
maskmask value reference PGC CPU mapping definition.
static void GPC_TimeSlotConfigureForPUS ( GPC_Type *  base,
uint8_t  slotIndex,
uint32_t  value 
)
inlinestatic
Parameters
baseGPC peripheral base address.
slotIndextime slot index.
valuevalue to be configured
void GPC_EnterWaitMode ( GPC_Type *  base,
gpc_lpm_config_t *  config 
)
Parameters
baseGPC peripheral base address.
configlpm mode configurations.
void GPC_EnterStopMode ( GPC_Type *  base,
gpc_lpm_config_t *  config 
)
Parameters
baseGPC peripheral base address.
configlpm mode configurations.
void GPC_Init ( GPC_Type *  base,
uint32_t  powerUpSlot,
uint32_t  powerDownSlot 
)
Parameters
baseGPC peripheral base address.
powerUpSlotpower up slot number.
powerDownSlotpower down slot number.