![]() |
MCUXpresso SDK API Reference Manual
Rev 2.14.2
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the LCD interface (LCDIF) module of MCUXpresso SDK devices.
Data Structures | |
struct | lcdif_dpi_config_t |
Configuration for LCDIF module to work in DBI mode. More... | |
struct | lcdif_fb_config_t |
LCDIF frame buffer configuration. More... | |
struct | lcdif_cursor_config_t |
LCDIF cursor configuration. More... | |
struct | lcdif_dither_config_t |
LCDIF dither configuration. More... | |
Macros | |
#define | LCDIF_MAKE_CURSOR_COLOR(r, g, b) (((r) << 16U) | ((g) << 8U) | ((b) << 0U)) |
Construct the cursor color, every element should be in the range of 0 ~ 255. More... | |
#define | LCDIF_MAKE_GAMMA_VALUE(r, g, b) (((r) << 16U) | ((g) << 8U) | ((b) << 0U)) |
Construct the gamma value set to LCDIF gamma table, every element should be in the range of 0~255. More... | |
#define | LCDIF_FB_ALIGN 128U |
The frame buffer should be 128 byte aligned. More... | |
#define | LCDIF_GAMMA_INDEX_MAX 256U |
Gamma index max value. More... | |
#define | LCDIF_CURSOR_SIZE 32U |
The cursor size is 32 x 32. | |
Functions | |
void | LCDIF_DpiModeGetDefaultConfig (lcdif_dpi_config_t *config) |
Get the default configuration for to initialize the LCDIF. More... | |
status_t | LCDIF_DpiModeSetConfig (LCDIF_Type *base, uint8_t displayIndex, const lcdif_dpi_config_t *config) |
Initialize the LCDIF to work in DPI mode. More... | |
Driver version | |
#define | FSL_LCDIF_DRIVER_VERSION (MAKE_VERSION(2, 1, 1)) |
Initialization and deinitialization | |
status_t | LCDIF_Init (LCDIF_Type *base) |
Initialize the LCDIF. More... | |
void | LCDIF_Deinit (LCDIF_Type *base) |
De-initialize the LCDIF. More... | |
Frame buffer | |
void | LCDIF_SetFrameBufferConfig (LCDIF_Type *base, uint8_t fbIndex, const lcdif_fb_config_t *config) |
Configure the LCDIF frame buffer. More... | |
void | LCDIF_FrameBufferGetDefaultConfig (lcdif_fb_config_t *config) |
Get default frame buffer configuration. More... | |
static void | LCDIF_SetFrameBufferAddr (LCDIF_Type *base, uint8_t fbIndex, uint32_t address) |
Set the frame buffer to LCDIF. More... | |
void | LCDIF_SetFrameBufferStride (LCDIF_Type *base, uint8_t fbIndex, uint32_t strideBytes) |
Set the frame buffer stride. More... | |
Dither | |
void | LCDIF_SetDitherConfig (LCDIF_Type *base, uint8_t displayIndex, const lcdif_dither_config_t *config) |
Set the dither configuration. More... | |
Gamma correction | |
void | LCDIF_SetGammaData (LCDIF_Type *base, uint8_t fbIndex, uint16_t startIndex, const uint32_t *gamma, uint16_t gammaLen) |
Set the gamma translation values to the LCDIF gamma table. More... | |
Interrupts | |
The interrupt must be enabled, otherwise the interrupt flags will not assert. | |
static void | LCDIF_EnableInterrupts (LCDIF_Type *base, uint32_t mask) |
Enables LCDIF interrupt requests. More... | |
static void | LCDIF_DisableInterrupts (LCDIF_Type *base, uint32_t mask) |
Disable LCDIF interrupt requests. More... | |
static uint32_t | LCDIF_GetAndClearInterruptPendingFlags (LCDIF_Type *base) |
Get and clear LCDIF interrupt pending status. More... | |
Cursor | |
Top-left point and Hot spot are two different cursor point. Top-left point is used as the base address for the cursor. Hot spot is used in a search for a corresponding screen coordinate when a selection is made, such as when the "Enter" key or left mouse button is pushed. Top-left point +-------------------------------+ | | | Hot spot | | +------- | | | \ | | | \ \ | | | \ \ | | \ \ | | \ \ | | \ \ | | \ \ | | \ | | | +-------------------------------+ For format masked, one cursor pixel is 2bits. 32x32 cursor pixels have 32 cursor color rows. Each cursor color row is 64bits. cursorColorRow_H[31:0] = colorRow[63:32] cursorColorRow_L[31:0] = colorRow[31:0] xorCursor = cursorColorRow_H[cursorXPos[4:0]] andCursor = cursorColorRow_L[cursorXPos[4:0]] The output cursor color is: andCursor xorCursor cursor color 0 0 Background register color 0 1 Foreground register color 1 0 Frame buffer pixel color 1 1 Invert frame buffer pixel color | |
void | LCDIF_CursorGetDefaultConfig (lcdif_cursor_config_t *config) |
Get the hardware cursor default configuration. More... | |
void | LCDIF_SetCursorConfig (LCDIF_Type *base, const lcdif_cursor_config_t *config) |
Configure the cursor. More... | |
static void | LCDIF_SetCursorHotspotPosition (LCDIF_Type *base, uint16_t x, uint16_t y) |
Set the cursor hotspot postion. More... | |
static void | LCDIF_SetCursorBufferAddress (LCDIF_Type *base, uint32_t address) |
Set the cursor memory address. More... | |
void | LCDIF_SetCursorColor (LCDIF_Type *base, uint32_t background, uint32_t foreground) |
Set the cursor color. More... | |
struct lcdif_dpi_config_t |
Data Fields | |
uint16_t | panelWidth |
Display panel width, pixels per line. More... | |
uint16_t | panelHeight |
Display panel height, how many lines per panel. More... | |
uint8_t | hsw |
HSYNC pulse width. More... | |
uint8_t | hfp |
Horizontal front porch. More... | |
uint8_t | hbp |
Horizontal back porch. More... | |
uint8_t | vsw |
VSYNC pulse width. More... | |
uint8_t | vfp |
Vrtical front porch. More... | |
uint8_t | vbp |
Vertical back porch. More... | |
uint32_t | polarityFlags |
OR'ed value of _lcdif_polarity_flags, used to contol the signal polarity. More... | |
lcdif_output_format_t | format |
DPI output format. More... | |
uint16_t lcdif_dpi_config_t::panelWidth |
uint16_t lcdif_dpi_config_t::panelHeight |
uint8_t lcdif_dpi_config_t::hsw |
uint8_t lcdif_dpi_config_t::hfp |
uint8_t lcdif_dpi_config_t::hbp |
uint8_t lcdif_dpi_config_t::vsw |
uint8_t lcdif_dpi_config_t::vfp |
uint8_t lcdif_dpi_config_t::vbp |
uint32_t lcdif_dpi_config_t::polarityFlags |
lcdif_output_format_t lcdif_dpi_config_t::format |
struct lcdif_fb_config_t |
Data Fields | |
bool | enable |
Enable the frame buffer output. More... | |
bool | enableGamma |
Enable the gamma correction. More... | |
lcdif_fb_format_t | format |
Frame buffer pixel format. More... | |
bool lcdif_fb_config_t::enable |
bool lcdif_fb_config_t::enableGamma |
lcdif_fb_format_t lcdif_fb_config_t::format |
struct lcdif_cursor_config_t |
Data Fields | |
bool | enable |
Enable the cursor or not. More... | |
lcdif_cursor_format_t | format |
Cursor format. More... | |
uint8_t | hotspotOffsetX |
Offset of the hotspot to top left point, range 0 ~ 31. | |
uint8_t | hotspotOffsetY |
Offset of the hotspot to top left point, range 0 ~ 31. | |
bool lcdif_cursor_config_t::enable |
lcdif_cursor_format_t lcdif_cursor_config_t::format |
struct lcdif_dither_config_t |
Data Fields | |
bool | enable |
Enable or not. More... | |
uint8_t | redSize |
Red color size, valid region 4-8. More... | |
uint8_t | greenSize |
Green color size, valid region 4-8. More... | |
uint8_t | blueSize |
Blue color size, valid region 4-8. More... | |
uint32_t | low |
Low part of the look up table. More... | |
uint32_t | high |
High part of the look up table. More... | |
bool lcdif_dither_config_t::enable |
uint8_t lcdif_dither_config_t::redSize |
uint8_t lcdif_dither_config_t::greenSize |
uint8_t lcdif_dither_config_t::blueSize |
uint32_t lcdif_dither_config_t::low |
uint32_t lcdif_dither_config_t::high |
#define LCDIF_MAKE_CURSOR_COLOR | ( | r, | |
g, | |||
b | |||
) | (((r) << 16U) | ((g) << 8U) | ((b) << 0U)) |
#define LCDIF_MAKE_GAMMA_VALUE | ( | r, | |
g, | |||
b | |||
) | (((r) << 16U) | ((g) << 8U) | ((b) << 0U)) |
#define LCDIF_FB_ALIGN 128U |
#define LCDIF_GAMMA_INDEX_MAX 256U |
enum lcdif_fb_format_t |
enum _lcdif_interrupt |
status_t LCDIF_Init | ( | LCDIF_Type * | base | ) |
This function initializes the LCDIF to work.
base | LCDIF peripheral base address. |
kStatus_Success | Initialize successfully. |
void LCDIF_Deinit | ( | LCDIF_Type * | base | ) |
This function disables the LCDIF peripheral clock.
base | LCDIF peripheral base address. |
void LCDIF_DpiModeGetDefaultConfig | ( | lcdif_dpi_config_t * | config | ) |
The default configuration value is:
config | Pointer to the LCDIF configuration. |
status_t LCDIF_DpiModeSetConfig | ( | LCDIF_Type * | base, |
uint8_t | displayIndex, | ||
const lcdif_dpi_config_t * | config | ||
) |
This function configures the LCDIF DPI display.
base | LCDIF peripheral base address. |
displayIndex | Display index. |
config | Pointer to the configuration structure. |
kStatus_Success | Initialize successfully. |
kStatus_InvalidArgument | Initialize failed because of invalid argument. |
void LCDIF_SetFrameBufferConfig | ( | LCDIF_Type * | base, |
uint8_t | fbIndex, | ||
const lcdif_fb_config_t * | config | ||
) |
base | LCDIF peripheral base address. |
fbIndex | Frame buffer index. |
config | Pointer to the configuration structure. |
void LCDIF_FrameBufferGetDefaultConfig | ( | lcdif_fb_config_t * | config | ) |
The default configuration is config->enable = true; config->enableGamma = false; config->format = kLCDIF_PixelFormatRGB565;
config | Pointer to the configuration structure. |
|
inlinestatic |
base | LCDIF peripheral base address. |
fbIndex | Frame buffer index. |
address | Frame buffer address. |
void LCDIF_SetFrameBufferStride | ( | LCDIF_Type * | base, |
uint8_t | fbIndex, | ||
uint32_t | strideBytes | ||
) |
base | LCDIF peripheral base address. |
fbIndex | Frame buffer index. |
strideBytes | The stride in byte. |
void LCDIF_SetDitherConfig | ( | LCDIF_Type * | base, |
uint8_t | displayIndex, | ||
const lcdif_dither_config_t * | config | ||
) |
base | LCDIF peripheral base address. |
displayIndex | Index to configure. |
config | Pointer to the configuration structure. |
void LCDIF_SetGammaData | ( | LCDIF_Type * | base, |
uint8_t | fbIndex, | ||
uint16_t | startIndex, | ||
const uint32_t * | gamma, | ||
uint16_t | gammaLen | ||
) |
base | LCDIF peripheral base address. |
fbIndex | The frame buffer index. |
startIndex | Start index in the gamma table that the value will be set to. |
gamma | The gamma values to set to the gamma table in LCDIF, could be defined using LCDIF_MAKE_GAMMA_VALUE. |
gammaLen | The length of the gamma . |
|
inlinestatic |
base | LCDIF peripheral base address. |
mask | The interrupts to enable, pass in as OR'ed value of _lcdif_interrupt. |
|
inlinestatic |
base | LCDIF peripheral base address. |
mask | The interrupts to disable, pass in as OR'ed value of _lcdif_interrupt. |
|
inlinestatic |
base | LCDIF peripheral base address. |
void LCDIF_CursorGetDefaultConfig | ( | lcdif_cursor_config_t * | config | ) |
The default configuration values are:
config | Pointer to the hardware cursor configuration structure. |
void LCDIF_SetCursorConfig | ( | LCDIF_Type * | base, |
const lcdif_cursor_config_t * | config | ||
) |
base | LCDIF peripheral base address. |
config | Cursor configuration. |
|
inlinestatic |
base | LCDIF peripheral base address. |
x | X coordinate of the hotspot, range 0 ~ 8191. |
y | Y coordinate of the hotspot, range 0 ~ 8191. |
|
inlinestatic |
base | LCDIF peripheral base address. |
address | Memory address. |
void LCDIF_SetCursorColor | ( | LCDIF_Type * | base, |
uint32_t | background, | ||
uint32_t | foreground | ||
) |
base | LCDIF peripheral base address. |
background | Background color, could be defined use LCDIF_MAKE_CURSOR_COLOR |
foreground | Foreground color, could be defined use LCDIF_MAKE_CURSOR_COLOR |