MCUXpresso SDK API Reference Manual  Rev 2.14.2
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
MU: Messaging Unit

Overview

The MCUXpresso SDK provides a driver for the MU module of MCUXpresso SDK devices.

Function description

The MU driver provides these functions:

MU initialization

The function MU_Init() initializes the MU module and enables the MU clock. It should be called before any other MU functions.
The function MU_Deinit() deinitializes the MU module and disables the MU clock. No MU functions can be called after this function.

MU message

The MU message must be sent when the transmit register is empty. The MU driver provides blocking API and non-blocking API to send message.
The MU_SendMsgNonBlocking() function writes a message to the MU transmit register without checking the transmit register status. The upper layer should check that the transmit register is empty before calling this function. This function can be used in the ISR for better performance.
The MU_SendMsg() function is a blocking function. It waits until the transmit register is empty and sends the message.
Correspondingly, there are blocking and non-blocking APIs for receiving a message. The MU_ReadMsgNonBlocking() function is a non-blocking API. The MU_ReadMsg() function is the blocking API.

MU flags

The MU driver provides 3-bit general purpose flags. When the flags are set on one side, they are reflected on the other side.
The MU flags must be set when the previous flags have been updated to the other side. The MU driver provides a non-blocking function and a blocking function. The blocking function MU_SetFlags() waits until previous flags have been updated to the other side and then sets flags. The non-blocking function sets the flags directly. Ensure that the kMU_FlagsUpdatingFlag is not pending before calling this function.
The function MU_GetFlags() gets the MU flags on the current side.

Status and interrupt

The function MU_GetStatusFlags() returns all MU status flags. Use the _mu_status_flags to check for specific flags, for example, to check RX0 and RX1 register full, use the following code:

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/mu The receive full flags are cleared automatically after messages are read out. The transmit empty flags are cleared automatically after new messages are written to the transmit register. The general purpose interrupt flags must be cleared manually using the function MU_ClearStatusFlags().
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/mu To enable or disable a specific interrupt, use MU_EnableInterrupts() and MU_DisableInterrupts() functions. The interrupts to enable or disable should be passed in as a bit mask of the _mu_interrupt_enable.
The MU_TriggerInterrupts() function triggers general purpose interrupts and NMI to the other core. The interrupts to trigger are passed in as a bit mask of the _mu_interrupt_trigger. If previously triggered interrupts have not been processed by the other side, this function returns an error.

MU misc functions

The MU_ResetBothSides() function resets MU at both A and B sides. However, only the A side can call this function.
If a core enters stop mode, the platform clock of this core is disabled by default. The function MU_SetClockOnOtherCoreEnable() forces the other core's platform clock to remain enabled even after that core has entered a stop mode. In this case, the other core's platform clock keeps running until the current core enters stop mode too.

Enumerations

enum  _mu_status_flags {
  kMU_Tx0EmptyFlag = MU_TX_FLAG(1UL << 0U),
  kMU_Tx1EmptyFlag = MU_TX_FLAG(1UL << 1U),
  kMU_Tx2EmptyFlag = MU_TX_FLAG(1UL << 2U),
  kMU_Tx3EmptyFlag = MU_TX_FLAG(1UL << 3U),
  kMU_Rx0FullFlag = MU_RX_FLAG(1UL << 0U),
  kMU_Rx1FullFlag = MU_RX_FLAG(1UL << 1U),
  kMU_Rx2FullFlag = MU_RX_FLAG(1UL << 2U),
  kMU_Rx3FullFlag = MU_RX_FLAG(1UL << 3U),
  kMU_GenInt0Flag = MU_GI_FLAG(1UL << 0U),
  kMU_GenInt1Flag = MU_GI_FLAG(1UL << 1U),
  kMU_GenInt2Flag = MU_GI_FLAG(1UL << 2U),
  kMU_GenInt3Flag = MU_GI_FLAG(1UL << 3U),
  kMU_RxFullPendingFlag = MU_STAT_FLAG(MU_SR_RFP_MASK),
  kMU_TxEmptyPendingFlag = MU_STAT_FLAG(MU_SR_TEP_MASK),
  kMU_GenIntPendingFlag = MU_STAT_FLAG(MU_SR_GIRP_MASK),
  kMU_EventPendingFlag = MU_STAT_FLAG(MU_SR_EP_MASK),
  kMU_FlagsUpdatingFlag = MU_STAT_FLAG(MU_SR_FUP_MASK),
  kMU_MuInResetFlag = MU_STAT_FLAG(MU_SR_MURS_MASK),
  kMU_MuResetInterruptFlag = MU_STAT_FLAG(MU_SR_MURIP_MASK)
}
 MU status flags. More...
 
enum  _mu_interrupt_enable {
  kMU_Tx0EmptyInterruptEnable = MU_TX_INTR(1UL << 0U),
  kMU_Tx1EmptyInterruptEnable = MU_TX_INTR(1UL << 1U),
  kMU_Tx2EmptyInterruptEnable = MU_TX_INTR(1UL << 2U),
  kMU_Tx3EmptyInterruptEnable = MU_TX_INTR(1UL << 3U),
  kMU_Rx0FullInterruptEnable = MU_RX_INTR(1UL << 0U),
  kMU_Rx1FullInterruptEnable = MU_RX_INTR(1UL << 1U),
  kMU_Rx2FullInterruptEnable = MU_RX_INTR(1UL << 2U),
  kMU_Rx3FullInterruptEnable = MU_RX_INTR(1UL << 3U),
  kMU_GenInt0InterruptEnable = MU_GI_INTR(1UL << 0U),
  kMU_GenInt1InterruptEnable = MU_GI_INTR(1UL << 1U),
  kMU_GenInt2InterruptEnable = MU_GI_INTR(1UL << 2U),
  kMU_GenInt3InterruptEnable = MU_GI_INTR(1UL << 3U),
  kMU_MuResetInterruptEnable = MU_MISC_INTR(MU_CR_MURIE_MASK)
}
 MU interrupt source to enable. More...
 
enum  _mu_interrupt_trigger {
  kMU_GenInt0InterruptTrigger = MU_GI_INTR(1UL << 0U),
  kMU_GenInt1InterruptTrigger = MU_GI_INTR(1UL << 1U),
  kMU_GenInt2InterruptTrigger = MU_GI_INTR(1UL << 2U),
  kMU_GenInt3InterruptTrigger = MU_GI_INTR(1UL << 3U)
}
 MU interrupt that could be triggered to the other core. More...
 
enum  mu_msg_reg_index_t
 MU message register index.
 

Driver version

#define FSL_MU_DRIVER_VERSION   (MAKE_VERSION(2, 2, 1))
 MU driver version. More...
 

MU initialization.

void MU_Init (MU_Type *base)
 Initializes the MU module. More...
 
void MU_Deinit (MU_Type *base)
 De-initializes the MU module. More...
 

MU Message

static void MU_SendMsgNonBlocking (MU_Type *base, uint32_t regIndex, uint32_t msg)
 Writes a message to the TX register. More...
 
void MU_SendMsg (MU_Type *base, uint32_t regIndex, uint32_t msg)
 Blocks to send a message. More...
 
static uint32_t MU_ReceiveMsgNonBlocking (MU_Type *base, uint32_t regIndex)
 Reads a message from the RX register. More...
 
uint32_t MU_ReceiveMsg (MU_Type *base, uint32_t regIndex)
 Blocks to receive a message. More...
 

MU Flags

static void MU_SetFlagsNonBlocking (MU_Type *base, uint32_t flags)
 Sets the 3-bit MU flags reflect on the other MU side. More...
 
void MU_SetFlags (MU_Type *base, uint32_t flags)
 Blocks setting the 3-bit MU flags reflect on the other MU side. More...
 
static uint32_t MU_GetFlags (MU_Type *base)
 Gets the current value of the 3-bit MU flags set by the other side. More...
 

Status and Interrupt.

uint32_t MU_GetStatusFlags (MU_Type *base)
 Gets the MU status flags. More...
 
static void MU_ClearStatusFlags (MU_Type *base, uint32_t flags)
 Clears the specific MU status flags. More...
 
static void MU_EnableInterrupts (MU_Type *base, uint32_t interrupts)
 Enables the specific MU interrupts. More...
 
static void MU_DisableInterrupts (MU_Type *base, uint32_t interrupts)
 Disables the specific MU interrupts. More...
 
status_t MU_TriggerInterrupts (MU_Type *base, uint32_t interrupts)
 Triggers interrupts to the other core. More...
 
status_t MU_TriggerNmi (MU_Type *base)
 Triggers NMI to the other core. More...
 
static void MU_ClearNmi (MU_Type *base)
 Clear non-maskable interrupt (NMI) sent by the other core. More...
 

MU misc functions

void MU_BootOtherCore (MU_Type *base, mu_core_boot_mode_t mode)
 Boots the other core. More...
 
void MU_HoldOtherCoreReset (MU_Type *base)
 Holds the other core reset. More...
 
static void MU_ResetBothSides (MU_Type *base)
 Resets the MU for both A side and B side. More...
 
static void MU_SetClockOnOtherCoreEnable (MU_Type *base, bool enable)
 Enables or disables the clock on the other core. More...
 
void MU_HardwareResetOtherCore (MU_Type *base, bool waitReset, bool holdReset, mu_core_boot_mode_t bootMode)
 Hardware reset the other core. More...
 
static void MU_MaskHardwareReset (MU_Type *base, bool mask)
 Mask hardware reset by the other core. More...
 

Macro Definition Documentation

#define FSL_MU_DRIVER_VERSION   (MAKE_VERSION(2, 2, 1))

Enumeration Type Documentation

Enumerator
kMU_Tx0EmptyFlag 

TX0 empty.

kMU_Tx1EmptyFlag 

TX1 empty.

kMU_Tx2EmptyFlag 

TX2 empty.

kMU_Tx3EmptyFlag 

TX3 empty.

kMU_Rx0FullFlag 

RX0 full.

kMU_Rx1FullFlag 

RX1 full.

kMU_Rx2FullFlag 

RX2 full.

kMU_Rx3FullFlag 

RX3 full.

kMU_GenInt0Flag 

General purpose interrupt 0 pending.

kMU_GenInt1Flag 

General purpose interrupt 1 pending.

kMU_GenInt2Flag 

General purpose interrupt 2 pending.

kMU_GenInt3Flag 

General purpose interrupt 3 pending.

kMU_RxFullPendingFlag 

Any RX full flag is pending.

kMU_TxEmptyPendingFlag 

Any TX empty flag is pending.

kMU_GenIntPendingFlag 

Any general interrupt flag is pending.

kMU_EventPendingFlag 

MU event pending.

kMU_FlagsUpdatingFlag 

MU flags update is on-going.

kMU_MuInResetFlag 

MU of any side is in reset.

kMU_MuResetInterruptFlag 

The other side initializes MU reset.

Enumerator
kMU_Tx0EmptyInterruptEnable 

TX0 empty.

kMU_Tx1EmptyInterruptEnable 

TX1 empty.

kMU_Tx2EmptyInterruptEnable 

TX2 empty.

kMU_Tx3EmptyInterruptEnable 

TX3 empty.

kMU_Rx0FullInterruptEnable 

RX0 full.

kMU_Rx1FullInterruptEnable 

RX1 full.

kMU_Rx2FullInterruptEnable 

RX2 full.

kMU_Rx3FullInterruptEnable 

RX3 full.

kMU_GenInt0InterruptEnable 

General purpose interrupt 0.

kMU_GenInt1InterruptEnable 

General purpose interrupt 1.

kMU_GenInt2InterruptEnable 

General purpose interrupt 2.

kMU_GenInt3InterruptEnable 

General purpose interrupt 3.

kMU_MuResetInterruptEnable 

The other side initializes MU reset.

Enumerator
kMU_GenInt0InterruptTrigger 

General purpose interrupt 0.

kMU_GenInt1InterruptTrigger 

General purpose interrupt 1.

kMU_GenInt2InterruptTrigger 

General purpose interrupt 2.

kMU_GenInt3InterruptTrigger 

General purpose interrupt 3.

Function Documentation

void MU_Init ( MU_Type *  base)

This function enables the MU clock only.

Parameters
baseMU peripheral base address.
void MU_Deinit ( MU_Type *  base)

This function disables the MU clock only.

Parameters
baseMU peripheral base address.
static void MU_SendMsgNonBlocking ( MU_Type *  base,
uint32_t  regIndex,
uint32_t  msg 
)
inlinestatic

This function writes a message to the specific TX register. It does not check whether the TX register is empty or not. The upper layer should make sure the TX register is empty before calling this function. This function can be used in ISR for better performance.

* while (!(kMU_Tx0EmptyFlag & MU_GetStatusFlags(base))) { } Wait for TX0 register empty.
* MU_SendMsgNonBlocking(base, kMU_MsgReg0, MSG_VAL); Write message to the TX0 register.
*
Parameters
baseMU peripheral base address.
regIndexTX register index, see mu_msg_reg_index_t.
msgMessage to send.
void MU_SendMsg ( MU_Type *  base,
uint32_t  regIndex,
uint32_t  msg 
)

This function waits until the TX register is empty and sends the message.

Parameters
baseMU peripheral base address.
regIndexMU message register, see mu_msg_reg_index_t
msgMessage to send.
static uint32_t MU_ReceiveMsgNonBlocking ( MU_Type *  base,
uint32_t  regIndex 
)
inlinestatic

This function reads a message from the specific RX register. It does not check whether the RX register is full or not. The upper layer should make sure the RX register is full before calling this function. This function can be used in ISR for better performance.

* uint32_t msg;
* while (!(kMU_Rx0FullFlag & MU_GetStatusFlags(base)))
* {
* } Wait for the RX0 register full.
*
* msg = MU_ReceiveMsgNonBlocking(base, kMU_MsgReg0); Read message from RX0 register.
*
Parameters
baseMU peripheral base address.
regIndexRX register index, see mu_msg_reg_index_t.
Returns
The received message.
uint32_t MU_ReceiveMsg ( MU_Type *  base,
uint32_t  regIndex 
)

This function waits until the RX register is full and receives the message.

Parameters
baseMU peripheral base address.
regIndexMU message register, see mu_msg_reg_index_t
Returns
The received message.
static void MU_SetFlagsNonBlocking ( MU_Type *  base,
uint32_t  flags 
)
inlinestatic

This function sets the 3-bit MU flags directly. Every time the 3-bit MU flags are changed, the status flag kMU_FlagsUpdatingFlag asserts indicating the 3-bit MU flags are updating to the other side. After the 3-bit MU flags are updated, the status flag kMU_FlagsUpdatingFlag is cleared by hardware. During the flags updating period, the flags cannot be changed. The upper layer should make sure the status flag kMU_FlagsUpdatingFlag is cleared before calling this function.

* {
* } Wait for previous MU flags updating.
*
* MU_SetFlagsNonBlocking(base, 0U); Set the mU flags.
*
Parameters
baseMU peripheral base address.
flagsThe 3-bit MU flags to set.
void MU_SetFlags ( MU_Type *  base,
uint32_t  flags 
)

This function blocks setting the 3-bit MU flags. Every time the 3-bit MU flags are changed, the status flag kMU_FlagsUpdatingFlag asserts indicating the 3-bit MU flags are updating to the other side. After the 3-bit MU flags are updated, the status flag kMU_FlagsUpdatingFlag is cleared by hardware. During the flags updating period, the flags cannot be changed. This function waits for the MU status flag kMU_FlagsUpdatingFlag cleared and sets the 3-bit MU flags.

Parameters
baseMU peripheral base address.
flagsThe 3-bit MU flags to set.
static uint32_t MU_GetFlags ( MU_Type *  base)
inlinestatic

This function gets the current 3-bit MU flags on the current side.

Parameters
baseMU peripheral base address.
Returns
flags Current value of the 3-bit flags.
uint32_t MU_GetStatusFlags ( MU_Type *  base)

This function returns the bit mask of the MU status flags. See _mu_status_flags.

* uint32_t flags;
* flags = MU_GetStatusFlags(base); Get all status flags.
* if (kMU_Tx0EmptyFlag & flags)
* {
* The TX0 register is empty. Message can be sent.
* MU_SendMsgNonBlocking(base, kMU_MsgReg0, MSG0_VAL);
* }
* if (kMU_Tx1EmptyFlag & flags)
* {
* The TX1 register is empty. Message can be sent.
* MU_SendMsgNonBlocking(base, kMU_MsgReg1, MSG1_VAL);
* }
*
Parameters
baseMU peripheral base address.
Returns
Bit mask of the MU status flags, see _mu_status_flags.
static void MU_ClearStatusFlags ( MU_Type *  base,
uint32_t  flags 
)
inlinestatic

This function clears the specific MU status flags. The flags to clear should be passed in as bit mask. See _mu_status_flags.

* Clear general interrupt 0 and general interrupt 1 pending flags.
*
Parameters
baseMU peripheral base address.
flagsBit mask of the MU status flags. See _mu_status_flags. Only the following flags can be cleared by software, other flags are cleared by hardware:
static void MU_EnableInterrupts ( MU_Type *  base,
uint32_t  interrupts 
)
inlinestatic

This function enables the specific MU interrupts. The interrupts to enable should be passed in as bit mask. See _mu_interrupt_enable.

* Enable general interrupt 0 and TX0 empty interrupt.
*
Parameters
baseMU peripheral base address.
interruptsBit mask of the MU interrupts. See _mu_interrupt_enable.
static void MU_DisableInterrupts ( MU_Type *  base,
uint32_t  interrupts 
)
inlinestatic

This function disables the specific MU interrupts. The interrupts to disable should be passed in as bit mask. See _mu_interrupt_enable.

* Disable general interrupt 0 and TX0 empty interrupt.
*
Parameters
baseMU peripheral base address.
interruptsBit mask of the MU interrupts. See _mu_interrupt_enable.
status_t MU_TriggerInterrupts ( MU_Type *  base,
uint32_t  interrupts 
)

This function triggers the specific interrupts to the other core. The interrupts to trigger are passed in as bit mask. See _mu_interrupt_trigger. The MU should not trigger an interrupt to the other core when the previous interrupt has not been processed by the other core. This function checks whether the previous interrupts have been processed. If not, it returns an error.

* {
* Previous general purpose interrupt 0 or general purpose interrupt 2
* has not been processed by the other core.
* }
*
Parameters
baseMU peripheral base address.
interruptsBit mask of the interrupts to trigger. See _mu_interrupt_trigger.
Return values
kStatus_SuccessInterrupts have been triggered successfully.
kStatus_FailPrevious interrupts have not been accepted.
status_t MU_TriggerNmi ( MU_Type *  base)

This function triggers the NMI to the other core. The MU should not trigger NMI to the other core when the previous interrupt has not been processed by the other core. This function checks whether the previous interrupts have been processed. If not, it returns an error.

Parameters
baseMU peripheral base address.
Return values
kStatus_SuccessInterrupts have been triggered successfully.
kStatus_FailPrevious interrupts have not been accepted.
static void MU_ClearNmi ( MU_Type *  base)
inlinestatic

This function clears non-maskable interrupt (NMI) sent by the other core.

Parameters
baseMU peripheral base address.
void MU_BootOtherCore ( MU_Type *  base,
mu_core_boot_mode_t  mode 
)

This function boots the other core with a boot configuration.

Parameters
baseMU peripheral base address.
modeThe other core boot mode.
void MU_HoldOtherCoreReset ( MU_Type *  base)

This function causes the other core to be held in reset following any reset event.

Parameters
baseMU peripheral base address.
static void MU_ResetBothSides ( MU_Type *  base)
inlinestatic

This function resets the MU for both A side and B side. Before reset, it is recommended to interrupt processor B, because this function may affect the ongoing processor B programs.

Parameters
baseMU peripheral base address.
static void MU_SetClockOnOtherCoreEnable ( MU_Type *  base,
bool  enable 
)
inlinestatic

This function enables or disables the platform clock on the other core when that core enters a stop mode. If disabled, the platform clock for the other core is disabled when it enters stop mode. If enabled, the platform clock keeps running on the other core in stop mode, until this core also enters stop mode.

Parameters
baseMU peripheral base address.
enableEnable or disable the clock on the other core.
void MU_HardwareResetOtherCore ( MU_Type *  base,
bool  waitReset,
bool  holdReset,
mu_core_boot_mode_t  bootMode 
)

This function resets the other core, the other core could mask the hardware reset by calling MU_MaskHardwareReset. The hardware reset mask feature is only available for some platforms. This function could be used together with MU_BootOtherCore to control the other core reset workflow.

Example 1: Reset the other core, and no hold reset

* MU_HardwareResetOtherCore(MU_A, true, false, bootMode);
*

In this example, the core at MU side B will reset with the specified boot mode.

Example 2: Reset the other core and hold it, then boot the other core later.

* Here the other core enters reset, and the reset is hold
* MU_HardwareResetOtherCore(MU_A, true, true, modeDontCare);
* Current core boot the other core when necessary.
* MU_BootOtherCore(MU_A, bootMode);
*
Note
The feature waitReset, holdReset, and bootMode might be not supported for some platforms. waitReset is only available for platforms that FSL_FEATURE_MU_NO_CORE_STATUS not defined as 1. holdReset is only available for platforms that FSL_FEATURE_MU_NO_RSTH not defined as 1. bootMode is only available for platforms that FSL_FEATURE_MU_NO_BOOT not defined as 1.
Parameters
baseMU peripheral base address.
waitResetWait the other core enters reset.
  • true: Wait until the other core enters reset, if the other core has masked the hardware reset, then this function will be blocked.
  • false: Don't wait the reset.
holdResetHold the other core reset or not.
  • true: Hold the other core in reset, this function returns directly when the other core enters reset.
  • false: Don't hold the other core in reset, this function waits until the other core out of reset.
bootModeBoot mode of the other core, if holdReset is true, this parameter is useless.
static void MU_MaskHardwareReset ( MU_Type *  base,
bool  mask 
)
inlinestatic

The other core could call MU_HardwareResetOtherCore() to reset current core. To mask the reset, call this function and pass in true.

Parameters
baseMU peripheral base address.
maskPass true to mask the hardware reset, pass false to unmask it.