![]() |
MCUXpresso SDK API Reference Manual
Rev 2.14.2
NXP Semiconductors
|
Macros | |
#define | SENTINEL_BASELINE_API_CMD_PING (0x01U) |
sentinel command definition. More... | |
Functions | |
void | SENTINEL_Init (void) |
Initialize MU interface for Sentinel access. | |
void | SENTINEL_Deinit (void) |
Deinitialize MU interface for Sentinel access. | |
void | SENTINEL_SendMessage (uint32_t *param, uint32_t paramCount) |
Send message to Sentinel. More... | |
void | SENTINEL_ReceiveMessage (uint32_t *pParam, uint32_t *pParamCount) |
Receive message from Sentinel. More... | |
uint32_t | SENTINEL_Command (uint32_t *cmdParam, uint32_t cmdParamCount, uint32_t *pRespParam, uint32_t *pRespParamCount) |
Send command to Sentinel and receive response. More... | |
uint32_t | SENTINEL_Ping (void) |
Ping Sentinel to see if it is alive. More... | |
uint32_t | SENTINEL_GetFirmwareVersion (uint32_t *pVersion, uint32_t *pCommitSha) |
Get Sentinel firmware version. More... | |
uint32_t | SENTINEL_GetFirmwareStatus (uint8_t *pStatus) |
Get Sentinel firmware status. More... | |
uint32_t | SENTINEL_SetPowerDown (uint32_t resumeAddr, uint32_t size) |
Request Sentinel to enter power down. More... | |
uint32_t | SENTINEL_GetSocInfo (uint16_t *pSoc_id, uint16_t *pSoc_rev) |
Get Sentinel cpu version. More... | |
Driver version | |
#define | FSL_SENTINEL_DRIVER_VERSION (MAKE_VERSION(2, 0, 3)) |
sentinel driver version 2.0.3. More... | |
#define SENTINEL_BASELINE_API_CMD_PING (0x01U) |
#define FSL_SENTINEL_DRIVER_VERSION (MAKE_VERSION(2, 0, 3)) |
void SENTINEL_SendMessage | ( | uint32_t * | param, |
uint32_t | paramCount | ||
) |
param | Command parameters pointer. Each parameter is a 32bit word. |
paramCount | Command parameter count. |
void SENTINEL_ReceiveMessage | ( | uint32_t * | pParam, |
uint32_t * | pParamCount | ||
) |
pParam | Pointer to save command parameters. Each parameter is a 32bit word. |
pParamCount | Inout pointer to command parameter count. |
uint32_t SENTINEL_Command | ( | uint32_t * | cmdParam, |
uint32_t | cmdParamCount, | ||
uint32_t * | pRespParam, | ||
uint32_t * | pRespParamCount | ||
) |
cmdParam | Command parameters pointer. Each parameter is a 32bit word. |
cmdParamCount | Command parameter count. |
pRespParam | Pointer to save response parameters. Each parameter is a 32bit word. |
pRespParamCount | Inout pointer to response parameter count. |
uint32_t SENTINEL_Ping | ( | void | ) |
uint32_t SENTINEL_GetFirmwareVersion | ( | uint32_t * | pVersion, |
uint32_t * | pCommitSha | ||
) |
pVersion | Pointer to save firmware version. |
pCommitSha | Pointer to save first 4 bytes of the git commit ID. |
uint32_t SENTINEL_GetFirmwareStatus | ( | uint8_t * | pStatus | ) |
pStatus | Pointer to save firmware status. 0: No firmware in place. 1: Firmware authenticated and operational. |
uint32_t SENTINEL_SetPowerDown | ( | uint32_t | resumeAddr, |
uint32_t | size | ||
) |
resumeAddr | Base address in memory for resume code |
size | Length of resume code in memory |
uint32_t SENTINEL_GetSocInfo | ( | uint16_t * | pSoc_id, |
uint16_t * | pSoc_rev | ||
) |
pSoc_id | Pointer to soc id. |
pSoc_rev | Pointer to soc revision number. |