![]() |
MCUXpresso SDK API Reference Manual
Rev 2.15.000
NXP Semiconductors
|
Data Structures | |
| struct | _mem_config |
| Memory user config. More... | |
Macros | |
| #define | MinimalHeapSize_c (uint32_t)4 |
| Provide Minimal heap size for application to execute correctly. More... | |
| #define | gMemManagerLight (1) |
| Configures the memory manager light enable. | |
| #define | MEM_MANAGER_ENABLE_TRACE (0) |
| Configures the memory manager trace debug enable. | |
| #define | MEM_MANAGER_PRE_CONFIGURE (1) |
| Configures the memory manager pre configure. | |
| #define | MEM_BLOCK_DATA_BUFFER_DEFINE(name, numberOfBlocks, blockSize, id) |
| Defines the memory buffer. More... | |
| #define | MEM_BLOCK_BUFFER(name) (uint8_t *)&g_poolHeadBuffer##name |
| \ More... | |
Typedefs | |
| typedef enum _mem_status | mem_status_t |
| Memory status. | |
| typedef struct _mem_config | mem_config_t |
| Memory user config. | |
| typedef struct _mem_area_cfg_s | memAreaCfg_t |
| Memory user config. | |
Enumerations | |
| enum | _mem_status |
| Memory status. | |
Functions | |
| mem_status_t | MEM_Init (void) |
| Initialises the Memory Manager. | |
| void * | MEM_BufferAllocWithId (uint32_t numBytes, uint8_t poolId) |
| Allocate a block from the memory pools. More... | |
| mem_status_t | MEM_BufferFree (void *buffer) |
| Memory buffer free . More... | |
| uint16_t | MEM_BufferGetSize (void *buffer) |
| Returns the size of a given buffer. More... | |
| mem_status_t | MEM_BufferFreeAllWithId (uint8_t poolId) |
| Frees all allocated blocks by selected source and in selected pool. More... | |
| void * | MEM_BufferRealloc (void *buffer, uint32_t new_size) |
| Memory buffer realloc. More... | |
| uint32_t | MEM_GetHeapUpperLimit (void) |
| Get the address after the last allocated block if MemManagerLight is used. More... | |
| uint32_t | MEM_GetHeapUpperLimitByAreaId (uint8_t id) |
| Get the address after the last allocated block in area defined by id. More... | |
| uint32_t | MEM_GetFreeHeapSizeLowWaterMark (void) |
| Get the free space low watermark. More... | |
| uint32_t | MEM_GetFreeHeapSizeLowWaterMarkByAreaId (uint8_t area_id) |
| Get the free space low watermark. More... | |
| uint32_t | MEM_ResetFreeHeapSizeLowWaterMark (void) |
| Reset the free space low watermark. More... | |
| uint32_t | MEM_ResetFreeHeapSizeLowWaterMarkByAreaId (uint8_t area_id) |
| Reset the free space low watermark. More... | |
| uint32_t | MEM_GetFreeHeapSizeByAreaId (uint8_t area_id) |
| Get the free space in the heap for a area id. More... | |
| uint32_t | MEM_GetFreeHeapSize (void) |
| Get the free space in the heap. More... | |
| void | MEM_ReinitRamBank (uint32_t startAddress, uint32_t endAddress) |
| Selective RAM bank reinit after low power, based on a requested address range Useful for ECC RAM banks Defined as weak and empty in fsl_component_mem_manager_light.c to be overloaded by user. More... | |
| mem_status_t | MEM_RegisterExtendedArea (memAreaCfg_t *area_desc, uint8_t *area_id, uint16_t flags) |
| Function to register additional areas to allocate memory from. More... | |
| mem_status_t | MEM_UnRegisterExtendedArea (uint8_t area_id) |
| Function to unregister an extended area. More... | |
| struct _mem_config |
| #define MinimalHeapSize_c (uint32_t)4 |
The application can define a minimal heap size for proper code exection at run time, This will issue a link error if the minimal heap size requirement is not fullfilled (not enough space in RAM) By Default, Minimal heap size is set to 4 bytes (unlikely enough to have application work correctly)
| #define MEM_BLOCK_DATA_BUFFER_DEFINE | ( | name, | |
| numberOfBlocks, | |||
| blockSize, | |||
| id | |||
| ) |
This macro is used to define the shell memory buffer for memory manager. And then uses the macro MEM_BLOCK_BUFFER to get the memory buffer pointer. The macro should not be used in any function.
This is a example,
| name | The name string of the memory buffer. |
| numberOfBlocks | The number Of Blocks. |
| blockSize | The memory block size. |
| id | The id Of memory buffer. |
| #define MEM_BLOCK_BUFFER | ( | name | ) | (uint8_t *)&g_poolHeadBuffer##name |
Gets the memory buffer pointer \ \ This macro is used to get the memory buffer pointer. The macro should \ not be used before the macro MEM_BLOCK_BUFFER_DEFINE is used. \ \
| name | The memory name string of the buffer. \ |
| void* MEM_BufferAllocWithId | ( | uint32_t | numBytes, |
| uint8_t | poolId | ||
| ) |
The function uses the numBytes argument to look up a pool with adequate block sizes.
| numBytes | The number of bytes will be allocated. |
| poolId | The ID of the pool where to search for a free buffer. |
| Memory | buffer address when allocate success, NULL when allocate fail. |
| mem_status_t MEM_BufferFree | ( | void * | buffer | ) |
| buffer | The memory buffer address will be free. |
| kStatus_MemSuccess | Memory free succeed. |
| kStatus_MemFreeError | Memory free error occurred. |
| uint16_t MEM_BufferGetSize | ( | void * | buffer | ) |
| buffer | The memory buffer address will be get size. |
| The | size of a given buffer. |
| mem_status_t MEM_BufferFreeAllWithId | ( | uint8_t | poolId | ) |
| poolId | Selected pool Id (4 LSBs of poolId parameter) and selected source Id (4 MSBs of poolId parameter). |
| kStatus_MemSuccess | Memory free succeed. |
| kStatus_MemFreeError | Memory free error occurred. |
| void* MEM_BufferRealloc | ( | void * | buffer, |
| uint32_t | new_size | ||
| ) |
| buffer | The memory buffer address will be reallocated. |
| new_size | The number of bytes will be reallocated |
| kStatus_MemSuccess | Memory free succeed. |
| kStatus_MemFreeError | Memory free error occurred. |
| uint32_t MEM_GetHeapUpperLimit | ( | void | ) |
| UpperLimit | Return the address after the last allocated block if MemManagerLight is used. |
| 0 | Return 0 in case of the legacy MemManager. |
| uint32_t MEM_GetHeapUpperLimitByAreaId | ( | uint8_t | id | ) |
| [in] | id | 0 means memHeap, other values depend on number of registered areas |
| UpperLimit | Return the address after the last allocated block if MemManagerLight is used. |
| 0 | Return 0 in case of the legacy MemManager. |
| uint32_t MEM_GetFreeHeapSizeLowWaterMark | ( | void | ) |
| FreeHeapSize | Return the heap space low water mark free if MemManagerLight is used. |
| 0 | Return 0 in case of the legacy MemManager. |
| uint32_t MEM_GetFreeHeapSizeLowWaterMarkByAreaId | ( | uint8_t | area_id | ) |
| area_id | Selected area Id |
| Return | the heap space low water mark free if MemManagerLight is used. |
| 0 | Return 0 in case of the legacy MemManager. |
| uint32_t MEM_ResetFreeHeapSizeLowWaterMark | ( | void | ) |
| FreeHeapSize | Return the heap space low water mark free at the time it was reset if MemManagerLight is used. |
| 0 | Return 0 in case of the legacy MemManager. |
| uint32_t MEM_ResetFreeHeapSizeLowWaterMarkByAreaId | ( | uint8_t | area_id | ) |
| area_id | Selected area Id |
| FreeHeapSize | Return the heap space low water mark free at the time it was reset if MemManagerLight is used. |
| 0 | Return 0 in case of the legacy MemManager. |
| uint32_t MEM_GetFreeHeapSizeByAreaId | ( | uint8_t | area_id | ) |
| area_id | area_id whose available size is requested (0 means generic pool) |
| FreeHeapSize | Return the free space in the heap if MemManagerLight is used. |
| 0 | Return 0 in case of the legacy MemManager. |
| uint32_t MEM_GetFreeHeapSize | ( | void | ) |
| FreeHeapSize | Return the free space in the heap if MemManagerLight is used. |
| 0 | Return 0 in case of the legacy MemManager. |
| void MEM_ReinitRamBank | ( | uint32_t | startAddress, |
| uint32_t | endAddress | ||
| ) |
| [in] | startAddress | Start address of the requested range |
| [in] | endAddress | End address of the requested range |
| mem_status_t MEM_RegisterExtendedArea | ( | memAreaCfg_t * | area_desc, |
| uint8_t * | area_id, | ||
| uint16_t | flags | ||
| ) |
| [in] | area_desc | memAreaCfg_t structure defining start address and end address of area. This atructure may not be in rodata becasue the next field and internal private context are reserved in this structure. If NULL defines the default memHeap area. |
| [out] | area_id | pointer to return id of area. Required if allocation from specific pool is required. |
| [in] | flags | BIT(0) means that allocations can be performed in pool only explicitly and it is not a member of the default pool (id 0). Invalid for initial registration call. |
| mem_status_t MEM_UnRegisterExtendedArea | ( | uint8_t | area_id | ) |
| [in] | area_id | must be different from 0 (main heap). |