MCUXpresso SDK API Reference Manual  Rev 2.15.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Power Driver

Overview

Power driver provides APIs to control peripherals power and control the system power mode.

Macros

#define LOWPOWER_SRAMRETCTRL_RETEN_RAMX0   (1UL << 0)
 SRAM instances retention control during low power modes. More...
 
#define LOWPOWER_SRAMRETCTRL_RETEN_RAMX1   (1UL << 1)
 Enable SRAMX_1 retention when entering in Low power modes.
 
#define LOWPOWER_SRAMRETCTRL_RETEN_RAMX2   (1UL << 2)
 Enable SRAMX_2 retention when entering in Low power modes.
 
#define LOWPOWER_SRAMRETCTRL_RETEN_RAMX3   (1UL << 3)
 Enable SRAMX_3 retention when entering in Low power modes.
 
#define LOWPOWER_SRAMRETCTRL_RETEN_RAM00   (1UL << 4)
 Enable SRAM0_0 retention when entering in Low power modes.
 
#define LOWPOWER_SRAMRETCTRL_RETEN_RAM01   (1UL << 5)
 Enable SRAM0_1 retention when entering in Low power modes.
 
#define LOWPOWER_SRAMRETCTRL_RETEN_RAM10   (1UL << 6)
 Enable SRAM1_0 retention when entering in Low power modes.
 
#define LOWPOWER_SRAMRETCTRL_RETEN_RAM20   (1UL << 7)
 Enable SRAM2_0 retention when entering in Low power modes.
 
#define LOWPOWER_SRAMRETCTRL_RETEN_RAM30   (1UL << 8)
 Enable SRAM3_0 retention when entering in Low power modes.
 
#define LOWPOWER_SRAMRETCTRL_RETEN_RAM31   (1UL << 9)
 Enable SRAM3_1 retention when entering in Low power modes.
 
#define LOWPOWER_SRAMRETCTRL_RETEN_RAM40   (1UL << 10)
 Enable SRAM4_0 retention when entering in Low power modes.
 
#define LOWPOWER_SRAMRETCTRL_RETEN_RAM41   (1UL << 11)
 Enable SRAM4_1 retention when entering in Low power modes.
 
#define LOWPOWER_SRAMRETCTRL_RETEN_RAM42   (1UL << 12)
 Enable SRAM4_2 retention when entering in Low power modes.
 
#define LOWPOWER_SRAMRETCTRL_RETEN_RAM43   (1UL << 13)
 Enable SRAM4_3 retention when entering in Low power modes.
 
#define LOWPOWER_SRAMRETCTRL_RETEN_RAM_USB_HS   (1UL << 14)
 Enable SRAM USB HS retention when entering in Low power modes.
 
#define LOWPOWER_SRAMRETCTRL_RETEN_RAM_PUF   (1UL << 15)
 Enable SRAM PUFF retention when entering in Low power modes.
 
#define WAKEUP_SYS   (1ULL << 0) /*!< [SLEEP, DEEP SLEEP ] */ /* WWDT0_IRQ and BOD_IRQ*/
 Low Power Modes Wake up sources.
 
#define WAKEUP_SDMA0   (1ULL << 1)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_GLOBALINT0   (1ULL << 2)
 [SLEEP, DEEP SLEEP, POWER DOWN ]
 
#define WAKEUP_GPIO_GLOBALINT1   (1ULL << 3)
 [SLEEP, DEEP SLEEP, POWER DOWN ]
 
#define WAKEUP_GPIO_INT0_0   (1ULL << 4)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_1   (1ULL << 5)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_2   (1ULL << 6)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_3   (1ULL << 7)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_UTICK   (1ULL << 8)
 [SLEEP, ]
 
#define WAKEUP_MRT   (1ULL << 9)
 [SLEEP, ]
 
#define WAKEUP_CTIMER0   (1ULL << 10)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_CTIMER1   (1ULL << 11)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_SCT   (1ULL << 12)
 [SLEEP, ]
 
#define WAKEUP_CTIMER3   (1ULL << 13)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM0   (1ULL << 14)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM1   (1ULL << 15)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM2   (1ULL << 16)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM3   (1ULL << 17)
 [SLEEP, DEEP SLEEP, POWER DOWN ]
 
#define WAKEUP_FLEXCOMM4   (1ULL << 18)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM5   (1ULL << 19)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM6   (1ULL << 20)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM7   (1ULL << 21)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_ADC   (1ULL << 22)
 [SLEEP, ]
 
#define WAKEUP_ACMP_CAPT   (1ULL << 24)
 [SLEEP, DEEP SLEEP, POWER DOWN ]
 
#define WAKEUP_USB0_NEEDCLK   (1ULL << 27)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_USB0   (1ULL << 28)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_RTC_LITE_ALARM_WAKEUP   (1ULL << 29)
 [SLEEP, DEEP SLEEP, POWER DOWN, DEEP POWER DOWN]
 
#define WAKEUP_EZH_ARCH_B   (1ULL << 30)
 [SLEEP, ]
 
#define WAKEUP_WAKEUP_MAILBOX   (1ULL << 31)
 [SLEEP, DEEP SLEEP, POWER DOWN ]
 
#define WAKEUP_GPIO_INT0_4   (1ULL << 32)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_5   (1ULL << 33)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_6   (1ULL << 34)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_7   (1ULL << 35)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_CTIMER2   (1ULL << 36)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_CTIMER4   (1ULL << 37)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_OS_EVENT_TIMER   (1ULL << 38)
 [SLEEP, DEEP SLEEP, POWER DOWN, DEEP POWER DOWN]
 
#define WAKEUP_SDIO   (1ULL << 42)
 [SLEEP, ]
 
#define WAKEUP_USB1   (1ULL << 47)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_USB1_NEEDCLK   (1ULL << 48)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_SEC_HYPERVISOR_CALL   (1ULL << 49)
 [SLEEP, ]
 
#define WAKEUP_SEC_GPIO_INT0_0   (1ULL << 50)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_SEC_GPIO_INT0_1   (1ULL << 51)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_PLU   (1ULL << 52)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_SHA   (1ULL << 54)
 [SLEEP, ]
 
#define WAKEUP_CASPER   (1ULL << 55)
 [SLEEP, ]
 
#define WAKEUP_PUFF   (1ULL << 56)
 [SLEEP, ]
 
#define WAKEUP_PQ   (1ULL << 57)
 [SLEEP, ]
 
#define WAKEUP_SDMA1   (1ULL << 58)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_LSPI_HS   (1ULL << 59)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_ALLWAKEUPIOS   (1ULL << 63)
 [ , DEEP POWER DOWN]
 
#define LOWPOWER_HWWAKE_FORCED   (1UL << 0)
 Sleep Postpone. More...
 
#define LOWPOWER_HWWAKE_PERIPHERALS   (1UL << 1)
 Wake for Flexcomms. More...
 
#define LOWPOWER_HWWAKE_SDMA0   (1UL << 3)
 Wake for DMA0. More...
 
#define LOWPOWER_HWWAKE_SDMA1   (1UL << 5)
 Wake for DMA1. More...
 
#define LOWPOWER_HWWAKE_ENABLE_FRO192M   (1UL << 31)
 Need to be set if FRO192M is disable - via PDCTRL0 - in Deep Sleep mode and any of \ LOWPOWER_HWWAKE_PERIPHERALS, LOWPOWER_HWWAKE_SDMA0 or LOWPOWER_HWWAKE_SDMA1 is set.
 
#define LOWPOWER_CPURETCTRL_ENA_DISABLE   0
 In POWER DOWN mode, CPU Retention is disabled.
 
#define LOWPOWER_CPURETCTRL_ENA_ENABLE   1
 In POWER DOWN mode, CPU Retention is enabled.
 
#define LOWPOWER_WAKEUPIOSRC_PIO0_INDEX   0
 Wake up I/O sources. More...
 
#define LOWPOWER_WAKEUPIOSRC_PIO1_INDEX   2
 Pin P0(28)
 
#define LOWPOWER_WAKEUPIOSRC_PIO2_INDEX   4
 Pin P1(18)
 
#define LOWPOWER_WAKEUPIOSRC_PIO3_INDEX   6
 Pin P1(30)
 
#define LOWPOWER_WAKEUPIOSRC_DISABLE   0
 Wake up is disable.
 
#define LOWPOWER_WAKEUPIOSRC_RISING   1
 Wake up on rising edge.
 
#define LOWPOWER_WAKEUPIOSRC_FALLING   2
 Wake up on falling edge.
 
#define LOWPOWER_WAKEUPIOSRC_RISING_FALLING   3
 Wake up on both rising or falling edges.
 
#define LOWPOWER_WAKEUPIO_PIO0_PULLUPDOWN_INDEX   8
 Wake-up I/O 0 pull-up/down configuration index.
 
#define LOWPOWER_WAKEUPIO_PIO1_PULLUPDOWN_INDEX   9
 Wake-up I/O 1 pull-up/down configuration index.
 
#define LOWPOWER_WAKEUPIO_PIO2_PULLUPDOWN_INDEX   10
 Wake-up I/O 2 pull-up/down configuration index.
 
#define LOWPOWER_WAKEUPIO_PIO3_PULLUPDOWN_INDEX   11
 Wake-up I/O 3 pull-up/down configuration index.
 
#define LOWPOWER_WAKEUPIO_PIO0_PULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO0_PULLUPDOWN_INDEX)
 Wake-up I/O 0 pull-up/down mask.
 
#define LOWPOWER_WAKEUPIO_PIO1_PULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO1_PULLUPDOWN_INDEX)
 Wake-up I/O 1 pull-up/down mask.
 
#define LOWPOWER_WAKEUPIO_PIO2_PULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO2_PULLUPDOWN_INDEX)
 Wake-up I/O 2 pull-up/down mask.
 
#define LOWPOWER_WAKEUPIO_PIO3_PULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO3_PULLUPDOWN_INDEX)
 Wake-up I/O 3 pull-up/down mask.
 
#define LOWPOWER_WAKEUPIO_PULLDOWN   0
 Select pull-down.
 
#define LOWPOWER_WAKEUPIO_PULLUP   1
 Select pull-up.
 
#define LOWPOWER_WAKEUPIO_PIO0_DISABLEPULLUPDOWN_INDEX   12
 Wake-up I/O 0 pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO1_DISABLEPULLUPDOWN_INDEX   13
 Wake-up I/O 1 pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO2_DISABLEPULLUPDOWN_INDEX   14
 Wake-up I/O 2 pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO3_DISABLEPULLUPDOWN_INDEX   15
 Wake-up I/O 3 pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO0_DISABLEPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO0_DISABLEPULLUPDOWN_INDEX)
 Wake-up I/O 0 pull-up/down disable/enable mask.
 
#define LOWPOWER_WAKEUPIO_PIO1_DISABLEPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO1_DISABLEPULLUPDOWN_INDEX)
 Wake-up I/O 1 pull-up/down disable/enable mask.
 
#define LOWPOWER_WAKEUPIO_PIO2_DISABLEPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO2_DISABLEPULLUPDOWN_INDEX)
 Wake-up I/O 2 pull-up/down disable/enable mask.
 
#define LOWPOWER_WAKEUPIO_PIO3_DISABLEPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO3_DISABLEPULLUPDOWN_INDEX)
 Wake-up I/O 3 pull-up/down disable/enable mask.
 
#define LOWPOWER_WAKEUPIO_PIO0_USEEXTERNALPULLUPDOWN_INDEX   (16)
 Wake-up I/O 0 use external pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO1_USEEXTERNALPULLUPDOWN_INDEX   (17)
 Wake-up I/O 1 use external pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO2_USEEXTERNALPULLUPDOWN_INDEX   (18)
 Wake-up I/O 2 use external pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO3_USEEXTERNALPULLUPDOWN_INDEX   (19)
 Wake-up I/O 3 use external pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO0_USEEXTERNALPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO0_USEEXTERNALPULLUPDOWN_INDEX)
 Wake-up I/O 0 use external pull-up/down \ disable/enable mask, 0: disable, 1: enable.
 
#define LOWPOWER_WAKEUPIO_PIO1_USEEXTERNALPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO1_USEEXTERNALPULLUPDOWN_INDEX)
 Wake-up I/O 1 use external pull-up/down \ disable/enable mask, 0: disable, 1: enable.
 
#define LOWPOWER_WAKEUPIO_PIO2_USEEXTERNALPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO2_USEEXTERNALPULLUPDOWN_INDEX)
 Wake-up I/O 2 use external pull-up/down \ disable/enable mask, 0: disable, 1: enable.
 
#define LOWPOWER_WAKEUPIO_PIO3_USEEXTERNALPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO3_USEEXTERNALPULLUPDOWN_INDEX)
 Wake-up I/O 3 use external pull-up/down \ disable/enable mask, 0: disable, 1: enable.
 

Typedefs

typedef enum pd_bits pd_bit_t
 Analog components power modes control during low power modes.
 
typedef enum _power_bod_vbat_level power_bod_vbat_level_t
 BOD VBAT level.
 
typedef enum _power_bod_hyst power_bod_hyst_t
 BOD Hysteresis control.
 
typedef enum _power_bod_core_level power_bod_core_level_t
 BOD core level.
 
typedef enum
_power_device_reset_cause 
power_device_reset_cause_t
 Device Reset Causes.
 
typedef enum
_power_device_boot_mode 
power_device_boot_mode_t
 Device Boot Modes.
 

Enumerations

enum  pd_bits
 Analog components power modes control during low power modes.
 
enum  _power_bod_vbat_level {
  kPOWER_BodVbatLevel1000mv = 0,
  kPOWER_BodVbatLevel1100mv = 1,
  kPOWER_BodVbatLevel1200mv = 2,
  kPOWER_BodVbatLevel1300mv = 3,
  kPOWER_BodVbatLevel1400mv = 4,
  kPOWER_BodVbatLevel1500mv = 5,
  kPOWER_BodVbatLevel1600mv = 6,
  kPOWER_BodVbatLevel1650mv = 7,
  kPOWER_BodVbatLevel1700mv = 8,
  kPOWER_BodVbatLevel1750mv = 9,
  kPOWER_BodVbatLevel1800mv = 10,
  kPOWER_BodVbatLevel1900mv = 11,
  kPOWER_BodVbatLevel2000mv = 12,
  kPOWER_BodVbatLevel2100mv = 13,
  kPOWER_BodVbatLevel2200mv = 14,
  kPOWER_BodVbatLevel2300mv = 15,
  kPOWER_BodVbatLevel2400mv = 16,
  kPOWER_BodVbatLevel2500mv = 17,
  kPOWER_BodVbatLevel2600mv = 18,
  kPOWER_BodVbatLevel2700mv = 19,
  kPOWER_BodVbatLevel2806mv = 20,
  kPOWER_BodVbatLevel2900mv = 21,
  kPOWER_BodVbatLevel3000mv = 22,
  kPOWER_BodVbatLevel3100mv = 23,
  kPOWER_BodVbatLevel3200mv = 24,
  kPOWER_BodVbatLevel3300mv = 25
}
 BOD VBAT level. More...
 
enum  _power_bod_hyst {
  kPOWER_BodHystLevel25mv = 0U,
  kPOWER_BodHystLevel50mv = 1U,
  kPOWER_BodHystLevel75mv = 2U,
  kPOWER_BodHystLevel100mv = 3U
}
 BOD Hysteresis control. More...
 
enum  _power_bod_core_level {
  kPOWER_BodCoreLevel600mv = 0,
  kPOWER_BodCoreLevel650mv = 1,
  kPOWER_BodCoreLevel700mv = 2,
  kPOWER_BodCoreLevel750mv = 3,
  kPOWER_BodCoreLevel800mv = 4,
  kPOWER_BodCoreLevel850mv = 5,
  kPOWER_BodCoreLevel900mv = 6,
  kPOWER_BodCoreLevel950mv = 7
}
 BOD core level. More...
 
enum  _power_device_reset_cause {
  kRESET_CAUSE_POR = 0UL,
  kRESET_CAUSE_PADRESET = 1UL,
  kRESET_CAUSE_BODRESET = 2UL,
  kRESET_CAUSE_ARMSYSTEMRESET = 3UL,
  kRESET_CAUSE_WDTRESET = 4UL,
  kRESET_CAUSE_SWRRESET = 5UL,
  kRESET_CAUSE_CDOGRESET = 6UL,
  kRESET_CAUSE_DPDRESET_WAKEUPIO = 7UL,
  kRESET_CAUSE_DPDRESET_RTC = 8UL,
  kRESET_CAUSE_DPDRESET_OSTIMER = 9UL,
  kRESET_CAUSE_DPDRESET_WAKEUPIO_RTC = 10UL,
  kRESET_CAUSE_DPDRESET_WAKEUPIO_OSTIMER = 11UL,
  kRESET_CAUSE_DPDRESET_RTC_OSTIMER = 12UL,
  kRESET_CAUSE_DPDRESET_WAKEUPIO_RTC_OSTIMER = 13UL,
  kRESET_CAUSE_NOT_RELEVANT,
  kRESET_CAUSE_NOT_DETERMINISTIC = 15UL
}
 Device Reset Causes. More...
 
enum  _power_device_boot_mode {
  kBOOT_MODE_POWER_UP,
  kBOOT_MODE_LP_DEEP_SLEEP = 1UL,
  kBOOT_MODE_LP_POWER_DOWN = 2UL,
  kBOOT_MODE_LP_DEEP_POWER_DOWN = 4UL
}
 Device Boot Modes. More...
 

Functions

static void POWER_EnablePD (pd_bit_t en)
 API to enable PDRUNCFG bit in the Syscon. More...
 
static void POWER_DisablePD (pd_bit_t en)
 API to disable PDRUNCFG bit in the Syscon. More...
 
static void POWER_SetBodVbatLevel (power_bod_vbat_level_t level, power_bod_hyst_t hyst, bool enBodVbatReset)
 set BOD VBAT level. More...
 
static void POWER_EnableDeepSleep (void)
 API to enable deep sleep bit in the ARM Core. More...
 
static void POWER_DisableDeepSleep (void)
 API to disable deep sleep bit in the ARM Core. More...
 
void POWER_CycleCpuAndFlash (void)
 Shut off the Flash and execute the _WFI(), then power up the Flash after wake-up event This MUST BE EXECUTED outside the Flash: either from ROM or from SRAM. The rest could stay in Flash. But, for consistency, it is preferable to have all functions defined in this file implemented in ROM. More...
 
void POWER_EnterDeepSleep (uint32_t exclude_from_pd, uint32_t sram_retention_ctrl, uint64_t wakeup_interrupts, uint32_t hardware_wake_ctrl)
 Configures and enters in DEEP-SLEEP low power mode. More...
 
void POWER_EnterPowerDown (uint32_t exclude_from_pd, uint32_t sram_retention_ctrl, uint64_t wakeup_interrupts, uint32_t cpu_retention_ctrl)
 Configures and enters in POWERDOWN low power mode. More...
 
void POWER_EnterDeepPowerDown (uint32_t exclude_from_pd, uint32_t sram_retention_ctrl, uint64_t wakeup_interrupts, uint32_t wakeup_io_ctrl)
 Configures and enters in DEEPPOWERDOWN low power mode. More...
 
void POWER_EnterSleep (void)
 Configures and enters in SLEEP low power mode. More...
 
void POWER_SetVoltageForFreq (uint32_t system_freq_hz)
 Power Library API to choose normal regulation and set the voltage for the desired operating frequency. More...
 
void POWER_Xtal16mhzCapabankTrim (int32_t pi32_16MfXtalIecLoadpF_x100, int32_t pi32_16MfXtalPPcbParCappF_x100, int32_t pi32_16MfXtalNPcbParCappF_x100)
 Sets board-specific trim values for 16MHz XTAL. More...
 
void POWER_Xtal32khzCapabankTrim (int32_t pi32_32kfXtalIecLoadpF_x100, int32_t pi32_32kfXtalPPcbParCappF_x100, int32_t pi32_32kfXtalNPcbParCappF_x100)
 Sets board-specific trim values for 32kHz XTAL. More...
 
void POWER_SetXtal16mhzLdo (void)
 Enables and sets LDO for 16MHz XTAL. More...
 
void POWER_GetWakeUpCause (power_device_reset_cause_t *p_reset_cause, power_device_boot_mode_t *p_boot_mode, uint32_t *p_wakeupio_cause)
 Return some key information related to the device reset causes / wake-up sources, for all power modes. More...
 

Driver version

#define FSL_POWER_DRIVER_VERSION   (MAKE_VERSION(1, 0, 0))
 power driver version 1.0.0. More...
 

Macro Definition Documentation

#define FSL_POWER_DRIVER_VERSION   (MAKE_VERSION(1, 0, 0))
#define LOWPOWER_SRAMRETCTRL_RETEN_RAMX0   (1UL << 0)

Enable SRAMX_0 retention when entering in Low power modes

#define LOWPOWER_HWWAKE_FORCED   (1UL << 0)

Force peripheral clocking to stay on during deep-sleep mode.

#define LOWPOWER_HWWAKE_PERIPHERALS   (1UL << 1)

Any Flexcomm FIFO reaching the level specified by its own TXLVL will cause \ peripheral clocking to wake up temporarily while the related status is asserted

#define LOWPOWER_HWWAKE_SDMA0   (1UL << 3)

DMA0 being busy will cause peripheral clocking to remain running until DMA \ completes. Used in conjonction with LOWPOWER_HWWAKE_PERIPHERALS

#define LOWPOWER_HWWAKE_SDMA1   (1UL << 5)

DMA0 being busy will cause peripheral clocking to remain running until DMA \ completes. Used in conjonction with LOWPOWER_HWWAKE_PERIPHERALS

#define LOWPOWER_WAKEUPIOSRC_PIO0_INDEX   0

Pin P1( 1)

Enumeration Type Documentation

Enumerator
kPOWER_BodVbatLevel1000mv 

Brown out detector VBAT level 1V.

kPOWER_BodVbatLevel1100mv 

Brown out detector VBAT level 1.1V.

kPOWER_BodVbatLevel1200mv 

Brown out detector VBAT level 1.2V.

kPOWER_BodVbatLevel1300mv 

Brown out detector VBAT level 1.3V.

kPOWER_BodVbatLevel1400mv 

Brown out detector VBAT level 1.4V.

kPOWER_BodVbatLevel1500mv 

Brown out detector VBAT level 1.5V.

kPOWER_BodVbatLevel1600mv 

Brown out detector VBAT level 1.6V.

kPOWER_BodVbatLevel1650mv 

Brown out detector VBAT level 1.65V.

kPOWER_BodVbatLevel1700mv 

Brown out detector VBAT level 1.7V.

kPOWER_BodVbatLevel1750mv 

Brown out detector VBAT level 1.75V.

kPOWER_BodVbatLevel1800mv 

Brown out detector VBAT level 1.8V.

kPOWER_BodVbatLevel1900mv 

Brown out detector VBAT level 1.9V.

kPOWER_BodVbatLevel2000mv 

Brown out detector VBAT level 2V.

kPOWER_BodVbatLevel2100mv 

Brown out detector VBAT level 2.1V.

kPOWER_BodVbatLevel2200mv 

Brown out detector VBAT level 2.2V.

kPOWER_BodVbatLevel2300mv 

Brown out detector VBAT level 2.3V.

kPOWER_BodVbatLevel2400mv 

Brown out detector VBAT level 2.4V.

kPOWER_BodVbatLevel2500mv 

Brown out detector VBAT level 2.5V.

kPOWER_BodVbatLevel2600mv 

Brown out detector VBAT level 2.6V.

kPOWER_BodVbatLevel2700mv 

Brown out detector VBAT level 2.7V.

kPOWER_BodVbatLevel2806mv 

Brown out detector VBAT level 2.806V.

kPOWER_BodVbatLevel2900mv 

Brown out detector VBAT level 2.9V.

kPOWER_BodVbatLevel3000mv 

Brown out detector VBAT level 3.0V.

kPOWER_BodVbatLevel3100mv 

Brown out detector VBAT level 3.1V.

kPOWER_BodVbatLevel3200mv 

Brown out detector VBAT level 3.2V.

kPOWER_BodVbatLevel3300mv 

Brown out detector VBAT level 3.3V.

Enumerator
kPOWER_BodHystLevel25mv 

BOD Hysteresis control level 25mv.

kPOWER_BodHystLevel50mv 

BOD Hysteresis control level 50mv.

kPOWER_BodHystLevel75mv 

BOD Hysteresis control level 75mv.

kPOWER_BodHystLevel100mv 

BOD Hysteresis control level 100mv.

Enumerator
kPOWER_BodCoreLevel600mv 

Brown out detector core level 600mV.

kPOWER_BodCoreLevel650mv 

Brown out detector core level 650mV.

kPOWER_BodCoreLevel700mv 

Brown out detector core level 700mV.

kPOWER_BodCoreLevel750mv 

Brown out detector core level 750mV.

kPOWER_BodCoreLevel800mv 

Brown out detector core level 800mV.

kPOWER_BodCoreLevel850mv 

Brown out detector core level 850mV.

kPOWER_BodCoreLevel900mv 

Brown out detector core level 900mV.

kPOWER_BodCoreLevel950mv 

Brown out detector core level 950mV.

Enumerator
kRESET_CAUSE_POR 

Power On Reset.

kRESET_CAUSE_PADRESET 

Hardware Pin Reset.

kRESET_CAUSE_BODRESET 

Brown-out Detector reset (either BODVBAT or BODCORE)

kRESET_CAUSE_ARMSYSTEMRESET 

ARM System Reset.

kRESET_CAUSE_WDTRESET 

Watchdog Timer Reset.

kRESET_CAUSE_SWRRESET 

Software Reset.

kRESET_CAUSE_CDOGRESET 

Code Watchdog Reset.

kRESET_CAUSE_DPDRESET_WAKEUPIO 

Any of the 4 wake-up pins.

kRESET_CAUSE_DPDRESET_RTC 

Real Time Counter (RTC)

kRESET_CAUSE_DPDRESET_OSTIMER 

OS Event Timer (OSTIMER)

kRESET_CAUSE_DPDRESET_WAKEUPIO_RTC 

Any of the 4 wake-up pins and RTC (it is not possible to distinguish which of these 2 events occured first)

kRESET_CAUSE_DPDRESET_WAKEUPIO_OSTIMER 

Any of the 4 wake-up pins and OSTIMER (it is not possible to distinguish which of these 2 events occured first)

kRESET_CAUSE_DPDRESET_RTC_OSTIMER 

Real Time Counter or OS Event Timer (it is not possible to distinguish which of these 2 events occured first)

kRESET_CAUSE_DPDRESET_WAKEUPIO_RTC_OSTIMER 

Any of the 4 wake-up pins (it is not possible to distinguish which of these 3 events occured first)

kRESET_CAUSE_NOT_RELEVANT 

No reset cause (for example, this code is used when waking up from DEEP-SLEEP low power mode)

kRESET_CAUSE_NOT_DETERMINISTIC 

Unknown Reset Cause.

Should be treated like "Hardware Pin Reset" from an application point of view.

Enumerator
kBOOT_MODE_POWER_UP 

All non Low Power Mode wake up (Power On Reset, Pin Reset, BoD Reset, ARM System Reset ...

)

kBOOT_MODE_LP_DEEP_SLEEP 

Wake up from DEEP-SLEEP Low Power mode.

kBOOT_MODE_LP_POWER_DOWN 

Wake up from POWER-DOWN Low Power mode.

kBOOT_MODE_LP_DEEP_POWER_DOWN 

Wake up from DEEP-POWER-DOWN Low Power mode.

Function Documentation

static void POWER_EnablePD ( pd_bit_t  en)
inlinestatic

Note that enabling the bit powers down the peripheral

Parameters
enperipheral for which to enable the PDRUNCFG bit
Returns
none
static void POWER_DisablePD ( pd_bit_t  en)
inlinestatic

Note that disabling the bit powers up the peripheral

Parameters
enperipheral for which to disable the PDRUNCFG bit
Returns
none
static void POWER_SetBodVbatLevel ( power_bod_vbat_level_t  level,
power_bod_hyst_t  hyst,
bool  enBodVbatReset 
)
inlinestatic
Parameters
levelBOD detect level
hystBoD Hysteresis control
enBodVbatResetVBAT brown out detect reset
static void POWER_EnableDeepSleep ( void  )
inlinestatic
Returns
none
static void POWER_DisableDeepSleep ( void  )
inlinestatic
Returns
none
void POWER_CycleCpuAndFlash ( void  )
Returns
Nothing
void POWER_EnterDeepSleep ( uint32_t  exclude_from_pd,
uint32_t  sram_retention_ctrl,
uint64_t  wakeup_interrupts,
uint32_t  hardware_wake_ctrl 
)
Parameters
exclude_from_pd,:
sram_retention_ctrl,:
wakeup_interrupts,:
hardware_wake_ctrl,:
Returns
Nothing
     !!! IMPORTANT NOTES :
0 - CPU0 & System CLock frequency is switched to FRO12MHz and is NOT restored back by the API. 1 - CPU0 Interrupt Enable registers (NVIC->ISER) are modified by this function. They are restored back in case of CPU retention or if POWERDOWN is not taken (for instance because an interrupt is pending). 2 - The Non Maskable Interrupt (NMI) is disabled and its configuration before calling this function will be restored back if POWERDOWN is not taken (for instance because an RTC or OSTIMER interrupt is pending). 3 - The HARD FAULT handler should execute from SRAM. (The Hard fault handler should initiate a full chip reset) reset)
void POWER_EnterPowerDown ( uint32_t  exclude_from_pd,
uint32_t  sram_retention_ctrl,
uint64_t  wakeup_interrupts,
uint32_t  cpu_retention_ctrl 
)
Parameters
exclude_from_pd,:
sram_retention_ctrl,:
wakeup_interrupts,:
cpu_retention_ctrl,:0 = CPU retention is disable / 1 = CPU retention is enabled, all other values are RESERVED.
Returns
Nothing
     !!! IMPORTANT NOTES :
0 - CPU0 & System CLock frequency is switched to FRO12MHz and is NOT restored back by the API. 1 - CPU0 Interrupt Enable registers (NVIC->ISER) are modified by this function. They are restored back in case of CPU retention or if POWERDOWN is not taken (for instance because an interrupt is pending). 2 - The Non Maskable Interrupt (NMI) is disabled and its configuration before calling this function will be restored back if POWERDOWN is not taken (for instance because an RTC or OSTIMER interrupt is pending). 3 - In case of CPU retention, it is the responsability of the user to make sure that SRAM instance containing the stack used to call this function WILL BE preserved during low power (via parameter "sram_retention_ctrl") 4 - The HARD FAULT handler should execute from SRAM. (The Hard fault handler should initiate a full chip reset) reset)
void POWER_EnterDeepPowerDown ( uint32_t  exclude_from_pd,
uint32_t  sram_retention_ctrl,
uint64_t  wakeup_interrupts,
uint32_t  wakeup_io_ctrl 
)
Parameters
exclude_from_pd,:
sram_retention_ctrl,:
wakeup_interrupts,:
wakeup_io_ctrl,:
Returns
Nothing
     !!! IMPORTANT NOTES :
0 - CPU0 & System CLock frequency is switched to FRO12MHz and is NOT restored back by the API. 1 - CPU0 Interrupt Enable registers (NVIC->ISER) are modified by this function. They are restored back if DEEPPOWERDOWN is not taken (for instance because an RTC or OSTIMER interrupt is pending). 2 - The Non Maskable Interrupt (NMI) is disabled and its configuration before calling this function will be restored back if DEEPPOWERDOWN is not taken (for instance because an RTC or OSTIMER interrupt is pending). 3 - The HARD FAULT handler should execute from SRAM. (The Hard fault handler should initiate a full chip reset)
void POWER_EnterSleep ( void  )
Parameters
:
Returns
Nothing
void POWER_SetVoltageForFreq ( uint32_t  system_freq_hz)
Parameters
system_freq_hz- The desired frequency (in Hertz) at which the part would like to operate, note that the voltage and flash wait states should be set before changing frequency
Returns
none
void POWER_Xtal16mhzCapabankTrim ( int32_t  pi32_16MfXtalIecLoadpF_x100,
int32_t  pi32_16MfXtalPPcbParCappF_x100,
int32_t  pi32_16MfXtalNPcbParCappF_x100 
)
Parameters
pi32_16MfXtalIecLoadpF_x100Load capacitance, pF x 100. For example, 6pF becomes 600, 1.2pF becomes 120
pi32_16MfXtalPPcbParCappF_x100PCB +ve parasitic capacitance, pF x 100. For example, 6pF becomes 600, 1.2pF becomes 120
pi32_16MfXtalNPcbParCappF_x100PCB -ve parasitic capacitance, pF x 100. For example, 6pF becomes 600, 1.2pF becomes 120
Returns
none
Note
Following default Values can be used: pi32_32MfXtalIecLoadpF_x100 Load capacitance, pF x 100 : 600 pi32_32MfXtalPPcbParCappF_x100 PCB +ve parasitic capacitance, pF x 100 : 20 pi32_32MfXtalNPcbParCappF_x100 PCB -ve parasitic capacitance, pF x 100 : 40
void POWER_Xtal32khzCapabankTrim ( int32_t  pi32_32kfXtalIecLoadpF_x100,
int32_t  pi32_32kfXtalPPcbParCappF_x100,
int32_t  pi32_32kfXtalNPcbParCappF_x100 
)
Parameters
pi32_32kfXtalIecLoadpF_x100Load capacitance, pF x 100. For example, 6pF becomes 600, 1.2pF becomes 120
pi32_32kfXtalPPcbParCappF_x100PCB +ve parasitic capacitance, pF x 100. For example, 6pF becomes 600, 1.2pF becomes 120
pi32_32kfXtalNPcbParCappF_x100PCB -ve parasitic capacitance, pF x 100. For example, 6pF becomes 600, 1.2pF becomes 120
Returns
none
Note
Following default Values can be used: pi32_32kfXtalIecLoadpF_x100 Load capacitance, pF x 100 : 600 pi32_32kfXtalPPcbParCappF_x100 PCB +ve parasitic capacitance, pF x 100 : 40 pi32_32kfXtalNPcbParCappF_x100 PCB -ve parasitic capacitance, pF x 100 : 40
void POWER_SetXtal16mhzLdo ( void  )
Returns
none
void POWER_GetWakeUpCause ( power_device_reset_cause_t p_reset_cause,
power_device_boot_mode_t p_boot_mode,
uint32_t *  p_wakeupio_cause 
)
Parameters
p_reset_cause: the device reset cause, according to the definition of power_device_reset_cause_t type.
p_boot_mode: the device boot mode, according to the definition of power_device_boot_mode_t type.
p_wakeupio_cause,:the wake-up pin sources, according to the definition of register PMC->WAKEIOCAUSE[3:0].
Returns
Nothing
    !!!  IMPORTANT ERRATA - IMPORTANT ERRATA - IMPORTANT ERRATA     !!!
    !!!   valid ONLY for LPC55S69 (not for LPC55S16 and LPC55S06)   !!!
    !!!   when FALLING EDGE DETECTION is enabled on wake-up pins:   !!!
    - 1. p_wakeupio_cause is NOT ACCURATE
    - 2. Spurious kRESET_CAUSE_DPDRESET_WAKEUPIO* event is reported when
         several wake-up sources are enabled during DEEP-POWER-DOWN
         (like enabling wake-up on RTC and Falling edge wake-up pins)