MCUXpresso SDK API Reference Manual  Rev 2.15.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Typical use case

More...

Overview

The SDMA multi fifo script support transfer data between multi peripheral fifos and memory, a typical user case is that receiving multi PDM channel data and put it into memory as

| channel 0 | channel 1 | channel 2 | channel 3 | channel 4 | ......... |

Multi fifo script is target to implement above feature, it can supports 1.configurable fifo watermark range from 1~(2^12-1), it is a value of fifo_watermark * channel_numbers 2.configurable fifo numbers, support up to 15 continuous fifos 3.configurable fifo address offset, support address offset up to 64

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/pdm/pdm_sai_sdma

Data Structures

struct  _pdm_sdma_handle
 PDM DMA transfer handle, users should not touch the content of the handle. More...
 

Typedefs

typedef void(* pdm_sdma_callback_t )(PDM_Type *base, pdm_sdma_handle_t *handle, status_t status, void *userData)
 PDM eDMA transfer callback function for finish and error.
 

Driver version

#define FSL_PDM_SDMA_DRIVER_VERSION   (MAKE_VERSION(2, 7, 0))
 Version 2.7.0.
 

eDMA Transactional

void PDM_TransferCreateHandleSDMA (PDM_Type *base, pdm_sdma_handle_t *handle, pdm_sdma_callback_t callback, void *userData, sdma_handle_t *dmaHandle, uint32_t eventSource)
 Initializes the PDM eDMA handle. More...
 
status_t PDM_TransferReceiveSDMA (PDM_Type *base, pdm_sdma_handle_t *handle, pdm_transfer_t *xfer)
 Performs a non-blocking PDM receive using eDMA. More...
 
void PDM_TransferAbortReceiveSDMA (PDM_Type *base, pdm_sdma_handle_t *handle)
 Aborts a PDM receive using eDMA. More...
 
void PDM_SetChannelConfigSDMA (PDM_Type *base, pdm_sdma_handle_t *handle, uint32_t channel, const pdm_channel_config_t *config)
 PDM channel configurations. More...
 
void PDM_TransferTerminateReceiveSDMA (PDM_Type *base, pdm_sdma_handle_t *handle)
 Terminate all the PDM sdma receive transfer. More...
 

Data Structure Documentation

struct _pdm_sdma_handle

Data Fields

sdma_handle_tdmaHandle
 DMA handler for PDM send.
 
uint8_t nbytes
 eDMA minor byte transfer count initially configured. More...
 
uint8_t fifoWidth
 fifo width
 
uint8_t endChannel
 The last enabled channel.
 
uint8_t channelNums
 total channel numbers
 
uint32_t count
 The transfer data count in a DMA request.
 
uint32_t state
 Internal state for PDM eDMA transfer.
 
uint32_t eventSource
 PDM event source number.
 
pdm_sdma_callback_t callback
 Callback for users while transfer finish or error occurs.
 
void * userData
 User callback parameter.
 
sdma_buffer_descriptor_t bdPool [PDM_XFER_QUEUE_SIZE]
 BD pool for SDMA transfer. More...
 
pdm_transfer_t pdmQueue [PDM_XFER_QUEUE_SIZE]
 Transfer queue storing queued transfer. More...
 
size_t transferSize [PDM_XFER_QUEUE_SIZE]
 Data bytes need to transfer.
 
volatile uint8_t queueUser
 Index for user to queue transfer. More...
 
volatile uint8_t queueDriver
 Index for driver to get the transfer data and size.
 

Field Documentation

uint8_t _pdm_sdma_handle::nbytes
sdma_buffer_descriptor_t _pdm_sdma_handle::bdPool[PDM_XFER_QUEUE_SIZE]
pdm_transfer_t _pdm_sdma_handle::pdmQueue[PDM_XFER_QUEUE_SIZE]
volatile uint8_t _pdm_sdma_handle::queueUser

Function Documentation

void PDM_TransferCreateHandleSDMA ( PDM_Type *  base,
pdm_sdma_handle_t handle,
pdm_sdma_callback_t  callback,
void *  userData,
sdma_handle_t dmaHandle,
uint32_t  eventSource 
)

This function initializes the PDM DMA handle, which can be used for other PDM master transactional APIs. Usually, for a specified PDM instance, call this API once to get the initialized handle.

Parameters
basePDM base pointer.
handlePDM eDMA handle pointer.
callbackPointer to user callback function.
userDataUser parameter passed to the callback function.
dmaHandleeDMA handle pointer, this handle shall be static allocated by users.
eventSourcePDM event source number.
status_t PDM_TransferReceiveSDMA ( PDM_Type *  base,
pdm_sdma_handle_t handle,
pdm_transfer_t xfer 
)
Note
This interface returns immediately after the transfer initiates. Call the PDM_GetReceiveRemainingBytes to poll the transfer status and check whether the PDM transfer is finished.
Parameters
basePDM base pointer
handlePDM eDMA handle pointer.
xferPointer to DMA transfer structure.
Return values
kStatus_SuccessStart a PDM eDMA receive successfully.
kStatus_InvalidArgumentThe input argument is invalid.
kStatus_RxBusyPDM is busy receiving data.
void PDM_TransferAbortReceiveSDMA ( PDM_Type *  base,
pdm_sdma_handle_t handle 
)
Parameters
basePDM base pointer
handlePDM eDMA handle pointer.
void PDM_SetChannelConfigSDMA ( PDM_Type *  base,
pdm_sdma_handle_t handle,
uint32_t  channel,
const pdm_channel_config_t config 
)
Parameters
basePDM base pointer.
handlePDM eDMA handle pointer.
channelchannel number.
configchannel configurations.
void PDM_TransferTerminateReceiveSDMA ( PDM_Type *  base,
pdm_sdma_handle_t handle 
)
Parameters
basePDM base pointer.
handlePDM SDMA handle pointer.