MCUXpresso SDK API Reference Manual  Rev 2.15.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
PWM: Pulse Width Modulation Driver

Overview

The MCUXpresso SDK provides a peripheral driver for the Pulse Width Modulation (PWM) module of MCUXpresso SDK devices.

PWM Driver

Initialization and deinitialization

The function PWM_Init() initializes the PWM with a specified configurations. The function PWM_GetDefaultConfig() gets the default configurations.The initialization function configures the PWM for the requested register update mode for registers with buffers.

The function PWM_Deinit() disables the PWM counter and turns off the module clock.

Typical use case

PWM output

Output PWM signal on PWM3 module with different dutycycles. Periodically update the PWM signal duty cycle. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/pwm

Typedefs

typedef enum _pwm_clock_source pwm_clock_source_t
 PWM clock source select. More...
 
typedef enum _pwm_fifo_water_mark pwm_fifo_water_mark_t
 PWM FIFO water mark select. More...
 
typedef enum _pwm_byte_data_swap pwm_byte_data_swap_t
 PWM byte data swap select. More...
 
typedef enum
_pwm_half_word_data_swap 
pwm_half_word_data_swap_t
 PWM half-word data swap select. More...
 
typedef enum
_pwm_output_configuration 
pwm_output_configuration_t
 PWM Output Configuration.
 
typedef enum _pwm_sample_repeat pwm_sample_repeat_t
 PWM FIFO sample repeat It determines the number of times each sample from the FIFO is to be used.
 
typedef enum _pwm_interrupt_enable pwm_interrupt_enable_t
 List of PWM interrupt options.
 
typedef enum _pwm_status_flags pwm_status_flags_t
 List of PWM status flags.
 
typedef enum _pwm_fifo_available pwm_fifo_available_t
 List of PWM FIFO available.
 

Enumerations

enum  _pwm_clock_source {
  kPWM_PeripheralClock = 1U,
  kPWM_HighFrequencyClock,
  kPWM_LowFrequencyClock
}
 PWM clock source select. More...
 
enum  _pwm_fifo_water_mark {
  kPWM_FIFOWaterMark_1 = 0U,
  kPWM_FIFOWaterMark_2,
  kPWM_FIFOWaterMark_3,
  kPWM_FIFOWaterMark_4
}
 PWM FIFO water mark select. More...
 
enum  _pwm_byte_data_swap {
  kPWM_ByteNoSwap = 0U,
  kPWM_ByteSwap
}
 PWM byte data swap select. More...
 
enum  _pwm_half_word_data_swap {
  kPWM_HalfWordNoSwap = 0U,
  kPWM_HalfWordSwap
}
 PWM half-word data swap select. More...
 
enum  _pwm_output_configuration {
  kPWM_SetAtRolloverAndClearAtcomparison = 0U,
  kPWM_ClearAtRolloverAndSetAtcomparison,
  kPWM_NoConfigure
}
 PWM Output Configuration. More...
 
enum  _pwm_sample_repeat {
  kPWM_EachSampleOnce = 0u,
  kPWM_EachSampletwice,
  kPWM_EachSampleFourTimes,
  kPWM_EachSampleEightTimes
}
 PWM FIFO sample repeat It determines the number of times each sample from the FIFO is to be used. More...
 
enum  _pwm_interrupt_enable {
  kPWM_FIFOEmptyInterruptEnable = (1U << 0),
  kPWM_RolloverInterruptEnable = (1U << 1),
  kPWM_CompareInterruptEnable = (1U << 2)
}
 List of PWM interrupt options. More...
 
enum  _pwm_status_flags {
  kPWM_FIFOEmptyFlag = (1U << 3),
  kPWM_RolloverFlag = (1U << 4),
  kPWM_CompareFlag = (1U << 5),
  kPWM_FIFOWriteErrorFlag
}
 List of PWM status flags. More...
 
enum  _pwm_fifo_available {
  kPWM_NoDataInFIFOFlag = 0U,
  kPWM_OneWordInFIFOFlag,
  kPWM_TwoWordsInFIFOFlag,
  kPWM_ThreeWordsInFIFOFlag,
  kPWM_FourWordsInFIFOFlag
}
 List of PWM FIFO available. More...
 

Functions

static void PWM_SoftwareReset (PWM_Type *base)
 Sofrware reset. More...
 
static void PWM_SetPeriodValue (PWM_Type *base, uint32_t value)
 Sets the PWM period value. More...
 
static uint32_t PWM_GetPeriodValue (PWM_Type *base)
 Gets the PWM period value. More...
 
static uint32_t PWM_GetCounterValue (PWM_Type *base)
 Gets the PWM counter value. More...
 

Driver version

#define FSL_PWM_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))
 Version 2.0.0.
 

Initialization and deinitialization

status_t PWM_Init (PWM_Type *base, const pwm_config_t *config)
 Ungates the PWM clock and configures the peripheral for basic operation. More...
 
void PWM_Deinit (PWM_Type *base)
 Gate the PWM submodule clock. More...
 
void PWM_GetDefaultConfig (pwm_config_t *config)
 Fill in the PWM config struct with the default settings. More...
 

PWM start and stop.

static void PWM_StartTimer (PWM_Type *base)
 Starts the PWM counter when the PWM is enabled. More...
 
static void PWM_StopTimer (PWM_Type *base)
 Stops the PWM counter when the pwm is disabled. More...
 

Interrupt Interface

static void PWM_EnableInterrupts (PWM_Type *base, uint32_t mask)
 Enables the selected PWM interrupts. More...
 
static void PWM_DisableInterrupts (PWM_Type *base, uint32_t mask)
 Disables the selected PWM interrupts. More...
 
static uint32_t PWM_GetEnabledInterrupts (PWM_Type *base)
 Gets the enabled PWM interrupts. More...
 

Status Interface

static uint32_t PWM_GetStatusFlags (PWM_Type *base)
 Gets the PWM status flags. More...
 
static void PWM_clearStatusFlags (PWM_Type *base, uint32_t mask)
 Clears the PWM status flags. More...
 
static uint32_t PWM_GetFIFOAvailable (PWM_Type *base)
 Gets the PWM FIFO available. More...
 

Sample Interface

static void PWM_SetSampleValue (PWM_Type *base, uint32_t value)
 Sets the PWM sample value. More...
 
static uint32_t PWM_GetSampleValue (PWM_Type *base)
 Gets the PWM sample value. More...
 

Typedef Documentation

Sets the data level at which the FIFO empty flag will be set

It determines the byte ordering of the 16-bit data when it goes into the FIFO from the sample register.

Enumeration Type Documentation

Enumerator
kPWM_PeripheralClock 

The Peripheral clock is used as the clock.

kPWM_HighFrequencyClock 

High-frequency reference clock is used as the clock.

kPWM_LowFrequencyClock 

Low-frequency reference clock(32KHz) is used as the clock.

Sets the data level at which the FIFO empty flag will be set

Enumerator
kPWM_FIFOWaterMark_1 

FIFO empty flag is set when there are more than or equal to 1 empty slots.

kPWM_FIFOWaterMark_2 

FIFO empty flag is set when there are more than or equal to 2 empty slots.

kPWM_FIFOWaterMark_3 

FIFO empty flag is set when there are more than or equal to 3 empty slots.

kPWM_FIFOWaterMark_4 

FIFO empty flag is set when there are more than or equal to 4 empty slots.

It determines the byte ordering of the 16-bit data when it goes into the FIFO from the sample register.

Enumerator
kPWM_ByteNoSwap 

byte ordering remains the same

kPWM_ByteSwap 

byte ordering is reversed

Enumerator
kPWM_HalfWordNoSwap 

Half word swapping does not take place.

kPWM_HalfWordSwap 

Half word from write data bus are swapped.

Enumerator
kPWM_SetAtRolloverAndClearAtcomparison 

Output pin is set at rollover and cleared at comparison.

kPWM_ClearAtRolloverAndSetAtcomparison 

Output pin is cleared at rollover and set at comparison.

kPWM_NoConfigure 

PWM output is disconnected.

Enumerator
kPWM_EachSampleOnce 

Use each sample once.

kPWM_EachSampletwice 

Use each sample twice.

kPWM_EachSampleFourTimes 

Use each sample four times.

kPWM_EachSampleEightTimes 

Use each sample eight times.

Enumerator
kPWM_FIFOEmptyInterruptEnable 

This bit controls the generation of the FIFO Empty interrupt.

kPWM_RolloverInterruptEnable 

This bit controls the generation of the Rollover interrupt.

kPWM_CompareInterruptEnable 

This bit controls the generation of the Compare interrupt.

Enumerator
kPWM_FIFOEmptyFlag 

This bit indicates the FIFO data level in comparison to the water level set by FWM field in the control register.

kPWM_RolloverFlag 

This bit shows that a roll-over event has occurred.

kPWM_CompareFlag 

This bit shows that a compare event has occurred.

kPWM_FIFOWriteErrorFlag 

This bit shows that an attempt has been made to write FIFO when it is full.

Enumerator
kPWM_NoDataInFIFOFlag 

No data available.

kPWM_OneWordInFIFOFlag 

1 word of data in FIFO

kPWM_TwoWordsInFIFOFlag 

2 word of data in FIFO

kPWM_ThreeWordsInFIFOFlag 

3 word of data in FIFO

kPWM_FourWordsInFIFOFlag 

4 word of data in FIFO

Function Documentation

status_t PWM_Init ( PWM_Type *  base,
const pwm_config_t *  config 
)
Note
This API should be called at the beginning of the application using the PWM driver.
Parameters
basePWM peripheral base address
configPointer to user's PWM config structure.
Returns
kStatus_Success means success; else failed.
void PWM_Deinit ( PWM_Type *  base)
Parameters
basePWM peripheral base address
void PWM_GetDefaultConfig ( pwm_config_t *  config)

The default values are:

* config->enableStopMode = false;
* config->enableDozeMode = false;
* config->enableWaitMode = false;
* config->enableDozeMode = false;
* config->clockSource = kPWM_LowFrequencyClock;
* config->prescale = 0U;
* config->outputConfig = kPWM_SetAtRolloverAndClearAtcomparison;
* config->fifoWater = kPWM_FIFOWaterMark_2;
* config->sampleRepeat = kPWM_EachSampleOnce;
* config->byteSwap = kPWM_ByteNoSwap;
* config->halfWordSwap = kPWM_HalfWordNoSwap;
*
Parameters
configPointer to user's PWM config structure.
static void PWM_StartTimer ( PWM_Type *  base)
inlinestatic

When the PWM is enabled, it begins a new period, the output pin is set to start a new period while the prescaler and counter are released and counting begins.

Parameters
basePWM peripheral base address
static void PWM_StopTimer ( PWM_Type *  base)
inlinestatic
Parameters
basePWM peripheral base address
static void PWM_SoftwareReset ( PWM_Type *  base)
inlinestatic

PWM is reset when this bit is set to 1. It is a self clearing bit. Setting this bit resets all the registers to their reset values except for the STOPEN, DOZEN, WAITEN, and DBGEN bits in this control register.

Parameters
basePWM peripheral base address
static void PWM_EnableInterrupts ( PWM_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
basePWM peripheral base address
maskThe interrupts to enable. This is a logical OR of members of the enumeration pwm_interrupt_enable_t
static void PWM_DisableInterrupts ( PWM_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
basePWM peripheral base address
maskThe interrupts to disable. This is a logical OR of members of the enumeration pwm_interrupt_enable_t
static uint32_t PWM_GetEnabledInterrupts ( PWM_Type *  base)
inlinestatic
Parameters
basePWM peripheral base address
Returns
The enabled interrupts. This is the logical OR of members of the enumeration pwm_interrupt_enable_t
static uint32_t PWM_GetStatusFlags ( PWM_Type *  base)
inlinestatic
Parameters
basePWM peripheral base address
Returns
The status flags. This is the logical OR of members of the enumeration pwm_status_flags_t
static void PWM_clearStatusFlags ( PWM_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
basePWM peripheral base address
maskThe status flags to clear. This is a logical OR of members of the enumeration pwm_status_flags_t
static uint32_t PWM_GetFIFOAvailable ( PWM_Type *  base)
inlinestatic
Parameters
basePWM peripheral base address
Returns
The status flags. This is the logical OR of members of the enumeration pwm_fifo_available_t
static void PWM_SetSampleValue ( PWM_Type *  base,
uint32_t  value 
)
inlinestatic
Parameters
basePWM peripheral base address
valueThe sample value. This is the input to the 4x16 FIFO. The value in this register denotes the value of the sample being currently used.
static uint32_t PWM_GetSampleValue ( PWM_Type *  base)
inlinestatic
Parameters
basePWM peripheral base address
Returns
The sample value. It can be read only when the PWM is enable.
static void PWM_SetPeriodValue ( PWM_Type *  base,
uint32_t  value 
)
inlinestatic
Parameters
basePWM peripheral base address
valueThe period value. The PWM period register (PWM_PWMPR) determines the period of the PWM output signal. Writing 0xFFFF to this register will achieve the same result as writing 0xFFFE. PWMO (Hz) = PCLK(Hz) / (period +2)
static uint32_t PWM_GetPeriodValue ( PWM_Type *  base)
inlinestatic
Parameters
basePWM peripheral base address
Returns
The period value. The PWM period register (PWM_PWMPR) determines the period of the PWM output signal.
static uint32_t PWM_GetCounterValue ( PWM_Type *  base)
inlinestatic
Parameters
basePWM peripheral base address
Returns
The counter value. The current count value.