The MCUXpresso SDK provides a driver for the TSTMR module of MCUXpresso SDK devices.
| static uint64_t TSTMR_ReadTimeStamp |
( |
TSTMR_Type * |
base | ) |
|
|
inlinestatic |
This function reads the low and high registers and returns the 56-bit free running counter value. This can be read by software at any time to determine the software ticks. TSTMR registers can be read with 32-bit accesses only. The TSTMR LOW read should occur first, followed by the TSTMR HIGH read.
- Parameters
-
| base | TSTMR peripheral base address. |
- Returns
- The 56-bit time stamp value.
| static void TSTMR_DelayUs |
( |
TSTMR_Type * |
base, |
|
|
uint32_t |
delayInUs |
|
) |
| |
|
inlinestatic |
This function repeatedly reads the timestamp register and waits for the user-specified delay value.
- Parameters
-
| base | TSTMR peripheral base address. |
| delayInUs | Delay value in microseconds. |