![]() |
MCUXpresso SDK API Reference Manual
Rev 2.14.0
NXP Semiconductors
|
The MCUXpresso SDK provides a driver for the Input multiplexing (INPUTMUX).
It configures the inputs to the pin interrupt block, DMA trigger, and frequency measure function. Once configured, the clock is not needed for the inputmux.
INPUTMUX_AttachSignal function configures the specified input
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/inputmux
Files | |
| file | fsl_inputmux.h |
| file | fsl_inputmux_connections.h |
Functions | |
| void | INPUTMUX_Init (INPUTMUX_Type *base) |
| Initialize INPUTMUX peripheral. More... | |
| void | INPUTMUX_AttachSignal (INPUTMUX_Type *base, uint32_t index, inputmux_connection_t connection) |
| Attaches a signal. More... | |
| void | INPUTMUX_EnableSignal (INPUTMUX_Type *base, inputmux_signal_t signal, bool enable) |
| Enable/disable a signal. More... | |
| void | INPUTMUX_Deinit (INPUTMUX_Type *base) |
| Deinitialize INPUTMUX peripheral. More... | |
Input multiplexing connections | |
| enum | inputmux_connection_t { kINPUTMUX_Sct0In0ToSct0 = 0U + (SCT0_INMUX0 << PMUX_SHIFT) , kINPUTMUX_Sai1RxBclkToSct0 = 76U + (SCT0_INMUX0 << PMUX_SHIFT) , kINPUTMUX_Sai1RxSyncOutToTimer0Captsel = 64U + (TIMER0CAPTSEL0 << PMUX_SHIFT) , kINPUTMUX_Sai1RxSyncOutToTimer1Captsel = 64U + (TIMER1CAPTSEL0 << PMUX_SHIFT) , kINPUTMUX_Sai1RxSyncOutToTimer2Captsel = 64U + (TIMER2CAPTSEL0 << PMUX_SHIFT) , kINPUTMUX_Sai1RxSyncOutToTimer3Captsel = 64U + (TIMER3CAPTSEL0 << PMUX_SHIFT) , kINPUTMUX_Sai1RxSyncOutToTimer4Captsel = 64U + (TIMER4CAPTSEL0 << PMUX_SHIFT) , kINPUTMUX_Sai1RxSyncOutToTimer0Trigger = 64U + (TIMER0TRIGIN << PMUX_SHIFT) , kINPUTMUX_Sai1RxSyncOutToTimer1Trigger = 64U + (TIMER1TRIGIN << PMUX_SHIFT) , kINPUTMUX_Sai1RxSyncOutToTimer2Trigger = 64U + (TIMER2TRIGIN << PMUX_SHIFT) , kINPUTMUX_Sai1RxSyncOutToTimer3Trigger = 64U + (TIMER3TRIGIN << PMUX_SHIFT) , kINPUTMUX_Sai1RxSyncOutToTimer4Trigger = 64U + (TIMER4TRIGIN << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToSmartDma = 70U + (SMARTDMAARCHB_INMUX0 << PMUX_SHIFT) , kINPUTMUX_GpioPort1Pin31ToPintsel = 63U + (PINTSEL0 << PMUX_SHIFT) , kINPUTMUX_EvtgOut1AToFreqmeasRef = 9u + (FREQMEAS_REF_REG << PMUX_SHIFT) , kINPUTMUX_EvtgOut1AToFreqmeasTar = 9u + (FREQMEAS_TAR_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToCmp0Trigger = 40U + (CMP0_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToCmp1Trigger = 40U + (CMP1_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToCmp2Trigger = 40U + (CMP2_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_WuuToAdc0Trigger = 65U + (ADC0_TRIG0 << PMUX_SHIFT) , kINPUTMUX_WuuToAdc1Trigger = 65U + (ADC1_TRIG0 << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToDac0Trigger = 31U + (DAC0_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToDac1Trigger = 31U + (DAC1_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToDac2Trigger = 31U + (DAC2_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_TrigIn9ToEnc0Trigger = 51U + (ENC0_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_TrigIn9ToEnc0Home = 51U + (ENC0_HOME_REG << PMUX_SHIFT) , kINPUTMUX_TrigIn9ToEnc0Index = 51U + (ENC0_INDEX_REG << PMUX_SHIFT) , kINPUTMUX_TrigIn9ToEnc0Phaseb = 51U + (ENC0_PHASEB_REG << PMUX_SHIFT) , kINPUTMUX_TrigIn9ToEnc0Phasea = 51U + (ENC0_PHASEA_REG << PMUX_SHIFT) , kINPUTMUX_TrigIn9ToEnc1Trigger = 51U + (ENC1_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_TrigIn9ToEnc1Home = 51U + (ENC1_HOME_REG << PMUX_SHIFT) , kINPUTMUX_TrigIn9ToEnc1Index = 51U + (ENC1_INDEX_REG << PMUX_SHIFT) , kINPUTMUX_TrigIn9ToEnc1Phaseb = 51U + (ENC1_PHASEB_REG << PMUX_SHIFT) , kINPUTMUX_TrigIn9ToEnc1Phasea = 51U + (ENC1_PHASEA_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm0Sm0ExtSync = 60U + (FlexPWM0_SM0_EXTSYNC_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm0Sm1ExtSync = 60U + (FlexPWM0_SM1_EXTSYNC_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm0Sm2ExtSync = 60U + (FlexPWM0_SM2_EXTSYNC_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm0Sm3ExtSync = 60U + (FlexPWM0_SM3_EXTSYNC_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm0Sm0Exta = 60U + (FlexPWM0_SM0_EXTA_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm0Sm1Exta = 60U + (FlexPWM0_SM1_EXTA_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm0Sm2Exta = 60U + (FlexPWM0_SM2_EXTA_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm0Sm3Exta = 60U + (FlexPWM0_SM3_EXTA_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm0ExtForce = 60U + (FlexPWM0_EXTFORCE_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm0Fault0 = 60U + (FlexPWM0_FAULT0_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm0Fault1 = 60U + (FlexPWM0_FAULT1_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm0Fault2 = 60U + (FlexPWM0_FAULT2_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm0Fault3 = 60U + (FlexPWM0_FAULT3_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm1Sm0ExtSync = 60U + (FlexPWM1_SM0_EXTSYNC_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm1Sm1ExtSync = 60U + (FlexPWM1_SM1_EXTSYNC_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm1Sm2ExtSync = 60U + (FlexPWM1_SM2_EXTSYNC_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm1Sm3ExtSync = 60U + (FlexPWM1_SM3_EXTSYNC_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm1Sm0Exta = 60U + (FlexPWM1_SM0_EXTA_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm1Sm1Exta = 60U + (FlexPWM1_SM1_EXTA_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm1Sm2Exta = 60U + (FlexPWM1_SM2_EXTA_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm1Sm3Exta = 60U + (FlexPWM1_SM3_EXTA_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm1ExtForce = 60U + (FlexPWM1_EXTFORCE_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm1Fault0 = 60U + (FlexPWM1_FAULT0_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm1Fault1 = 60U + (FlexPWM1_FAULT1_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm1Fault2 = 60U + (FlexPWM1_FAULT2_REG << PMUX_SHIFT) , kINPUTMUX_Gpio3PinEventTrig1ToFlexPwm1Fault3 = 60U + (FlexPWM1_FAULT3_REG << PMUX_SHIFT) , kINPUTMUX_ExttrigIn1ToPwm0ExtClk = 5U + (PWM0_EXT_CLK_REG << PMUX_SHIFT) , kINPUTMUX_ExttrigIn1ToPwm1ExtClk = 5U + (PWM1_EXT_CLK_REG << PMUX_SHIFT) , kINPUTMUX_SincFilterCh4ToEvtgTrigger = 55U + (EVTG_TRIG0_REG << PMUX_SHIFT) , kINPUTMUX_Lpflexcomm9Trig3ToUsbfsTrigger = 9U + (USBFS_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_Lptmr1ToTsiTrigger = 1U + (TSI_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_EnetPpsOut0ToExtTrigger = 47U + (EXT_TRIG0_REG << PMUX_SHIFT) , kINPUTMUX_WuuToSincFilterChTrigger = 56U + (SINC_FILTER_CH0_REG << PMUX_SHIFT) , kINPUTMUX_FlexioCh7ToOpamp0Trigger = 54U + (OPAMP0_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_FlexioCh7ToOpamp1Trigger = 54U + (OPAMP1_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_FlexioCh7ToOpamp2Trigger = 54U + (OPAMP2_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_WuuToFlexcomm0Trigger = 42U + (FLEXCOMM0_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_WuuToFlexcomm1Trigger = 42U + (FLEXCOMM1_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_WuuToFlexcomm2Trigger = 42U + (FLEXCOMM2_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_WuuToFlexcomm3Trigger = 42U + (FLEXCOMM3_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_WuuToFlexcomm4Trigger = 42U + (FLEXCOMM4_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_WuuToFlexcomm5Trigger = 42U + (FLEXCOMM5_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_WuuToFlexcomm6Trigger = 42U + (FLEXCOMM6_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_WuuToFlexcomm7Trigger = 42U + (FLEXCOMM7_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_WuuToFlexcomm8Trigger = 42U + (FLEXCOMM8_TRIG_REG << PMUX_SHIFT) , kINPUTMUX_WuuToFlexcomm9Trigger = 42U + (FLEXCOMM9_TRIG_REG << PMUX_SHIFT) } |
| INPUTMUX connections type. More... | |
| enum | inputmux_signal_t { kINPUTMUX_FlexSpi0RxToDma0Ch1Ena = 1U + (DMA0_REQ_ENABLE0_REG << ENA_SHIFT) , kINPUTMUX_Evtg0Out0AToDma0Ch31Ena = 31U + (DMA0_REQ_ENABLE0_REG << ENA_SHIFT) , kINPUTMUX_FlexIO0ShiftRegister2RequestToDma0Ch63Ena = 31U + (DMA0_REQ_ENABLE1_REG << ENA_SHIFT) , kINPUTMUX_I3c0RxToDma0Ch95Ena = 31U + (DMA0_REQ_ENABLE2_REG << ENA_SHIFT) , kINPUTMUX_Tsi0OutOfRangeToDma0Ch121Ena = 25U + (DMA0_REQ_ENABLE3_REG << ENA_SHIFT) , kINPUTMUX_Evtg0Out0AToDma1Ch31Ena = 31U + (DMA1_REQ_ENABLE0_REG << ENA_SHIFT) , kINPUTMUX_FlexIO0ShiftRegister2RequestToDma1Ch63Ena = 31U + (DMA1_REQ_ENABLE1_REG << ENA_SHIFT) , kINPUTMUX_I3c0RxToDma1Ch95Ena = 31U + (DMA1_REQ_ENABLE2_REG << ENA_SHIFT) } |
| INPUTMUX signal enable/disable type. More... | |
| #define | SCT0_INMUX0 0x00U |
| Periphinmux IDs. | |
| #define | TIMER0CAPTSEL0 0x20U |
| #define | TIMER0TRIGIN 0x30U |
| #define | TIMER1CAPTSEL0 0x40U |
| #define | TIMER1TRIGIN 0x50U |
| #define | TIMER2CAPTSEL0 0x60U |
| #define | TIMER2TRIGIN 0x70U |
| #define | SMARTDMAARCHB_INMUX0 0xA0U |
| #define | PINTSEL0 0xC0U |
| #define | FREQMEAS_REF_REG 0x180U |
| #define | FREQMEAS_TAR_REG 0x184U |
| #define | TIMER3CAPTSEL0 0x1A0U |
| #define | TIMER3TRIGIN 0x1B0U |
| #define | TIMER4CAPTSEL0 0x1C0U |
| #define | TIMER4TRIGIN 0x1D0U |
| #define | CMP0_TRIG_REG 0x260U |
| #define | ADC0_TRIG0 0x280U |
| #define | ADC1_TRIG0 0x2C0U |
| #define | DAC0_TRIG_REG 0x300U |
| #define | DAC1_TRIG_REG 0x320U |
| #define | DAC2_TRIG_REG 0x340U |
| #define | ENC0_TRIG_REG 0x360U |
| #define | ENC0_HOME_REG 0x364U |
| #define | ENC0_INDEX_REG 0x368U |
| #define | ENC0_PHASEB_REG 0x36CU |
| #define | ENC0_PHASEA_REG 0x370U |
| #define | ENC1_TRIG_REG 0x380U |
| #define | ENC1_HOME_REG 0x384U |
| #define | ENC1_INDEX_REG 0x388U |
| #define | ENC1_PHASEB_REG 0x38CU |
| #define | ENC1_PHASEA_REG 0x390U |
| #define | FlexPWM0_SM0_EXTSYNC_REG 0x3A0U |
| #define | FlexPWM0_SM1_EXTSYNC_REG 0x3A4U |
| #define | FlexPWM0_SM2_EXTSYNC_REG 0x3A8U |
| #define | FlexPWM0_SM3_EXTSYNC_REG 0x3ACU |
| #define | FlexPWM0_SM0_EXTA_REG 0x3B0U |
| #define | FlexPWM0_SM1_EXTA_REG 0x3B4U |
| #define | FlexPWM0_SM2_EXTA_REG 0x3B8U |
| #define | FlexPWM0_SM3_EXTA_REG 0x3BCU |
| #define | FlexPWM0_EXTFORCE_REG 0x3C0U |
| #define | FlexPWM0_FAULT0_REG 0x3C4U |
| #define | FlexPWM0_FAULT1_REG 0x3C8U |
| #define | FlexPWM0_FAULT2_REG 0x3CCU |
| #define | FlexPWM0_FAULT3_REG 0x3D0U |
| #define | FlexPWM1_SM0_EXTSYNC_REG 0x3E0U |
| #define | FlexPWM1_SM1_EXTSYNC_REG 0x3E4U |
| #define | FlexPWM1_SM2_EXTSYNC_REG 0x3E8U |
| #define | FlexPWM1_SM3_EXTSYNC_REG 0x3ECU |
| #define | FlexPWM1_SM0_EXTA_REG 0x3F0U |
| #define | FlexPWM1_SM1_EXTA_REG 0x3F4U |
| #define | FlexPWM1_SM2_EXTA_REG 0x3F8U |
| #define | FlexPWM1_SM3_EXTA_REG 0x3FCU |
| #define | FlexPWM1_EXTFORCE_REG 0x400U |
| #define | FlexPWM1_FAULT0_REG 0x404U |
| #define | FlexPWM1_FAULT1_REG 0x408U |
| #define | FlexPWM1_FAULT2_REG 0x40CU |
| #define | FlexPWM1_FAULT3_REG 0x410U |
| #define | PWM0_EXT_CLK_REG 0x420U |
| #define | PWM1_EXT_CLK_REG 0x424U |
| #define | EVTG_TRIG0_REG 0x440U |
| #define | USBFS_TRIG_REG 0x480U |
| #define | TSI_TRIG_REG 0x4A0U |
| #define | EXT_TRIG0_REG 0x4C0U |
| #define | CMP1_TRIG_REG 0x4E0U |
| #define | CMP2_TRIG_REG 0x500U |
| #define | SINC_FILTER_CH0_REG 0x520U |
| #define | OPAMP0_TRIG_REG 0x580U |
| #define | OPAMP1_TRIG_REG 0x584U |
| #define | OPAMP2_TRIG_REG 0x588U |
| #define | FLEXCOMM0_TRIG_REG 0x5A0U |
| #define | FLEXCOMM1_TRIG_REG 0x5C0U |
| #define | FLEXCOMM2_TRIG_REG 0x5E0U |
| #define | FLEXCOMM3_TRIG_REG 0x600U |
| #define | FLEXCOMM4_TRIG_REG 0x620U |
| #define | FLEXCOMM5_TRIG_REG 0x640U |
| #define | FLEXCOMM6_TRIG_REG 0x660U |
| #define | FLEXCOMM7_TRIG_REG 0x680U |
| #define | FLEXCOMM8_TRIG_REG 0x6A0U |
| #define | FLEXCOMM9_TRIG_REG 0x6C0U |
| #define | FLEXIO_TRIG0_REG 0x6E0U |
| #define | DMA0_REQ_ENABLE0_REG 0x700U |
| #define | DMA0_REQ_ENABLE1_REG 0x710U |
| #define | DMA0_REQ_ENABLE2_REG 0x720U |
| #define | DMA0_REQ_ENABLE3_REG 0x730U |
| #define | DMA1_REQ_ENABLE0_REG 0x780U |
| #define | DMA1_REQ_ENABLE1_REG 0x790U |
| #define | DMA1_REQ_ENABLE2_REG 0x7A0U |
| #define | DMA1_REQ_ENABLE3_REG 0x7B0U |
| #define | ENA_SHIFT 8U |
| #define | PMUX_SHIFT 20U |
Driver version | |
| #define | FSL_INPUTMUX_DRIVER_VERSION (MAKE_VERSION(2, 0, 7)) |
| Group interrupt driver version for SDK. | |
| enum inputmux_signal_t |
| void INPUTMUX_Init | ( | INPUTMUX_Type * | base | ) |
This function enables the INPUTMUX clock.
| base | Base address of the INPUTMUX peripheral. |
| None. |
| void INPUTMUX_AttachSignal | ( | INPUTMUX_Type * | base, |
| uint32_t | index, | ||
| inputmux_connection_t | connection | ||
| ) |
This function attaches multiplexed signals from INPUTMUX to target signals. For example, to attach GPIO PORT0 Pin 5 to PINT peripheral, do the following:
In this example, INTMUX has 8 registers for PINT, PINT_SEL0~PINT_SEL7. With parameter index specified as 2, this function configures register PINT_SEL2.
| base | Base address of the INPUTMUX peripheral. |
| index | The serial number of destination register in the group of INPUTMUX registers with same name. |
| connection | Applies signal from source signals collection to target signal. |
| None. |
| void INPUTMUX_EnableSignal | ( | INPUTMUX_Type * | base, |
| inputmux_signal_t | signal, | ||
| bool | enable | ||
| ) |
This function gates the INPUTPMUX clock.
| base | Base address of the INPUTMUX peripheral. |
| signal | Enable signal register id and bit offset. |
| enable | Selects enable or disable. |
| None. |
| void INPUTMUX_Deinit | ( | INPUTMUX_Type * | base | ) |
This function disables the INPUTMUX clock.
| base | Base address of the INPUTMUX peripheral. |
| None. |