MCUXpresso SDK API Reference Manual  Rev 2.14.0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Mailbox

Overview

The MCUXpresso SDK provides a peripheral driver for the Mailbox module of MCUXpresso SDK devices.

The mailbox driver API provide:

Typical use case

Example of code on primary core, which cause interrupt on secondary core by writing to mailbox register.

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/mailbox

Example of code on secondary core to handle interrupt from primary core.

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/mailbox

Example of code to get/set mutex.

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/mailbox

Files

file  fsl_mailbox.h
 

Functions

static uint32_t MAILBOX_GetMutex (MAILBOX_Type *base)
 Get MUTEX state and lock mutex. More...
 
static void MAILBOX_SetMutex (MAILBOX_Type *base)
 Set MUTEX state. More...
 

Driver version

#define FSL_MAILBOX_DRIVER_VERSION   (MAKE_VERSION(2, 3, 2))
 MAILBOX driver version 2.3.0. More...
 

MAILBOX initialization

CPU ID.

static void MAILBOX_Init (MAILBOX_Type *base)
 Initializes the MAILBOX module. More...
 
static void MAILBOX_Deinit (MAILBOX_Type *base)
 De-initializes the MAILBOX module. More...
 

Macro Definition Documentation

#define FSL_MAILBOX_DRIVER_VERSION   (MAKE_VERSION(2, 3, 2))

Function Documentation

static void MAILBOX_Init ( MAILBOX_Type *  base)
inlinestatic

This function enables the MAILBOX clock only.

Parameters
baseMAILBOX peripheral base address.
static void MAILBOX_Deinit ( MAILBOX_Type *  base)
inlinestatic

This function disables the MAILBOX clock only.

Parameters
baseMAILBOX peripheral base address.
static uint32_t MAILBOX_GetMutex ( MAILBOX_Type *  base)
inlinestatic
Parameters
baseMAILBOX peripheral base address.
Returns
See note
Note
Returns '1' if the mutex was taken or '0' if another resources has the mutex locked. Once a mutex is taken, it can be returned with the MAILBOX_SetMutex() function.
static void MAILBOX_SetMutex ( MAILBOX_Type *  base)
inlinestatic
Parameters
baseMAILBOX peripheral base address.
Note
Sets mutex state to '1' and allows other resources to get the mutex.