MCUXpresso SDK API Reference Manual  Rev 2.12.7
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
CCM32K: 32kHz Clock Control Module

Overview

The MCUxpreeso SDK provides a driver for the 32kHz Clock Control Module (CCM32K)

Control 32kHz free-running oscillator

The function CCM32K_Enable32kFro() can be used to enable/disable 32kHz free-running oscillator. To trim the frequency of output clock when the clock source is selected as 32kHz free-running oscillator, the function CCM32K_Get32kFroTrimValue() has been provided to realize this feature.

Control 32kHz crystal oscillator

The function CCM32K_Set32kOscConfig() can be used to enable/disable/bypass 32kHz Crystal Oscillator. If the parameter "mode" is selected as kCCM32K_Disable32kHzCrystalOsc it means to disable the 32kHz Crystal Oscillator. If the parameter "mode" is selected as kCCM32K_Bypass32kHzCrystalOsc, it means the application uses the 32kHz Oscillator or 32kHz external clock from EXTAL pin.

Data Structures

struct  ccm32k_clock_monitor_config_t
 Clock monitor configuration structure. More...
 
struct  ccm32k_osc_config_t
 The structure of oscillator configuration. More...
 

Enumerations

enum  ccm32k_osc_xtal_cap_t {
  kCCM32K_OscXtal0pFCap = 0x0U,
  kCCM32K_OscXtal2pFCap = 0x1U,
  kCCM32K_OscXtal4pFCap = 0x2U,
  kCCM32K_OscXtal6pFCap = 0x3U,
  kCCM32K_OscXtal8pFCap = 0x4U,
  kCCM32K_OscXtal10pFCap = 0x5U,
  kCCM32K_OscXtal12pFCap = 0x6U,
  kCCM32K_OscXtal14pFCap = 0x7U,
  kCCM32K_OscXtal16pFCap = 0x8U,
  kCCM32K_OscXtal18pFCap = 0x9U,
  kCCM32K_OscXtal20pFCap = 0xAU,
  kCCM32K_OscXtal22pFCap = 0xBU,
  kCCM32K_OscXtal24pFCap = 0xCU,
  kCCM32K_OscXtal26pFCap = 0xDU,
  kCCM32K_OscXtal28pFCap = 0xEU,
  kCCM32K_OscXtal30pFCap = 0xFU
}
 The enumerator of internal capacitance of OSC's XTAL pin. More...
 
enum  ccm32k_osc_extal_cap_t {
  kCCM32K_OscExtal0pFCap = 0x0U,
  kCCM32K_OscExtal2pFCap = 0x1U,
  kCCM32K_OscExtal4pFCap = 0x2U,
  kCCM32K_OscExtal6pFCap = 0x3U,
  kCCM32K_OscExtal8pFCap = 0x4U,
  kCCM32K_OscExtal10pFCap = 0x5U,
  kCCM32K_OscExtal12pFCap = 0x6U,
  kCCM32K_OscExtal14pFCap = 0x7U,
  kCCM32K_OscExtal16pFCap = 0x8U,
  kCCM32K_OscExtal18pFCap = 0x9U,
  kCCM32K_OscExtal20pFCap = 0xAU,
  kCCM32K_OscExtal22pFCap = 0xBU,
  kCCM32K_OscExtal24pFCap = 0xCU,
  kCCM32K_OscExtal26pFCap = 0xDU,
  kCCM32K_OscExtal28pFCap = 0xEU,
  kCCM32K_OscExtal30pFCap = 0xFU
}
 The enumerator of internal capacitance of OSC's EXTAL pin. More...
 
enum  ccm32k_osc_coarse_adjustment_value_t
 The enumerator of osc amplifier coarse fine adjustment. More...
 
enum  ccm32k_osc_mode_t {
  kCCM32K_Disable32kHzCrystalOsc = 0x0U,
  kCCM32K_Enable32kHzCrystalOsc = 0x1U,
  kCCM32K_Bypass32kHzCrystalOsc = 0x3U
}
 The enumerator of 32kHz oscillator. More...
 
enum  {
  kCCM32K_32kOscReadyStatusFlag = CCM32K_STATUS_OSC32K_RDY_MASK,
  kCCM32K_32kOscActiveStatusFlag = CCM32K_STATUS_OSC32K_ACTIVE_MASK,
  kCCM32K_32kFroActiveStatusFlag = CCM32K_STATUS_FRO32K_ACTIVE_MASK,
  kCCM32K_ClockDetectStatusFlag = CCM32K_STATUS_CLOCK_DET_MASK
}
 The enumerator of CCM32K status flag. More...
 
enum  ccm32k_state_t {
  kCCM32K_Both32kFro32kOscDisabled,
  kCCM32K_Only32kFroEnabled = 0x1U,
  kCCM32K_Only32kOscEnabled = 0x2U,
  kCCM32K_Both32kFro32kOscEnabled = ((uint8_t)kCCM32K_Only32kFroEnabled | (uint8_t)kCCM32K_Only32kOscEnabled)
}
 The enumerator of module state. More...
 
enum  ccm32k_clock_source_t {
  kCCM32K_ClockSourceNone = 0x0U,
  kCCM32K_ClockSource32kFro = 0x1U,
  kCCM32K_ClockSource32kOsc = 0x2U
}
 The enumerator of clock source. More...
 
enum  ccm32k_clock_monitor_freq_trim_value_t {
  kCCM32K_ClockMonitor2CycleAssert = 0x0U,
  kCCM32K_ClockMonitor4CycleAssert,
  kCCM32K_ClockMonitor6CycleAssert,
  kCCM32K_ClockMonitor8CycleAssert
}
 Clock monitor frequency trim values. More...
 
enum  ccm32k_clock_monitor_divide_trim_value_t {
  kCCM32K_ClockMonitor_1kHzFro32k_1kHzOsc32k = 0x0U,
  kCCM32K_ClockMonitor_64HzFro32k_1kHzOsc32k = 0x1U,
  kCCM32K_ClockMonitor_1KHzFro32k_64HzOsc32k = 0x2U,
  kCCM32K_ClockMonitor_64HzFro32k_64HzOsc32k = 0x3U
}
 Clock monitor divide trim values. More...
 
enum  ccm32k_clock_source_select_t {
  kCCM32K_ClockSourceSelectFro32k = 0x0U,
  kCCM32K_ClockSourceSelectOsc32k
}
 CCM32K clock source enumeration. More...
 
enum  ccm32k_clock_output_peripheral_t {
  kCCM32K_ClockOutToRtc = 1U << 0U,
  kCCM32K_ClockOutToRfmc = 1U << 1U,
  kCCM32K_ClockOutToNbu = 1U << 2U,
  kCCM32K_ClockOutToWuuRmcPortD = 1U << 3U,
  kCCM32K_ClockOutToOtherModules = 1U << 4U
}
 32kHz clock output peripheral bit map. More...
 

Driver version

#define FSL_CCM32K_DRIVER_VERSION   (MAKE_VERSION(2, 2, 0))
 CCM32K driver version 2.2.0. More...
 

32kHz Free-running Oscillator Interfaces

void CCM32K_Enable32kFro (CCM32K_Type *base, bool enable)
 Enable/Disable 32kHz free-running oscillator. More...
 
static void CCM32K_Lock32kFroWriteAccess (CCM32K_Type *base)
 Lock all further write accesses to the FRO32K_CTRL register until a POR occurs. More...
 
static uint16_t CCM32K_Get32kFroTrimValue (CCM32K_Type *base)
 Get frequency trim value of 32kHz free-running oscillator. More...
 
void CCM32K_Set32kFroTrimValue (CCM32K_Type *base, uint16_t trimValue)
 Set the frequency trim value of 32kHz free-running oscillator by software. More...
 
static void CCM32K_Disable32kFroIFRLoad (CCM32K_Type *base, bool disable)
 Disable/Enable the function of setting 32kHz free-running oscillator trim value when IFR value gets loaded in the SOC. More...
 
static void CCM32K_Lock32kFroTrimWriteAccess (CCM32K_Type *base)
 Lock all further write accesses to the FRO32K_TRIM register until a POR occurs. More...
 

32kHz Crystal Oscillator Interfaces

void CCM32K_Set32kOscConfig (CCM32K_Type *base, ccm32k_osc_mode_t mode, const ccm32k_osc_config_t *config)
 Config 32k Crystal Oscillator. More...
 
static void CCM32K_Lock32kOscWriteAccess (CCM32K_Type *base)
 Lock all further write accesses to the OSC32K_CTRL register until a POR occurs. More...
 

Clock Monitor Control Interfaces

void CCM32K_EnableClockMonitor (CCM32K_Type *base, bool enable)
 Enable/disable clock monitor. More...
 
static void CCM32K_SetClockMonitorFreqTrimValue (CCM32K_Type *base, ccm32k_clock_monitor_freq_trim_value_t trimValue)
 Set clock monitor frequency trim value. More...
 
static void CCM32K_SetClockMonitorDivideTrimValue (CCM32K_Type *base, ccm32k_clock_monitor_divide_trim_value_t trimValue)
 Set clock monitor divide trim value. More...
 
void CCM32K_SetClockMonitorConfig (CCM32K_Type *base, const ccm32k_clock_monitor_config_t *config)
 Config clock monitor one time, including frequency trim value, divide trim value. More...
 
static void CCM32K_LockClockMonitorWriteAccess (CCM32K_Type *base)
 Lock all further write accesses to the CLKMON_CTRL register until a POR occurs. More...
 

Clock Gate Control Interfaces

static void CCM32K_EnableCLKOutToPeripherals (CCM32K_Type *base, uint8_t peripheralMask)
 Enable 32kHz clock output to selected peripherals. More...
 
static void CCM32K_DisableCLKOutToPeripherals (CCM32K_Type *base, uint8_t peripheralMask)
 Disable 32kHz clock output to selected peripherals. More...
 
static void CCM32K_SelectClockSource (CCM32K_Type *base, ccm32k_clock_source_select_t clockSource)
 Select CCM32K module's clock source which will be provide to the device. More...
 
static void CCM32K_LockClockGateWriteAccess (CCM32K_Type *base)
 Lock all further write access to the CGC32K register until a POR occurs. More...
 

Status Interface

static uint32_t CCM32K_GetStatusFlag (CCM32K_Type *base)
 Get the status flag. More...
 

State/Clock Source Interfaces

ccm32k_state_t CCM32K_GetCurrentState (CCM32K_Type *base)
 Get current state. More...
 
ccm32k_clock_source_t CCM32K_GetClockSource (CCM32K_Type *base)
 Return current clock source. More...
 

Data Structure Documentation

struct ccm32k_clock_monitor_config_t

Data Fields

bool enableClockMonitor
 Used to enable/disable clock monitor. More...
 
ccm32k_clock_monitor_freq_trim_value_t freqTrimValue
 Clock minitor frequency trim value. More...
 
ccm32k_clock_monitor_divide_trim_value_t divideTrimValue
 Clock minitor divide trim value. More...
 

Field Documentation

bool ccm32k_clock_monitor_config_t::enableClockMonitor
ccm32k_clock_monitor_freq_trim_value_t ccm32k_clock_monitor_config_t::freqTrimValue
ccm32k_clock_monitor_divide_trim_value_t ccm32k_clock_monitor_config_t::divideTrimValue
struct ccm32k_osc_config_t

Data Fields

bool enableInternalCapBank
 enable/disable the internal capacitance bank. More...
 
ccm32k_osc_xtal_cap_t xtalCap
 The internal capacitance for the OSC XTAL pin from the capacitor bank, only useful when the internal capacitance bank is enabled. More...
 
ccm32k_osc_extal_cap_t extalCap
 The internal capacitance for the OSC EXTAL pin from the capacitor bank, only useful when the internal capacitance bank is enabled. More...
 
ccm32k_osc_coarse_adjustment_value_t coarseAdjustment
 32kHz crystal oscillator amplifier coarse adjustment value. More...
 

Field Documentation

bool ccm32k_osc_config_t::enableInternalCapBank
ccm32k_osc_xtal_cap_t ccm32k_osc_config_t::xtalCap
ccm32k_osc_extal_cap_t ccm32k_osc_config_t::extalCap
ccm32k_osc_coarse_adjustment_value_t ccm32k_osc_config_t::coarseAdjustment

Macro Definition Documentation

#define FSL_CCM32K_DRIVER_VERSION   (MAKE_VERSION(2, 2, 0))

Enumeration Type Documentation

Enumerator
kCCM32K_OscXtal0pFCap 

The internal capacitance for XTAL pin is 0pF.

kCCM32K_OscXtal2pFCap 

The internal capacitance for XTAL pin is 2pF.

kCCM32K_OscXtal4pFCap 

The internal capacitance for XTAL pin is 4pF.

kCCM32K_OscXtal6pFCap 

The internal capacitance for XTAL pin is 6pF.

kCCM32K_OscXtal8pFCap 

The internal capacitance for XTAL pin is 8pF.

kCCM32K_OscXtal10pFCap 

The internal capacitance for XTAL pin is 10pF.

kCCM32K_OscXtal12pFCap 

The internal capacitance for XTAL pin is 12pF.

kCCM32K_OscXtal14pFCap 

The internal capacitance for XTAL pin is 14pF.

kCCM32K_OscXtal16pFCap 

The internal capacitance for XTAL pin is 16pF.

kCCM32K_OscXtal18pFCap 

The internal capacitance for XTAL pin is 18pF.

kCCM32K_OscXtal20pFCap 

The internal capacitance for XTAL pin is 20pF.

kCCM32K_OscXtal22pFCap 

The internal capacitance for XTAL pin is 22pF.

kCCM32K_OscXtal24pFCap 

The internal capacitance for XTAL pin is 24pF.

kCCM32K_OscXtal26pFCap 

The internal capacitance for XTAL pin is 26pF.

kCCM32K_OscXtal28pFCap 

The internal capacitance for XTAL pin is 28pF.

kCCM32K_OscXtal30pFCap 

The internal capacitance for XTAL pin is 30pF.

Enumerator
kCCM32K_OscExtal0pFCap 

The internal capacitance for EXTAL pin is 0pF.

kCCM32K_OscExtal2pFCap 

The internal capacitance for EXTAL pin is 2pF.

kCCM32K_OscExtal4pFCap 

The internal capacitance for EXTAL pin is 4pF.

kCCM32K_OscExtal6pFCap 

The internal capacitance for EXTAL pin is 6pF.

kCCM32K_OscExtal8pFCap 

The internal capacitance for EXTAL pin is 8pF.

kCCM32K_OscExtal10pFCap 

The internal capacitance for EXTAL pin is 10pF.

kCCM32K_OscExtal12pFCap 

The internal capacitance for EXTAL pin is 12pF.

kCCM32K_OscExtal14pFCap 

The internal capacitance for EXTAL pin is 14pF.

kCCM32K_OscExtal16pFCap 

The internal capacitance for EXTAL pin is 16pF.

kCCM32K_OscExtal18pFCap 

The internal capacitance for EXTAL pin is 18pF.

kCCM32K_OscExtal20pFCap 

The internal capacitance for EXTAL pin is 20pF.

kCCM32K_OscExtal22pFCap 

The internal capacitance for EXTAL pin is 22pF.

kCCM32K_OscExtal24pFCap 

The internal capacitance for EXTAL pin is 24pF.

kCCM32K_OscExtal26pFCap 

The internal capacitance for EXTAL pin is 26pF.

kCCM32K_OscExtal28pFCap 

The internal capacitance for EXTAL pin is 28pF.

kCCM32K_OscExtal30pFCap 

The internal capacitance for EXTAL pin is 30pF.

Tunes the internal transconductance (gm) by increasing the current.

Enumerator
kCCM32K_Disable32kHzCrystalOsc 

Disable 32kHz Crystal Oscillator.

kCCM32K_Enable32kHzCrystalOsc 

Enable 32kHz Crystal Oscillator.

kCCM32K_Bypass32kHzCrystalOsc 

Bypass 32kHz Crystal Oscillator, use the 32kHz Oscillator or external 32kHz clock.

anonymous enum
Enumerator
kCCM32K_32kOscReadyStatusFlag 

Indicates the 32kHz crystal oscillator is stable.

kCCM32K_32kOscActiveStatusFlag 

Indicates the 32kHz crystal oscillator is active and in use.

kCCM32K_32kFroActiveStatusFlag 

Indicates the 32kHz free running oscillator is active and in use.

kCCM32K_ClockDetectStatusFlag 

Indicates the clock monitor has detected an error.

Enumerator
kCCM32K_Both32kFro32kOscDisabled 

Indicates both 32kHz free running oscillator and 32kHz crystal oscillator are disabled.

kCCM32K_Only32kFroEnabled 

Indicates only 32kHz free running oscillator is enabled.

kCCM32K_Only32kOscEnabled 

Indicates only 32kHz crystal oscillator is enabled.

kCCM32K_Both32kFro32kOscEnabled 

Indicates both 32kHz free running oscillator and 32kHz crystal oscillator are enabled.

Enumerator
kCCM32K_ClockSourceNone 

None clock source.

kCCM32K_ClockSource32kFro 

32kHz free running oscillator is the clock source.

kCCM32K_ClockSource32kOsc 

32kHz crystal oscillator is the clock source.

Enumerator
kCCM32K_ClockMonitor2CycleAssert 

Clock monitor asserts 2 cycle after expected edge (assert after 10 cycles with no edge).

kCCM32K_ClockMonitor4CycleAssert 

Clock monitor asserts 4 cycle after expected edge (assert after 12 cycles with no edge).

kCCM32K_ClockMonitor6CycleAssert 

Clock monitor asserts 6 cycle after expected edge (assert after 14 cycles with no edge).

kCCM32K_ClockMonitor8CycleAssert 

Clock monitor asserts 8 cycle after expected edge (assert after 16 cycles with no edge).

Enumerator
kCCM32K_ClockMonitor_1kHzFro32k_1kHzOsc32k 

Clock monitor operates at 1 kHz for both FRO32K and OSC32K.

kCCM32K_ClockMonitor_64HzFro32k_1kHzOsc32k 

Clock monitor operates at 64 Hz for FRO32K and clock monitor operates at 1 kHz for OSC32K.

kCCM32K_ClockMonitor_1KHzFro32k_64HzOsc32k 

Clock monitor operates at 1K Hz for FRO32K and clock monitor operates at 64 Hz for OSC32K.

kCCM32K_ClockMonitor_64HzFro32k_64HzOsc32k 

Clock monitor operates at 64 Hz for FRO32K and clock monitor operates at 64 Hz for OSC32K.

Enumerator
kCCM32K_ClockSourceSelectFro32k 

FRO32K clock output is selected as clock source.

kCCM32K_ClockSourceSelectOsc32k 

OSC32K clock output is selected as clock source.

Enumerator
kCCM32K_ClockOutToRtc 

32kHz clock output to RTC.

kCCM32K_ClockOutToRfmc 

32kHz clock output to Rfmc.

kCCM32K_ClockOutToNbu 

32kHz clock output to NBU.

kCCM32K_ClockOutToWuuRmcPortD 

32kHz clock output to WUU/RMC/PORTD.

kCCM32K_ClockOutToOtherModules 

32kHz clock output to Other modules.

Function Documentation

void CCM32K_Enable32kFro ( CCM32K_Type *  base,
bool  enable 
)
Note
There is a start up time before clocks are output from the FRO.
To enable FRO32k and set it as 32kHz clock source please follow steps:
* CCM32K_Enable32kFro(base, true); //Enable FRO analog oscillator.
* CCM32K_DisableCLKOutToPeripherals(base, mask); //Disable clock out.
* CCM32K_SelectClockSource(base, kCCM32K_ClockSourceSelectFro32k); //Select FRO32k as clock source.
* while(CCM32K_GetStatus(base) != kCCM32K_32kFroActiveStatusFlag); //Check FOR32k is active and in used.
* CCM32K_EnableCLKOutToPeripherals(base, mask); //Enable clock out if needed.
*
Parameters
baseCCM32K peripheral base address.
enableBoolean value to enable or disable the 32kHz free-running oscillator. true – Enable 32kHz free-running oscillator. false – Disable 32kHz free-running oscillator.
static void CCM32K_Lock32kFroWriteAccess ( CCM32K_Type *  base)
inlinestatic
Parameters
baseCCM32K peripheral base address.
static uint16_t CCM32K_Get32kFroTrimValue ( CCM32K_Type *  base)
inlinestatic
Parameters
baseCCM32K peripheral base address.
Returns
The current trim value.
void CCM32K_Set32kFroTrimValue ( CCM32K_Type *  base,
uint16_t  trimValue 
)
Note
The frequency is decreased monotonically when the trimValue is changed progressively from 0x0U to 0x7FFU.
If the FRO32 is enabled before invoking this function, then in this function the FRO32 will be disabled, after updating trim value the FRO32 will be re-enabled.
Parameters
baseCCM32K peripheral base address.
trimValueThe frequency trim value.
static void CCM32K_Disable32kFroIFRLoad ( CCM32K_Type *  base,
bool  disable 
)
inlinestatic
Parameters
baseCCM32K peripheral base address.
disableBoolean value to disable or enable IFR loading function. true – Disable IFR loading function. false – Enable IFR loading function.
static void CCM32K_Lock32kFroTrimWriteAccess ( CCM32K_Type *  base)
inlinestatic
Parameters
baseCCM32K peripheral base address.
void CCM32K_Set32kOscConfig ( CCM32K_Type *  base,
ccm32k_osc_mode_t  mode,
const ccm32k_osc_config_t *  config 
)
Note
When the mode selected as kCCM32K_Disable32kHzCrystalOsc or kCCM32K_Bypass32kHzCrystalOsc the parameter config is useless, so it can be set as "NULL".
To enable OSC32K and select it as clock source of 32kHz please follow steps:
* CCM32K_Set32kOscConfig(base, kCCM32K_Enable32kHzCrystalOsc, config); //Enable OSC32k and set config.
* while((CCM32K_GetStatus(base) & kCCM32K_32kOscReadyStatusFlag) == 0UL); //Check if OSC32K is stable.
* CCM32K_DisableCLKOutToPeripherals(base, mask); //Disable clock out.
* CCM32K_SelectClockSource(base, kCCM32K_ClockSourceSelectOsc32k); //Select OSC32k as clock source.
* while((CCM32K_GetStatus(base) & kCCM32K_32kOscActiveStatusFlag) == 0UL); //Check if OSC32K is used as clock source.
* CCM32K_EnableCLKOutToPeripherals(base, mask); //Enable clock out.
*
Parameters
baseCCM32K peripheral base address.
modeThe mode of 32k crystal oscillator.
configThe pointer to the structure ccm32k_osc_config_t.
static void CCM32K_Lock32kOscWriteAccess ( CCM32K_Type *  base)
inlinestatic
Parameters
baseCCM32K peripheral base address.
void CCM32K_EnableClockMonitor ( CCM32K_Type *  base,
bool  enable 
)
Parameters
baseCCM32K peripheral base address.
enableUsed to enable/disable clock monitor.
  • turn Enable clock monitor.
  • false Disable clock monitor.
static void CCM32K_SetClockMonitorFreqTrimValue ( CCM32K_Type *  base,
ccm32k_clock_monitor_freq_trim_value_t  trimValue 
)
inlinestatic
Parameters
baseCCM32K peripheral base address.
trimValueClock minitor frequency trim value, please refer to ccm32k_clock_monitor_freq_trim_value_t.
static void CCM32K_SetClockMonitorDivideTrimValue ( CCM32K_Type *  base,
ccm32k_clock_monitor_divide_trim_value_t  trimValue 
)
inlinestatic
Parameters
baseCCM32K peripheral base address.
trimValueClock minitor divide trim value, please refer to ccm32k_clock_monitor_divide_trim_value_t.
void CCM32K_SetClockMonitorConfig ( CCM32K_Type *  base,
const ccm32k_clock_monitor_config_t *  config 
)
Parameters
baseCCM32K peripheral base address.
configPointer to ccm32k_clock_monitor_config_t structure.
static void CCM32K_LockClockMonitorWriteAccess ( CCM32K_Type *  base)
inlinestatic
Parameters
baseCCM32K peripheral base address.
static void CCM32K_EnableCLKOutToPeripherals ( CCM32K_Type *  base,
uint8_t  peripheralMask 
)
inlinestatic
Parameters
baseCCM32K peripheral base address.
peripheralMaskThe mask of peripherals to enable 32kHz clock output, should be the OR'ed value of ccm32k_clock_output_peripheral_t.
static void CCM32K_DisableCLKOutToPeripherals ( CCM32K_Type *  base,
uint8_t  peripheralMask 
)
inlinestatic
Parameters
baseCCM32K peripheral base address.
peripheralMaskThe mask of peripherals to disable 32kHz clock output, should be the OR'ed value of ccm32k_clock_output_peripheral_t.
static void CCM32K_SelectClockSource ( CCM32K_Type *  base,
ccm32k_clock_source_select_t  clockSource 
)
inlinestatic
Parameters
baseCCM32K peripheral base address.
clockSourceUsed to select clock source, please refer to ccm32k_clock_source_select_t for details.
static void CCM32K_LockClockGateWriteAccess ( CCM32K_Type *  base)
inlinestatic
Parameters
baseCCM32K peripheral base address.
static uint32_t CCM32K_GetStatusFlag ( CCM32K_Type *  base)
inlinestatic
Parameters
baseCCM32K peripheral base address.
Returns
The status flag of the current node. The enumerator of status flags have been provided, please see the Enumerations title for details.
ccm32k_state_t CCM32K_GetCurrentState ( CCM32K_Type *  base)
Parameters
baseCCM32K peripheral base address.
Returns
The CCM32K's current state, please refer to ccm32k_state_t for details.
ccm32k_clock_source_t CCM32K_GetClockSource ( CCM32K_Type *  base)
Parameters
baseCCM32K peripheral base address.
Return values
kCCM32K_ClockSourceNoneThe none clock source is selected.
kCCM32K_ClockSource32kFro32kHz free-running oscillator is selected as clock source.
kCCM32K_ClockSource32kOsc32kHz crystal oscillator is selected as clock source..