The MCUXpresso SDK provides a peripheral driver for the eeprom emulation module of MCUXpresso SDK devices.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/eeprom_emulation
|
|
void | EE_GetDefaultConfig (eeprom_emulation_config_t *config) |
| |
|
void | EE_SetEepromEmulationInfo (eeprom_emulation_handle_t *handle, eeprom_emulation_config_t *config) |
| |
|
uint32_t | EE_Init (eeprom_emulation_handle_t *handle) |
| |
|
uint32_t | EE_WriteData (eeprom_emulation_handle_t *handle, uint16_t dataID, uint32_t source) |
| |
|
uint32_t | EE_ReadData (eeprom_emulation_handle_t *handle, uint16_t dataID, uint32_t *recordAddr) |
| |
|
uint32_t | EE_ReportStatus (eeprom_emulation_handle_t *handle) |
| |
|
uint32_t | EE_Deinit (eeprom_emulation_handle_t *handle) |
| |
|
uint32_t | EE_Main (eeprom_emulation_handle_t *handle) |
| |
|
uint32_t | EE_NextSector (eeprom_emulation_handle_t *handle, uint32_t addr) |
| |
|
uint32_t | EE_PrevSector (eeprom_emulation_handle_t *handle, uint32_t addr) |
| |
|
uint32_t | EE_VerifyRecordStatus (eeprom_emulation_handle_t *handle, uint32_t dest, uint32_t expData) |
| |
|
uint32_t | EE_VerifySectorHeader (eeprom_emulation_handle_t *handle, uint32_t dest, uint32_t expData) |
| |
|
uint32_t | EE_MultiProgram (eeprom_emulation_handle_t *handle, uint32_t dest, uint32_t size, uint8_t *pData) |
| |
|
uint32_t | EE_CopyRecord (eeprom_emulation_handle_t *handle, eeprom_emulation_data_record_t dataRecord, uint8_t remainData[]) |
| |
|
uint32_t | EE_SwapSector (eeprom_emulation_handle_t *handle) |
| |
|
uint32_t | EE_SearchInSector (eeprom_emulation_handle_t *handle, uint16_t expID, uint32_t sectorAddress) |
| |
|
uint32_t | EE_SearchBlankSpace (eeprom_emulation_handle_t *handle, uint32_t sectorAddress) |
| |
|
uint32_t | EE_SearchInAllActives (eeprom_emulation_handle_t *handle, uint16_t dataID) |
| |
|
uint32_t | EE_SearchLoop (eeprom_emulation_handle_t *handle, uint16_t dataID) |
| |
|
uint32_t | EE_BlankCheck (eeprom_emulation_handle_t *handle, uint32_t address, uint32_t size) |
| |
|
uint8_t | EE_GetSectorStatus (eeprom_emulation_handle_t *handle, uint32_t sectorAddress) |
| |
|
uint32_t | EE_FindActSector (eeprom_emulation_handle_t *handle, uint32_t sectorAddress, bool closestFlag, bool nextFlag) |
| |
|
uint8_t | EE_GetSectorNumber (eeprom_emulation_handle_t *handle, uint8_t expStatus) |
| |
|
uint32_t | EE_ValidateDeadIndicator (eeprom_emulation_handle_t *handle, uint32_t sectorAddress) |
| |
|
uint32_t | EE_ValidateEraseCycle (eeprom_emulation_handle_t *handle, uint32_t sectorAddress, uint8_t *pData) |
| |
|
uint32_t | EE_ValidateActIndicator (eeprom_emulation_handle_t *handle, uint32_t sectorAddress) |
| |
|
uint32_t | EE_ReEraseEeprom (eeprom_emulation_handle_t *handle, uint32_t sectorAddress) |
| |
|
uint32_t | EE_CheckAvailabilityStatus (eeprom_emulation_handle_t *handle) |
| |
|
| AT_QUICKACCESS_SECTION_CODE (uint32_t EE_FlashEraseAll(eeprom_emulation_handle_t *handle)) |
| |
|
uint32_t | EE_FlashCheckErrorCode (void) |
| |
|
| AT_QUICKACCESS_SECTION_CODE (uint32_t EE_SyncFlashErase(eeprom_emulation_handle_t *handle, uint32_t destination)) |
| |
|
| AT_QUICKACCESS_SECTION_CODE (uint32_t EE_FlashEraseVerifySection(eeprom_emulation_handle_t *handle, uint32_t destination, uint16_t Number, uint8_t marginLevel)) |
| |
|
| AT_QUICKACCESS_SECTION_CODE (uint32_t EE_SingleProgram(eeprom_emulation_handle_t *handle, uint32_t destination, uint8_t *pData)) |
| |
|
uint32_t | EE_SingleProgramCheck (eeprom_emulation_handle_t *handle, uint32_t destination, uint8_t *pExpectedData, uint8_t marginLevel) |
| |
|
void | FLASH_CACHE_Disable (void) |
| |