MCUXpresso SDK API Reference Manual  Rev 2.15.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
IOMUXC: IOMUX Controller

Overview

IOMUXC driver provides APIs for pin configuration. It also supports the miscellaneous functions integrated in IOMUXC.

The MCUXpresso SDK provides a peripheral driver for the Input/Output Multiplexing Controller.

The IOMUXC, working in conjunction with the IOMUX, enables the chip to share one pad for multiple signals from different peripheral interfaces.

Files

file  fsl_iomuxc.h
 

Data Structures

struct  iomux_pin_config_t
 IOMUXC pin configuration structure. More...
 
struct  iomuxc_input_pin_config_t
 IOMUXC pin configuration and mux for input function. More...
 
struct  iomux_pin_reset_config_t
 IOMUXC pin configuration reset value structure. More...
 

Enumerations

enum  _iomuxc_pull {
  kIOMUXC_PullDisable = 0U,
  kIOMUXC_PullDown = 2U,
  kIOMUXC_PullUp = 3U
}
 Internal resistor pull feature selection. More...
 
enum  _iomuxc_slew_rate {
  kIOMUXC_StandardSlewRate = 0U,
  kIOMUXC_SlowSlewRate = 1U
}
 Slew rate selection. More...
 
enum  _iomuxc_open_drain_enable {
  kIOMUXC_OpenDrainDisable = 0U,
  kIOMUXC_OpenDrainEnable = 1U
}
 Internal resistor pull feature enable/disable. More...
 
enum  _iomuxc_drive_strength {
  kIOMUXC_StandardDriveStrength = 0U,
  kIOMUXC_HighDriveStrength = 1U
}
 Configures the drive strength. More...
 
enum  _iomuxc_mux {
  kIOMUXC_MuxAlt0 = 0U,
  kIOMUXC_MuxAlt1 = 1U,
  kIOMUXC_MuxAlt2 = 2U,
  kIOMUXC_MuxAlt3 = 3U,
  kIOMUXC_MuxAlt4 = 4U,
  kIOMUXC_MuxAlt5 = 5U,
  kIOMUXC_MuxAlt6 = 6U,
  kIOMUXC_MuxAlt7 = 7U,
  kIOMUXC_MuxAlt8 = 8U,
  kIOMUXC_MuxAlt9 = 9U,
  kIOMUXC_MuxAlt10 = 10U,
  kIOMUXC_MuxAlt11 = 11U,
  kIOMUXC_MuxAlt12 = 12U,
  kIOMUXC_MuxAlt13 = 13U,
  kIOMUXC_MuxAlt14 = 14U,
  kIOMUXC_MuxAlt15 = 15U
}
 Pin mux selection. More...
 
enum  _iomuxc_lock_register {
  kIOMUXC_UnlockRegister = 0U,
  kIOMUXC_LockRegister = 1U
}
 Unlock/lock the pin control register field[15:0]. More...
 
enum  _iomuxc_input_buffer_enable {
  kIOMUXC_InputBufferDisable = 0U,
  kIOMUXC_InputBufferEnable = 1U
}
 Input buffer feature enable/disable. More...
 
enum  _iomuxc_output_buffer_enable {
  kIOMUXC_outputBufferDisable = 0U,
  kIOMUXC_outputBufferEnable = 1U
}
 output buffer feature enable/disable More...
 
enum  iomux_digital_filter_clock_select_t {
  kIOMUXC_IPGClock = 0U,
  kIOMUXC_1KhzClock = 1U
}
 Digital filter clock selection. More...
 
enum  _iomuxc_inputpin_mux {
  kIOMUXC_InputMuxAlt0 = 0u,
  kIOMUXC_InputMuxAlt1 = 1U,
  kIOMUXC_InputMuxAlt2 = 2U,
  kIOMUXC_InputMuxAlt3 = 3U
}
 Input pin mux selection(DAISY). More...
 
enum  _iomuxc_input_inversion_enable {
  kIOMUXC_InputInversionDisable = 0U,
  kIOMUXC_InputInversionEnable = 1U
}
 Input inversion feature enable/disable. More...
 

Driver version

#define FSL_IOMUXC_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))
 < Version 2.0.0. More...
 

Configuration

#define IOMUXC_SET_MUX_CONTROL_PAD(instance, iomuxc_port, pin, config)   (instance)->SW_MUX_CTL_PAD[(iomuxc_port)*32U + (pin)] = *((const uint32_t *)(&config));
 Sets the IOMUXC SW MUX Control Register. More...
 
#define IOMUXC_SET_INPUTPIN_CONFIG(instance, index, config)   (instance)->SELECT_INPUT[index] = *((const uint32_t *)(&config));
 Sets the IOMUXC input function pin configuration: the N_SELECT_INPUT_DAISY_Register. More...
 
#define IOMUXC_SET_MUX_CONTROL_PAD_RESET(instance, config)
 Sets the reset value for IOMUXC0 SW MUX Control Register. More...
 

Data Structure Documentation

struct iomux_pin_config_t
Note
for i.MX7ULP, the SW_MUX_CTL_PAD of IOMUXC0 and IOMUXC1 is a little different in the digital filter feature. The SW_MUX_CTL_PAD of IOMUXC1 has no digital filter feature. For this case, just ignore the digital filter fields.

Data Fields

uint32_t pullSelect: 2
 No-pull/pull-down/pull-up select.
 
uint32_t slewRate: 1
 Standard/slow slew rate Configure.
 
uint32_t openDrainEnable: 1
 Open drain enable/disable.
 
uint32_t driveStrength: 1
 Standard/slow drive strength configure.
 
uint32_t mux: 4
 Pin mux Configure.
 
uint32_t lockRegister: 1
 Lock/unlock the PCR field[15:0].
 
uint32_t inputBufferEnable: 1
 Input buffer is enable/disable. More...
 
uint32_t outputBufferEnable: 1
 Output buffer is enable/disable. More...
 
uint32_t digitalFilterEnable: 1
 Digital filters are enable/disable. More...
 
uint32_t digitalFilterSelect: 1
 Set digital filter clockSource.
 
uint32_t digitalFilterDuration: 5
 Set digital filter duration.
 

Field Documentation

uint32_t iomux_pin_config_t::inputBufferEnable
uint32_t iomux_pin_config_t::outputBufferEnable
uint32_t iomux_pin_config_t::digitalFilterEnable
struct iomuxc_input_pin_config_t

Data Fields

uint32_t daisy: 2
 Selects source pad for Module Input Function. More...
 
uint32_t inversion: 1
 Controls the inversion of the pad->module input to instance.
 

Field Documentation

uint32_t iomuxc_input_pin_config_t::daisy

Refer to "Input SSS" column from "Input Mux" IOMUX Sheet.

struct iomux_pin_reset_config_t

Data Fields

uint32_t pullSelect: 2
 No-pull/pull-down/pull-up select.
 
uint32_t slewRate: 1
 Standard/slow slew rate Configure.
 
uint32_t openDrainEnable: 1
 Open drain enable/disable.
 
uint32_t driveStrength: 1
 Standard/slow drive strength configure.
 
uint32_t lockRegister: 1
 Lock/unlock the PCR field[15:0].
 

Macro Definition Documentation

#define FSL_IOMUXC_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))
#define IOMUXC_SET_MUX_CONTROL_PAD (   instance,
  iomuxc_port,
  pin,
  config 
)    (instance)->SW_MUX_CTL_PAD[(iomuxc_port)*32U + (pin)] = *((const uint32_t *)(&config));
Note
Uses macro instead of inline function is to avoid the parameter type check, because the IOMUXC0 and IOMUXC1 is differnt.
Parameters
instanceIOMUXC instance. It's pointer to IOMUXC0_Type or IOMUXC1_Type in the soc head file.
iomuxc_portIOMUXC PORT name, please refer the enum iomuxc0_port_t and iomuxc1_port_t.
pinpin number.
configstructure object of iomux_pin_config_t, not a pointer.
#define IOMUXC_SET_INPUTPIN_CONFIG (   instance,
  index,
  config 
)    (instance)->SELECT_INPUT[index] = *((const uint32_t *)(&config));
Parameters
instanceIOMUXC instance. It's pointer to IOMUXC0_Type or IOMUXC1_Type in the soc head file.
indexregister index, please refer the iomuxc0_select_input_t and iomuxc1_select_input_t.
configstructure object of iomuxc_input_pin_config_t, not a pointer.
#define IOMUXC_SET_MUX_CONTROL_PAD_RESET (   instance,
  config 
)
Value:
if ((uint32_t)instance == IOMUXC0_BASE) \
{ \
((IOMUXC0_Type *)instance)->SW_MUX_CTL_PAD_RESET0_b = *((const uint32_t *)(&config)); \
} \
else \
{ \
((IOMUXC1_Type *)instance)->SW_MUX_CTL_PAD_RESET1_b = *((const uint32_t *)(&config)); \
}
Parameters
instanceIOMUXC instance. It's pointer to IOMUXC0_Type or IOMUXC1_Type in the soc head file.
configstructure object of iomux_pin_config_t, not a pointer.

Enumeration Type Documentation

Enumerator
kIOMUXC_PullDisable 

Internal pull-up/down resistor is disabled.

kIOMUXC_PullDown 

Internal pull-down resistor is enabled.

kIOMUXC_PullUp 

Internal pull-up resistor is enabled.

Enumerator
kIOMUXC_StandardSlewRate 

Standard slew rate is configured.

kIOMUXC_SlowSlewRate 

Slow slew rate is configured.

Enumerator
kIOMUXC_OpenDrainDisable 

Internal pull-down resistor is disabled.

kIOMUXC_OpenDrainEnable 

Internal pull-up resistor is enabled.

Enumerator
kIOMUXC_StandardDriveStrength 

Standard-drive strength is configured.

kIOMUXC_HighDriveStrength 

High-drive strength is configured.

Enumerator
kIOMUXC_MuxAlt0 

Chip-specific.

kIOMUXC_MuxAlt1 

Chip-specific.

kIOMUXC_MuxAlt2 

Chip-specific.

kIOMUXC_MuxAlt3 

Chip-specific.

kIOMUXC_MuxAlt4 

Chip-specific.

kIOMUXC_MuxAlt5 

Chip-specific.

kIOMUXC_MuxAlt6 

Chip-specific.

kIOMUXC_MuxAlt7 

Chip-specific.

kIOMUXC_MuxAlt8 

Chip-specific.

kIOMUXC_MuxAlt9 

Chip-specific.

kIOMUXC_MuxAlt10 

Chip-specific.

kIOMUXC_MuxAlt11 

Chip-specific.

kIOMUXC_MuxAlt12 

Chip-specific.

kIOMUXC_MuxAlt13 

Chip-specific.

kIOMUXC_MuxAlt14 

Chip-specific.

kIOMUXC_MuxAlt15 

Chip-specific.

Enumerator
kIOMUXC_UnlockRegister 

Pin Control Register fields [15:0] are not locked.

kIOMUXC_LockRegister 

Pin Control Register fields [15:0] are locked.

Enumerator
kIOMUXC_InputBufferDisable 

Input buffer is disabled.

kIOMUXC_InputBufferEnable 

Output buffer is enabled.

Enumerator
kIOMUXC_outputBufferDisable 

Output buffer is disabled.

kIOMUXC_outputBufferEnable 

Output buffer is enabled.

Enumerator
kIOMUXC_IPGClock 

Digital filters are clocked by the IPG clock.

kIOMUXC_1KhzClock 

Digital filters are clocked by the 1kHz clock.

Refer to "Input SSS" column from "Input Mux" IOMUX Sheet.

Enumerator
kIOMUXC_InputMuxAlt0 

Chip-specific.

kIOMUXC_InputMuxAlt1 

Chip-specific.

kIOMUXC_InputMuxAlt2 

Chip-specific.

kIOMUXC_InputMuxAlt3 

Chip-specific.

Enumerator
kIOMUXC_InputInversionDisable 

Input inversion is disabled.

kIOMUXC_InputInversionEnable 

Output inversion is enabled.