MCUXpresso SDK API Reference Manual  Rev 2.15.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Sentinel

Overview

Macros

#define SENTINEL_BASELINE_API_CMD_PING   (0x01U)
 sentinel command definition. More...
 

Functions

void SENTINEL_Init (void)
 Initialize MU interface for Sentinel access.
 
void SENTINEL_Deinit (void)
 Deinitialize MU interface for Sentinel access.
 
void SENTINEL_SendMessage (uint32_t *param, uint32_t paramCount)
 Send message to Sentinel. More...
 
void SENTINEL_ReceiveMessage (uint32_t *pParam, uint32_t *pParamCount)
 Receive message from Sentinel. More...
 
uint32_t SENTINEL_Command (uint32_t *cmdParam, uint32_t cmdParamCount, uint32_t *pRespParam, uint32_t *pRespParamCount)
 Send command to Sentinel and receive response. More...
 
uint32_t SENTINEL_Ping (void)
 Ping Sentinel to see if it is alive. More...
 
uint32_t SENTINEL_GetFirmwareVersion (uint32_t *pVersion, uint32_t *pCommitSha)
 Get Sentinel firmware version. More...
 
uint32_t SENTINEL_GetFirmwareStatus (uint8_t *pStatus)
 Get Sentinel firmware status. More...
 
uint32_t SENTINEL_SetPowerDown (uint32_t resumeAddr, uint32_t size)
 Request Sentinel to enter power down. More...
 
uint32_t SENTINEL_GetSocInfo (uint16_t *pSoc_id, uint16_t *pSoc_rev)
 Get Sentinel cpu version. More...
 

Driver version

#define FSL_SENTINEL_DRIVER_VERSION   (MAKE_VERSION(2, 0, 3))
 sentinel driver version 2.0.3. More...
 

Macro Definition Documentation

#define SENTINEL_BASELINE_API_CMD_PING   (0x01U)
#define FSL_SENTINEL_DRIVER_VERSION   (MAKE_VERSION(2, 0, 3))

Function Documentation

void SENTINEL_SendMessage ( uint32_t *  param,
uint32_t  paramCount 
)
Parameters
paramCommand parameters pointer. Each parameter is a 32bit word.
paramCountCommand parameter count.
void SENTINEL_ReceiveMessage ( uint32_t *  pParam,
uint32_t *  pParamCount 
)
Parameters
pParamPointer to save command parameters. Each parameter is a 32bit word.
pParamCountInout pointer to command parameter count.
uint32_t SENTINEL_Command ( uint32_t *  cmdParam,
uint32_t  cmdParamCount,
uint32_t *  pRespParam,
uint32_t *  pRespParamCount 
)
Parameters
cmdParamCommand parameters pointer. Each parameter is a 32bit word.
cmdParamCountCommand parameter count.
pRespParamPointer to save response parameters. Each parameter is a 32bit word.
pRespParamCountInout pointer to response parameter count.
Returns
0 for success, otherwise return error code.
uint32_t SENTINEL_Ping ( void  )
Returns
0 for success, otherwise return error code.
uint32_t SENTINEL_GetFirmwareVersion ( uint32_t *  pVersion,
uint32_t *  pCommitSha 
)
Parameters
pVersionPointer to save firmware version.
pCommitShaPointer to save first 4 bytes of the git commit ID.
Returns
0 for success, otherwise return error code.
uint32_t SENTINEL_GetFirmwareStatus ( uint8_t *  pStatus)
Parameters
pStatusPointer to save firmware status. 0: No firmware in place. 1: Firmware authenticated and operational.
Returns
0 for success, otherwise return error code.
uint32_t SENTINEL_SetPowerDown ( uint32_t  resumeAddr,
uint32_t  size 
)
Parameters
resumeAddrBase address in memory for resume code
sizeLength of resume code in memory
Returns
0 for success, otherwise return error code.
uint32_t SENTINEL_GetSocInfo ( uint16_t *  pSoc_id,
uint16_t *  pSoc_rev 
)
Parameters
pSoc_idPointer to soc id.
pSoc_revPointer to soc revision number.
Returns
0 for success, otherwise return error code.