![]() |
MCUXpresso SDK API Reference Manual
Rev 2.15.100
NXP Semiconductors
|
Data Structures | |
| struct | _flexio_uart_edma_handle |
| UART eDMA handle. More... | |
Typedefs | |
| typedef void(* | flexio_uart_edma_transfer_callback_t )(FLEXIO_UART_Type *base, flexio_uart_edma_handle_t *handle, status_t status, void *userData) |
| UART transfer callback function. More... | |
Driver version | |
| #define | FSL_FLEXIO_UART_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 4, 1)) |
| FlexIO UART EDMA driver version. More... | |
| struct _flexio_uart_edma_handle |
Data Fields | |
| flexio_uart_edma_transfer_callback_t | callback |
| Callback function. More... | |
| void * | userData |
| UART callback function parameter. More... | |
| size_t | txDataSizeAll |
| Total bytes to be sent. More... | |
| size_t | rxDataSizeAll |
| Total bytes to be received. More... | |
| edma_handle_t * | txEdmaHandle |
| The eDMA TX channel used. More... | |
| edma_handle_t * | rxEdmaHandle |
| The eDMA RX channel used. More... | |
| uint8_t | nbytes |
| eDMA minor byte transfer count initially configured. More... | |
| volatile uint8_t | txState |
| TX transfer state. More... | |
| volatile uint8_t | rxState |
| RX transfer state. | |
| flexio_uart_edma_transfer_callback_t _flexio_uart_edma_handle::callback |
| void* _flexio_uart_edma_handle::userData |
| size_t _flexio_uart_edma_handle::txDataSizeAll |
| size_t _flexio_uart_edma_handle::rxDataSizeAll |
| edma_handle_t* _flexio_uart_edma_handle::txEdmaHandle |
| edma_handle_t* _flexio_uart_edma_handle::rxEdmaHandle |
| uint8_t _flexio_uart_edma_handle::nbytes |
| volatile uint8_t _flexio_uart_edma_handle::txState |
| #define FSL_FLEXIO_UART_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 4, 1)) |
| typedef void(* flexio_uart_edma_transfer_callback_t)(FLEXIO_UART_Type *base, flexio_uart_edma_handle_t *handle, status_t status, void *userData) |
| status_t FLEXIO_UART_TransferCreateHandleEDMA | ( | FLEXIO_UART_Type * | base, |
| flexio_uart_edma_handle_t * | handle, | ||
| flexio_uart_edma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | txEdmaHandle, | ||
| edma_handle_t * | rxEdmaHandle | ||
| ) |
| base | Pointer to FLEXIO_UART_Type. |
| handle | Pointer to flexio_uart_edma_handle_t structure. |
| callback | The callback function. |
| userData | The parameter of the callback function. |
| rxEdmaHandle | User requested DMA handle for RX DMA transfer. |
| txEdmaHandle | User requested DMA handle for TX DMA transfer. |
| kStatus_Success | Successfully create the handle. |
| kStatus_OutOfRange | The FlexIO SPI eDMA type/handle table out of range. |
| status_t FLEXIO_UART_TransferSendEDMA | ( | FLEXIO_UART_Type * | base, |
| flexio_uart_edma_handle_t * | handle, | ||
| flexio_uart_transfer_t * | xfer | ||
| ) |
This function sends data using eDMA. This is a non-blocking function, which returns right away. When all data is sent out, the send callback function is called.
| base | Pointer to FLEXIO_UART_Type |
| handle | UART handle pointer. |
| xfer | UART eDMA transfer structure, see flexio_uart_transfer_t. |
| kStatus_Success | if succeed, others failed. |
| kStatus_FLEXIO_UART_TxBusy | Previous transfer on going. |
| status_t FLEXIO_UART_TransferReceiveEDMA | ( | FLEXIO_UART_Type * | base, |
| flexio_uart_edma_handle_t * | handle, | ||
| flexio_uart_transfer_t * | xfer | ||
| ) |
This function receives data using eDMA. This is a non-blocking function, which returns right away. When all data is received, the receive callback function is called.
| base | Pointer to FLEXIO_UART_Type |
| handle | Pointer to flexio_uart_edma_handle_t structure |
| xfer | UART eDMA transfer structure, see flexio_uart_transfer_t. |
| kStatus_Success | if succeed, others failed. |
| kStatus_UART_RxBusy | Previous transfer on going. |
| void FLEXIO_UART_TransferAbortSendEDMA | ( | FLEXIO_UART_Type * | base, |
| flexio_uart_edma_handle_t * | handle | ||
| ) |
This function aborts sent data which using eDMA.
| base | Pointer to FLEXIO_UART_Type |
| handle | Pointer to flexio_uart_edma_handle_t structure |
| void FLEXIO_UART_TransferAbortReceiveEDMA | ( | FLEXIO_UART_Type * | base, |
| flexio_uart_edma_handle_t * | handle | ||
| ) |
This function aborts the receive data which using eDMA.
| base | Pointer to FLEXIO_UART_Type |
| handle | Pointer to flexio_uart_edma_handle_t structure |
| status_t FLEXIO_UART_TransferGetSendCountEDMA | ( | FLEXIO_UART_Type * | base, |
| flexio_uart_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
This function gets the number of bytes sent out.
| base | Pointer to FLEXIO_UART_Type |
| handle | Pointer to flexio_uart_edma_handle_t structure |
| count | Number of bytes sent so far by the non-blocking transaction. |
| kStatus_NoTransferInProgress | transfer has finished or no transfer in progress. |
| kStatus_Success | Successfully return the count. |
| status_t FLEXIO_UART_TransferGetReceiveCountEDMA | ( | FLEXIO_UART_Type * | base, |
| flexio_uart_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
This function gets the number of bytes received.
| base | Pointer to FLEXIO_UART_Type |
| handle | Pointer to flexio_uart_edma_handle_t structure |
| count | Number of bytes received so far by the non-blocking transaction. |
| kStatus_NoTransferInProgress | transfer has finished or no transfer in progress. |
| kStatus_Success | Successfully return the count. |