![]() |
MCUXpresso SDK API Reference Manual
Rev 2.15.100
NXP Semiconductors
|
Data Structures | |
| struct | _flexspi_edma_handle |
| FLEXSPI DMA transfer handle, users should not touch the content of the handle. More... | |
Typedefs | |
| typedef void(* | flexspi_edma_callback_t )(FLEXSPI_Type *base, flexspi_edma_handle_t *handle, status_t status, void *userData) |
| FLEXSPI eDMA transfer callback function for finish and error. | |
|
typedef enum _flexspi_edma_ntransfer_size | flexspi_edma_transfer_nsize_t |
| eDMA transfer configuration | |
Enumerations | |
| enum | _flexspi_edma_ntransfer_size { kFLEXPSI_EDMAnSize1Bytes = 0x1U, kFLEXPSI_EDMAnSize2Bytes = 0x2U, kFLEXPSI_EDMAnSize4Bytes = 0x4U, kFLEXPSI_EDMAnSize8Bytes = 0x8U, kFLEXPSI_EDMAnSize32Bytes = 0x20U } |
| eDMA transfer configuration More... | |
Driver version | |
| #define | FSL_FLEXSPI_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 3, 3)) |
| FLEXSPI EDMA driver version. More... | |
FLEXSPI eDMA Transactional | |
| void | FLEXSPI_TransferCreateHandleEDMA (FLEXSPI_Type *base, flexspi_edma_handle_t *handle, flexspi_edma_callback_t callback, void *userData, edma_handle_t *txDmaHandle, edma_handle_t *rxDmaHandle) |
| Initializes the FLEXSPI handle for transfer which is used in transactional functions and set the callback. More... | |
| void | FLEXSPI_TransferUpdateSizeEDMA (FLEXSPI_Type *base, flexspi_edma_handle_t *handle, flexspi_edma_transfer_nsize_t nsize) |
| Update FLEXSPI EDMA transfer source data transfer size(SSIZE) and destination data transfer size(DSIZE). More... | |
| status_t | FLEXSPI_TransferEDMA (FLEXSPI_Type *base, flexspi_edma_handle_t *handle, flexspi_transfer_t *xfer) |
| Transfers FLEXSPI data using an eDMA non-blocking method. More... | |
| void | FLEXSPI_TransferAbortEDMA (FLEXSPI_Type *base, flexspi_edma_handle_t *handle) |
| Aborts the transfer data using eDMA. More... | |
| status_t | FLEXSPI_TransferGetTransferCountEDMA (FLEXSPI_Type *base, flexspi_edma_handle_t *handle, size_t *count) |
| Gets the transferred counts of transfer. More... | |
| struct _flexspi_edma_handle |
Data Fields | |
| edma_handle_t * | txDmaHandle |
| eDMA handler for FLEXSPI Tx. More... | |
| edma_handle_t * | rxDmaHandle |
| eDMA handler for FLEXSPI Rx. More... | |
| size_t | transferSize |
| Bytes need to transfer. More... | |
| flexspi_edma_transfer_nsize_t | nsize |
| eDMA SSIZE/DSIZE in each transfer. More... | |
| uint8_t | nbytes |
| eDMA minor byte transfer count initially configured. More... | |
| uint8_t | count |
| The transfer data count in a DMA request. More... | |
| uint32_t | state |
| Internal state for FLEXSPI eDMA transfer. More... | |
| flexspi_edma_callback_t | completionCallback |
| A callback function called after the eDMA transfer is finished. More... | |
| void * | userData |
| User callback parameter. | |
| edma_handle_t* _flexspi_edma_handle::txDmaHandle |
| edma_handle_t* _flexspi_edma_handle::rxDmaHandle |
| size_t _flexspi_edma_handle::transferSize |
| flexspi_edma_transfer_nsize_t _flexspi_edma_handle::nsize |
| uint8_t _flexspi_edma_handle::nbytes |
| uint8_t _flexspi_edma_handle::count |
| uint32_t _flexspi_edma_handle::state |
| flexspi_edma_callback_t _flexspi_edma_handle::completionCallback |
| #define FSL_FLEXSPI_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 3, 3)) |
| void FLEXSPI_TransferCreateHandleEDMA | ( | FLEXSPI_Type * | base, |
| flexspi_edma_handle_t * | handle, | ||
| flexspi_edma_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | txDmaHandle, | ||
| edma_handle_t * | rxDmaHandle | ||
| ) |
| base | FLEXSPI peripheral base address |
| handle | Pointer to flexspi_edma_handle_t structure |
| callback | FLEXSPI callback, NULL means no callback. |
| userData | User callback function data. |
| txDmaHandle | User requested DMA handle for TX DMA transfer. |
| rxDmaHandle | User requested DMA handle for RX DMA transfer. |
| void FLEXSPI_TransferUpdateSizeEDMA | ( | FLEXSPI_Type * | base, |
| flexspi_edma_handle_t * | handle, | ||
| flexspi_edma_transfer_nsize_t | nsize | ||
| ) |
| base | FLEXSPI peripheral base address |
| handle | Pointer to flexspi_edma_handle_t structure |
| nsize | FLEXSPI DMA transfer data transfer size(SSIZE/DSIZE), by default the size is kFLEXPSI_EDMAnSize1Bytes(one byte). |
| status_t FLEXSPI_TransferEDMA | ( | FLEXSPI_Type * | base, |
| flexspi_edma_handle_t * | handle, | ||
| flexspi_transfer_t * | xfer | ||
| ) |
This function writes/receives data to/from the FLEXSPI transmit/receive FIFO. This function is non-blocking.
| base | FLEXSPI peripheral base address. |
| handle | Pointer to flexspi_edma_handle_t structure |
| xfer | FLEXSPI transfer structure. |
| kStatus_FLEXSPI_Busy | FLEXSPI is busy transfer. |
| kStatus_InvalidArgument | The watermark configuration is invalid, the watermark should be power of 2 to do successfully EDMA transfer. |
| kStatus_Success | FLEXSPI successfully start edma transfer. |
| void FLEXSPI_TransferAbortEDMA | ( | FLEXSPI_Type * | base, |
| flexspi_edma_handle_t * | handle | ||
| ) |
This function aborts the transfer data using eDMA.
| base | FLEXSPI peripheral base address. |
| handle | Pointer to flexspi_edma_handle_t structure |
| status_t FLEXSPI_TransferGetTransferCountEDMA | ( | FLEXSPI_Type * | base, |
| flexspi_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | FLEXSPI peripheral base address. |
| handle | Pointer to flexspi_edma_handle_t structure. |
| count | Bytes transfer. |
| kStatus_Success | Succeed get the transfer count. |
| kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress. |