![]() |
MCUXpresso SDK API Reference Manual
Rev 2.15.100
NXP Semiconductors
|
Data Structures | |
| struct | _iee_config |
| IEE configuration structure. More... | |
Typedefs | |
| typedef enum _iee_region | iee_region_t |
| IEE region. More... | |
| typedef enum _iee_aes_bypass | iee_aes_bypass_t |
| IEE AES enablement/bypass. More... | |
| typedef enum _iee_aes_mode | iee_aes_mode_t |
| IEE AES mode. More... | |
| typedef enum _iee_aes_key_size | iee_aes_key_size_t |
| IEE AES key size. More... | |
| typedef enum _iee_aes_key_num | iee_aes_key_num_t |
| IEE AES ke number. More... | |
| typedef struct _iee_config | iee_config_t |
| IEE configuration structure. More... | |
Enumerations | |
| enum | _iee_region { kIEE_Region0 = 0U, kIEE_Region1 = 1U, kIEE_Region2 = 2U, kIEE_Region3 = 3U, kIEE_Region4 = 4U, kIEE_Region5 = 5U, kIEE_Region6 = 6U, kIEE_Region7 = 7U } |
| IEE region. More... | |
| enum | _iee_aes_bypass { kIEE_AesUseMdField = 0U, kIEE_AesBypass = 1U } |
| IEE AES enablement/bypass. More... | |
| enum | _iee_aes_mode { kIEE_ModeNone = 0U, kIEE_ModeAesXTS = 1U, kIEE_ModeAesCTRWAddress = 2U, kIEE_ModeAesCTRWOAddress = 3U, kIEE_ModeAesCTRkeystream = 4U } |
| IEE AES mode. More... | |
| enum | _iee_aes_key_size { kIEE_AesCTR128XTS256 = 0U, kIEE_AesCTR256XTS512 = 1U } |
| IEE AES key size. More... | |
| enum | _iee_aes_key_num { kIEE_AesKey1 = 1U, kIEE_AesKey2 = 2U } |
| IEE AES ke number. More... | |
Functions | |
| void | IEE_Init (IEE_Type *base) |
| Resets IEE module to factory default values. More... | |
| void | IEE_GetDefaultConfig (iee_config_t *config) |
| Loads default values to the IEE configuration structure. More... | |
| void | IEE_SetRegionConfig (IEE_Type *base, iee_region_t region, iee_config_t *config) |
| Sets the IEE module according to the configuration structure. More... | |
| status_t | IEE_SetRegionKey (IEE_Type *base, iee_region_t region, iee_aes_key_num_t keyNum, const uint8_t *key, size_t keySize) |
| Sets the IEE module key. More... | |
| static uint32_t | IEE_GetOffset (uint32_t addressIee, uint32_t addressMemory) |
| Computes IEE offset to be set for specifed memory location. More... | |
| void | IEE_LockRegionConfig (IEE_Type *base, iee_region_t region) |
| Lock the IEE region configuration. More... | |
Driver version | |
| #define | FSL_IEE_DRIVER_VERSION (MAKE_VERSION(2, 1, 1)) |
| IEE driver version. More... | |
| struct _iee_config |
Data Fields | |
| iee_aes_bypass_t | bypass |
| AES encryption/decryption bypass. | |
| iee_aes_mode_t | mode |
| AES mode. | |
| iee_aes_key_size_t | keySize |
| size of AES key | |
| uint32_t | pageOffset |
| Offset to physical memory location from IEE start address. | |
| #define FSL_IEE_DRIVER_VERSION (MAKE_VERSION(2, 1, 1)) |
Version 2.1.1.
Current version: 2.1.1
Change log:
| typedef enum _iee_region iee_region_t |
| typedef enum _iee_aes_bypass iee_aes_bypass_t |
| typedef enum _iee_aes_mode iee_aes_mode_t |
| typedef enum _iee_aes_key_size iee_aes_key_size_t |
| typedef enum _iee_aes_key_num iee_aes_key_num_t |
| typedef struct _iee_config iee_config_t |
| enum _iee_region |
| enum _iee_aes_bypass |
| enum _iee_aes_mode |
| enum _iee_aes_key_size |
| enum _iee_aes_key_num |
| void IEE_Init | ( | IEE_Type * | base | ) |
This function performs hardware reset of IEE module. Attributes and keys of all regions are cleared.
| base | IEER peripheral address. |
| void IEE_GetDefaultConfig | ( | iee_config_t * | config | ) |
Loads default values to the IEE region configuration structure. The default values are as follows.
| config | Configuration for the selected IEE region. |
| void IEE_SetRegionConfig | ( | IEE_Type * | base, |
| iee_region_t | region, | ||
| iee_config_t * | config | ||
| ) |
This function configures IEE region according to configuration structure.
| base | IEE peripheral address. |
| region | Selection of the IEE region to be configured. |
| config | Configuration for the selected IEE region. |
| status_t IEE_SetRegionKey | ( | IEE_Type * | base, |
| iee_region_t | region, | ||
| iee_aes_key_num_t | keyNum, | ||
| const uint8_t * | key, | ||
| size_t | keySize | ||
| ) |
This function sets specified AES key for the given region.
| base | IEE peripheral address. |
| region | Selection of the IEE region to be configured. |
| keyNum | Selection of AES KEY1 or KEY2. |
| key | AES key. |
| keySize | Size of AES key. |
|
inlinestatic |
This function calculates offset that must be set for IEE region to access physical memory location.
| addressIee | Address of IEE peripheral. |
| addressMemory | Address of physical memory location. |
| void IEE_LockRegionConfig | ( | IEE_Type * | base, |
| iee_region_t | region | ||
| ) |
This function locks IEE region registers for Key, Offset and Attribute. Only system reset can clear the Lock bit.
| base | IEE peripheral address. |
| region | Selection of the IEE region to be locked. |