![]() |
MCUXpresso SDK API Reference Manual
Rev 2.15.100
NXP Semiconductors
|
Data Structures | |
| struct | _lpi2c_master_config |
| Structure with settings to initialize the LPI2C master module. More... | |
| struct | _lpi2c_match_config |
| LPI2C master data match configuration structure. More... | |
| struct | _lpi2c_master_transfer |
| Non-blocking transfer descriptor structure. More... | |
| struct | _lpi2c_master_handle |
| Driver handle for master non-blocking APIs. More... | |
Typedefs | |
| typedef enum _lpi2c_direction | lpi2c_direction_t |
| Direction of master and slave transfers. More... | |
| typedef enum _lpi2c_master_pin_config | lpi2c_master_pin_config_t |
| LPI2C pin configuration. More... | |
| typedef enum _lpi2c_host_request_source | lpi2c_host_request_source_t |
| LPI2C master host request selection. More... | |
| typedef enum _lpi2c_host_request_polarity | lpi2c_host_request_polarity_t |
| LPI2C master host request pin polarity configuration. More... | |
| typedef struct _lpi2c_master_config | lpi2c_master_config_t |
| Structure with settings to initialize the LPI2C master module. More... | |
| typedef enum _lpi2c_data_match_config_mode | lpi2c_data_match_config_mode_t |
| LPI2C master data match configuration modes. More... | |
| typedef struct _lpi2c_match_config | lpi2c_data_match_config_t |
| LPI2C master data match configuration structure. More... | |
| typedef struct _lpi2c_master_transfer | lpi2c_master_transfer_t |
| LPI2C master descriptor of the transfer. More... | |
| typedef struct _lpi2c_master_handle | lpi2c_master_handle_t |
| LPI2C master handle of the transfer. More... | |
| typedef void(* | lpi2c_master_transfer_callback_t )(LPI2C_Type *base, lpi2c_master_handle_t *handle, status_t completionStatus, void *userData) |
| Master completion callback function pointer type. More... | |
| typedef void(* | lpi2c_master_isr_t )(LPI2C_Type *base, void *handle) |
| Typedef for master interrupt handler, used internally for LPI2C master interrupt and EDMA transactional APIs. | |
Initialization and deinitialization | |
| void | LPI2C_MasterGetDefaultConfig (lpi2c_master_config_t *masterConfig) |
| Provides a default configuration for the LPI2C master peripheral. More... | |
| void | LPI2C_MasterInit (LPI2C_Type *base, const lpi2c_master_config_t *masterConfig, uint32_t sourceClock_Hz) |
| Initializes the LPI2C master peripheral. More... | |
| void | LPI2C_MasterDeinit (LPI2C_Type *base) |
| Deinitializes the LPI2C master peripheral. More... | |
| void | LPI2C_MasterConfigureDataMatch (LPI2C_Type *base, const lpi2c_data_match_config_t *matchConfig) |
| Configures LPI2C master data match feature. More... | |
| status_t | LPI2C_MasterCheckAndClearError (LPI2C_Type *base, uint32_t status) |
| Convert provided flags to status code, and clear any errors if present. More... | |
| status_t | LPI2C_CheckForBusyBus (LPI2C_Type *base) |
| Make sure the bus isn't already busy. More... | |
| static void | LPI2C_MasterReset (LPI2C_Type *base) |
| Performs a software reset. More... | |
| static void | LPI2C_MasterEnable (LPI2C_Type *base, bool enable) |
| Enables or disables the LPI2C module as master. More... | |
Status | |
| static uint32_t | LPI2C_MasterGetStatusFlags (LPI2C_Type *base) |
| Gets the LPI2C master status flags. More... | |
| static void | LPI2C_MasterClearStatusFlags (LPI2C_Type *base, uint32_t statusMask) |
| Clears the LPI2C master status flag state. More... | |
Interrupts | |
| static void | LPI2C_MasterEnableInterrupts (LPI2C_Type *base, uint32_t interruptMask) |
| Enables the LPI2C master interrupt requests. More... | |
| static void | LPI2C_MasterDisableInterrupts (LPI2C_Type *base, uint32_t interruptMask) |
| Disables the LPI2C master interrupt requests. More... | |
| static uint32_t | LPI2C_MasterGetEnabledInterrupts (LPI2C_Type *base) |
| Returns the set of currently enabled LPI2C master interrupt requests. More... | |
DMA control | |
| static void | LPI2C_MasterEnableDMA (LPI2C_Type *base, bool enableTx, bool enableRx) |
| Enables or disables LPI2C master DMA requests. More... | |
| static uint32_t | LPI2C_MasterGetTxFifoAddress (LPI2C_Type *base) |
| Gets LPI2C master transmit data register address for DMA transfer. More... | |
| static uint32_t | LPI2C_MasterGetRxFifoAddress (LPI2C_Type *base) |
| Gets LPI2C master receive data register address for DMA transfer. More... | |
FIFO control | |
| static void | LPI2C_MasterSetWatermarks (LPI2C_Type *base, size_t txWords, size_t rxWords) |
| Sets the watermarks for LPI2C master FIFOs. More... | |
| static void | LPI2C_MasterGetFifoCounts (LPI2C_Type *base, size_t *rxCount, size_t *txCount) |
| Gets the current number of words in the LPI2C master FIFOs. More... | |
Bus operations | |
| void | LPI2C_MasterSetBaudRate (LPI2C_Type *base, uint32_t sourceClock_Hz, uint32_t baudRate_Hz) |
| Sets the I2C bus frequency for master transactions. More... | |
| static bool | LPI2C_MasterGetBusIdleState (LPI2C_Type *base) |
| Returns whether the bus is idle. More... | |
| status_t | LPI2C_MasterStart (LPI2C_Type *base, uint8_t address, lpi2c_direction_t dir) |
| Sends a START signal and slave address on the I2C bus. More... | |
| static status_t | LPI2C_MasterRepeatedStart (LPI2C_Type *base, uint8_t address, lpi2c_direction_t dir) |
| Sends a repeated START signal and slave address on the I2C bus. More... | |
| status_t | LPI2C_MasterSend (LPI2C_Type *base, void *txBuff, size_t txSize) |
| Performs a polling send transfer on the I2C bus. More... | |
| status_t | LPI2C_MasterReceive (LPI2C_Type *base, void *rxBuff, size_t rxSize) |
| Performs a polling receive transfer on the I2C bus. More... | |
| status_t | LPI2C_MasterStop (LPI2C_Type *base) |
| Sends a STOP signal on the I2C bus. More... | |
| status_t | LPI2C_MasterTransferBlocking (LPI2C_Type *base, lpi2c_master_transfer_t *transfer) |
| Performs a master polling transfer on the I2C bus. More... | |
Non-blocking | |
| void | LPI2C_MasterTransferCreateHandle (LPI2C_Type *base, lpi2c_master_handle_t *handle, lpi2c_master_transfer_callback_t callback, void *userData) |
| Creates a new handle for the LPI2C master non-blocking APIs. More... | |
| status_t | LPI2C_MasterTransferNonBlocking (LPI2C_Type *base, lpi2c_master_handle_t *handle, lpi2c_master_transfer_t *transfer) |
| Performs a non-blocking transaction on the I2C bus. More... | |
| status_t | LPI2C_MasterTransferGetCount (LPI2C_Type *base, lpi2c_master_handle_t *handle, size_t *count) |
| Returns number of bytes transferred so far. More... | |
| void | LPI2C_MasterTransferAbort (LPI2C_Type *base, lpi2c_master_handle_t *handle) |
| Terminates a non-blocking LPI2C master transmission early. More... | |
IRQ handler | |
| void | LPI2C_MasterTransferHandleIRQ (LPI2C_Type *base, void *lpi2cMasterHandle) |
| Reusable routine to handle master interrupts. More... | |
| struct _lpi2c_master_config |
This structure holds configuration settings for the LPI2C peripheral. To initialize this structure to reasonable defaults, call the LPI2C_MasterGetDefaultConfig() function and pass a pointer to your configuration structure instance.
The configuration structure can be made constant so it resides in flash.
Data Fields | |
| bool | enableMaster |
| Whether to enable master mode. More... | |
| bool | enableDoze |
| Whether master is enabled in doze mode. More... | |
| bool | debugEnable |
| Enable transfers to continue when halted in debug mode. More... | |
| bool | ignoreAck |
| Whether to ignore ACK/NACK. More... | |
| lpi2c_master_pin_config_t | pinConfig |
| The pin configuration option. More... | |
| uint32_t | baudRate_Hz |
| Desired baud rate in Hertz. More... | |
| uint32_t | busIdleTimeout_ns |
| Bus idle timeout in nanoseconds. More... | |
| uint32_t | pinLowTimeout_ns |
| Pin low timeout in nanoseconds. More... | |
| uint8_t | sdaGlitchFilterWidth_ns |
| Width in nanoseconds of glitch filter on SDA pin. More... | |
| uint8_t | sclGlitchFilterWidth_ns |
| Width in nanoseconds of glitch filter on SCL pin. More... | |
| struct { | |
| bool enable | |
| Enable host request. More... | |
| lpi2c_host_request_source_t source | |
| Host request source. More... | |
| lpi2c_host_request_polarity_t polarity | |
| Host request pin polarity. More... | |
| } | hostRequest |
| Host request options. More... | |
| bool _lpi2c_master_config::enableMaster |
| bool _lpi2c_master_config::enableDoze |
| bool _lpi2c_master_config::debugEnable |
| bool _lpi2c_master_config::ignoreAck |
| lpi2c_master_pin_config_t _lpi2c_master_config::pinConfig |
| uint32_t _lpi2c_master_config::baudRate_Hz |
| uint32_t _lpi2c_master_config::busIdleTimeout_ns |
Set to 0 to disable.
| uint32_t _lpi2c_master_config::pinLowTimeout_ns |
Set to 0 to disable.
| uint8_t _lpi2c_master_config::sdaGlitchFilterWidth_ns |
Set to 0 to disable.
| uint8_t _lpi2c_master_config::sclGlitchFilterWidth_ns |
Set to 0 to disable.
| bool _lpi2c_master_config::enable |
| lpi2c_host_request_source_t _lpi2c_master_config::source |
| lpi2c_host_request_polarity_t _lpi2c_master_config::polarity |
| struct { ... } _lpi2c_master_config::hostRequest |
| struct _lpi2c_match_config |
Data Fields | |
| lpi2c_data_match_config_mode_t | matchMode |
| Data match configuration setting. More... | |
| bool | rxDataMatchOnly |
| When set to true, received data is ignored until a successful match. More... | |
| uint32_t | match0 |
| Match value 0. More... | |
| uint32_t | match1 |
| Match value 1. More... | |
| lpi2c_data_match_config_mode_t _lpi2c_match_config::matchMode |
| bool _lpi2c_match_config::rxDataMatchOnly |
| uint32_t _lpi2c_match_config::match0 |
| uint32_t _lpi2c_match_config::match1 |
| struct _lpi2c_master_transfer |
This structure is used to pass transaction parameters to the LPI2C_MasterTransferNonBlocking() API.
Data Fields | |
| uint32_t | flags |
| Bit mask of options for the transfer. More... | |
| uint16_t | slaveAddress |
| The 7-bit slave address. More... | |
| lpi2c_direction_t | direction |
| Either kLPI2C_Read or kLPI2C_Write. More... | |
| uint32_t | subaddress |
| Sub address. More... | |
| size_t | subaddressSize |
| Length of sub address to send in bytes. More... | |
| void * | data |
| Pointer to data to transfer. More... | |
| size_t | dataSize |
| Number of bytes to transfer. More... | |
| uint32_t _lpi2c_master_transfer::flags |
See enumeration _lpi2c_master_transfer_flags for available options. Set to 0 or kLPI2C_TransferDefaultFlag for normal transfers.
| uint16_t _lpi2c_master_transfer::slaveAddress |
| lpi2c_direction_t _lpi2c_master_transfer::direction |
| uint32_t _lpi2c_master_transfer::subaddress |
Transferred MSB first.
| size_t _lpi2c_master_transfer::subaddressSize |
Maximum size is 4 bytes.
| void* _lpi2c_master_transfer::data |
| size_t _lpi2c_master_transfer::dataSize |
| struct _lpi2c_master_handle |
Data Fields | |
| uint8_t | state |
| Transfer state machine current state. More... | |
| uint16_t | remainingBytes |
| Remaining byte count in current state. More... | |
| uint8_t * | buf |
| Buffer pointer for current state. More... | |
| uint16_t | commandBuffer [6] |
| LPI2C command sequence. More... | |
| lpi2c_master_transfer_t | transfer |
| Copy of the current transfer info. More... | |
| lpi2c_master_transfer_callback_t | completionCallback |
| Callback function pointer. More... | |
| void * | userData |
| Application data passed to callback. More... | |
| uint8_t _lpi2c_master_handle::state |
| uint16_t _lpi2c_master_handle::remainingBytes |
| uint8_t* _lpi2c_master_handle::buf |
| uint16_t _lpi2c_master_handle::commandBuffer[6] |
When all 6 command words are used: Start&addr&write[1 word] + subaddr[4 words] + restart&addr&read[1 word]
| lpi2c_master_transfer_t _lpi2c_master_handle::transfer |
| lpi2c_master_transfer_callback_t _lpi2c_master_handle::completionCallback |
| void* _lpi2c_master_handle::userData |
| typedef enum _lpi2c_direction lpi2c_direction_t |
| typedef enum _lpi2c_master_pin_config lpi2c_master_pin_config_t |
| typedef enum _lpi2c_host_request_source lpi2c_host_request_source_t |
| typedef struct _lpi2c_master_config lpi2c_master_config_t |
This structure holds configuration settings for the LPI2C peripheral. To initialize this structure to reasonable defaults, call the LPI2C_MasterGetDefaultConfig() function and pass a pointer to your configuration structure instance.
The configuration structure can be made constant so it resides in flash.
| typedef struct _lpi2c_match_config lpi2c_data_match_config_t |
| typedef struct _lpi2c_master_transfer lpi2c_master_transfer_t |
| typedef struct _lpi2c_master_handle lpi2c_master_handle_t |
| typedef void(* lpi2c_master_transfer_callback_t)(LPI2C_Type *base, lpi2c_master_handle_t *handle, status_t completionStatus, void *userData) |
This callback is used only for the non-blocking master transfer API. Specify the callback you wish to use in the call to LPI2C_MasterTransferCreateHandle().
| base | The LPI2C peripheral base address. |
| handle | Pointer to the LPI2C master driver handle. |
| completionStatus | Either kStatus_Success or an error code describing how the transfer completed. |
| userData | Arbitrary pointer-sized value passed from the application. |
| enum _lpi2c_master_flags |
The following status register flags can be cleared:
All flags except kLPI2C_MasterBusyFlag and kLPI2C_MasterBusBusyFlag can be enabled as interrupts.
| enum _lpi2c_direction |
| void LPI2C_MasterGetDefaultConfig | ( | lpi2c_master_config_t * | masterConfig | ) |
This function provides the following default configuration for the LPI2C master peripheral:
After calling this function, you can override any settings in order to customize the configuration, prior to initializing the master driver with LPI2C_MasterInit().
| [out] | masterConfig | User provided configuration structure for default values. Refer to lpi2c_master_config_t. |
| void LPI2C_MasterInit | ( | LPI2C_Type * | base, |
| const lpi2c_master_config_t * | masterConfig, | ||
| uint32_t | sourceClock_Hz | ||
| ) |
This function enables the peripheral clock and initializes the LPI2C master peripheral as described by the user provided configuration. A software reset is performed prior to configuration.
| base | The LPI2C peripheral base address. |
| masterConfig | User provided peripheral configuration. Use LPI2C_MasterGetDefaultConfig() to get a set of defaults that you can override. |
| sourceClock_Hz | Frequency in Hertz of the LPI2C functional clock. Used to calculate the baud rate divisors, filter widths, and timeout periods. |
| void LPI2C_MasterDeinit | ( | LPI2C_Type * | base | ) |
This function disables the LPI2C master peripheral and gates the clock. It also performs a software reset to restore the peripheral to reset conditions.
| base | The LPI2C peripheral base address. |
| void LPI2C_MasterConfigureDataMatch | ( | LPI2C_Type * | base, |
| const lpi2c_data_match_config_t * | matchConfig | ||
| ) |
| base | The LPI2C peripheral base address. |
| matchConfig | Settings for the data match feature. |
| status_t LPI2C_MasterCheckAndClearError | ( | LPI2C_Type * | base, |
| uint32_t | status | ||
| ) |
| base | The LPI2C peripheral base address. |
| status | Current status flags value that will be checked. |
| status_t LPI2C_CheckForBusyBus | ( | LPI2C_Type * | base | ) |
A busy bus is allowed if we are the one driving it.
| base | The LPI2C peripheral base address. |
| kStatus_Success | |
| kStatus_LPI2C_Busy |
|
inlinestatic |
Restores the LPI2C master peripheral to reset conditions.
| base | The LPI2C peripheral base address. |
|
inlinestatic |
| base | The LPI2C peripheral base address. |
| enable | Pass true to enable or false to disable the specified LPI2C as master. |
|
inlinestatic |
A bit mask with the state of all LPI2C master status flags is returned. For each flag, the corresponding bit in the return value is set if the flag is asserted.
| base | The LPI2C peripheral base address. |
|
inlinestatic |
The following status register flags can be cleared:
Attempts to clear other flags has no effect.
| base | The LPI2C peripheral base address. |
| statusMask | A bitmask of status flags that are to be cleared. The mask is composed of _lpi2c_master_flags enumerators OR'd together. You may pass the result of a previous call to LPI2C_MasterGetStatusFlags(). |
|
inlinestatic |
All flags except kLPI2C_MasterBusyFlag and kLPI2C_MasterBusBusyFlag can be enabled as interrupts.
| base | The LPI2C peripheral base address. |
| interruptMask | Bit mask of interrupts to enable. See _lpi2c_master_flags for the set of constants that should be OR'd together to form the bit mask. |
|
inlinestatic |
All flags except kLPI2C_MasterBusyFlag and kLPI2C_MasterBusBusyFlag can be enabled as interrupts.
| base | The LPI2C peripheral base address. |
| interruptMask | Bit mask of interrupts to disable. See _lpi2c_master_flags for the set of constants that should be OR'd together to form the bit mask. |
|
inlinestatic |
| base | The LPI2C peripheral base address. |
|
inlinestatic |
| base | The LPI2C peripheral base address. |
| enableTx | Enable flag for transmit DMA request. Pass true for enable, false for disable. |
| enableRx | Enable flag for receive DMA request. Pass true for enable, false for disable. |
|
inlinestatic |
| base | The LPI2C peripheral base address. |
|
inlinestatic |
| base | The LPI2C peripheral base address. |
|
inlinestatic |
| base | The LPI2C peripheral base address. |
| txWords | Transmit FIFO watermark value in words. The kLPI2C_MasterTxReadyFlag flag is set whenever the number of words in the transmit FIFO is equal or less than txWords. Writing a value equal or greater than the FIFO size is truncated. |
| rxWords | Receive FIFO watermark value in words. The kLPI2C_MasterRxReadyFlag flag is set whenever the number of words in the receive FIFO is greater than rxWords. Writing a value equal or greater than the FIFO size is truncated. |
|
inlinestatic |
| base | The LPI2C peripheral base address. | |
| [out] | txCount | Pointer through which the current number of words in the transmit FIFO is returned. Pass NULL if this value is not required. |
| [out] | rxCount | Pointer through which the current number of words in the receive FIFO is returned. Pass NULL if this value is not required. |
| void LPI2C_MasterSetBaudRate | ( | LPI2C_Type * | base, |
| uint32_t | sourceClock_Hz, | ||
| uint32_t | baudRate_Hz | ||
| ) |
The LPI2C master is automatically disabled and re-enabled as necessary to configure the baud rate. Do not call this function during a transfer, or the transfer is aborted.
| base | The LPI2C peripheral base address. |
| sourceClock_Hz | LPI2C functional clock frequency in Hertz. |
| baudRate_Hz | Requested bus frequency in Hertz. |
|
inlinestatic |
Requires the master mode to be enabled.
| base | The LPI2C peripheral base address. |
| true | Bus is busy. |
| false | Bus is idle. |
| status_t LPI2C_MasterStart | ( | LPI2C_Type * | base, |
| uint8_t | address, | ||
| lpi2c_direction_t | dir | ||
| ) |
This function is used to initiate a new master mode transfer. First, the bus state is checked to ensure that another master is not occupying the bus. Then a START signal is transmitted, followed by the 7-bit address specified in the address parameter. Note that this function does not actually wait until the START and address are successfully sent on the bus before returning.
| base | The LPI2C peripheral base address. |
| address | 7-bit slave device address, in bits [6:0]. |
| dir | Master transfer direction, either kLPI2C_Read or kLPI2C_Write. This parameter is used to set the R/w bit (bit 0) in the transmitted slave address. |
| kStatus_Success | START signal and address were successfully enqueued in the transmit FIFO. |
| kStatus_LPI2C_Busy | Another master is currently utilizing the bus. |
|
inlinestatic |
This function is used to send a Repeated START signal when a transfer is already in progress. Like LPI2C_MasterStart(), it also sends the specified 7-bit address.
| base | The LPI2C peripheral base address. |
| address | 7-bit slave device address, in bits [6:0]. |
| dir | Master transfer direction, either kLPI2C_Read or kLPI2C_Write. This parameter is used to set the R/w bit (bit 0) in the transmitted slave address. |
| kStatus_Success | Repeated START signal and address were successfully enqueued in the transmit FIFO. |
| kStatus_LPI2C_Busy | Another master is currently utilizing the bus. |
| status_t LPI2C_MasterSend | ( | LPI2C_Type * | base, |
| void * | txBuff, | ||
| size_t | txSize | ||
| ) |
Sends up to txSize number of bytes to the previously addressed slave device. The slave may reply with a NAK to any byte in order to terminate the transfer early. If this happens, this function returns kStatus_LPI2C_Nak.
| base | The LPI2C peripheral base address. |
| txBuff | The pointer to the data to be transferred. |
| txSize | The length in bytes of the data to be transferred. |
| kStatus_Success | Data was sent successfully. |
| kStatus_LPI2C_Busy | Another master is currently utilizing the bus. |
| kStatus_LPI2C_Nak | The slave device sent a NAK in response to a byte. |
| kStatus_LPI2C_FifoError | FIFO under run or over run. |
| kStatus_LPI2C_ArbitrationLost | Arbitration lost error. |
| kStatus_LPI2C_PinLowTimeout | SCL or SDA were held low longer than the timeout. |
| status_t LPI2C_MasterReceive | ( | LPI2C_Type * | base, |
| void * | rxBuff, | ||
| size_t | rxSize | ||
| ) |
| base | The LPI2C peripheral base address. |
| rxBuff | The pointer to the data to be transferred. |
| rxSize | The length in bytes of the data to be transferred. |
| kStatus_Success | Data was received successfully. |
| kStatus_LPI2C_Busy | Another master is currently utilizing the bus. |
| kStatus_LPI2C_Nak | The slave device sent a NAK in response to a byte. |
| kStatus_LPI2C_FifoError | FIFO under run or overrun. |
| kStatus_LPI2C_ArbitrationLost | Arbitration lost error. |
| kStatus_LPI2C_PinLowTimeout | SCL or SDA were held low longer than the timeout. |
| status_t LPI2C_MasterStop | ( | LPI2C_Type * | base | ) |
This function does not return until the STOP signal is seen on the bus, or an error occurs.
| base | The LPI2C peripheral base address. |
| kStatus_Success | The STOP signal was successfully sent on the bus and the transaction terminated. |
| kStatus_LPI2C_Busy | Another master is currently utilizing the bus. |
| kStatus_LPI2C_Nak | The slave device sent a NAK in response to a byte. |
| kStatus_LPI2C_FifoError | FIFO under run or overrun. |
| kStatus_LPI2C_ArbitrationLost | Arbitration lost error. |
| kStatus_LPI2C_PinLowTimeout | SCL or SDA were held low longer than the timeout. |
| status_t LPI2C_MasterTransferBlocking | ( | LPI2C_Type * | base, |
| lpi2c_master_transfer_t * | transfer | ||
| ) |
| base | The LPI2C peripheral base address. |
| transfer | Pointer to the transfer structure. |
| kStatus_Success | Data was received successfully. |
| kStatus_LPI2C_Busy | Another master is currently utilizing the bus. |
| kStatus_LPI2C_Nak | The slave device sent a NAK in response to a byte. |
| kStatus_LPI2C_FifoError | FIFO under run or overrun. |
| kStatus_LPI2C_ArbitrationLost | Arbitration lost error. |
| kStatus_LPI2C_PinLowTimeout | SCL or SDA were held low longer than the timeout. |
| void LPI2C_MasterTransferCreateHandle | ( | LPI2C_Type * | base, |
| lpi2c_master_handle_t * | handle, | ||
| lpi2c_master_transfer_callback_t | callback, | ||
| void * | userData | ||
| ) |
The creation of a handle is for use with the non-blocking APIs. Once a handle is created, there is not a corresponding destroy handle. If the user wants to terminate a transfer, the LPI2C_MasterTransferAbort() API shall be called.
| base | The LPI2C peripheral base address. | |
| [out] | handle | Pointer to the LPI2C master driver handle. |
| callback | User provided pointer to the asynchronous callback function. | |
| userData | User provided pointer to the application callback data. |
| status_t LPI2C_MasterTransferNonBlocking | ( | LPI2C_Type * | base, |
| lpi2c_master_handle_t * | handle, | ||
| lpi2c_master_transfer_t * | transfer | ||
| ) |
| base | The LPI2C peripheral base address. |
| handle | Pointer to the LPI2C master driver handle. |
| transfer | The pointer to the transfer descriptor. |
| kStatus_Success | The transaction was started successfully. |
| kStatus_LPI2C_Busy | Either another master is currently utilizing the bus, or a non-blocking transaction is already in progress. |
| status_t LPI2C_MasterTransferGetCount | ( | LPI2C_Type * | base, |
| lpi2c_master_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | The LPI2C peripheral base address. | |
| handle | Pointer to the LPI2C master driver handle. | |
| [out] | count | Number of bytes transferred so far by the non-blocking transaction. |
| kStatus_Success | |
| kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress. |
| void LPI2C_MasterTransferAbort | ( | LPI2C_Type * | base, |
| lpi2c_master_handle_t * | handle | ||
| ) |
| base | The LPI2C peripheral base address. |
| handle | Pointer to the LPI2C master driver handle. |
| void LPI2C_MasterTransferHandleIRQ | ( | LPI2C_Type * | base, |
| void * | lpi2cMasterHandle | ||
| ) |
| base | The LPI2C peripheral base address. |
| lpi2cMasterHandle | Pointer to the LPI2C master driver handle. |