![]() |
MCUXpresso SDK API Reference Manual
Rev 2.15.100
NXP Semiconductors
|
This function constructs a job descriptor capable of performing a key blackening operation on a plaintext secure memory resident object.
Functions | |
| status_t | CAAM_BLACK_GetKeyBlacken (CAAM_Type *base, caam_handle_t *handle, const uint8_t *data, size_t dataSize, caam_fifost_type_t fifostType, uint8_t *blackdata) |
| Construct a black key. More... | |
| status_t CAAM_BLACK_GetKeyBlacken | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | data, | ||
| size_t | dataSize, | ||
| caam_fifost_type_t | fifostType, | ||
| uint8_t * | blackdata | ||
| ) |
This function constructs a job descriptor capable of performing a key blackening operation on a plaintext secure memory resident object.
| base | CAAM peripheral base address | |
| handle | jobRing used for this request | |
| data | Pointer address uses to pointed the plaintext. | |
| dataSize | Size of the buffer pointed by the data parameter | |
| fifostType | Type of AES-CBC or AEC-CCM to encrypt plaintext | |
| [out] | blackdata | Pointer address uses to pointed the black key |