MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Qspi_edma_driver

Overview

Data Structures

struct  qspi_edma_handle_t
 QSPI DMA transfer handle, users should not touch the content of the handle. More...
 

Typedefs

typedef void(* qspi_edma_callback_t )(QuadSPI_Type *base, qspi_edma_handle_t *handle, status_t status, void *userData)
 QSPI eDMA transfer callback function for finish and error.
 

Driver version

#define FSL_QSPI_EDMA_DRIVER_VERSION   (MAKE_VERSION(2, 2, 2))
 QSPI EDMA driver version 2.2.2. More...
 

eDMA Transactional

void QSPI_TransferTxCreateHandleEDMA (QuadSPI_Type *base, qspi_edma_handle_t *handle, qspi_edma_callback_t callback, void *userData, edma_handle_t *dmaHandle)
 Initializes the QSPI handle for send which is used in transactional functions and set the callback. More...
 
void QSPI_TransferRxCreateHandleEDMA (QuadSPI_Type *base, qspi_edma_handle_t *handle, qspi_edma_callback_t callback, void *userData, edma_handle_t *dmaHandle)
 Initializes the QSPI handle for receive which is used in transactional functions and set the callback. More...
 
status_t QSPI_TransferSendEDMA (QuadSPI_Type *base, qspi_edma_handle_t *handle, qspi_transfer_t *xfer)
 Transfers QSPI data using an eDMA non-blocking method. More...
 
status_t QSPI_TransferReceiveEDMA (QuadSPI_Type *base, qspi_edma_handle_t *handle, qspi_transfer_t *xfer)
 Receives data using an eDMA non-blocking method. More...
 
void QSPI_TransferAbortSendEDMA (QuadSPI_Type *base, qspi_edma_handle_t *handle)
 Aborts the sent data using eDMA. More...
 
void QSPI_TransferAbortReceiveEDMA (QuadSPI_Type *base, qspi_edma_handle_t *handle)
 Aborts the receive data using eDMA. More...
 
status_t QSPI_TransferGetSendCountEDMA (QuadSPI_Type *base, qspi_edma_handle_t *handle, size_t *count)
 Gets the transferred counts of send. More...
 
status_t QSPI_TransferGetReceiveCountEDMA (QuadSPI_Type *base, qspi_edma_handle_t *handle, size_t *count)
 Gets the status of the receive transfer. More...
 

Data Structure Documentation

struct _qspi_edma_handle

Data Fields

edma_handle_t * dmaHandle
 eDMA handler for QSPI send
 
size_t transferSize
 Bytes need to transfer. More...
 
uint8_t nbytes
 eDMA minor byte transfer count initially configured. More...
 
uint8_t count
 The transfer data count in a DMA request.
 
uint32_t state
 Internal state for QSPI eDMA transfer.
 
qspi_edma_callback_t callback
 Callback for users while transfer finish or error occurred.
 
void * userData
 User callback parameter.
 

Field Documentation

size_t qspi_edma_handle_t::transferSize
uint8_t qspi_edma_handle_t::nbytes

Macro Definition Documentation

#define FSL_QSPI_EDMA_DRIVER_VERSION   (MAKE_VERSION(2, 2, 2))

Function Documentation

void QSPI_TransferTxCreateHandleEDMA ( QuadSPI_Type *  base,
qspi_edma_handle_t *  handle,
qspi_edma_callback_t  callback,
void *  userData,
edma_handle_t *  dmaHandle 
)
Parameters
baseQSPI peripheral base address
handlePointer to qspi_edma_handle_t structure
callbackQSPI callback, NULL means no callback.
userDataUser callback function data.
dmaHandleUser requested eDMA handle for eDMA transfer
void QSPI_TransferRxCreateHandleEDMA ( QuadSPI_Type *  base,
qspi_edma_handle_t *  handle,
qspi_edma_callback_t  callback,
void *  userData,
edma_handle_t *  dmaHandle 
)
Parameters
baseQSPI peripheral base address
handlePointer to qspi_edma_handle_t structure
callbackQSPI callback, NULL means no callback.
userDataUser callback function data.
dmaHandleUser requested eDMA handle for eDMA transfer
status_t QSPI_TransferSendEDMA ( QuadSPI_Type *  base,
qspi_edma_handle_t *  handle,
qspi_transfer_t *  xfer 
)

This function writes data to the QSPI transmit FIFO. This function is non-blocking.

Parameters
basePointer to QuadSPI Type.
handlePointer to qspi_edma_handle_t structure
xferQSPI transfer structure.
status_t QSPI_TransferReceiveEDMA ( QuadSPI_Type *  base,
qspi_edma_handle_t *  handle,
qspi_transfer_t *  xfer 
)

This function receive data from the QSPI receive buffer/FIFO. This function is non-blocking. Users shall notice that this receive size shall not bigger than 64 bytes. As this interface is used to read flash status registers. For flash contents read, please use AHB bus read, this is much more efficiency.

Parameters
basePointer to QuadSPI Type.
handlePointer to qspi_edma_handle_t structure
xferQSPI transfer structure.
void QSPI_TransferAbortSendEDMA ( QuadSPI_Type *  base,
qspi_edma_handle_t *  handle 
)

This function aborts the sent data using eDMA.

Parameters
baseQSPI peripheral base address.
handlePointer to qspi_edma_handle_t structure
void QSPI_TransferAbortReceiveEDMA ( QuadSPI_Type *  base,
qspi_edma_handle_t *  handle 
)

This function abort receive data which using eDMA.

Parameters
baseQSPI peripheral base address.
handlePointer to qspi_edma_handle_t structure
status_t QSPI_TransferGetSendCountEDMA ( QuadSPI_Type *  base,
qspi_edma_handle_t *  handle,
size_t *  count 
)
Parameters
basePointer to QuadSPI Type.
handlePointer to qspi_edma_handle_t structure.
countBytes sent.
Return values
kStatus_SuccessSucceed get the transfer count.
kStatus_NoTransferInProgressThere is not a non-blocking transaction currently in progress.
status_t QSPI_TransferGetReceiveCountEDMA ( QuadSPI_Type *  base,
qspi_edma_handle_t *  handle,
size_t *  count 
)
Parameters
basePointer to QuadSPI Type.
handlePointer to qspi_edma_handle_t structure
countBytes received.
Return values
kStatus_SuccessSucceed get the transfer count.
kStatus_NoTransferInProgressThere is not a non-blocking transaction currently in progress.