This chapter describes the programming interface of the debug console driver.
The debug console enables debug log messages to be output via the specified peripheral with frequency of the peripheral source clock and base address at the specified baud rate. Additionally, it provides input and output functions to scan and print formatted data.
Function groups
Initialization
To initialize the debug console, call the DbgConsole_Init() function with these parameters. This function automatically enables the module and the clock.
Selects the supported debug console hardware device type, such as
typedef enum _serial_port_type
{
After the initialization is successful, stdout and stdin are connected to the selected peripheral. The debug console state is stored in the debug_console_state_t structure, such as shown here.
typedef struct DebugConsoleState
{
uint8_t uartHandleBuffer[HAL_UART_HANDLE_SIZE];
hal_uart_status_t (*putChar)(hal_uart_handle_t handle, const uint8_t *data, size_t length);
hal_uart_status_t (*getChar)(hal_uart_handle_t handle, uint8_t *data, size_t length);
serial_port_type_t type;
} debug_console_state_t;
This example shows how to call the DbgConsole_Init() given the user configuration structure.
DbgConsole_Init(BOARD_DEBUG_USART_INSTANCE, BOARD_DEBUG_USART_BAUDRATE, BOARD_DEBUG_USART_TYPE,
BOARD_DEBUG_USART_CLK_FREQ);
Advanced Feature
The debug console provides input and output functions to scan and print formatted data.
- Support a format specifier for PRINTF following this prototype " %[flags][width][.precision][length]specifier", which is explained below
| flags | Description |
| - | Left-justified within the given field width. Right-justified is the default. |
| + | Forces to precede the result with a plus or minus sign (+ or -) even for positive numbers. By default, only negative numbers are preceded with a - sign. |
| (space) | If no sign is written, a blank space is inserted before the value. |
| # | Used with o, x, or X specifiers the value is preceded with 0, 0x, or 0X respectively for values other than zero. Used with e, E and f, it forces the written output to contain a decimal point even if no digits would follow. By default, if no digits follow, no decimal point is written. Used with g or G the result is the same as with e or E but trailing zeros are not removed. |
| 0 | Left-pads the number with zeroes (0) instead of spaces, where padding is specified (see width sub-specifier). |
| Width | Description |
| (number) | A minimum number of characters to be printed. If the value to be printed is shorter than this number, the result is padded with blank spaces. The value is not truncated even if the result is larger. |
| * | The width is not specified in the format string, but as an additional integer value argument preceding the argument that has to be formatted. |
| .precision | Description |
| .number | For integer specifiers (d, i, o, u, x, X) − precision specifies the minimum number of digits to be written. If the value to be written is shorter than this number, the result is padded with leading zeros. The value is not truncated even if the result is longer. A precision of 0 means that no character is written for the value 0. For e, E, and f specifiers − this is the number of digits to be printed after the decimal point. For g and G specifiers − This is the maximum number of significant digits to be printed. For s − this is the maximum number of characters to be printed. By default, all characters are printed until the ending null character is encountered. For c type − it has no effect. When no precision is specified, the default is 1. If the period is specified without an explicit value for precision, 0 is assumed. |
| .* | The precision is not specified in the format string, but as an additional integer value argument preceding the argument that has to be formatted. |
| length | Description |
| Do not support |
| specifier | Description |
| d or i | Signed decimal integer |
| f | Decimal floating point |
| F | Decimal floating point capital letters |
| x | Unsigned hexadecimal integer |
| X | Unsigned hexadecimal integer capital letters |
| o | Signed octal |
| b | Binary value |
| p | Pointer address |
| u | Unsigned decimal integer |
| c | Character |
| s | String of characters |
| n | Nothing printed |
- Support a format specifier for SCANF following this prototype " %[*][width][length]specifier", which is explained below
| * | Description |
| An optional starting asterisk indicates that the data is to be read from the stream but ignored. In other words, it is not stored in the corresponding argument. |
| width | Description |
| This specifies the maximum number of characters to be read in the current reading operation. |
| length | Description |
| hh | The argument is interpreted as a signed character or unsigned character (only applies to integer specifiers: i, d, o, u, x, and X). |
| h | The argument is interpreted as a short integer or unsigned short integer (only applies to integer specifiers: i, d, o, u, x, and X). |
| l | The argument is interpreted as a long integer or unsigned long integer for integer specifiers (i, d, o, u, x, and X) and as a wide character or wide character string for specifiers c and s. |
| ll | The argument is interpreted as a long long integer or unsigned long long integer for integer specifiers (i, d, o, u, x, and X) and as a wide character or wide character string for specifiers c and s. |
| L | The argument is interpreted as a long double (only applies to floating point specifiers: e, E, f, g, and G). |
| j or z or t | Not supported |
| specifier | Qualifying Input | Type of argument |
| c | Single character: Reads the next character. If a width different from 1 is specified, the function reads width characters and stores them in the successive locations of the array passed as argument. No null character is appended at the end. | char * |
| i | Integer: : Number optionally preceded with a + or - sign | int * |
| d | Decimal integer: Number optionally preceded with a + or - sign | int * |
| a, A, e, E, f, F, g, G | Floating point: Decimal number containing a decimal point, optionally preceded by a + or - sign and optionally followed by the e or E character and a decimal number. Two examples of valid entries are -732.103 and 7.12e4 | float * |
| o | Octal Integer: | int * |
| s | String of characters. This reads subsequent characters until a white space is found (white space characters are considered to be blank, newline, and tab). | char * |
| u | Unsigned decimal integer. | unsigned int * |
The debug console has its own printf/scanf/putchar/getchar functions which are defined in the header file.
This utility supports selecting toolchain's printf/scanf or the MCUXpresso SDK printf/scanf.
#if SDK_DEBUGCONSOLE == DEBUGCONSOLE_DISABLE
#define PRINTF
#define SCANF
#define PUTCHAR
#define GETCHAR
#elif SDK_DEBUGCONSOLE == DEBUGCONSOLE_REDIRECT_TO_SDK
#define PRINTF DbgConsole_Printf
#define SCANF DbgConsole_Scanf
#define PUTCHAR DbgConsole_Putchar
#define GETCHAR DbgConsole_Getchar
#elif SDK_DEBUGCONSOLE == DEBUGCONSOLE_REDIRECT_TO_TOOLCHAIN
#define PRINTF printf
#define SCANF scanf
#define PUTCHAR putchar
#define GETCHAR getchar
#endif
SDK_DEBUGCONSOLE and SDK_DEBUGCONSOLE_UART
There are two macros SDK_DEBUGCONSOLE and SDK_DEBUGCONSOLE_UART added to configure PRINTF and low level output perihperal.
- The macro SDK_DEBUGCONSOLE is used for forntend. Whether debug console redirect to toolchain or SDK or disabled, it decides which is the frontend of the debug console, Tool chain or SDK. The fucntion can be set by the macro SDK_DEBUGCONSOLE.
- The macro SDK_DEBUGCONSOLE_UART is used for backend. It is use to decide whether provide low level IO implementation to toolchain printf and scanf. For example, within MCUXpresso, if the macro SDK_DEBUGCONSOLE_UART is defined, __sys_write and __sys_readc will be used when __REDLIB__ is defined; _write and _read will be used in other cases.The macro does not specifically refer to the perihpheral "UART". It refers to the external perihperal UART. So if the macro SDK_DEBUGCONSOLE_UART is not defined when tool-chain printf is calling, the semihosting will be used.
The following the matrix show the effects of SDK_DEBUGCONSOLE and SDK_DEBUGCONSOLE_UART on PRINTF and printf. The green mark is the default setting of the debug console.
| SDK_DEBUGCONSOLE | SDK_DEBUGCONSOLE_UART | PRINTF | printf |
| DEBUGCONSOLE_REDIRECT_TO_SDK | defined | UART | UART |
| DEBUGCONSOLE_REDIRECT_TO_SDK | undefined | UART | semihost |
| DEBUGCONSOLE_REDIRECT_TO_TOOLCHAIN | defined | UART | UART |
| DEBUGCONSOLE_REDIRECT_TO_TOOLCHAIN | undefined | semihost | semihost |
| DEBUGCONSOLE_DISABLE | defined | No ouput | UART |
| DEBUGCONSOLE_DISABLE | undefined | No ouput | semihost |
Typical use case
Some examples use the PUTCHAR & GETCHAR function
ch = GETCHAR();
PUTCHAR(ch);
Some examples use the PRINTF function
Statement prints the string format.
PRINTF(
"%s %s\r\n",
"Hello",
"world!");
Statement prints the hexadecimal format/
PRINTF(
"0x%02X hexadecimal number equivalents 255", 255);
Statement prints the decimal floating point and unsigned decimal.
PRINTF(
"Execution timer: %s\n\rTime: %u ticks %2.5f milliseconds\n\rDONE\n\r",
"1 day", 86400, 86.4);
Some examples use the SCANF function
PRINTF(
"Enter a decimal number: ");
SCANF("%d", &i);
PRINTF(
"\r\nYou have entered %d.\r\n", i, i);
PRINTF(
"Enter a hexadecimal number: ");
SCANF("%x", &i);
PRINTF(
"\r\nYou have entered 0x%X (%d).\r\n", i, i);
Print out failure messages using MCUXpresso SDK __assert_func:
void __assert_func(const char *file, int line, const char *func, const char *failedExpr)
{
PRINTF(
"ASSERT ERROR \" %s \": file \"%s\" Line \"%d\" function name \"%s\" \n", failedExpr, file , line, func);
for (;;)
{}
}
Note:
To use 'printf' and 'scanf' for GNUC Base, add file 'fsl_sbrk.c' in path: ..\{package}\devices\{subset}\utilities\fsl_sbrk.c to your project.
| #define DEBUGCONSOLE_REDIRECT_TO_TOOLCHAIN 0U |
Select toolchain printf and scanf.
| #define DEBUGCONSOLE_REDIRECT_TO_SDK 1U |
| #define DEBUGCONSOLE_DISABLE 2U |
| #define PRINTF_FLOAT_ENABLE 0U |
| #define SCANF_FLOAT_ENABLE 0U |
| #define PRINTF_ADVANCED_ENABLE 0U |
| #define SCANF_ADVANCED_ENABLE 0U |
if SDK_DEBUGCONSOLE defined to 0,it represents select toolchain printf, scanf. if SDK_DEBUGCONSOLE defined to 1,it represents select SDK version printf, scanf. if SDK_DEBUGCONSOLE defined to 2,it represents disable debugconsole function.
Call this function to enable debug log messages to be output via the specified peripheral, frequency of peripheral source clock, and base address at the specified baud rate. After this function has returned, stdout and stdin are connected to the selected peripheral.
- Parameters
-
| instance | The instance of the module.If the device is kSerialPort_Uart, the instance is UART peripheral instance. The UART hardware peripheral type is determined by UART adapter. For example, if the instance is 1, if the lpuart_adapter.c is added to the current project, the UART periheral is LPUART1. If the uart_adapter.c is added to the current project, the UART periheral is UART1. |
| baudRate | The desired baud rate in bits per second. |
| device | Low level device type for the debug console, can be one of the following.
|
| clkSrcFreq | Frequency of peripheral source clock. |
- Returns
- Indicates whether initialization was successful or not.
- Return values
-
| kStatus_Success | Execution successfully |
| kStatus_Fail | Execution failure |
Call this function to disable debug log messages to be output via the specified peripheral base address and at the specified baud rate.
- Returns
- Indicates whether de-initialization was successful or not.
| status_t DbgConsole_EnterLowpower |
( |
void |
| ) |
|
This function is used to prepare to enter low power consumption.
- Returns
- Indicates whether de-initialization was successful or not.
| status_t DbgConsole_ExitLowpower |
( |
void |
| ) |
|
This function is used to restore from low power consumption.
- Returns
- Indicates whether de-initialization was successful or not.
| int DbgConsole_Printf |
( |
const char * |
fmt_s, |
|
|
|
... |
|
) |
| |
Call this function to write a formatted output to the standard output stream.
- Parameters
-
| fmt_s | Format control string. |
- Returns
- Returns the number of characters printed or a negative value if an error occurs.
| int DbgConsole_Vprintf |
( |
const char * |
fmt_s, |
|
|
va_list |
formatStringArg |
|
) |
| |
Call this function to write a formatted output to the standard output stream.
- Parameters
-
| fmt_s | Format control string. |
| formatStringArg | Format arguments. |
- Returns
- Returns the number of characters printed or a negative value if an error occurs.
| int DbgConsole_Putchar |
( |
int |
dbgConsoleCh | ) |
|
Call this function to write a character to stdout.
- Parameters
-
| dbgConsoleCh | Character to be written. |
- Returns
- Returns the character written.
| int DbgConsole_Scanf |
( |
char * |
fmt_s, |
|
|
|
... |
|
) |
| |
Call this function to read formatted data from the standard input stream.
- Parameters
-
| fmt_s | Format control string. |
- Returns
- Returns the number of fields successfully converted and assigned.
| int DbgConsole_Getchar |
( |
void |
| ) |
|
Call this function to read a character from standard input.
- Returns
- Returns the character read.