![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
Data Structures | |
| struct | _asrc_p2p_sdma_config |
| destination peripheral configuration More... | |
| struct | _asrc_sdma_in_handle |
| ASRC sdma in handle. More... | |
| struct | _asrc_sdma_out_handle |
| ASRC sdma out handle. More... | |
| struct | _asrc_sdma_handle |
| ASRC DMA transfer handle, users should not touch the content of the handle. More... | |
Macros | |
| #define | ASRC_XFER_IN_QUEUE_SIZE 4U |
| ASRC xfer queue size. | |
Typedefs | |
| typedef struct _asrc_sdma_handle | asrc_sdma_handle_t |
| ASRC sdma handle prototype. | |
| typedef void(* | asrc_sdma_callback_t )(ASRC_Type *base, asrc_sdma_handle_t *handle, status_t status, void *userData) |
| ASRC SDMA transfer callback function for finish and error. | |
| typedef void(* | asrc_start_peripheral_t )(bool start) |
| ASRC trigger peripheral function pointer. | |
|
typedef struct _asrc_p2p_sdma_config | asrc_p2p_sdma_config_t |
| destination peripheral configuration | |
| typedef struct _asrc_sdma_in_handle | asrc_sdma_in_handle_t |
| ASRC sdma in handle. | |
|
typedef struct _asrc_sdma_out_handle | asrc_sdma_out_handle_t |
| ASRC sdma out handle. | |
Driver version | |
| #define | FSL_ASRC_SDMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 3)) |
| Version 2.0.3. | |
ASRC SDMA Transactional | |
| void | ASRC_TransferInCreateHandleSDMA (ASRC_Type *base, asrc_sdma_handle_t *handle, asrc_sdma_callback_t callback, sdma_handle_t *dmaHandle, uint32_t eventSource, asrc_context_t context, const asrc_p2p_sdma_config_t *periphConfig, void *userData) |
| Initializes the ASRC input SDMA handle. More... | |
| void | ASRC_TransferOutCreateHandleSDMA (ASRC_Type *base, asrc_sdma_handle_t *handle, asrc_sdma_callback_t callback, sdma_handle_t *dmaHandle, uint32_t eventSource, asrc_context_t context, const asrc_p2p_sdma_config_t *periphConfig, void *userData) |
| Initializes the ASRC output SDMA handle. More... | |
| status_t | ASRC_TransferSetContextConfigSDMA (ASRC_Type *base, asrc_sdma_handle_t *handle, asrc_context_config_t *asrcConfig) |
| Configures the ASRC context. More... | |
| status_t | ASRC_TransferSDMA (ASRC_Type *base, asrc_sdma_handle_t *handle, asrc_transfer_t *xfer) |
| Performs a non-blocking ASRC transfer using DMA. More... | |
| void | ASRC_TransferAbortInSDMA (ASRC_Type *base, asrc_sdma_handle_t *handle) |
| Aborts a ASRC in transfer using SDMA. More... | |
| void | ASRC_TransferAbortOutSDMA (ASRC_Type *base, asrc_sdma_handle_t *handle) |
| brief Aborts a ASRC out transfer using SDMA. More... | |
| struct _asrc_p2p_sdma_config |
Data Fields | |
| uint32_t | eventSource |
| peripheral event source | |
| uint8_t | watermark |
| peripheral watermark | |
| uint8_t | channel |
| peripheral channel number | |
| uint8_t | fifoWidth |
| peripheral fifo width | |
| bool | enableContinuous |
true is the amount of samples to be transferred is unknown and script will keep on transferring as long as both events are detected and script must be stopped by application, false is The amount of samples to be transferred is equal to the count field of mode word | |
| asrc_start_peripheral_t | startPeripheral |
| trigger peripheral start | |
| struct _asrc_sdma_in_handle |
Data Fields | |
| sdma_handle_t * | sdmaHandle |
| DMA handler for ASRC. | |
| uint32_t | eventSource |
| ASRC event source number. | |
| asrc_sdma_callback_t | callback |
| Callback for users while transfer finish or error occurs. | |
| void * | userData |
| User callback parameter. | |
| sdma_buffer_descriptor_t | bdPool [ASRC_XFER_IN_QUEUE_SIZE] |
| BD pool for SDMA transfer. More... | |
| uint8_t | asrcInWatermark |
| The transfer data count in a DMA request. | |
| uint8_t | bytesPerSample |
| Bytes in a sample. | |
| uint32_t * | asrcQueue [ASRC_XFER_IN_QUEUE_SIZE] |
| Transfer queue storing queued transfer. More... | |
| size_t | sdmaTransferSize [ASRC_XFER_IN_QUEUE_SIZE] |
| Data bytes need to transfer. | |
| volatile uint8_t | queueUser |
| Index for user to queue transfer. More... | |
| volatile uint8_t | queueDriver |
| Index for driver to get the transfer data and size. | |
| const asrc_p2p_sdma_config_t * | peripheralConfig |
| peripheral configuration | |
| uint32_t | state |
| Internal state for ASRC SDMA transfer. | |
| sdma_buffer_descriptor_t _asrc_sdma_in_handle::bdPool[ASRC_XFER_IN_QUEUE_SIZE] |
| uint32_t* _asrc_sdma_in_handle::asrcQueue[ASRC_XFER_IN_QUEUE_SIZE] |
| volatile uint8_t _asrc_sdma_in_handle::queueUser |
| struct _asrc_sdma_out_handle |
Data Fields | |
| sdma_handle_t * | sdmaHandle |
| DMA handler for ASRC. | |
| void * | userData |
| User callback parameter. | |
| uint32_t | state |
| Internal state for ASRC SDMA transfer. | |
| uint8_t | bytesPerSample |
| Bytes in a sample. | |
| uint32_t | eventSource |
| ASRC event source number. | |
| asrc_sdma_callback_t | callback |
| Callback for users while transfer finish or error occurs. | |
| uint8_t | asrcOutWatermark |
| The transfer data count in a DMA request. | |
| sdma_buffer_descriptor_t | bdPool [ASRC_XFER_OUT_QUEUE_SIZE] |
| BD pool for SDMA transfer. More... | |
| uint32_t * | asrcQueue [ASRC_XFER_OUT_QUEUE_SIZE] |
| Transfer queue storing queued transfer. More... | |
| size_t | sdmaTransferSize [ASRC_XFER_OUT_QUEUE_SIZE] |
| Data bytes need to transfer. | |
| volatile uint8_t | queueUser |
| Index for user to queue transfer. More... | |
| volatile uint8_t | queueDriver |
| Index for driver to get the transfer data and size. | |
| const asrc_p2p_sdma_config_t * | peripheralConfig |
| peripheral configuration | |
| uint32_t | nonAlignSize |
| non align size | |
| void * | nonAlignAddr |
| non align address | |
| sdma_buffer_descriptor_t _asrc_sdma_out_handle::bdPool[ASRC_XFER_OUT_QUEUE_SIZE] |
| uint32_t* _asrc_sdma_out_handle::asrcQueue[ASRC_XFER_OUT_QUEUE_SIZE] |
| volatile uint8_t _asrc_sdma_out_handle::queueUser |
| struct _asrc_sdma_handle |
Data Fields | |
| asrc_sdma_in_handle_t | inDMAHandle |
| input dma handle | |
| asrc_sdma_out_handle_t | outDMAHandle |
| output dma handle | |
| asrc_context_t | context |
| ASRC context number. | |
| uint8_t | dataChannels |
| ASRC process data channel number. | |
| void ASRC_TransferInCreateHandleSDMA | ( | ASRC_Type * | base, |
| asrc_sdma_handle_t * | handle, | ||
| asrc_sdma_callback_t | callback, | ||
| sdma_handle_t * | dmaHandle, | ||
| uint32_t | eventSource, | ||
| asrc_context_t | context, | ||
| const asrc_p2p_sdma_config_t * | periphConfig, | ||
| void * | userData | ||
| ) |
This function initializes the ASRC input DMA handle, which can be used for other ASRC transactional APIs. Usually, for a specified ASRC context, call this API once to get the initialized handle.
| base | ASRC base pointer. |
| handle | ASRC SDMA handle pointer. |
| base | ASRC peripheral base address. |
| callback | Pointer to user callback function. |
| dmaHandle | SDMA handle pointer, this handle shall be static allocated by users. |
| eventSource | ASRC input sdma event source. |
| context | ASRC context number. |
| periphConfig | peripheral configurations, used for case. |
| userData | User parameter passed to the callback function. |
| void ASRC_TransferOutCreateHandleSDMA | ( | ASRC_Type * | base, |
| asrc_sdma_handle_t * | handle, | ||
| asrc_sdma_callback_t | callback, | ||
| sdma_handle_t * | dmaHandle, | ||
| uint32_t | eventSource, | ||
| asrc_context_t | context, | ||
| const asrc_p2p_sdma_config_t * | periphConfig, | ||
| void * | userData | ||
| ) |
This function initializes the ASRC out DMA handle, which can be used for other ASRC transactional APIs. Usually, for a specified ASRC context, call this API once to get the initialized handle.
| base | ASRC base pointer. |
| handle | ASRC SDMA handle pointer. |
| callback | ASRC outcallback. |
| dmaHandle | SDMA handle pointer, this handle shall be static allocated by users. |
| eventSource | ASRC output event source. |
| context | ASRC context number. |
| periphConfig | peripheral configurations, used for case. |
| userData | User parameter passed to the callback function. |
| status_t ASRC_TransferSetContextConfigSDMA | ( | ASRC_Type * | base, |
| asrc_sdma_handle_t * | handle, | ||
| asrc_context_config_t * | asrcConfig | ||
| ) |
| base | ASRC base pointer. |
| handle | ASRC SDMA handle pointer. |
| asrcConfig | asrc context configurations. |
| status_t ASRC_TransferSDMA | ( | ASRC_Type * | base, |
| asrc_sdma_handle_t * | handle, | ||
| asrc_transfer_t * | xfer | ||
| ) |
| base | ASRC base pointer. |
| handle | ASRC SDMA handle pointer. |
| xfer | ASRC xfer configurations pointer. |
| kStatus_Success | Start a ASRC SDMA send successfully. |
| kStatus_InvalidArgument | The input argument is invalid. |
| kStatus_TxBusy | ASRC is busy sending data. |
| void ASRC_TransferAbortInSDMA | ( | ASRC_Type * | base, |
| asrc_sdma_handle_t * | handle | ||
| ) |
| base | ASRC base pointer. |
| handle | ASRC SDMA handle pointer. |
| void ASRC_TransferAbortOutSDMA | ( | ASRC_Type * | base, |
| asrc_sdma_handle_t * | handle | ||
| ) |
param base ASRC base pointer. param handle ASRC SDMA handle pointer.