MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
CACHE: LPLMEM CACHE Memory Controller

Overview

The SDK provides a peripheral driver for the CACHE Controller of MCUXpresso SDK devices.

CACHE driver is created to help user to operate the cache memory more easy. The LPLMEM contains code bus cache and system bus cache if the system bus cache is supported (the system bus cache is soc specific). The code bus cache is ranged from 0x00000000 ~ 0x1FFFFFFF and the system bus is ranged from 0x20000000 ~ 0xFFFFFFFF.

The APIs for basic operations are including the following three groups: 1L. The L1 specific cache driver API. This group provides the IP specific cache controller drivers. The L1 caches in this arch is the AHB Low-Power Local Memory Controller (LPLMEM). The driver API name in this level is L1 cache controller specific.

2L. The unified L1 cache driver API. For ease of use, we try to unify the L1 cache driver API as much as possible in this group. APIs of this type directly call the L1 specific cache driver API and are unified to the same name. Due to the cache controller specification, it is impossible to provide all L1 cache unified APIs for LPLMEM.

3L. The unified cache driver API. This group is provided for unified cache driver APIs for combining L1 and L2 cache maintain operations. This is provided for SDK drivers (DMA, ENET, USDHC, etc) which should do the cache maintenance in their transactional APIs. This is because in this arch, there is no L2 cache so the unified cache driver API directly call only L1 cache driver APIs.

Function groups

L1 CACHE Operation

This function group provides Enable/Disable APIs. This function group only provides the cache invalidate operation beacuse the LPLMEM is write through mode. By default, the cache mode is write through with allocation. The above cache maintains are provided for code bus cache and might provide for system bus cache if it is supported in the future.

Driver version

#define FSL_CACHE_DRIVER_VERSION   (MAKE_VERSION(2, 1, 1))
 cache driver version 2.1.1. More...
 

cache control for the L1 low power local memory controller

static void L1CACHE_EnableCodeCache (void)
 Enables the processor code bus cache.
 
static void L1CACHE_DisableCodeCache (void)
 Disables the processor code bus cache.
 
static void L1CACHE_InvalidateCodeCache (void)
 Invalidates the processor code bus cache.
 

The unified L1 cache controller

The LPLMEM is write-through design, so there is no cache maintain by range control operation.

So all cache maintain by range unified functions are directly call the cache maintain all functions since they have the same effect.

void L1CACHE_InvalidateICacheByRange (uint32_t address, uint32_t size_byte)
 Invalidates L1 instrument cache by range. More...
 
static void L1CACHE_InvalidateDCacheByRange (uint32_t address, uint32_t size_byte)
 Invalidates L1 data cache by range. More...
 
static void L1CACHE_CleanDCacheByRange (uint32_t address, uint32_t size_byte)
 Cleans L1 data cache by range. More...
 
static void L1CACHE_CleanInvalidateDCacheByRange (uint32_t address, uint32_t size_byte)
 Cleans and Invalidates L1 data cache by range. More...
 

Unified Cache Control for caches in all levels

static void ICACHE_InvalidateByRange (uint32_t address, uint32_t size_byte)
 Invalidates instruction cache by range. More...
 
static void DCACHE_InvalidateByRange (uint32_t address, uint32_t size_byte)
 Invalidates data cache by range. More...
 
static void DCACHE_CleanByRange (uint32_t address, uint32_t size_byte)
 Clean data cache by range. More...
 
static void DCACHE_CleanInvalidateByRange (uint32_t address, uint32_t size_byte)
 Cleans and Invalidates data cache by range. More...
 

Macro Definition Documentation

#define FSL_CACHE_DRIVER_VERSION   (MAKE_VERSION(2, 1, 1))

Function Documentation

void L1CACHE_InvalidateICacheByRange ( uint32_t  address,
uint32_t  size_byte 
)
Parameters
addressThe start address of the memory to be invalidated.
size_byteThe memory size.
static void L1CACHE_InvalidateDCacheByRange ( uint32_t  address,
uint32_t  size_byte 
)
inlinestatic
Parameters
addressThe start address of the memory to be invalidated.
size_byteThe memory size.
static void L1CACHE_CleanDCacheByRange ( uint32_t  address,
uint32_t  size_byte 
)
inlinestatic

The cache is write through mode, so there is nothing to do with the cache flush/clean operation.

Parameters
addressThe start address of the memory to be cleaned.
size_byteThe memory size.
static void L1CACHE_CleanInvalidateDCacheByRange ( uint32_t  address,
uint32_t  size_byte 
)
inlinestatic
Parameters
addressThe start address of the memory to be clean and invalidated.
size_byteThe memory size.
static void ICACHE_InvalidateByRange ( uint32_t  address,
uint32_t  size_byte 
)
inlinestatic
Parameters
addressThe physical address.
size_bytesize of the memory to be invalidated.
static void DCACHE_InvalidateByRange ( uint32_t  address,
uint32_t  size_byte 
)
inlinestatic
Parameters
addressThe physical address.
size_bytesize of the memory to be invalidated.
static void DCACHE_CleanByRange ( uint32_t  address,
uint32_t  size_byte 
)
inlinestatic
Parameters
addressThe physical address.
size_bytesize of the memory to be cleaned.
static void DCACHE_CleanInvalidateByRange ( uint32_t  address,
uint32_t  size_byte 
)
inlinestatic
Parameters
addressThe physical address.
size_bytesize of the memory to be Cleaned and Invalidated.