![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev 2.16.000
    
   NXP Semiconductors 
   | 
 
Modules | |
| ftfx utilities | |
Data Structures | |
| struct | ftfx_spec_mem_t | 
| ftfx special memory access information.  More... | |
| struct | ftfx_mem_desc_t | 
| Flash memory descriptor.  More... | |
| struct | ftfx_ops_config_t | 
| Active FTFx information for the current operation.  More... | |
| struct | ftfx_ifr_desc_t | 
| Flash IFR memory descriptor.  More... | |
| struct | ftfx_config_t | 
| Flash driver state information.  More... | |
Macros | |
| #define | kFTFx_ResourceOptionFlashIfr 0x00U | 
| Macro for the two possible options of flash read resource command.  More... | |
| #define | kFTFx_ResourceOptionVersionId 0x01U | 
| Select code for the version ID.  | |
| #define | kFTFx_MarginValueNormal 0x0U | 
| Macro for supported FTFx margin levels.  | |
| #define | kFTFx_MarginValueUser 0x1U | 
| Apply the 'User' margin to the normal read-1 level.  More... | |
| #define | kFTFx_MarginValueFactory 0x2U | 
| Apply the 'Factory' margin to the normal read-1 level.  More... | |
| #define | kFTFx_MarginValueInvalid 0x3U | 
| Not real margin level, Used to determine the range of valid margin level.  More... | |
Initialization | |
| void | FTFx_API_Init (ftfx_config_t *config) | 
| Initializes the global flash properties structure members.  More... | |
Erasing | |
| status_t | FTFx_CMD_Erase (ftfx_config_t *config, uint32_t start, uint32_t lengthInBytes, uint32_t key) | 
| Erases the flash sectors encompassed by parameters passed into function.  More... | |
| status_t | FTFx_CMD_EraseAll (ftfx_config_t *config, uint32_t key) | 
| Erases entire flash.  More... | |
Programming | |
| status_t | FTFx_CMD_Program (ftfx_config_t *config, uint32_t start, const uint8_t *src, uint32_t lengthInBytes) | 
| Programs flash with data at locations passed in through parameters.  More... | |
| status_t | FTFx_CMD_ProgramOnce (ftfx_config_t *config, uint8_t index, const uint8_t *src, uint32_t lengthInBytes) | 
| Programs Program Once Field through parameters.  More... | |
Reading | |
| status_t | FTFx_CMD_ReadOnce (ftfx_config_t *config, uint8_t index, uint8_t *dst, uint32_t lengthInBytes) | 
| Reads the Program Once Field through parameters.  More... | |
Verification | |
| status_t | FTFx_CMD_VerifyErase (ftfx_config_t *config, uint32_t start, uint32_t lengthInBytes, uint8_t margin) | 
| Verifies an erasure of the desired flash area at a specified margin level.  More... | |
| status_t | FTFx_CMD_VerifyEraseAll (ftfx_config_t *config, uint8_t margin) | 
| Verifies erasure of the entire flash at a specified margin level.  More... | |
| status_t | FTFx_CMD_VerifyProgram (ftfx_config_t *config, uint32_t start, uint32_t lengthInBytes, const uint8_t *expectedData, uint8_t margin, uint32_t *failedAddress, uint32_t *failedData) | 
| Verifies programming of the desired flash area at a specified margin level.  More... | |
Security | |
| status_t | FTFx_REG_GetSecurityState (ftfx_config_t *config, ftfx_security_state_t *state) | 
| Returns the security state via the pointer passed into the function.  More... | |
| struct ftfx_spec_mem_t | 
| struct ftfx_mem_desc_t | 
Data Fields | |
| uint32_t | blockBase | 
| A base address of the flash block.  | |
| uint32_t | totalSize | 
| The size of the flash block.  More... | |
| uint32_t | sectorSize | 
| The size in bytes of a sector of flash.  More... | |
| uint32_t | blockCount | 
| A number of flash blocks.  More... | |
| uint8_t | type | 
| Type of flash block.  More... | |
| uint8_t | index | 
| Index of flash block.  More... | |
| uint8_t ftfx_mem_desc_t::type | 
| uint8_t ftfx_mem_desc_t::index | 
| uint32_t ftfx_mem_desc_t::totalSize | 
| uint32_t ftfx_mem_desc_t::sectorSize | 
| uint32_t ftfx_mem_desc_t::blockCount | 
| struct ftfx_ops_config_t | 
Data Fields | |
| uint32_t | convertedAddress | 
| A converted address for the current flash type.  More... | |
| uint32_t ftfx_ops_config_t::convertedAddress | 
| struct ftfx_ifr_desc_t | 
| struct ftfx_config_t | 
An instance of this structure is allocated by the user of the flash driver and passed into each of the driver APIs.
Data Fields | |
| uint32_t | flexramBlockBase | 
| The base address of the FlexRAM/acceleration RAM.  | |
| uint32_t | flexramTotalSize | 
| The size of the FlexRAM/acceleration RAM.  | |
| uint16_t | eepromTotalSize | 
| The size of EEPROM area which was partitioned from FlexRAM.  | |
| function_ptr_t | runCmdFuncAddr | 
| An buffer point to the flash execute-in-RAM function.  More... | |
| function_ptr_t ftfx_config_t::runCmdFuncAddr | 
| #define kStatusGroupGeneric 0 | 
| #define kFTFx_ResourceOptionFlashIfr 0x00U | 
Select code for Program flash 0 IFR, Program flash swap 0 IFR, Data flash 0 IFR
| #define kFTFx_MarginValueUser 0x1U | 
| #define kFTFx_MarginValueFactory 0x2U | 
| #define kFTFx_MarginValueInvalid 0x3U | 
| anonymous enum | 
| enum ftfx_swap_state_t | 
| void FTFx_API_Init | ( | ftfx_config_t * | config | ) | 
This function checks and initializes the Flash module for the other Flash APIs.
| config | Pointer to the storage for the driver runtime state. | 
| status_t FTFx_CMD_Erase | ( | ftfx_config_t * | config, | 
| uint32_t | start, | ||
| uint32_t | lengthInBytes, | ||
| uint32_t | key | ||
| ) | 
This function erases the appropriate number of flash sectors based on the desired start address and length.
| config | The pointer to the storage for the driver runtime state. | 
| start | The start address of the desired flash memory to be erased. The start address does not need to be sector-aligned but must be word-aligned. | 
| lengthInBytes | The length, given in bytes (not words or long-words) to be erased. Must be word-aligned. | 
| key | The value used to validate all flash erase APIs. | 
| kStatus_FTFx_Success | API was executed successfully. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_AlignmentError | The parameter is not aligned with the specified baseline. | 
| kStatus_FTFx_AddressError | The address is out of range. | 
| kStatus_FTFx_EraseKeyError | The API erase key is invalid. | 
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| kStatus_FTFx_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FTFx_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FTFx_CommandFailure | Run-time error during the command execution. | 
| status_t FTFx_CMD_EraseAll | ( | ftfx_config_t * | config, | 
| uint32_t | key | ||
| ) | 
| config | Pointer to the storage for the driver runtime state. | 
| key | A value used to validate all flash erase APIs. | 
| kStatus_FTFx_Success | API was executed successfully. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_EraseKeyError | API erase key is invalid. | 
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| kStatus_FTFx_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FTFx_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FTFx_CommandFailure | Run-time error during command execution. | 
| kStatus_FTFx_PartitionStatusUpdateFailure | Failed to update the partition status. | 
| status_t FTFx_CMD_Program | ( | ftfx_config_t * | config, | 
| uint32_t | start, | ||
| const uint8_t * | src, | ||
| uint32_t | lengthInBytes | ||
| ) | 
This function programs the flash memory with the desired data for a given flash area as determined by the start address and the length.
| config | A pointer to the storage for the driver runtime state. | 
| start | The start address of the desired flash memory to be programmed. Must be word-aligned. | 
| src | A pointer to the source buffer of data that is to be programmed into the flash. | 
| lengthInBytes | The length, given in bytes (not words or long-words), to be programmed. Must be word-aligned. | 
| kStatus_FTFx_Success | API was executed successfully. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_AlignmentError | Parameter is not aligned with the specified baseline. | 
| kStatus_FTFx_AddressError | Address is out of range. | 
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| kStatus_FTFx_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FTFx_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FTFx_CommandFailure | Run-time error during the command execution. | 
| status_t FTFx_CMD_ProgramOnce | ( | ftfx_config_t * | config, | 
| uint8_t | index, | ||
| const uint8_t * | src, | ||
| uint32_t | lengthInBytes | ||
| ) | 
This function programs the Program Once Field with the desired data for a given flash area as determined by the index and length.
| config | A pointer to the storage for the driver runtime state. | 
| index | The index indicating which area of the Program Once Field to be programmed. | 
| src | A pointer to the source buffer of data that is to be programmed into the Program Once Field. | 
| lengthInBytes | The length, given in bytes (not words or long-words), to be programmed. Must be word-aligned. | 
| kStatus_FTFx_Success | API was executed successfully. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| kStatus_FTFx_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FTFx_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FTFx_CommandFailure | Run-time error during the command execution. | 
| status_t FTFx_CMD_ReadOnce | ( | ftfx_config_t * | config, | 
| uint8_t | index, | ||
| uint8_t * | dst, | ||
| uint32_t | lengthInBytes | ||
| ) | 
This function reads the read once feild with given index and length.
| config | A pointer to the storage for the driver runtime state. | 
| index | The index indicating the area of program once field to be read. | 
| dst | A pointer to the destination buffer of data that is used to store data to be read. | 
| lengthInBytes | The length, given in bytes (not words or long-words), to be programmed. Must be word-aligned. | 
| kStatus_FTFx_Success | API was executed successfully. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| kStatus_FTFx_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FTFx_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FTFx_CommandFailure | Run-time error during the command execution. | 
| status_t FTFx_CMD_VerifyErase | ( | ftfx_config_t * | config, | 
| uint32_t | start, | ||
| uint32_t | lengthInBytes, | ||
| uint8_t | margin | ||
| ) | 
This function checks the appropriate number of flash sectors based on the desired start address and length to check whether the flash is erased to the specified read margin level.
| config | A pointer to the storage for the driver runtime state. | 
| start | The start address of the desired flash memory to be verified. The start address does not need to be sector-aligned but must be word-aligned. | 
| lengthInBytes | The length, given in bytes (not words or long-words), to be verified. Must be word-aligned. | 
| margin | Read margin choice. | 
| kStatus_FTFx_Success | API was executed successfully. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_AlignmentError | Parameter is not aligned with specified baseline. | 
| kStatus_FTFx_AddressError | Address is out of range. | 
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| kStatus_FTFx_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FTFx_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FTFx_CommandFailure | Run-time error during the command execution. | 
| status_t FTFx_CMD_VerifyEraseAll | ( | ftfx_config_t * | config, | 
| uint8_t | margin | ||
| ) | 
This function checks whether the flash is erased to the specified read margin level.
| config | A pointer to the storage for the driver runtime state. | 
| margin | Read margin choice. | 
| kStatus_FTFx_Success | API was executed successfully. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| kStatus_FTFx_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FTFx_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FTFx_CommandFailure | Run-time error during the command execution. | 
| status_t FTFx_CMD_VerifyProgram | ( | ftfx_config_t * | config, | 
| uint32_t | start, | ||
| uint32_t | lengthInBytes, | ||
| const uint8_t * | expectedData, | ||
| uint8_t | margin, | ||
| uint32_t * | failedAddress, | ||
| uint32_t * | failedData | ||
| ) | 
This function verifies the data programed in the flash memory using the Flash Program Check Command and compares it to the expected data for a given flash area as determined by the start address and length.
| config | A pointer to the storage for the driver runtime state. | 
| start | The start address of the desired flash memory to be verified. Must be word-aligned. | 
| lengthInBytes | The length, given in bytes (not words or long-words), to be verified. Must be word-aligned. | 
| expectedData | A pointer to the expected data that is to be verified against. | 
| margin | Read margin choice. | 
| failedAddress | A pointer to the returned failing address. | 
| failedData | A pointer to the returned failing data. Some derivatives do not include failed data as part of the FCCOBx registers. In this case, zeros are returned upon failure. | 
| kStatus_FTFx_Success | API was executed successfully. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_AlignmentError | Parameter is not aligned with specified baseline. | 
| kStatus_FTFx_AddressError | Address is out of range. | 
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| kStatus_FTFx_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FTFx_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FTFx_CommandFailure | Run-time error during the command execution. | 
| status_t FTFx_REG_GetSecurityState | ( | ftfx_config_t * | config, | 
| ftfx_security_state_t * | state | ||
| ) | 
This function retrieves the current flash security status, including the security enabling state and the backdoor key enabling state.
| config | A pointer to storage for the driver runtime state. | 
| state | A pointer to the value returned for the current security status code: | 
| kStatus_FTFx_Success | API was executed successfully. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. |