![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev 2.16.000
    
   NXP Semiconductors 
   | 
 
The I2C_DMA module provide a method for I2C transfer operation based on DMA.
Data Structures | |
| struct | i2c_master_dma_transfer_handle_t | 
| I2C master DMA transfer structure.  More... | |
Typedefs | |
| typedef void(* | i2c_master_dma_transfer_callback_t )(i2c_master_dma_transfer_handle_t *handle) | 
| I2C master DMA transfer callback typedef.  More... | |
Driver version | |
| #define | FSL_I2C_DMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) | 
| I2C DMA driver version.  More... | |
I2C Block DMA Transfer Operation | |
| void | I2C_MasterCreateDMAHandle (I2C_Type *base, i2c_master_dma_transfer_handle_t *psHandle, i2c_master_dma_transfer_callback_t pfCallback, void *pUserData, DMA_Type *dmaBase, dma_channel_t eChannel) | 
| Initializes the I2C handle which is used in transactional functions.  More... | |
| status_t | I2C_MasterTransferDMA (i2c_master_dma_transfer_handle_t *psHandle, i2c_master_transfer_t *psTransfer) | 
| Performs a master DMA non-blocking transfer on the I2C bus.  More... | |
| status_t | I2C_MasterTransferGetCountDMA (i2c_master_dma_transfer_handle_t *psHandle, uint16_t *pu16Count) | 
| Gets a master transfer status during the DMA non-blocking transfer.  More... | |
| void | I2C_MasterTransferAbortDMA (i2c_master_dma_transfer_handle_t *psHandle) | 
| Aborts a master DMA non-blocking transfer early.  More... | |
| struct _i2c_master_dma_transfer_handle | 
Retry times for waiting flag.
I2C master DMA handle typedef.
Data Fields | |
| I2C_Type * | base | 
| I2C base pointer to the I2C instance that assigned to this handle.  More... | |
| i2c_master_transfer_t | sTransfer | 
| I2C master transfer structure.  More... | |
| uint16_t | u16TransferSize | 
| Total bytes to be transferred.  More... | |
| uint8_t | u8State | 
| I2C master transfer status.  More... | |
| dma_handle_t | sDmaHandle | 
| The DMA handler used.  More... | |
| status_t | completionStatus | 
| I2C master transfer complete status, indicating how the transfer ends.  More... | |
| i2c_master_dma_transfer_callback_t | pfCallback | 
| A callback function called after the DMA transfer is finished.  More... | |
| void * | pUserData | 
User configurable pointer to any data, function, structure etc that user wish to use in the  callback   | |
| I2C_Type* i2c_master_dma_transfer_handle_t::base | 
| i2c_master_transfer_t i2c_master_dma_transfer_handle_t::sTransfer | 
| uint16_t i2c_master_dma_transfer_handle_t::u16TransferSize | 
| uint8_t i2c_master_dma_transfer_handle_t::u8State | 
| dma_handle_t i2c_master_dma_transfer_handle_t::sDmaHandle | 
| status_t i2c_master_dma_transfer_handle_t::completionStatus | 
| i2c_master_dma_transfer_callback_t i2c_master_dma_transfer_handle_t::pfCallback | 
| #define FSL_I2C_DMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) | 
| typedef void(* i2c_master_dma_transfer_callback_t)(i2c_master_dma_transfer_handle_t *handle) | 
| void I2C_MasterCreateDMAHandle | ( | I2C_Type * | base, | 
| i2c_master_dma_transfer_handle_t * | psHandle, | ||
| i2c_master_dma_transfer_callback_t | pfCallback, | ||
| void * | pUserData, | ||
| DMA_Type * | dmaBase, | ||
| dma_channel_t | eChannel | ||
| ) | 
| base | I2C peripheral base address. | 
| psHandle | A pointer to the i2c_master_dma_transfer_handle_t structure. | 
| pfCallback | A pointer to the user callback function. | 
| pUserData | A user parameter passed to the callback function. | 
| dmaBase | DMA base address. | 
| eChannel | DMA channel for master transfer. | 
| status_t I2C_MasterTransferDMA | ( | i2c_master_dma_transfer_handle_t * | psHandle, | 
| i2c_master_transfer_t * | psTransfer | ||
| ) | 
| psHandle | A pointer to the i2c_master_dma_transfer_handle_t structure. | 
| psTransfer | A pointer to the transfer structure of i2c_master_transfer_t. | 
| kStatus_Success | Successfully completed the data transmission. | 
| kStatus_I2C_Busy | A previous transmission is still not finished. | 
| kStatus_I2C_Timeout | Transfer error, waits for a signal timeout. | 
| kStatus_I2C_ArbitrationLost | Transfer error, arbitration lost. | 
| kStataus_I2C_Nak | Transfer error, receive NAK during transfer. | 
| status_t I2C_MasterTransferGetCountDMA | ( | i2c_master_dma_transfer_handle_t * | psHandle, | 
| uint16_t * | pu16Count | ||
| ) | 
| psHandle | A pointer to the i2c_master_dma_transfer_handle_t structure. | 
| pu16Count | A number of bytes transferred by the non-blocking transaction. | 
| void I2C_MasterTransferAbortDMA | ( | i2c_master_dma_transfer_handle_t * | psHandle | ) | 
| psHandle | A pointer to the i2c_master_dma_transfer_handle_t structure. |