![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
Data Structures | |
| struct | _hal_uart_config |
| UART configuration structure. More... | |
| struct | _hal_uart_transfer |
| UART transfer structure. More... | |
Macros | |
| #define | UART_ADAPTER_NON_BLOCKING_MODE (1U) |
| Enable or disable UART adapter non-blocking mode (1 - enable, 0 - disable) | |
| #define | HAL_UART_ADAPTER_FIFO (1U) |
| Enable or disable uart hardware FIFO mode (1 - enable, 0 - disable) | |
| #define | HAL_UART_DMA_INIT_ENABLE (1U) |
| Enable or disable uart DMA adapter int mode (1 - enable, 0 - disable) | |
| #define | HAL_UART_DMA_IDLELINE_TIMEOUT (1U) |
| Definition of uart dma adapter software idleline detection timeout value in ms. More... | |
| #define | HAL_UART_HANDLE_SIZE (92U + HAL_UART_ADAPTER_LOWPOWER * 16U + HAL_UART_DMA_ENABLE * 4U) |
| Definition of uart adapter handle size. More... | |
| #define | UART_HANDLE_DEFINE(name) uint32_t name[((HAL_UART_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))] |
| Definition of uart dma adapter handle size. More... | |
| #define | HAL_UART_TRANSFER_MODE (0U) |
| Whether enable transactional function of the UART. More... | |
Typedefs | |
| typedef void * | hal_uart_handle_t |
| The handle of uart adapter. More... | |
| typedef void * | hal_uart_dma_handle_t |
| The handle of uart dma adapter. More... | |
| typedef enum _hal_uart_status | hal_uart_status_t |
| UART status. | |
| typedef enum _hal_uart_parity_mode | hal_uart_parity_mode_t |
| UART parity mode. More... | |
| typedef enum _hal_uart_stop_bit_count | hal_uart_stop_bit_count_t |
| UART stop bit count. More... | |
| typedef struct _hal_uart_config | hal_uart_config_t |
| UART configuration structure. More... | |
| typedef void(* | hal_uart_transfer_callback_t )(hal_uart_handle_t handle, hal_uart_status_t status, void *callbackParam) |
| UART transfer callback function. More... | |
| typedef struct _hal_uart_transfer | hal_uart_transfer_t |
| UART transfer structure. More... | |
Enumerations | |
| enum | _hal_uart_status { kStatus_HAL_UartSuccess = kStatus_Success, kStatus_HAL_UartTxBusy = MAKE_STATUS(kStatusGroup_HAL_UART, 1), kStatus_HAL_UartRxBusy = MAKE_STATUS(kStatusGroup_HAL_UART, 2), kStatus_HAL_UartTxIdle = MAKE_STATUS(kStatusGroup_HAL_UART, 3), kStatus_HAL_UartRxIdle = MAKE_STATUS(kStatusGroup_HAL_UART, 4), kStatus_HAL_UartBaudrateNotSupport, kStatus_HAL_UartProtocolError, kStatus_HAL_UartError = MAKE_STATUS(kStatusGroup_HAL_UART, 7) } |
| UART status. More... | |
| enum | _hal_uart_parity_mode { kHAL_UartParityDisabled = 0x0U, kHAL_UartParityEven = 0x2U, kHAL_UartParityOdd = 0x3U } |
| UART parity mode. More... | |
| enum | _hal_uart_stop_bit_count { kHAL_UartOneStopBit = 0U, kHAL_UartTwoStopBit = 1U } |
| UART stop bit count. More... | |
Functions | |
| hal_uart_status_t | HAL_UartEnterLowpower (hal_uart_handle_t handle) |
| Prepares to enter low power consumption. More... | |
| hal_uart_status_t | HAL_UartExitLowpower (hal_uart_handle_t handle) |
| Restores from low power consumption. More... | |
| void | HAL_UartIsrFunction (hal_uart_handle_t handle) |
| UART IRQ handle function. More... | |
Initialization and deinitialization | |
| hal_uart_status_t | HAL_UartInit (hal_uart_handle_t handle, const hal_uart_config_t *uart_config) |
| Initializes a UART instance with the UART handle and the user configuration structure. More... | |
| hal_uart_status_t | HAL_UartDeinit (hal_uart_handle_t handle) |
| Deinitializes a UART instance. More... | |
Blocking bus Operations | |
| hal_uart_status_t | HAL_UartReceiveBlocking (hal_uart_handle_t handle, uint8_t *data, size_t length) |
| Reads RX data register using a blocking method. More... | |
| hal_uart_status_t | HAL_UartSendBlocking (hal_uart_handle_t handle, const uint8_t *data, size_t length) |
| Writes to the TX register using a blocking method. More... | |
Functional API with non-blocking mode. | |
| |
| hal_uart_status_t | HAL_UartInstallCallback (hal_uart_handle_t handle, hal_uart_transfer_callback_t callback, void *callbackParam) |
| Installs a callback and callback parameter. More... | |
| hal_uart_status_t | HAL_UartReceiveNonBlocking (hal_uart_handle_t handle, uint8_t *data, size_t length) |
| Receives a buffer of data using an interrupt method. More... | |
| hal_uart_status_t | HAL_UartSendNonBlocking (hal_uart_handle_t handle, uint8_t *data, size_t length) |
| Transmits a buffer of data using the interrupt method. More... | |
| hal_uart_status_t | HAL_UartGetReceiveCount (hal_uart_handle_t handle, uint32_t *reCount) |
| Gets the number of bytes that have been received. More... | |
| hal_uart_status_t | HAL_UartGetSendCount (hal_uart_handle_t handle, uint32_t *seCount) |
| Gets the number of bytes written to the UART TX register. More... | |
| hal_uart_status_t | HAL_UartAbortReceive (hal_uart_handle_t handle) |
| Aborts the interrupt-driven data receiving. More... | |
| hal_uart_status_t | HAL_UartAbortSend (hal_uart_handle_t handle) |
| Aborts the interrupt-driven data sending. More... | |
| struct _hal_uart_config |
Data Fields | |
| uint32_t | srcClock_Hz |
| Source clock. | |
| uint32_t | baudRate_Bps |
| Baud rate. | |
| hal_uart_parity_mode_t | parityMode |
| Parity mode, disabled (default), even, odd. | |
| hal_uart_stop_bit_count_t | stopBitCount |
| Number of stop bits, 1 stop bit (default) or 2 stop bits. | |
| uint8_t | enableRx |
| Enable RX. | |
| uint8_t | enableTx |
| Enable TX. | |
| uint8_t | enableRxRTS |
| Enable RX RTS. | |
| uint8_t | enableTxCTS |
| Enable TX CTS. | |
| uint8_t | instance |
| Instance (0 - UART0, 1 - UART1, ...), detail information please refer to the SOC corresponding RM. More... | |
| uint8_t _hal_uart_config::instance |
Invalid instance value will cause initialization failure.
| struct _hal_uart_transfer |
| #define HAL_UART_DMA_IDLELINE_TIMEOUT (1U) |
| #define HAL_UART_HANDLE_SIZE (92U + HAL_UART_ADAPTER_LOWPOWER * 16U + HAL_UART_DMA_ENABLE * 4U) |
| #define UART_HANDLE_DEFINE | ( | name | ) | uint32_t name[((HAL_UART_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))] |
Defines the uart handle
This macro is used to define a 4 byte aligned uart handle. Then use "(hal_uart_handle_t)name" to get the uart handle.
The macro should be global and could be optional. You could also define uart handle by yourself.
This is an example,
| name | The name string of the uart handle. |
| #define HAL_UART_TRANSFER_MODE (0U) |
(0 - disable, 1 - enable)
| typedef void* hal_uart_handle_t |
| typedef void* hal_uart_dma_handle_t |
| typedef enum _hal_uart_parity_mode hal_uart_parity_mode_t |
| typedef enum _hal_uart_stop_bit_count hal_uart_stop_bit_count_t |
| typedef struct _hal_uart_config hal_uart_config_t |
| typedef void(* hal_uart_transfer_callback_t)(hal_uart_handle_t handle, hal_uart_status_t status, void *callbackParam) |
| typedef struct _hal_uart_transfer hal_uart_transfer_t |
| enum _hal_uart_status |
| hal_uart_status_t HAL_UartInit | ( | hal_uart_handle_t | handle, |
| const hal_uart_config_t * | uart_config | ||
| ) |
This function configures the UART module with user-defined settings. The user can configure the configuration structure. The parameter handle is a pointer to point to a memory space of size HAL_UART_HANDLE_SIZE allocated by the caller. Example below shows how to use this API to configure the UART.
| handle | Pointer to point to a memory space of size HAL_UART_HANDLE_SIZE allocated by the caller. The handle should be 4 byte aligned, because unaligned access doesn't be supported on some devices. You can define the handle in the following two ways: UART_HANDLE_DEFINE(handle); or uint32_t handle[((HAL_UART_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))]; |
| uart_config | Pointer to user-defined configuration structure. |
| kStatus_HAL_UartBaudrateNotSupport | Baudrate is not support in current clock source. |
| kStatus_HAL_UartSuccess | UART initialization succeed |
| hal_uart_status_t HAL_UartDeinit | ( | hal_uart_handle_t | handle | ) |
This function waits for TX complete, disables TX and RX, and disables the UART clock.
| handle | UART handle pointer. |
| kStatus_HAL_UartSuccess | UART de-initialization succeed |
| hal_uart_status_t HAL_UartReceiveBlocking | ( | hal_uart_handle_t | handle, |
| uint8_t * | data, | ||
| size_t | length | ||
| ) |
This function polls the RX register, waits for the RX register to be full or for RX FIFO to have data, and reads data from the RX register.
| handle | UART handle pointer. |
| data | Start address of the buffer to store the received data. |
| length | Size of the buffer. |
| kStatus_HAL_UartError | An error occurred while receiving data. |
| kStatus_HAL_UartParityError | A parity error occurred while receiving data. |
| kStatus_HAL_UartSuccess | Successfully received all data. |
| hal_uart_status_t HAL_UartSendBlocking | ( | hal_uart_handle_t | handle, |
| const uint8_t * | data, | ||
| size_t | length | ||
| ) |
This function polls the TX register, waits for the TX register to be empty or for the TX FIFO to have room and writes data to the TX buffer.
| handle | UART handle pointer. |
| data | Start address of the data to write. |
| length | Size of the data to write. |
| kStatus_HAL_UartSuccess | Successfully sent all data. |
| hal_uart_status_t HAL_UartInstallCallback | ( | hal_uart_handle_t | handle, |
| hal_uart_transfer_callback_t | callback, | ||
| void * | callbackParam | ||
| ) |
This function is used to install the callback and callback parameter for UART module. When non-blocking sending or receiving finished, the adapter will notify the upper layer by the installed callback function. And the status is also passed as status parameter when the callback is called.
| handle | UART handle pointer. |
| callback | The callback function. |
| callbackParam | The parameter of the callback function. |
| kStatus_HAL_UartSuccess | Successfully install the callback. |
| hal_uart_status_t HAL_UartReceiveNonBlocking | ( | hal_uart_handle_t | handle, |
| uint8_t * | data, | ||
| size_t | length | ||
| ) |
This function receives data using an interrupt method. This is a non-blocking function, which returns directly without waiting for all data to be received. The receive request is saved by the UART adapter. When the new data arrives, the receive request is serviced first. When all data is received, the UART adapter notifies the upper layer through a callback function and passes the status parameter kStatus_HAL_UartRxIdle.
| handle | UART handle pointer. |
| data | Start address of the data to write. |
| length | Size of the data to write. |
| kStatus_HAL_UartSuccess | Successfully queue the transfer into transmit queue. |
| kStatus_HAL_UartRxBusy | Previous receive request is not finished. |
| kStatus_HAL_UartError | An error occurred. |
| hal_uart_status_t HAL_UartSendNonBlocking | ( | hal_uart_handle_t | handle, |
| uint8_t * | data, | ||
| size_t | length | ||
| ) |
This function sends data using an interrupt method. This is a non-blocking function, which returns directly without waiting for all data to be written to the TX register. When all data is written to the TX register in the ISR, the UART driver calls the callback function and passes the kStatus_HAL_UartTxIdle as status parameter.
| handle | UART handle pointer. |
| data | Start address of the data to write. |
| length | Size of the data to write. |
| kStatus_HAL_UartSuccess | Successfully start the data transmission. |
| kStatus_HAL_UartTxBusy | Previous transmission still not finished; data not all written to TX register yet. |
| kStatus_HAL_UartError | An error occurred. |
| hal_uart_status_t HAL_UartGetReceiveCount | ( | hal_uart_handle_t | handle, |
| uint32_t * | reCount | ||
| ) |
This function gets the number of bytes that have been received.
| handle | UART handle pointer. |
| reCount | Receive bytes count. |
| kStatus_HAL_UartError | An error occurred. |
| kStatus_Success | Get successfully through the parameter count. |
| hal_uart_status_t HAL_UartGetSendCount | ( | hal_uart_handle_t | handle, |
| uint32_t * | seCount | ||
| ) |
This function gets the number of bytes written to the UART TX register by using the interrupt method.
| handle | UART handle pointer. |
| seCount | Send bytes count. |
| kStatus_HAL_UartError | An error occurred. |
| kStatus_Success | Get successfully through the parameter count. |
| hal_uart_status_t HAL_UartAbortReceive | ( | hal_uart_handle_t | handle | ) |
This function aborts the interrupt-driven data receiving. The user can get the remainBytes to know how many bytes are not received yet.
| handle | UART handle pointer. |
| kStatus_Success | Get successfully abort the receiving. |
| hal_uart_status_t HAL_UartAbortSend | ( | hal_uart_handle_t | handle | ) |
This function aborts the interrupt-driven data sending. The user can get the remainBytes to find out how many bytes are not sent out.
| handle | UART handle pointer. |
| kStatus_Success | Get successfully abort the sending. |
| hal_uart_status_t HAL_UartEnterLowpower | ( | hal_uart_handle_t | handle | ) |
This function is used to prepare to enter low power consumption.
| handle | UART handle pointer. |
| kStatus_HAL_UartSuccess | Successful operation. |
| kStatus_HAL_UartError | An error occurred. |
| hal_uart_status_t HAL_UartExitLowpower | ( | hal_uart_handle_t | handle | ) |
This function is used to restore from low power consumption.
| handle | UART handle pointer. |
| kStatus_HAL_UartSuccess | Successful operation. |
| kStatus_HAL_UartError | An error occurred. |
| void HAL_UartIsrFunction | ( | hal_uart_handle_t | handle | ) |
This function handles the UART transmit and receive IRQ request.
| handle | UART handle pointer. |