![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the Enhanced Quadrature Encoder/Decoder () module of MCUXpresso SDK devices.
This section describes the programming interface of the EQDC Peripheral driver. The EQDC driver configures the EQDC module and provides a functional interface for the user to build the EQDC application.
This function group initializes default configuration structure for the EQDC counter and initializes EQDC counter with the normal configuration and de-initialize EQDC module. Some APIs are also created to control the features.
This function group get/clear the EQDC status.
This function group enable/disable the EQDC interrupts.
This function group get the counter/hold value of positions.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/eqdc
Data Structures | |
| struct | eqdc_config_t |
| Define user configuration structure for EQDC module. More... | |
Macros | |
| #define | EQDC_CTRL_W1C_FLAGS (EQDC_CTRL_HIRQ_MASK | EQDC_CTRL_XIRQ_MASK | EQDC_CTRL_WDIRQ_MASK) |
| W1C bits in EQDC CTRL registers. More... | |
| #define | EQDC_INTCTRL_W1C_FLAGS |
| W1C bits in EQDC INTCTRL registers. More... | |
| #define | EQDC_CTRL_INT_EN (EQDC_CTRL_HIE_MASK | EQDC_CTRL_XIE_MASK | EQDC_CTRL_WDIE_MASK) |
| Interrupt enable bits in EQDC CTRL registers. More... | |
| #define | EQDC_INTCTRL_INT_EN |
| Interrupt enable bits in EQDC INTCTRL registers. More... | |
| #define | EQDC_CTRL_INT_FLAGS (EQDC_CTRL_HIRQ_MASK | EQDC_CTRL_XIRQ_MASK | EQDC_CTRL_WDIRQ_MASK) |
| Interrupt flag bits in EQDC CTRL registers. More... | |
| #define | EQDC_INTCTRL_INT_FLAGS |
| Interrupt flag bits in EQDC INTCTRL registers. More... | |
Initialization and deinitialization Interfaces | |
| void | EQDC_Init (EQDC_Type *base, const eqdc_config_t *psConfig) |
| Initializes the EQDC module. More... | |
| void | EQDC_GetDefaultConfig (eqdc_config_t *psConfig) |
| Gets an available pre-defined configuration. More... | |
| void | EQDC_Deinit (EQDC_Type *base) |
| De-initializes the EQDC module. More... | |
| void | EQDC_SetOperateMode (EQDC_Type *base, eqdc_operate_mode_t operateMode) |
| Initializes the mode of operation. More... | |
| static void | EQDC_SetCountMode (EQDC_Type *base, eqdc_count_mode_t countMode) |
| Initializes the mode of count. More... | |
Watchdog | |
| static void | EQDC_EnableWatchdog (EQDC_Type *base, bool bEnable) |
| Enable watchdog for EQDC module. More... | |
| static void | EQDC_SetWatchdogTimeout (EQDC_Type *base, uint16_t u16Timeout) |
| Set watchdog timeout value. More... | |
DMA | |
| static void | EQDC_EnableDMA (EQDC_Type *base, bool bEnable) |
| Enable DMA for EQDC module. More... | |
Double-set Registers Loading Operation | |
| static void | EQDC_SetBufferedRegisterLoadUpdateMode (EQDC_Type *base) |
| Set Buffered Register Load (Update) Mode. More... | |
| static void | EQDC_ClearBufferedRegisterLoadUpdateMode (EQDC_Type *base) |
| Clear Buffered Register Load (Update) Mode. More... | |
| static void | EQDC_SetEqdcLdok (EQDC_Type *base) |
| Set load okay. More... | |
| static uint8_t | EQDC_GetEqdcLdok (EQDC_Type *base) |
| Get load okay. More... | |
| static void | EQDC_ClearEqdcLdok (EQDC_Type *base) |
| Clear load okay. More... | |
Status | |
| static uint32_t | EQDC_GetStatusFlags (EQDC_Type *base) |
| Get the status flags. More... | |
| static void | EQDC_ClearStatusFlags (EQDC_Type *base, uint32_t u32Flags) |
| Clear the status flags. More... | |
| static uint16_t | EQDC_GetSignalStatusFlags (EQDC_Type *base) |
| Get the signals' real-time status. More... | |
| static eqdc_count_direction_flag_t | EQDC_GetLastCountDirection (EQDC_Type *base) |
| Get the direction of the last count. More... | |
Interrupts | |
| static void | EQDC_EnableInterrupts (EQDC_Type *base, uint32_t u32Interrupts) |
| Enable the interrupts. More... | |
| static void | EQDC_DisableInterrupts (EQDC_Type *base, uint32_t u32Interrupts) |
| Disable the interrupts. More... | |
Counter Operation | |
| static void | EQDC_DoSoftwareLoadInitialPositionValue (EQDC_Type *base) |
| Load the initial position value to position counter. More... | |
| static void | EQDC_SetInitialPositionValue (EQDC_Type *base, uint32_t u32PositionInitValue) |
| Set initial position value for EQDC module. More... | |
| static void | EQDC_SetPositionCounterValue (EQDC_Type *base, uint32_t positionCounterValue) |
| Set position counter value. More... | |
| static void | EQDC_SetPositionModulusValue (EQDC_Type *base, uint32_t positionModulusValue) |
| Set position counter modulus value. More... | |
| static void | EQDC_SetPositionCompare0Value (EQDC_Type *base, uint32_t u32PositionComp0Value) |
| Set position counter compare 0 value. More... | |
| static void | EQDC_SetPositionCompare1Value (EQDC_Type *base, uint32_t u32PositionComp1Value) |
| Set position counter compare 1 value. More... | |
| static void | EQDC_SetPositionCompare2Value (EQDC_Type *base, uint32_t u32PositionComp2Value) |
| Set position counter compare 2 value. More... | |
| static void | EQDC_SetPositionCompare3Value (EQDC_Type *base, uint32_t u32PositionComp3Value) |
| Set position counter compare 3 value. More... | |
| static uint32_t | EQDC_GetPosition (EQDC_Type *base) |
| Get the current position counter's value. More... | |
| static uint32_t | EQDC_GetHoldPosition (EQDC_Type *base) |
| Get the hold position counter's value. More... | |
| static uint32_t | EQDC_GetHoldPosition1 (EQDC_Type *base) |
| Get the hold position counter1's value. More... | |
| static uint32_t | EQDC_GetHoldPosition2 (EQDC_Type *base) |
| Get the hold position counter2's value. More... | |
| static uint32_t | EQDC_GetHoldPosition3 (EQDC_Type *base) |
| Get the hold position counter3's value. More... | |
| static uint16_t | EQDC_GetPositionDifference (EQDC_Type *base) |
| Get the position difference counter's value. More... | |
| static uint16_t | EQDC_GetHoldPositionDifference (EQDC_Type *base) |
| Get the hold position difference counter's value. More... | |
| static uint16_t | EQDC_GetRevolution (EQDC_Type *base) |
| Get the revolution counter's value. More... | |
| static uint16_t | EQDC_GetHoldRevolution (EQDC_Type *base) |
| Get the hold revolution counter's value. More... | |
| static uint16_t | EQDC_GetLastEdgeTime (EQDC_Type *base) |
| Get the last edge time. More... | |
| static uint16_t | EQDC_GetHoldLastEdgeTime (EQDC_Type *base) |
| Get the hold last edge time. More... | |
| static uint16_t | EQDC_GetPositionDifferencePeriod (EQDC_Type *base) |
| Get the Position Difference Period counter value. More... | |
| static uint16_t | EQDC_GetBufferedPositionDifferencePeriod (EQDC_Type *base) |
| Get buffered Position Difference Period counter value. More... | |
| static uint16_t | EQDC_GetHoldPositionDifferencePeriod (EQDC_Type *base) |
| Get Hold Position Difference Period counter value. More... | |
| struct eqdc_config_t |
Data Fields | |
| bool | enableReverseDirection |
| Enable reverse direction counting. More... | |
| bool | countOnce |
| Selects modulo loop or one shot counting mode. More... | |
| bool | enableDma |
| Enable DMA for new written buffer values of COMPx/INIT/MOD(x range is 0-3) | |
| bool | bufferedRegisterLoadMode |
| selects the loading time point of the buffered compare registers UCOMPx/LCOMPx, x=0~3, initial register (UINIT/LINIT), and modulus register (UMOD/LMOD). More... | |
| bool | enableTriggerInitPositionCounter |
Initialize position counter with initial register(UINIT, LINIT) value on TRIGGER's rising edge. More... | |
| bool | enableIndexInitPositionCounter |
| Enables the feature that the position counter to be initialized by Index Event Edge Mark. More... | |
| bool | enableTriggerClearPositionRegisters |
| Clear position counter(POS), revolution counter(REV), position difference counter (POSD) on TRIGGER's rising edge. More... | |
| bool | enableTriggerHoldPositionRegisters |
| Load position counter(POS), revolution counter(REV), position difference counter (POSD) values to hold registers on TRIGGER's rising edge. More... | |
| bool | filterPhaseA |
| Filter operation on PHASEA input, when write 1, it means filter for PHASEA input is bypassed. More... | |
| bool | filterPhaseB |
| Filter operation on PHASEB input, when write 1, it means filter for PHASEB input is bypassed. More... | |
| bool | filterIndPre |
| Filter operation on INDEX/PRESET input, when write 1, it means filter for INDEX/PRESET input is bypassed. More... | |
| bool | filterHomEna |
| Filter operation on HOME/ENABLE input, when write 1, it means filter for HOME/ENABLE input is bypassed. More... | |
| bool | enableWatchdog |
| Enable the watchdog to detect if the target is moving or not. More... | |
| uint16_t | watchdogTimeoutValue |
| Watchdog timeout count value. More... | |
| eqdc_prescaler_t | prescaler |
| Prescaler. More... | |
| bool | filterClockSourceselection |
| Filter Clock Source selection. More... | |
| eqdc_filter_sample_count_t | filterSampleCount |
| Input Filter Sample Count. More... | |
| uint8_t | filterSamplePeriod |
| Input Filter Sample Period. More... | |
| eqdc_operate_mode_t | operateMode |
| Selects operation mode. More... | |
| eqdc_count_mode_t | countMode |
| Selects count mode. More... | |
| eqdc_home_enable_init_pos_counter_mode_t | homeEnableInitPosCounterMode |
Select how HOME/Enable signal used to initialize position counters. More... | |
| eqdc_index_preset_init_pos_counter_mode_t | indexPresetInitPosCounterMode |
Select how INDEX/Preset signal used to initialize position counters. More... | |
| eqdc_output_pulse_mode_t | outputPulseMode |
| The condition of POSMATCH pulses. More... | |
| uint32_t | positionCompareValue [4] |
| Position compare 0 ~ 3 value. More... | |
| eqdc_revolution_count_condition_t | revolutionCountCondition |
| Revolution Counter Modulus Enable. More... | |
| uint32_t | positionModulusValue |
| Position modulus value. More... | |
| uint32_t | positionInitialValue |
| Position initial value. More... | |
| uint32_t | positionCounterValue |
| Position counter value. More... | |
| bool | enablePeriodMeasurement |
| Enable period measurement. More... | |
| uint16_t | enabledInterruptsMask |
| Mask of interrupts to be enabled, should be OR'ed value of _eqdc_interrupt_enable. More... | |
| bool eqdc_config_t::enableReverseDirection |
| bool eqdc_config_t::countOnce |
| bool eqdc_config_t::bufferedRegisterLoadMode |
| bool eqdc_config_t::enableTriggerInitPositionCounter |
| bool eqdc_config_t::enableIndexInitPositionCounter |
This option works together with _eqdc_index_preset_init_pos_counter_mode and enableReverseDirection; If enabled, the behavior is like this:
When PHA leads PHB (Clockwise): If _eqdc_index_preset_init_pos_counter_mode is kEQDC_IndexInitPosCounterOnRisingEdge, then INDEX rising edge reset position counter. If _eqdc_index_preset_init_pos_counter_mode is kEQDC_IndexInitPosCounterOnFallingEdge, then INDEX falling edge reset position counter. If enableReverseDirection is false, then Reset position counter to initial value. If enableReverseDirection is true, then reset position counter to modulus value.
When PHA lags PHB (Counter Clockwise): If _eqdc_index_preset_init_pos_counter_mode is kEQDC_IndexInitPosCounterOnRisingEdge, then INDEX falling edge reset position counter. If _eqdc_index_preset_init_pos_counter_mode is kEQDC_IndexInitPosCounterOnFallingEdge, then INDEX rising edge reset position counter. If enableReverseDirection is false, then Reset position counter to modulus value. If enableReverseDirection is true, then reset position counter to initial value.
| bool eqdc_config_t::enableTriggerClearPositionRegisters |
| bool eqdc_config_t::enableTriggerHoldPositionRegisters |
| bool eqdc_config_t::filterPhaseA |
| bool eqdc_config_t::filterPhaseB |
| bool eqdc_config_t::filterIndPre |
| bool eqdc_config_t::filterHomEna |
| bool eqdc_config_t::enableWatchdog |
| uint16_t eqdc_config_t::watchdogTimeoutValue |
It stores the timeout count for the quadrature decoder module watchdog timer.
| eqdc_prescaler_t eqdc_config_t::prescaler |
| bool eqdc_config_t::filterClockSourceselection |
| eqdc_filter_sample_count_t eqdc_config_t::filterSampleCount |
This value should be chosen to reduce the probability of noisy samples causing an incorrect transition to be recognized. The value represent the number of consecutive samples that must agree prior to the input filter accepting an input transition.
| uint8_t eqdc_config_t::filterSamplePeriod |
This value should be set such that the sampling period is larger than the period of the expected noise. This value represents the sampling period (in IPBus clock cycles) of the decoder input signals. The available range is 0 - 255.
| eqdc_operate_mode_t eqdc_config_t::operateMode |
| eqdc_count_mode_t eqdc_config_t::countMode |
| eqdc_home_enable_init_pos_counter_mode_t eqdc_config_t::homeEnableInitPosCounterMode |
| eqdc_index_preset_init_pos_counter_mode_t eqdc_config_t::indexPresetInitPosCounterMode |
| eqdc_output_pulse_mode_t eqdc_config_t::outputPulseMode |
| uint32_t eqdc_config_t::positionCompareValue[4] |
The available value is a 32-bit number.
| eqdc_revolution_count_condition_t eqdc_config_t::revolutionCountCondition |
| uint32_t eqdc_config_t::positionModulusValue |
The available value is a 32-bit number.
| uint32_t eqdc_config_t::positionInitialValue |
The available value is a 32-bit number.
| uint32_t eqdc_config_t::positionCounterValue |
When Modulo mode enabled, the positionCounterValue should be in the range of positionInitialValue and positionModulusValue.
| bool eqdc_config_t::enablePeriodMeasurement |
When enabled, the position difference hold register (POSDH) is only updated when position difference register (POSD) is read.
| uint16_t eqdc_config_t::enabledInterruptsMask |
| #define EQDC_CTRL_W1C_FLAGS (EQDC_CTRL_HIRQ_MASK | EQDC_CTRL_XIRQ_MASK | EQDC_CTRL_WDIRQ_MASK) |
| #define EQDC_INTCTRL_W1C_FLAGS |
| #define EQDC_CTRL_INT_EN (EQDC_CTRL_HIE_MASK | EQDC_CTRL_XIE_MASK | EQDC_CTRL_WDIE_MASK) |
| #define EQDC_INTCTRL_INT_EN |
| #define EQDC_CTRL_INT_FLAGS (EQDC_CTRL_HIRQ_MASK | EQDC_CTRL_XIRQ_MASK | EQDC_CTRL_WDIRQ_MASK) |
| #define EQDC_INTCTRL_INT_FLAGS |
| enum _eqdc_status_flags |
| enum _eqdc_signal_status |
| enum eqdc_operate_mode_t |
The Quadrature Decoder operates in following 4 operation modes: 1.Quadrature Decode(QDC) Operation Mode (CTRL[PH1] = 0,CTRL2[OPMODE] = 0) In QDC operation mode, Module uses PHASEA, PHASEB, INDEX, HOME, TRIGGER and ICAP[3:1] to decode the PHASEA and PHASEB signals from Speed/Position sensor. 2.Quadrature Count(QCT) Operation Mode (CTRL[PH1] = 0,CTRL2[OPMODE] = 1) In QCT operation mode, Module uses PHASEA, PHASEB, PRESET, ENABLE, TRIGGER and ICAP[3:1] to count the PHASEA and PHASEB signals from Speed/Position sensor. 3.Single Phase Decode(PH1DC) Operation Mode (CTRL[PH1] = 1,CTRL2[OPMODE] = 0) In PH1DC operation mode, the module uses PHASEA, PHASEB, INDEX, HOME, TRIGGER and ICAP[3:1] to decode the PHASEA and PHASEB signals from Speed/Position sensor. 4.Single Phase Count(PH1CT) Operation Mode (CTRL[PH1] = 1,CTRL2[OPMODE] = 1) In PH1CT operation mode, the module uses PHASEA, PHASEB, PRESET, ENABLE, TRIGGER and ICAP[3:1] to count the PHASEA and PHASEB signals from Speed/Position sensor.
| enum eqdc_count_mode_t |
In decode mode, it uses the standard quadrature decoder with PHASEA and PHASEB, PHASEA = 0 and PHASEB = 0 mean reverse direction.
The Input Filter Sample Count represents the number of consecutive samples that must agree, before the input filter accepts an input transition
| enum eqdc_prescaler_t |
| void EQDC_Init | ( | EQDC_Type * | base, |
| const eqdc_config_t * | psConfig | ||
| ) |
This function initializes the EQDC by enabling the IP bus clock (optional).
| base | EQDC peripheral base address. |
| psConfig | Pointer to configuration structure. |
| void EQDC_GetDefaultConfig | ( | eqdc_config_t * | psConfig | ) |
The default value are:
| psConfig | Pointer to configuration structure. |
| void EQDC_Deinit | ( | EQDC_Type * | base | ) |
This function deinitializes the EQDC by disabling the IP bus clock (optional).
| base | EQDC peripheral base address. |
| void EQDC_SetOperateMode | ( | EQDC_Type * | base, |
| eqdc_operate_mode_t | operateMode | ||
| ) |
This function initializes mode of operation by enabling the IP bus clock (optional).
| base | EQDC peripheral base address. |
| operateMode | Select operation mode. |
|
inlinestatic |
These bits control the basic counting and behavior of Position Counter and Position Difference Counter. Setting CTRL[REV] to 1 can reverse the counting direction. 1.In quadrature Mode (CTRL[PH1] = 0): 00b - CM0: Normal/Reverse Quadrature X4 01b - CM1: Normal/Reverse Quadrature X2 10b - CM2: Normal/Reverse Quadrature X1 11b - CM3: Reserved 2.In Single Phase Mode (CTRL[PH1] = 1): 00b - CM0: UP/DOWN Pulse Count Mode 01b - CM1: Signed Mode, count PHASEA rising/falling edge, position counter counts up when PHASEB is low and counts down when PHASEB is high 10b - CM2: Signed Count Mode,count PHASEA rising edge only, position counter counts up when PHASEB is low and counts down when PHASEB is high 11b - CM3: Reserved
| base | EQDC peripheral base address. |
| countMode | Select count mode. |
|
inlinestatic |
| base | EQDC peripheral base address |
| bEnable | Enables or disables the watchdog |
|
inlinestatic |
| base | EQDC peripheral base address |
| u16Timeout | Number of clock cycles, plus one clock cycle that the watchdog timer counts before timing out |
|
inlinestatic |
| base | EQDC peripheral base address |
| bEnable | Enables or disables the DMA |
|
inlinestatic |
This bit selects the loading time point of the buffered compare registers UCOMPx/LCOMPx, x=0~3, initial register (UINIT/LINIT), and modulus register (UMOD/LMOD). Buffered registers are loaded and take effect at the next roll-over or roll-under if CTRL[LDOK] is set.
| base | EQDC peripheral base address |
|
inlinestatic |
Buffered Register Load (Update) Mode bit selects the loading time point of the buffered compare registers UCOMPx/LCOMPx, x=0~3, initial register (UINIT/LINIT), and modulus register (UMOD/LMOD). Buffered registers are loaded and take effect immediately upon CTRL[LDOK] is set.
| base | EQDC peripheral base address |
|
inlinestatic |
Load okay enables that the outer-set values of buffered compare registers (UCOMPx/LCOMPx, x=0~3), initial register(UINIT/LINIT) and modulus register(UMOD/LMOD) can be loaded into their inner-sets and take effect. When LDOK is set, this loading action occurs at the next position counter roll-over or roll-under if CTRL2[LDMOD] is set, or it occurs immediately if CTRL2[LDMOD] is cleared. LDOK is automatically cleared after the values in outer-set is loaded into the inner-set.
| base | EQDC peripheral base address. |
|
inlinestatic |
| base | EQDC peripheral base address. |
|
inlinestatic |
| base | EQDC peripheral base address. |
|
inlinestatic |
| base | EQDC peripheral base address. |
|
inlinestatic |
| base | EQDC peripheral base address. |
| u32Flags | Logical OR'ed value of the flags to clear, _eqdc_status_flags. |
|
inlinestatic |
| base | EQDC peripheral base address. |
|
inlinestatic |
| base | EQDC peripheral base address. |
|
inlinestatic |
| base | EQDC peripheral base address. |
| u32Interrupts | Logical OR'ed value of the interrupts, _eqdc_interrupt_enable. |
|
inlinestatic |
| base | EQDC peripheral base address. |
| u32Interrupts | Logical OR'ed value of the interrupts, _eqdc_interrupt_enable. |
|
inlinestatic |
Software trigger to load the initial position value (UINIT and LINIT) contents to position counter (UPOS and LPOS), so that to provide the consistent operation the position counter registers.
| base | EQDC peripheral base address. |
|
inlinestatic |
Set the position counter initial value (UINIT, LINIT). After writing values to the UINIT and LINIT registers, the values are "buffered" into outer-set registers temporarily. Values will be loaded into inner-set registers and take effect using the following two methods:
| base | EQDC peripheral base address |
| u32PositionInitValue | Position initial value |
|
inlinestatic |
Set the position counter value (POS or UPOS, LPOS).
| base | EQDC peripheral base address |
| positionCounterValue | Position counter value |
|
inlinestatic |
Set the position counter modulus value (UMOD, LMOD). After writing values to the UMOD and LMOD registers, the values are "buffered" into outer-set registers temporarily. Values will be loaded into inner-set registers and take effect using the following two methods:
| base | EQDC peripheral base address |
| positionModulusValue | Position modulus value |
|
inlinestatic |
Set the position counter compare 0 value (UCOMP0, LCOMP0). After writing values to the UCOMP0 and LCOMP0 registers, the values are "buffered" into outer-set registers temporarily. Values will be loaded into inner-set registers and take effect using the following two methods:
| base | EQDC peripheral base address |
| u32PositionComp0Value | Position modulus value |
|
inlinestatic |
Set the position counter compare 1 value (UCOMP1, LCOMP1). After writing values to the UCOMP1 and LCOMP1 registers, the values are "buffered" into outer-set registers temporarily. Values will be loaded into inner-set registers and take effect using the following two methods:
| base | EQDC peripheral base address |
| u32PositionComp1Value | Position modulus value |
|
inlinestatic |
Set the position counter compare 2 value (UCOMP2, LCOMP2). After writing values to the UCOMP2 and LCOMP2 registers, the values are "buffered" into outer-set registers temporarily. Values will be loaded into inner-set registers and take effect using the following two methods:
| base | EQDC peripheral base address |
| u32PositionComp2Value | Position modulus value |
|
inlinestatic |
Set the position counter compare 3 value (UCOMP3, LCOMP3). After writing values to the UCOMP3 and LCOMP3 registers, the values are "buffered" into outer-set registers temporarily. Values will be loaded into inner-set registers and take effect using the following two methods:
| base | EQDC peripheral base address |
| u32PositionComp3Value | Position modulus value |
|
inlinestatic |
| base | EQDC peripheral base address. |
|
inlinestatic |
The position counter (POS or UPOS, LPOS) value is loaded to hold position (POSH or UPOSH, LPOSH) when:
| base | EQDC peripheral base address. |
|
inlinestatic |
The Upper Position Counter Hold Register 1(UPOSH1) shares the same address with UCOMP1. When read, this register means the value of UPOSH1, which is the upper 16 bits of POSH1. The Lower Position Counter Hold Register 1(LPOSH1) shares the same address with LCOMP1. When read, this register means the value of LPOSH1, which is the lower 16 bits of POSH1. Position counter is captured into POSH1 on the rising edge of ICAP[1].
| base | EQDC peripheral base address. |
|
inlinestatic |
The Upper Position Counter Hold Register 2(UPOSH2) shares the same address with UCOMP2. When read,this register means the value of UPOSH2, which is the upper 16 bits of POSH2. The Lower Position Counter Hold Register 2(LPOSH2) shares the same address with LCOMP2. When read, this register means the value of LPOSH2, which is the lower 16 bits of POSH2. Position counter is captured into POSH2 on the rising edge of ICAP[2].
| base | EQDC peripheral base address. |
|
inlinestatic |
The Upper Position Counter Hold Register 3(UPOSH3) shares the same address with UCOMP3. When read,this register means the value of UPOSH3, which is the upper 16 bits of POSH3. The Lower Position Counter Hold Register 3(LPOSH3) shares the same address with LCOMP3. When read, this register means the value of LPOSH3, which is the lower 16 bits of POSH3. Position counter is captured into POSH3 on the rising edge of ICAP[3].
| base | EQDC peripheral base address. |
|
inlinestatic |
| base | EQDC peripheral base address. |
|
inlinestatic |
The position difference (POSD) value is loaded to hold position difference (POSDH) when:
| base | EQDC peripheral base address. |
|
inlinestatic |
Get the revolution counter (REV) value.
| base | EQDC peripheral base address. |
|
inlinestatic |
The revolution counter (REV) value is loaded to hold revolution (REVH) when:
| base | EQDC peripheral base address. |
|
inlinestatic |
Last edge time (LASTEDGE) is the time since the last edge occurred on PHASEA or PHASEB. The last edge time register counts up using the peripheral clock after prescaler. Any edge on PHASEA or PHASEB will reset this register to 0 and start counting. If the last edge timer count reaches 0xffff, the counting will stop in order to prevent an overflow.Counting will continue when an edge occurs on PHASEA or PHASEB.
| base | EQDC peripheral base address. |
|
inlinestatic |
The hold of last edge time(LASTEDGEH) is update to last edge time(LASTEDGE) when the position difference register register (POSD) is read.
| base | EQDC peripheral base address. |
|
inlinestatic |
The Position Difference Period counter (POSDPER) counts up using the prescaled peripheral clock. When reading the position difference register(POSD), the last edge time (LASTEDGE) will be loaded to position difference period counter(POSDPER). If the POSDPER count reaches 0xffff, the counting will stop in order to prevent an overflow. Counting will continue when an edge occurs on PHASEA or PHASEB.
| base | EQDC peripheral base address. |
|
inlinestatic |
The Bufferd Position Difference Period (POSDPERBFR) value is updated with the position difference period counter(POSDPER) when any edge occurs on PHASEA or PHASEB.
| base | EQDC peripheral base address. |
|
inlinestatic |
The hold position difference period(POSDPERH) is updated with the value of buffered position difference period(POSDPERBFR) when the position difference(POSD) register is read.
| base | EQDC peripheral base address. |