![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
Files | |
file | fsl_dmic.h |
Data Structures | |
struct | dmic_channel_config_t |
DMIC Channel configuration structure. More... | |
Typedefs | |
typedef void(* | dmic_callback_t )(void) |
DMIC Callback function. More... | |
typedef void(* | dmic_hwvad_callback_t )(void) |
HWVAD Callback function. More... | |
DMIC version | |
#define | FSL_DMIC_DRIVER_VERSION (MAKE_VERSION(2, 3, 2)) |
DMIC driver version 2.3.2. More... | |
Initialization and deinitialization | |
uint32_t | DMIC_GetInstance (DMIC_Type *base) |
Get the DMIC instance from peripheral base address. More... | |
void | DMIC_Init (DMIC_Type *base) |
Turns DMIC Clock on. More... | |
void | DMIC_DeInit (DMIC_Type *base) |
Turns DMIC Clock off. More... | |
void | DMIC_SetOperationMode (DMIC_Type *base, operation_mode_t mode) |
Set DMIC operating mode. More... | |
void | DMIC_Use2fs (DMIC_Type *base, bool use2fs) |
Configure Clock scaling. More... | |
Channel configuration | |
void | DMIC_CfgChannelDc (DMIC_Type *base, dmic_channel_t channel, dc_removal_t dc_cut_level, uint32_t post_dc_gain_reduce, bool saturate16bit) |
Configure DMIC channel. More... | |
static void | DMIC_EnableChannelSignExtend (DMIC_Type *base, dmic_channel_t channel, bool enable) |
Enbale channel sign extend which allows processing of 24bit audio data on 32bit machines. More... | |
void | DMIC_ConfigChannel (DMIC_Type *base, dmic_channel_t channel, stereo_side_t side, dmic_channel_config_t *channel_config) |
Configure DMIC channel. More... | |
void | DMIC_EnableChannnel (DMIC_Type *base, uint32_t channelmask) |
Enable a particualr channel. More... | |
void | DMIC_FifoChannel (DMIC_Type *base, uint32_t channel, uint32_t trig_level, uint32_t enable, uint32_t resetn) |
Configure fifo settings for DMIC channel. More... | |
static void | DMIC_EnableChannelInterrupt (DMIC_Type *base, dmic_channel_t channel, bool enable) |
Enable a particualr channel interrupt request. More... | |
static void | DMIC_EnableChannelDma (DMIC_Type *base, dmic_channel_t channel, bool enable) |
Enable a particualr channel dma request. More... | |
static void | DMIC_EnableChannelFifo (DMIC_Type *base, dmic_channel_t channel, bool enable) |
Enable a particualr channel fifo. More... | |
static void | DMIC_DoFifoReset (DMIC_Type *base, dmic_channel_t channel) |
Channel fifo reset. More... | |
static uint32_t | DMIC_FifoGetStatus (DMIC_Type *base, uint32_t channel) |
Get FIFO status. More... | |
static void | DMIC_FifoClearStatus (DMIC_Type *base, uint32_t channel, uint32_t mask) |
Clear FIFO status. More... | |
static uint32_t | DMIC_FifoGetData (DMIC_Type *base, uint32_t channel) |
Get FIFO data. More... | |
static uint32_t | DMIC_FifoGetAddress (DMIC_Type *base, uint32_t channel) |
Get FIFO address. More... | |
void | DMIC_ResetChannelDecimator (DMIC_Type *base, uint32_t channelMask, bool reset) |
DMIC channel Decimator reset. More... | |
Register callback. | |
void | DMIC_EnableIntCallback (DMIC_Type *base, dmic_callback_t cb) |
Enable callback. More... | |
void | DMIC_DisableIntCallback (DMIC_Type *base, dmic_callback_t cb) |
Disable callback. More... | |
HWVAD | |
static void | DMIC_SetGainNoiseEstHwvad (DMIC_Type *base, uint32_t value) |
Sets the gain value for the noise estimator. More... | |
static void | DMIC_SetGainSignalEstHwvad (DMIC_Type *base, uint32_t value) |
Sets the gain value for the signal estimator. More... | |
static void | DMIC_SetFilterCtrlHwvad (DMIC_Type *base, uint32_t value) |
Sets the hwvad filter cutoff frequency parameter. More... | |
static void | DMIC_SetInputGainHwvad (DMIC_Type *base, uint32_t value) |
Sets the input gain of hwvad. More... | |
static void | DMIC_CtrlClrIntrHwvad (DMIC_Type *base, bool st10) |
Clears hwvad internal interrupt flag. More... | |
static void | DMIC_FilterResetHwvad (DMIC_Type *base, bool rstt) |
Resets hwvad filters. More... | |
static uint16_t | DMIC_GetNoiseEnvlpEst (DMIC_Type *base) |
Gets the value from output of the filter z7. More... | |
void | DMIC_HwvadEnableIntCallback (DMIC_Type *base, dmic_hwvad_callback_t vadcb) |
Enable hwvad callback. More... | |
void | DMIC_HwvadDisableIntCallback (DMIC_Type *base, dmic_hwvad_callback_t vadcb) |
Disable callback. More... | |
struct dmic_channel_config_t |
Data Fields | |
pdm_div_t | divhfclk |
DMIC Clock pre-divider values. | |
uint32_t | osr |
oversampling rate(CIC decimation rate) for PCM | |
int32_t | gainshft |
4FS PCM data gain control | |
compensation_t | preac2coef |
Pre-emphasis Filter coefficient value for 2FS. | |
compensation_t | preac4coef |
Pre-emphasis Filter coefficient value for 4FS. | |
dc_removal_t | dc_cut_level |
DMIC DC filter control values. More... | |
uint32_t | post_dc_gain_reduce |
Fine gain adjustment in the form of a number of bits to downshift. | |
dmic_phy_sample_rate_t | sample_rate |
DMIC and decimator sample rates. | |
bool | saturate16bit |
Selects 16-bit saturation. More... | |
bool | enableSignExtend |
sign extend feature which allows processing of 24bit audio data on 32bit machine | |
dc_removal_t dmic_channel_config_t::dc_cut_level |
bool dmic_channel_config_t::saturate16bit |
0 means results roll over if out range and do not saturate. 1 means if the result overflows, it saturates at 0xFFFF for positive overflow and 0x8000 for negative overflow.
#define FSL_DMIC_DRIVER_VERSION (MAKE_VERSION(2, 3, 2)) |
typedef void(* dmic_callback_t)(void) |
typedef void(* dmic_hwvad_callback_t)(void) |
anonymous enum |
enum operation_mode_t |
enum stereo_side_t |
enum pdm_div_t |
enum compensation_t |
enum dc_removal_t |
enum dmic_channel_t |
anonymous enum |
uint32_t DMIC_GetInstance | ( | DMIC_Type * | base | ) |
base | DMIC peripheral base address. |
void DMIC_Init | ( | DMIC_Type * | base | ) |
base | : DMIC base |
void DMIC_DeInit | ( | DMIC_Type * | base | ) |
base | : DMIC base |
void DMIC_SetOperationMode | ( | DMIC_Type * | base, |
operation_mode_t | mode | ||
) |
base | : The base address of DMIC interface |
mode | : DMIC mode |
void DMIC_Use2fs | ( | DMIC_Type * | base, |
bool | use2fs | ||
) |
base | : The base address of DMIC interface |
use2fs | : clock scaling |
void DMIC_CfgChannelDc | ( | DMIC_Type * | base, |
dmic_channel_t | channel, | ||
dc_removal_t | dc_cut_level, | ||
uint32_t | post_dc_gain_reduce, | ||
bool | saturate16bit | ||
) |
base | : The base address of DMIC interface |
channel | : DMIC channel |
dc_cut_level | : dc_removal_t, Cut off Frequency |
post_dc_gain_reduce | : Fine gain adjustment in the form of a number of bits to downshift. |
saturate16bit | : If selects 16-bit saturation. |
|
inlinestatic |
base | : The base address of DMIC interface |
channel | : DMIC channel |
enable | : true is enable sign extend, false is disable sign extend |
void DMIC_ConfigChannel | ( | DMIC_Type * | base, |
dmic_channel_t | channel, | ||
stereo_side_t | side, | ||
dmic_channel_config_t * | channel_config | ||
) |
base | : The base address of DMIC interface |
channel | : DMIC channel |
side | : stereo_side_t, choice of left or right |
channel_config | : Channel configuration |
void DMIC_EnableChannnel | ( | DMIC_Type * | base, |
uint32_t | channelmask | ||
) |
base | : The base address of DMIC interface |
channelmask | reference _dmic_channel_mask |
void DMIC_FifoChannel | ( | DMIC_Type * | base, |
uint32_t | channel, | ||
uint32_t | trig_level, | ||
uint32_t | enable, | ||
uint32_t | resetn | ||
) |
base | : The base address of DMIC interface |
channel | : DMIC channel |
trig_level | : FIFO trigger level |
enable | : FIFO level |
resetn | : FIFO reset |
|
inlinestatic |
base | : The base address of DMIC interface |
channel | : Channel selection |
enable | : true is enable, false is disable |
|
inlinestatic |
base | : The base address of DMIC interface |
channel | : Channel selection |
enable | : true is enable, false is disable |
|
inlinestatic |
base | : The base address of DMIC interface |
channel | : Channel selection |
enable | : true is enable, false is disable |
|
inlinestatic |
base | : The base address of DMIC interface |
channel | : Channel selection |
|
inlinestatic |
base | : The base address of DMIC interface |
channel | : DMIC channel |
|
inlinestatic |
base | : The base address of DMIC interface |
channel | : DMIC channel |
mask | : Bits to be cleared |
|
inlinestatic |
base | : The base address of DMIC interface |
channel | : DMIC channel |
|
inlinestatic |
base | : The base address of DMIC interface |
channel | : DMIC channel |
void DMIC_ResetChannelDecimator | ( | DMIC_Type * | base, |
uint32_t | channelMask, | ||
bool | reset | ||
) |
base | : The base address of DMIC interface |
channelMask | : DMIC channel mask, reference _dmic_channel_mask |
reset | : true is reset decimator, false is release decimator. |
void DMIC_EnableIntCallback | ( | DMIC_Type * | base, |
dmic_callback_t | cb | ||
) |
This function enables the interrupt for the selected DMIC peripheral. The callback function is not enabled until this function is called.
base | Base address of the DMIC peripheral. |
cb | callback Pointer to store callback function. |
None. |
void DMIC_DisableIntCallback | ( | DMIC_Type * | base, |
dmic_callback_t | cb | ||
) |
This function disables the interrupt for the selected DMIC peripheral.
base | Base address of the DMIC peripheral. |
cb | callback Pointer to store callback function.. |
None. |
|
inlinestatic |
base | DMIC base pointer |
value | gain value for the noise estimator. |
None. |
|
inlinestatic |
base | DMIC base pointer |
value | gain value for the signal estimator. |
None. |
|
inlinestatic |
base | DMIC base pointer |
value | cut off frequency value. |
None. |
|
inlinestatic |
base | DMIC base pointer |
value | input gain value for hwvad. |
None. |
|
inlinestatic |
base | DMIC base pointer |
st10 | bit value. |
None. |
|
inlinestatic |
base | DMIC base pointer |
rstt | Reset bit value. |
None. |
|
inlinestatic |
base | DMIC base pointer |
output | of filter z7. |
void DMIC_HwvadEnableIntCallback | ( | DMIC_Type * | base, |
dmic_hwvad_callback_t | vadcb | ||
) |
This function enables the hwvad interrupt for the selected DMIC peripheral. The callback function is not enabled until this function is called.
base | Base address of the DMIC peripheral. |
vadcb | callback Pointer to store callback function. |
None. |
void DMIC_HwvadDisableIntCallback | ( | DMIC_Type * | base, |
dmic_hwvad_callback_t | vadcb | ||
) |
This function disables the hwvad interrupt for the selected DMIC peripheral.
base | Base address of the DMIC peripheral. |
vadcb | callback Pointer to store callback function.. |
None. |