MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
TMU: Thermal Management Unit Driver

Overview

The MCUXpresso SDK provides a peripheral driver for the thermal management unit (TMU) module of MCUXpresso SDK devices.

Typical use case

Monitor and report Configuration

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/tmu

Data Structures

struct  tmu_thresold_config_t
 configuration for TMU thresold. More...
 
struct  tmu_interrupt_status_t
 TMU interrupt status. More...
 
struct  tmu_config_t
 Configuration for TMU module. More...
 

Macros

#define FSL_TMU_DRIVER_VERSION   (MAKE_VERSION(2, 0, 3))
 TMU driver version. More...
 

Enumerations

enum  _tmu_interrupt_enable {
  kTMU_ImmediateTemperatureInterruptEnable,
  kTMU_AverageTemperatureInterruptEnable,
  kTMU_AverageTemperatureCriticalInterruptEnable
}
 TMU interrupt enable. More...
 
enum  _tmu_interrupt_status_flags {
  kTMU_ImmediateTemperatureStatusFlags = TMU_TIDR_ITTE_MASK,
  kTMU_AverageTemperatureStatusFlags = TMU_TIDR_ATTE_MASK,
  kTMU_AverageTemperatureCriticalStatusFlags
}
 TMU interrupt status flags. More...
 
enum  _tmu_status_flags {
  kTMU_IntervalExceededStatusFlags = TMU_TSR_MIE_MASK,
  kTMU_OutOfLowRangeStatusFlags = TMU_TSR_ORL_MASK,
  kTMU_OutOfHighRangeStatusFlags
}
 TMU status flags. More...
 
enum  tmu_average_low_pass_filter_t {
  kTMU_AverageLowPassFilter1_0 = 0U,
  kTMU_AverageLowPassFilter0_5 = 1U,
  kTMU_AverageLowPassFilter0_25 = 2U,
  kTMU_AverageLowPassFilter0_125 = 3U
}
 Average low pass filter setting. More...
 

Functions

void TMU_Init (TMU_Type *base, const tmu_config_t *config)
 Enable the access to TMU registers and Initialize TMU module. More...
 
void TMU_Deinit (TMU_Type *base)
 De-initialize TMU module and Disable the access to DCDC registers. More...
 
void TMU_GetDefaultConfig (tmu_config_t *config)
 Gets the default configuration for TMU. More...
 
static void TMU_Enable (TMU_Type *base, bool enable)
 Enable/Disable the TMU module. More...
 
static void TMU_EnableInterrupts (TMU_Type *base, uint32_t mask)
 Enable the TMU interrupts. More...
 
static void TMU_DisableInterrupts (TMU_Type *base, uint32_t mask)
 Disable the TMU interrupts. More...
 
void TMU_GetInterruptStatusFlags (TMU_Type *base, tmu_interrupt_status_t *status)
 Get interrupt status flags. More...
 
void TMU_ClearInterruptStatusFlags (TMU_Type *base, uint32_t mask)
 Clear interrupt status flags and corresponding interrupt critical site capture register. More...
 
static uint32_t TMU_GetStatusFlags (TMU_Type *base)
 Get TMU status flags. More...
 
status_t TMU_GetHighestTemperature (TMU_Type *base, uint32_t *temperature)
 Get the highest temperature reached for any enabled monitored site within the temperature sensor range. More...
 
status_t TMU_GetLowestTemperature (TMU_Type *base, uint32_t *temperature)
 Get the lowest temperature reached for any enabled monitored site within the temperature sensor range. More...
 
status_t TMU_GetImmediateTemperature (TMU_Type *base, uint32_t siteIndex, uint32_t *temperature)
 Get the last immediate temperature at site n. More...
 
status_t TMU_GetAverageTemperature (TMU_Type *base, uint32_t siteIndex, uint32_t *temperature)
 Get the last average temperature at site n. More...
 
void TMU_SetHighTemperatureThresold (TMU_Type *base, const tmu_thresold_config_t *config)
 Configure the high temperature thresold value and enable/disable relevant thresold. More...
 

Data Structure Documentation

struct tmu_thresold_config_t

Data Fields

bool immediateThresoldEnable
 Enable high temperature immediate threshold. More...
 
bool AverageThresoldEnable
 Enable high temperature average threshold. More...
 
bool AverageCriticalThresoldEnable
 Enable high temperature average critical threshold. More...
 
uint8_t immediateThresoldValue
 Range:0U-125U. More...
 
uint8_t averageThresoldValue
 Range:0U-125U. More...
 
uint8_t averageCriticalThresoldValue
 Range:0U-125U. More...
 

Field Documentation

bool tmu_thresold_config_t::immediateThresoldEnable
bool tmu_thresold_config_t::AverageThresoldEnable
bool tmu_thresold_config_t::AverageCriticalThresoldEnable
uint8_t tmu_thresold_config_t::immediateThresoldValue

Valid when corresponding thresold is enabled. High temperature immediate threshold value. Determines the current upper temperature threshold, for anyenabled monitored site.

uint8_t tmu_thresold_config_t::averageThresoldValue

Valid when corresponding thresold is enabled. High temperature average threshold value. Determines the average upper temperature threshold, for any enabled monitored site.

uint8_t tmu_thresold_config_t::averageCriticalThresoldValue

Valid when corresponding thresold is enabled. High temperature average critical threshold value. Determines the average upper critical temperature threshold, for any enabled monitored site.

struct tmu_interrupt_status_t

Data Fields

uint32_t interruptDetectMask
 The mask of interrupt status flags. More...
 
uint16_t immediateInterruptsSiteMask
 The mask of the temperature sensor site associated with a detected ITTE event. More...
 
uint16_t AverageInterruptsSiteMask
 The mask of the temperature sensor site associated with a detected ATTE event. More...
 
uint16_t AverageCriticalInterruptsSiteMask
 The mask of the temperature sensor site associated with a detected ATCTE event. More...
 

Field Documentation

uint32_t tmu_interrupt_status_t::interruptDetectMask

Refer to "_tmu_interrupt_status_flags" enumeration.

uint16_t tmu_interrupt_status_t::immediateInterruptsSiteMask

Please refer to "_tmu_monitor_site" enumeration.

uint16_t tmu_interrupt_status_t::AverageInterruptsSiteMask

Please refer to "_tmu_monitor_site" enumeration.

uint16_t tmu_interrupt_status_t::AverageCriticalInterruptsSiteMask

Please refer to "_tmu_monitor_site" enumeration.

struct tmu_config_t

Data Fields

uint8_t monitorInterval
 Temperature monitoring interval in seconds. More...
 
uint16_t monitorSiteSelection
 By setting the select bit for a temperature sensor site, it is enabled and included in all monitoring functions. More...
 
tmu_average_low_pass_filter_t averageLPF
 The average temperature is calculated as: ALPF x Current_Temp + (1 - ALPF) x Average_Temp. More...
 

Field Documentation

uint8_t tmu_config_t::monitorInterval

Please refer to specific table in RM.

uint16_t tmu_config_t::monitorSiteSelection

If no site is selected, site 0 is monitored by default. Refer to "_tmu_monitor_site" enumeration. Please look up relevant table in reference manual.

tmu_average_low_pass_filter_t tmu_config_t::averageLPF

For proper operation, this field should only change when monitoring is disabled.

Macro Definition Documentation

#define FSL_TMU_DRIVER_VERSION   (MAKE_VERSION(2, 0, 3))

Version 2.0.3.

Enumeration Type Documentation

Enumerator
kTMU_ImmediateTemperatureInterruptEnable 

Immediate temperature threshold exceeded interrupt enable.

kTMU_AverageTemperatureInterruptEnable 

Average temperature threshold exceeded interrupt enable.

kTMU_AverageTemperatureCriticalInterruptEnable 

Average temperature critical threshold exceeded interrupt enable.

>

Enumerator
kTMU_ImmediateTemperatureStatusFlags 

Immediate temperature threshold exceeded(ITTE).

kTMU_AverageTemperatureStatusFlags 

Average temperature threshold exceeded(ATTE).

kTMU_AverageTemperatureCriticalStatusFlags 

Average temperature critical threshold exceeded.

(ATCTE)

Enumerator
kTMU_IntervalExceededStatusFlags 

Monitoring interval exceeded.

The time required to perform measurement of all monitored sites has exceeded the monitoring interval as defined by TMTMIR.

kTMU_OutOfLowRangeStatusFlags 

Out-of-range low temperature measurement detected.

A temperature sensor detected a temperature reading below the lowest measurable temperature of 0 °C.

kTMU_OutOfHighRangeStatusFlags 

Out-of-range high temperature measurement detected.

A temperature sensor detected a temperature reading above the highest measurable temperature of 125 °C.

Enumerator
kTMU_AverageLowPassFilter1_0 

Average low pass filter = 1.

kTMU_AverageLowPassFilter0_5 

Average low pass filter = 0.5.

kTMU_AverageLowPassFilter0_25 

Average low pass filter = 0.25.

kTMU_AverageLowPassFilter0_125 

Average low pass filter = 0.125.

Function Documentation

void TMU_Init ( TMU_Type *  base,
const tmu_config_t *  config 
)
Parameters
baseTMU peripheral base address.
configPointer to configuration structure. Refer to "tmu_config_t" structure.
void TMU_Deinit ( TMU_Type *  base)
Parameters
baseTMU peripheral base address.
void TMU_GetDefaultConfig ( tmu_config_t *  config)

This function initializes the user configuration structure to default value. The default value are:

Example:

config->monitorInterval = 0U;
config->monitorSiteSelection = 0U;
config->averageLPF = kTMU_AverageLowPassFilter1_0;
Parameters
configPointer to TMU configuration structure.
static void TMU_Enable ( TMU_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseTMU peripheral base address.
enableSwitcher to enable/disable TMU.
static void TMU_EnableInterrupts ( TMU_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseTMU peripheral base address.
maskThe interrupt mask. Refer to "_tmu_interrupt_enable" enumeration.
static void TMU_DisableInterrupts ( TMU_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseTMU peripheral base address.
maskThe interrupt mask. Refer to "_tmu_interrupt_enable" enumeration.
void TMU_GetInterruptStatusFlags ( TMU_Type *  base,
tmu_interrupt_status_t *  status 
)
Parameters
baseTMU peripheral base address.
statusThe pointer to interrupt status structure. Record the current interrupt status. Please refer to "tmu_interrupt_status_t" structure.
void TMU_ClearInterruptStatusFlags ( TMU_Type *  base,
uint32_t  mask 
)
Parameters
baseTMU peripheral base address.
maskThe mask of interrupt status flags. Refer to "_tmu_interrupt_status_flags" enumeration.
static uint32_t TMU_GetStatusFlags ( TMU_Type *  base)
inlinestatic
Parameters
baseTMU peripheral base address.
Returns
The mask of status flags. Refer to "_tmu_status_flags" enumeration.
status_t TMU_GetHighestTemperature ( TMU_Type *  base,
uint32_t *  temperature 
)
Parameters
baseTMU peripheral base address.
temperatureHighest temperature recorded in degrees Celsius by any enabled monitored site.
Returns
Execution status.
Return values
kStatus_SuccessTemperature reading is valid.
kStatus_FailTemperature reading is not valid due to no measured temperature within the sensor range of 0-125 °C for an enabled monitored site.
status_t TMU_GetLowestTemperature ( TMU_Type *  base,
uint32_t *  temperature 
)
Parameters
baseTMU peripheral base address.
temperatureLowest temperature recorded in degrees Celsius by any enabled monitored site.
Returns
Execution status.
Return values
kStatus_SuccessTemperature reading is valid.
kStatus_FailTemperature reading is not valid due to no measured temperature within the sensor range of 0-125 °C for an enabled monitored site.
status_t TMU_GetImmediateTemperature ( TMU_Type *  base,
uint32_t  siteIndex,
uint32_t *  temperature 
)

The site must be part of the list of enabled monitored sites as defined by monitorSiteSelection in "tmu_config_t" structure.

Parameters
baseTMU peripheral base address.
siteIndexThe index of the site user want to read. 0U: site0 ~ 15U: site15.
temperatureLast immediate temperature reading at site n .
Returns
Execution status.
Return values
kStatus_SuccessTemperature reading is valid.
kStatus_FailTemperature reading is not valid because temperature out of sensor range or first measurement still pending.
status_t TMU_GetAverageTemperature ( TMU_Type *  base,
uint32_t  siteIndex,
uint32_t *  temperature 
)

The site must be part of the list of enabled monitored sites as defined by monitorSiteSelection in "tmu_config_t" structure.

Parameters
baseTMU peripheral base address.
siteIndexThe index of the site user want to read. 0U: site0 ~ 15U: site15.
temperatureLast average temperature reading at site n .
Returns
Execution status.
Return values
kStatus_SuccessTemperature reading is valid.
kStatus_FailTemperature reading is not valid because temperature out of sensor range or first measurement still pending.
void TMU_SetHighTemperatureThresold ( TMU_Type *  base,
const tmu_thresold_config_t *  config 
)
Parameters
baseTMU peripheral base address.
configPointer to configuration structure. Refer to "tmu_thresold_config_t" structure.