![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
The MCUXpresso SDK provides a driver for the MECC module of MCUXpresso SDK devices.
The MECC64 module supports Single Error Correction and Double Error Detection(SECDED) ECC function to provide reliability for 4 banks On-Chip RAM(OCRAM) access.
This example code shows how to correct single error and detect multiple error using the MECC driver.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/mecc
Data Structures | |
| struct | _mecc_config |
| MECC user configuration. More... | |
| struct | _mecc_single_error_info |
| MECC ocram single error information, including single error address, ECC code, error data and error bit position. More... | |
| struct | _mecc_multi_error_info |
| MECC ocram multiple error information, including multiple error address, ECC code, error data. More... | |
Typedefs | |
| typedef struct _mecc_config | mecc_config_t |
| MECC user configuration. More... | |
|
typedef struct _mecc_single_error_info | mecc_single_error_info_t |
| MECC ocram single error information, including single error address, ECC code, error data and error bit position. | |
|
typedef struct _mecc_multi_error_info | mecc_multi_error_info_t |
| MECC ocram multiple error information, including multiple error address, ECC code, error data. | |
Enumerations | |
| enum | { kStatus_MECC_BankMiss = MAKE_STATUS(kStatusGroup_MECC, 0) } |
| Error codes for the MECC driver. More... | |
| enum | { kMECC_SingleError0InterruptEnable = MECC_ERR_SIG_EN_SINGLE_ERR0_SIG_EN_MASK, kMECC_SingleError1InterruptEnable = MECC_ERR_SIG_EN_SINGLE_ERR1_SIG_EN_MASK, kMECC_SingleError2InterruptEnable = MECC_ERR_SIG_EN_SINGLE_ERR2_SIG_EN_MASK, kMECC_SingleError3InterruptEnable = MECC_ERR_SIG_EN_SINGLE_ERR3_SIG_EN_MASK, kMECC_MultiError0InterruptEnable = MECC_ERR_SIG_EN_MULTI_ERR0_SIG_EN_MASK, kMECC_MultiError1InterruptEnable = MECC_ERR_SIG_EN_MULTI_ERR1_SIG_EN_MASK, kMECC_MultiError2InterruptEnable = MECC_ERR_SIG_EN_MULTI_ERR2_SIG_EN_MASK, kMECC_MultiError3InterruptEnable = MECC_ERR_SIG_EN_MULTI_ERR3_SIG_EN_MASK, kMECC_StrobeError0InterruptEnable = MECC_ERR_SIG_EN_STRB_ERR0_SIG_EN_MASK, kMECC_StrobeError1InterruptEnable = MECC_ERR_SIG_EN_STRB_ERR1_SIG_EN_MASK, kMECC_StrobeError2InterruptEnable = MECC_ERR_SIG_EN_STRB_ERR2_SIG_EN_MASK, kMECC_StrobeError3InterruptEnable = MECC_ERR_SIG_EN_STRB_ERR3_SIG_EN_MASK, kMECC_AccessError0InterruptEnable = MECC_ERR_SIG_EN_ADDR_ERR0_SIG_EN_MASK, kMECC_AccessError1InterruptEnable = MECC_ERR_SIG_EN_ADDR_ERR1_SIG_EN_MASK, kMECC_AccessError2InterruptEnable = MECC_ERR_SIG_EN_ADDR_ERR2_SIG_EN_MASK, kMECC_AccessError3InterruptEnable = MECC_ERR_SIG_EN_ADDR_ERR3_SIG_EN_MASK, kMECC_AllInterruptsEnable = 0xFFFF } |
| MECC interrupt configuration structure, default settings all disabled. More... | |
| enum | { kMECC_SingleError0InterruptStatusEnable = MECC_ERR_STAT_EN_SINGLE_ERR0_STAT_EN_MASK, kMECC_SingleError1InterruptStatusEnable = MECC_ERR_STAT_EN_SINGLE_ERR1_STAT_EN_MASK, kMECC_SingleError2InterruptStatusEnable = MECC_ERR_STAT_EN_SINGLE_ERR2_STAT_EN_MASK, kMECC_SingleError3InterruptStatusEnable = MECC_ERR_STAT_EN_SINGLE_ERR3_STAT_EN_MASK, kMECC_MultiError0InterruptStatusEnable = MECC_ERR_STAT_EN_MULTI_ERR0_STAT_EN_MASK, kMECC_MultiError1InterruptStatusEnable = MECC_ERR_STAT_EN_MULTI_ERR1_STAT_EN_MASK, kMECC_MultiError2InterruptStatusEnable = MECC_ERR_STAT_EN_MULTI_ERR2_STAT_EN_MASK, kMECC_MultiError3InterruptStatusEnable = MECC_ERR_STAT_EN_MULTI_ERR3_STAT_EN_MASK, kMECC_StrobeError0InterruptStatusEnable = MECC_ERR_STAT_EN_STRB_ERR0_STAT_EN_MASK, kMECC_StrobeError1InterruptStatusEnable = MECC_ERR_STAT_EN_STRB_ERR1_STAT_EN_MASK, kMECC_StrobeError2InterruptStatusEnable = MECC_ERR_STAT_EN_STRB_ERR2_STAT_EN_MASK, kMECC_StrobeError3InterruptStatusEnable = MECC_ERR_STAT_EN_STRB_ERR3_STAT_EN_MASK, kMECC_AccessError0InterruptStatusEnable = MECC_ERR_STAT_EN_ADDR_ERR0_STAT_EN_MASK, kMECC_AccessError1InterruptStatusEnable = MECC_ERR_STAT_EN_ADDR_ERR1_STAT_EN_MASK, kMECC_AccessError2InterruptStatusEnable = MECC_ERR_STAT_EN_ADDR_ERR2_STAT_EN_MASK, kMECC_AccessError3InterruptStatusEnable = MECC_ERR_STAT_EN_ADDR_ERR3_STAT_EN_MASK, kMECC_AllInterruptsStatusEnable = 0xFFFF } |
| MECC interrupt status configuration structure, default settings all disabled. More... | |
| enum | { kMECC_SingleError0InterruptFlag = MECC_ERR_STATUS_SINGLE_ERR0_MASK, kMECC_SingleError1InterruptFlag = MECC_ERR_STATUS_SINGLE_ERR1_MASK, kMECC_SingleError2InterruptFlag = MECC_ERR_STATUS_SINGLE_ERR2_MASK, kMECC_SingleError3InterruptFlag = MECC_ERR_STATUS_SINGLE_ERR3_MASK, kMECC_MultiError0InterruptFlag = MECC_ERR_STATUS_MULTI_ERR0_MASK, kMECC_MultiError1InterruptFlag = MECC_ERR_STATUS_MULTI_ERR1_MASK, kMECC_MultiError2InterruptFlag = MECC_ERR_STATUS_MULTI_ERR2_MASK, kMECC_MultiError3InterruptFlag = MECC_ERR_STATUS_MULTI_ERR3_MASK, kMECC_StrobeError0InterruptFlag = MECC_ERR_STATUS_STRB_ERR0_MASK, kMECC_StrobeError1InterruptFlag = MECC_ERR_STATUS_STRB_ERR1_MASK, kMECC_StrobeError2InterruptFlag = MECC_ERR_STATUS_STRB_ERR2_MASK, kMECC_StrobeError3InterruptFlag = MECC_ERR_STATUS_STRB_ERR3_MASK, kMECC_AccessError0InterruptFlag = MECC_ERR_STATUS_ADDR_ERR0_MASK, kMECC_AccessError1InterruptFlag = MECC_ERR_STATUS_ADDR_ERR1_MASK, kMECC_AccessError2InterruptFlag = MECC_ERR_STATUS_ADDR_ERR2_MASK, kMECC_AccessError3InterruptFlag = MECC_ERR_STATUS_ADDR_ERR3_MASK, kMECC_AllInterruptsFlag = 0xFFFF } |
| MECC status flags. More... | |
| enum | { kMECC_OcramBank0 = 0U, kMECC_OcramBank1 = 1U, kMECC_OcramBank2 = 2U, kMECC_OcramBank3 = 3U } |
| MECC ocram bank number. More... | |
| enum | _mecc_pending_flag { kMECC_ReadDataWaitPendingFlag = 0x1U, kMECC_ReadAddrPipelinePendingFlag = 0x2U, kMECC_WriteDataPipelinePendingFlag = 0x4U, kMECC_WriteAddrPipelinePendingFlag = 0x8U, kMECC_AllPendingFlags = 0xFU } |
| Pending flags for OCRAM wait and pipeline enable. More... | |
Driver version | |
| #define | FSL_MECC_DRIVER_VERSION (MAKE_VERSION(2U, 1U, 0U)) |
| Driver version 2.1.0. More... | |
Initialization and deinitialization | |
| void | MECC_Init (MECC_Type *base, mecc_config_t *config) |
| MECC module initialization function. More... | |
| void | MECC_Deinit (MECC_Type *base) |
| Deinitializes the MECC. More... | |
| void | MECC_GetDefaultConfig (mecc_config_t *config) |
| Sets the MECC configuration structure to default values. More... | |
Status | |
| static uint32_t | MECC_GetStatusFlags (MECC_Type *base) |
| Gets MECC status flags. More... | |
| static void | MECC_ClearStatusFlags (MECC_Type *base, uint32_t mask) |
| MECC module clear interrupt status. More... | |
| static void | MECC_EnableInterruptStatus (MECC_Type *base, uint32_t mask) |
| MECC module enable interrupt status. More... | |
| static void | MECC_DisableInterruptStatus (MECC_Type *base, uint32_t mask) |
| MECC module disable interrupt status. More... | |
Interrupts | |
| static void | MECC_EnableInterrupts (MECC_Type *base, uint32_t mask) |
| MECC module enable interrupt. More... | |
| static void | MECC_DisableInterrupts (MECC_Type *base, uint32_t mask) |
| MECC module disable interrupt. More... | |
functional | |
| status_t | MECC_ErrorInjection (MECC_Type *base, uint32_t lowerrordata, uint32_t higherrordata, uint8_t eccdata, uint8_t banknumber) |
| MECC module error injection. More... | |
| status_t | MECC_GetSingleErrorInfo (MECC_Type *base, mecc_single_error_info_t *info, uint8_t banknumber) |
| MECC module get single error information. More... | |
| status_t | MECC_GetMultiErrorInfo (MECC_Type *base, mecc_multi_error_info_t *info, uint8_t banknumber) |
| MECC module get multiple error information. More... | |
| static uint32_t | MECC_GetPendingFlags (MECC_Type *base) |
| Get pending flags for OCRAM wait and pipeline enable. More... | |
| struct _mecc_config |
Data Fields | |
| bool | enableMecc |
| Enable the MECC function. More... | |
| uint32_t | startAddress |
| Start address of corresponding OCRAM memory region to enable ECC. More... | |
| uint32_t | endAddress |
| end address of corresponding OCRAM memory region to enable ECC. More... | |
| bool | enableReadDataWait |
| uint32_t Ocram1StartAddress; Ocram 1 start address, deprecated since 2.1.0 More... | |
| bool | enableReadAddrPipeline |
| If enabled, the read address will be registered before can be applied to memory cell: More... | |
| bool | enableWriteDataPipeline |
| If enabled, the write data will be registered before can be applied to memory cell: More... | |
| bool | enableWriteAddrPipeline |
| If enabled, write address will be registered before can be applied to memory cell: More... | |
| bool _mecc_config::enableMecc |
| uint32_t _mecc_config::startAddress |
| uint32_t _mecc_config::endAddress |
| bool _mecc_config::enableReadDataWait |
uint32_t Ocram1EndAddress; Ocram 1 end address, deprecated since 2.1.0
uint32_t Ocram2StartAddress; Ocram 2 start address, deprecated since 2.1.0.
uint32_t Ocram2EndAddress; Ocram 2 end address, deprecated since 2.1.0 If enabled, 1-cycle wait state will be inserted into each read access:
| bool _mecc_config::enableReadAddrPipeline |
| bool _mecc_config::enableWriteDataPipeline |
| bool _mecc_config::enableWriteAddrPipeline |
| struct _mecc_single_error_info |
Data Fields | |
| uint32_t | singleErrorAddress |
| Single error address on Ocram bank n. | |
| uint32_t | singleErrorDataLow |
| Single error low 32 bits uncorrected read data on Ocram bank n. | |
| uint32_t | singleErrorDataHigh |
| Single error high 32 bits uncorrected read data on Ocram bank n. | |
| uint32_t | singleErrorPosLow |
| Single error bit postion of low 32 bits read data on Ocram bank n. | |
| uint32_t | singleErrorPosHigh |
| Single error bit postion of high 32 bits read data on Ocram bank n. | |
| uint8_t | singleErrorEccCode |
| Single error ECC code on Ocram bank n. | |
| struct _mecc_multi_error_info |
Data Fields | |
| uint32_t | multiErrorAddress |
| Multiple error address on Ocram bank n. | |
| uint32_t | multiErrorDataLow |
| Multiple error low 32 bits read data on Ocram bank n. | |
| uint32_t | multiErrorDataHigh |
| Multiple error high 32 bits read data on Ocram bank n. | |
| uint8_t | multiErrorEccCode |
| Multiple error ECC code on Ocram bank n. | |
| #define FSL_MECC_DRIVER_VERSION (MAKE_VERSION(2U, 1U, 0U)) |
| typedef struct _mecc_config mecc_config_t |
| anonymous enum |
This structure contains the settings for all of the MECC interrupt configurations.
| anonymous enum |
This structure contains the settings for all of the MECC interrupt status configurations.
| anonymous enum |
This provides constants for the MECC status flags for use in the MECC functions.
| anonymous enum |
| enum _mecc_pending_flag |
| void MECC_Init | ( | MECC_Type * | base, |
| mecc_config_t * | config | ||
| ) |
| base | MECC base address. |
| config | pointer to the MECC configuration structure. |
| void MECC_Deinit | ( | MECC_Type * | base | ) |
| base | MECC base address. |
| void MECC_GetDefaultConfig | ( | mecc_config_t * | config | ) |
| config | pointer to the MECC configuration structure. |
|
inlinestatic |
| base | MECC peripheral base address. |
|
inlinestatic |
| base | MECC base address. |
| mask | status to clear. |
|
inlinestatic |
| base | MECC base address. |
| mask | status to enable. |
|
inlinestatic |
| base | MECC base address. |
| mask | status to disable. |
|
inlinestatic |
| base | MECC base address. |
| mask | The interrupts to enable. |
|
inlinestatic |
| base | MECC base address. |
| mask | The interrupts to disable. |
| status_t MECC_ErrorInjection | ( | MECC_Type * | base, |
| uint32_t | lowerrordata, | ||
| uint32_t | higherrordata, | ||
| uint8_t | eccdata, | ||
| uint8_t | banknumber | ||
| ) |
| base | MECC base address. |
| lowerrordata | low 32 bits data. |
| higherrordata | high 32 bits data. |
| eccdata | ecc code. |
| banknumber | ocram bank number. |
| kStatus_Success. | Bank0: ocram_base_address+0x20*i Bank1: ocram_base_address+0x20*i+0x8 Bank2: ocram_base_address+0x20*i+0x10 Bank3: ocram_base_address+0x20*i+0x18 i = 0,1,2,3,4..... |
| status_t MECC_GetSingleErrorInfo | ( | MECC_Type * | base, |
| mecc_single_error_info_t * | info, | ||
| uint8_t | banknumber | ||
| ) |
| base | MECC base address. |
| info | single error information. |
| banknumber | ocram bank number. |
| kStatus_Success. | |
| kStatus_MECC_BankMiss. | Bank0: ocram_base_address+0x20*i Bank1: ocram_base_address+0x20*i+0x8 Bank2: ocram_base_address+0x20*i+0x10 Bank3: ocram_base_address+0x20*i+0x18 i = 0,1,2,3,4..... |
| status_t MECC_GetMultiErrorInfo | ( | MECC_Type * | base, |
| mecc_multi_error_info_t * | info, | ||
| uint8_t | banknumber | ||
| ) |
| base | MECC base address. |
| info | multiple error information. |
| banknumber | ocram bank number. |
| kStatus_Success. | |
| kStatus_MECC_BankMiss. | Bank0: ocram_base_address+0x20*i Bank1: ocram_base_address+0x20*i+0x8 Bank2: ocram_base_address+0x20*i+0x10 Bank3: ocram_base_address+0x20*i+0x18 i = 0,1,2,3,4..... |
|
inlinestatic |
| base | MECC base address. |