![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
Macros | |
| #define | SMARTCARD_ATR_DURATION_ADJUSTMENT (360u) |
| Smart card definition which specifies the adjustment number of clock cycles during which an ATR string has to be received. | |
| #define | SMARTCARD_INIT_DELAY_CLOCK_CYCLES_ADJUSTMENT (4200u) |
| Smart card definition which specifies the adjustment number of clock cycles until an initial 'TS' character has to be received. More... | |
Functions | |
| void | SMARTCARD_PHY_GetDefaultConfig (smartcard_interface_config_t *config) |
| Fills in the configuration structure with default values. More... | |
| status_t | SMARTCARD_PHY_Init (void *base, smartcard_interface_config_t const *config, uint32_t srcClock_Hz) |
| Initializes a Smart card interface instance. More... | |
| void | SMARTCARD_PHY_Deinit (void *base, smartcard_interface_config_t const *config) |
| De-initializes a Smart card interface, stops the Smart card clock, and disables the VCC. More... | |
| status_t | SMARTCARD_PHY_Activate (void *base, smartcard_context_t *context, smartcard_reset_type_t resetType) |
| Activates the Smart card IC. More... | |
| status_t | SMARTCARD_PHY_Deactivate (void *base, smartcard_context_t *context) |
| De-activates the Smart card IC. More... | |
| status_t | SMARTCARD_PHY_Control (void *base, smartcard_context_t *context, smartcard_interface_control_t control, uint32_t param) |
| Controls the Smart card interface IC. More... | |
| #define SMARTCARD_INIT_DELAY_CLOCK_CYCLES_ADJUSTMENT (4200u) |
| void SMARTCARD_PHY_GetDefaultConfig | ( | smartcard_interface_config_t * | config | ) |
| config | The Smart card user configuration structure which contains configuration structure of type smartcard_interface_config_t. Function fill in members: clockToResetDelay = 42000, vcc = kSmartcardVoltageClassB3_3V, with default values. |
| status_t SMARTCARD_PHY_Init | ( | void * | base, |
| smartcard_interface_config_t const * | config, | ||
| uint32_t | srcClock_Hz | ||
| ) |
| base | The Smart card peripheral base address. |
| config | The user configuration structure of type smartcard_interface_config_t. Call the function SMARTCARD_PHY_GetDefaultConfig() to fill the configuration structure. |
| srcClock_Hz | Smart card clock generation module source clock. |
| kStatus_SMARTCARD_Success | or kStatus_SMARTCARD_OtherError in case of error. |
| void SMARTCARD_PHY_Deinit | ( | void * | base, |
| smartcard_interface_config_t const * | config | ||
| ) |
| base | The Smart card peripheral module base address. |
| config | The user configuration structure of type smartcard_interface_config_t. |
| status_t SMARTCARD_PHY_Activate | ( | void * | base, |
| smartcard_context_t * | context, | ||
| smartcard_reset_type_t | resetType | ||
| ) |
| base | The Smart card peripheral module base address. |
| context | A pointer to a Smart card driver context structure. |
| resetType | type of reset to be performed, possible values = kSmartcardColdReset, kSmartcardWarmReset |
| kStatus_SMARTCARD_Success | or kStatus_SMARTCARD_OtherError in case of error. |
| status_t SMARTCARD_PHY_Deactivate | ( | void * | base, |
| smartcard_context_t * | context | ||
| ) |
| base | The Smart card peripheral module base address. |
| context | A pointer to a Smart card driver context structure. |
| kStatus_SMARTCARD_Success | or kStatus_SMARTCARD_OtherError in case of error. |
| status_t SMARTCARD_PHY_Control | ( | void * | base, |
| smartcard_context_t * | context, | ||
| smartcard_interface_control_t | control, | ||
| uint32_t | param | ||
| ) |
| base | The Smart card peripheral module base address. |
| context | A pointer to a Smart card driver context structure. |
| control | A interface command type. |
| param | Integer value specific to control type |
| kStatus_SMARTCARD_Success | or kStatus_SMARTCARD_OtherError in case of error. |