![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
Files | |
file | fsl_cdog.h |
Driver version | |
#define | FSL_CDOG_DRIVER_VERSION (MAKE_VERSION(2, 1, 3)) |
Defines CDOG driver version 2.1.3. More... | |
CDOG Functional Operation | |
status_t | CDOG_Init (CDOG_Type *base, cdog_config_t *conf) |
Initialize CDOG. More... | |
void | CDOG_Deinit (CDOG_Type *base) |
Deinitialize CDOG. More... | |
void | CDOG_GetDefaultConfig (cdog_config_t *conf) |
Sets the default configuration of CDOG. More... | |
void | CDOG_Stop (CDOG_Type *base, uint32_t stop) |
Stops secure counter and instruction timer. More... | |
void | CDOG_Start (CDOG_Type *base, uint32_t reload, uint32_t start) |
Sets secure counter and instruction timer values. More... | |
void | CDOG_Check (CDOG_Type *base, uint32_t check) |
Checks secure counter. More... | |
void | CDOG_Set (CDOG_Type *base, uint32_t stop, uint32_t reload, uint32_t start) |
Sets secure counter and instruction timer values. More... | |
void | CDOG_Add (CDOG_Type *base, uint32_t add) |
Add value to secure counter. More... | |
void | CDOG_Add1 (CDOG_Type *base) |
Add 1 to secure counter. More... | |
void | CDOG_Add16 (CDOG_Type *base) |
Add 16 to secure counter. More... | |
void | CDOG_Add256 (CDOG_Type *base) |
Add 256 to secure counter. More... | |
void | CDOG_Sub (CDOG_Type *base, uint32_t sub) |
brief Substract value to secure counter More... | |
void | CDOG_Sub1 (CDOG_Type *base) |
Substract 1 from secure counter. More... | |
void | CDOG_Sub16 (CDOG_Type *base) |
Substract 16 from secure counter. More... | |
void | CDOG_Sub256 (CDOG_Type *base) |
Substract 256 from secure counter. More... | |
void | CDOG_WritePersistent (CDOG_Type *base, uint32_t value) |
Set the CDOG persistent word. More... | |
uint32_t | CDOG_ReadPersistent (CDOG_Type *base) |
Get the CDOG persistent word. More... | |
#define FSL_CDOG_DRIVER_VERSION (MAKE_VERSION(2, 1, 3)) |
Change log:
status_t CDOG_Init | ( | CDOG_Type * | base, |
cdog_config_t * | conf | ||
) |
This function initializes CDOG block and setting.
base | CDOG peripheral base address |
conf | CDOG configuration structure |
void CDOG_Deinit | ( | CDOG_Type * | base | ) |
This function deinitializes CDOG secure counter.
base | CDOG peripheral base address |
void CDOG_GetDefaultConfig | ( | cdog_config_t * | conf | ) |
This function initialize CDOG config structure to default values.
conf | CDOG configuration structure |
void CDOG_Stop | ( | CDOG_Type * | base, |
uint32_t | stop | ||
) |
This function stops instruction timer and secure counter. This also change state od CDOG to IDLE.
base | CDOG peripheral base address |
stop | expected value which will be compared with value of secure counter |
void CDOG_Start | ( | CDOG_Type * | base, |
uint32_t | reload, | ||
uint32_t | start | ||
) |
This function sets value in RELOAD and START registers for instruction timer and secure counter
base | CDOG peripheral base address |
reload | reload value |
start | start value |
void CDOG_Check | ( | CDOG_Type * | base, |
uint32_t | check | ||
) |
This function compares stop value in handler with secure counter value by writting to RELOAD refister.
base | CDOG peripheral base address |
check | expected (stop) value |
void CDOG_Set | ( | CDOG_Type * | base, |
uint32_t | stop, | ||
uint32_t | reload, | ||
uint32_t | start | ||
) |
This function sets value in STOP, RELOAD and START registers for instruction timer and secure counter.
base | CDOG peripheral base address |
stop | expected value which will be compared with value of secure counter |
reload | reload value for instruction timer |
start | start value for secure timer |
void CDOG_Add | ( | CDOG_Type * | base, |
uint32_t | add | ||
) |
This function add specified value to secure counter.
base | CDOG peripheral base address. |
add | Value to be added. |
void CDOG_Add1 | ( | CDOG_Type * | base | ) |
This function add 1 to secure counter.
base | CDOG peripheral base address. |
void CDOG_Add16 | ( | CDOG_Type * | base | ) |
This function add 16 to secure counter.
base | CDOG peripheral base address. |
void CDOG_Add256 | ( | CDOG_Type * | base | ) |
This function add 256 to secure counter.
base | CDOG peripheral base address. |
void CDOG_Sub | ( | CDOG_Type * | base, |
uint32_t | sub | ||
) |
This function substract specified value to secure counter.
param base CDOG peripheral base address. param sub Value to be substracted.
void CDOG_Sub1 | ( | CDOG_Type * | base | ) |
This function substract specified 1 from secure counter.
base | CDOG peripheral base address. |
void CDOG_Sub16 | ( | CDOG_Type * | base | ) |
This function substract specified 16 from secure counter.
base | CDOG peripheral base address. |
void CDOG_Sub256 | ( | CDOG_Type * | base | ) |
This function substract specified 256 from secure counter.
base | CDOG peripheral base address. |
void CDOG_WritePersistent | ( | CDOG_Type * | base, |
uint32_t | value | ||
) |
base | CDOG peripheral base address. |
value | The value to be written. |
uint32_t CDOG_ReadPersistent | ( | CDOG_Type * | base | ) |
base | CDOG peripheral base address. |