MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

Data Structures

struct  _asrc_data_format
 asrc context data format More...
 
struct  _asrc_access_ctrl
 asrc context access control The ASRC provides interleaving support in hardware to ensure that a variety of sample source can be internally combined tp confir with this format. More...
 
struct  _asrc_context_input_config
 asrc context input configuration More...
 
struct  _asrc_context_output_config
 asrc context output configuration More...
 
struct  _asrc_context_prefilter_config
 asrc context prefilter configuration More...
 
struct  _asrc_context_resampler_config
 asrc context resampler configuration More...
 
struct  _asrc_context_config
 asrc context configuration More...
 
struct  _asrc_transfer
 ASRC transfer. More...
 

Macros

#define FSL_ASRC_INPUT_FIFO_DEPTH   (128U)
 ASRC fifo depth.
 
#define ASRC_SUPPORT_MAXIMUM_CONTEXT_PROCESSOR_NUMBER   4U
 ASRC support maximum channel number of context.
 

Typedefs

typedef enum _asrc_context asrc_context_t
 asrc context id
 
typedef enum _asrc_data_endianness asrc_data_endianness_t
 arsc data endianness
 
typedef enum _asrc_data_width asrc_data_width_t
 data width
 
typedef enum _asrc_data_type asrc_data_type_t
 data type
 
typedef enum _asrc_data_sign asrc_data_sign_t
 sign extension
 
typedef enum
_asrc_sampleBuffer_init_mode 
asrc_sampleBuffer_init_mode_t
 asrc prefilter and resampler sample buffer init mode
 
typedef enum
_asrc_sampleBuffer_stop_mode 
asrc_sampleBuffer_stop_mode_t
 asrc prefilter and resampler sample buffer stop mode
 
typedef enum
_asrc_prefilter_stage1_result 
asrc_prefilter_stage1_result_t
 ASRC prefilter stage1 result format.
 
typedef enum _asrc_resampler_taps asrc_resampler_taps_t
 ASRC resampler taps.
 
typedef struct _asrc_data_format asrc_data_format_t
 asrc context data format
 
typedef struct _asrc_access_ctrl asrc_access_ctrl_t
 asrc context access control The ASRC provides interleaving support in hardware to ensure that a variety of sample source can be internally combined tp confir with this format. More...
 
typedef struct
_asrc_context_input_config 
asrc_context_input_config_t
 asrc context input configuration
 
typedef struct
_asrc_context_output_config 
asrc_context_output_config_t
 asrc context output configuration
 
typedef struct
_asrc_context_prefilter_config 
asrc_context_prefilter_config_t
 asrc context prefilter configuration
 
typedef struct
_asrc_context_resampler_config 
asrc_context_resampler_config_t
 asrc context resampler configuration
 
typedef struct _asrc_context_config asrc_context_config_t
 asrc context configuration
 
typedef struct _asrc_transfer asrc_transfer_t
 ASRC transfer.
 

Enumerations

enum  {
  kStatus_ASRCIdle = MAKE_STATUS(kStatusGroup_ASRC, 0),
  kStatus_ASRCBusy = MAKE_STATUS(kStatusGroup_ASRC, 1),
  kStatus_ASRCInvalidArgument = MAKE_STATUS(kStatusGroup_ASRC, 2),
  kStatus_ASRCConfigureFailed = MAKE_STATUS(kStatusGroup_ASRC, 3),
  kStatus_ASRCConvertError = MAKE_STATUS(kStatusGroup_ASRC, 4),
  kStatus_ASRCNotSupport = MAKE_STATUS(kStatusGroup_ASRC, 5),
  kStatus_ASRCQueueFull = MAKE_STATUS(kStatusGroup_ASRC, 6),
  kStatus_ASRCQueueIdle = MAKE_STATUS(kStatusGroup_ASRC, 7),
  kStatus_ASRCLoadFirmwareFailed = MAKE_STATUS(kStatusGroup_ASRC, 8),
  kStatus_ASRCResamplerConfigureFailed = MAKE_STATUS(kStatusGroup_ASRC, 9),
  kStatus_ASRCPrefilterConfigureFailed = MAKE_STATUS(kStatusGroup_ASRC, 10)
}
 ASRC return status, _asrc_status. More...
 
enum  _asrc_context {
  kASRC_Context0 = 0,
  kASRC_Context1 = 1,
  kASRC_Context2 = 2,
  kASRC_Context3 = 3
}
 asrc context id More...
 
enum  {
  kASRC_Context0InputFifoOverflow = 1U,
  kASRC_Context1InputFifoOverflow = 1U << 1U,
  kASRC_Context2InputFifoOverflow = 1U << 2U,
  kASRC_Context3InputFifoOverflow = 1U << 3U,
  kASRC_Context0OutFifoReadEmpty = 1U << 4U,
  kASRC_Context1OutFifoReadEmpty = 1U << 5U,
  kASRC_Context2OutFifoReadEmpty = 1U << 6U,
  kASRC_Context3OutFifoReadEmpty = 1U << 7U,
  kASRC_Context0RunStopDone = 1U << 8U,
  kASRC_Context1RunStopDone = 1U << 9U,
  kASRC_Context2RunStopDone = 1U << 10U,
  kASRC_Context3RunStopDone = 1U << 11U,
  kASRC_ContextAllInterruptStatus = 0xFFFU
}
 The ASRC interrupt enable flag, _asrc_interrupt_mask. More...
 
enum  {
  kASRC_FifoStatusInputFifoWatermarkFlag,
  kASRC_FifoStatusOutputFifoWatermarkFlag
}
 ASRC fifo status, _asrc_fifo_status. More...
 
enum  _asrc_data_endianness {
  kASRC_DataEndianLittle = 0U,
  kASRC_DataEndianBig = 1U
}
 arsc data endianness More...
 
enum  _asrc_data_width {
  kASRC_DataWidth32Bit = 3U,
  kASRC_DataWidth24Bit = 2U,
  kASRC_DataWidth20Bit = 1U,
  kASRC_DataWidth16Bit = 0U
}
 data width More...
 
enum  _asrc_data_type {
  kASRC_DataTypeInteger = 0U,
  kASRC_DataTypeFloat = 1U
}
 data type More...
 
enum  _asrc_data_sign {
  kASRC_DataSigned = 0U,
  kASRC_DataUnsigned = 1U
}
 sign extension More...
 
enum  _asrc_sampleBuffer_init_mode {
  kASRC_SampleBufferNoPreFillOnInit = 0U,
  kASRC_SampleBufferFillFirstSampleOnInit,
  kASRC_SampleBufferFillZeroOnInit = 2U
}
 asrc prefilter and resampler sample buffer init mode More...
 
enum  _asrc_sampleBuffer_stop_mode {
  kASRC_SampleBufferFillLastSampleOnStop,
  kASRC_SampleBufferFillZeroOnStop = 1U
}
 asrc prefilter and resampler sample buffer stop mode More...
 
enum  _asrc_prefilter_stage1_result {
  kASRC_PrefilterStage1ResultInt = 0U,
  kASRC_PrefilterStage1ResultFloat = 1U
}
 ASRC prefilter stage1 result format. More...
 
enum  _asrc_resampler_taps {
  kASRC_ResamplerTaps_32 = 32U,
  kASRC_ResamplerTaps_64 = 64U,
  kASRC_ResamplerTaps_128 = 128U
}
 ASRC resampler taps. More...
 
enum  {
  kASRC_SampleRate_8000 = 8000,
  kASRC_SampleRate_11025 = 11025,
  kASRC_SampleRate_12000 = 12000,
  kASRC_SampleRate_16000 = 16000,
  kASRC_SampleRate_22050 = 22050,
  kASRC_SampleRate_24000 = 24000,
  kASRC_SampleRate_32000 = 32000,
  kASRC_SampleRate_44100 = 44100,
  kASRC_SampleRate_48000 = 48000,
  kASRC_SampleRate_64000 = 64000,
  kASRC_SampleRate_88200 = 88200,
  kASRC_SampleRate_96000 = 96000,
  kASRC_SampleRate_128000 = 128000,
  kASRC_SampleRate_176400 = 176400,
  kASRC_SampleRate_192000 = 192000,
  kASRC_SampleRate_256000 = 256000,
  kASRC_SampleRate_352800 = 352800,
  kASRC_SampleRate_384000 = 384000,
  kASRC_SampleRate_768000 = 768000
}
 ASRC support sample rate, _asrc_sample_rate. More...
 

Driver version

#define FSL_ASRC_DRIVER_VERSION   (MAKE_VERSION(2, 0, 6))
 Version 2.0.6.
 

Initialization and deinitialization

uint32_t ASRC_GetInstance (ASRC_Type *base)
 Get instance number of the ASRC peripheral. More...
 
void ASRC_Init (ASRC_Type *base)
 brief Initializes the asrc peripheral. More...
 
void ASRC_Deinit (ASRC_Type *base)
 De-initializes the ASRC peripheral. More...
 
void ASRC_GetContextDefaultConfig (asrc_context_config_t *config, uint32_t channels, uint32_t inSampleRate, uint32_t outSampleRate)
 ASRC get context default configuration. More...
 
status_t ASRC_SetContextConfig (ASRC_Type *base, asrc_context_t context, asrc_context_config_t *config)
 ASRC configure context. More...
 
status_t ASRC_SetContextOutputConfig (ASRC_Type *base, asrc_context_t context, asrc_context_output_config_t *config)
 ASRC configure context output. More...
 
status_t ASRC_SetContextInputConfig (ASRC_Type *base, asrc_context_t context, asrc_context_input_config_t *config)
 ASRC configure context input. More...
 
static void ASRC_EnableContextRun (ASRC_Type *base, asrc_context_t context, bool enable)
 ASRC context enable run. More...
 
static void ASRC_EnableContextRunStop (ASRC_Type *base, asrc_context_t context, bool enable)
 ASRC context enable run stop. More...
 
static void ASRC_EnableContextInDMA (ASRC_Type *base, asrc_context_t context, bool enable)
 ASRC context input DMA request enable. More...
 
static void ASRC_EnableContextOutDMA (ASRC_Type *base, asrc_context_t context, bool enable)
 ASRC context output DMA request enable. More...
 
static void ASRC_EnablePreFilterBypass (ASRC_Type *base, asrc_context_t context, bool bypass)
 ASRC prefilter bypass mode This function enable or disable the ASRC prefilter bypass mode. More...
 
static void ASRC_EnableResamplerBypass (ASRC_Type *base, asrc_context_t context, bool bypass)
 ASRC resampler bypass mode This function enable or disable the ASRC resampler bypass mode. More...
 
static void ASRC_SetContextChannelNumber (ASRC_Type *base, asrc_context_t context, uint32_t channels)
 ASRC set context channel number. More...
 
uint32_t ASRC_GetContextOutSampleSize (uint32_t inSampleRate, uint32_t inSamplesSize, uint32_t inWidth, uint32_t outSampleRate, uint32_t outWidth)
 ASRC get output sample count. More...
 

Interrupts

static void ASRC_EnableInterrupt (ASRC_Type *base, uint32_t mask)
 ASRC interrupt enable This function enable the ASRC interrupt with the provided mask. More...
 
static void ASRC_DisableInterrupt (ASRC_Type *base, uint32_t mask)
 ASRC interrupt disable This function disable the ASRC interrupt with the provided mask. More...
 

Status

static uint32_t ASRC_GetInterruptStatus (ASRC_Type *base)
 Gets the ASRC interrupt status flag state. More...
 
static void ASRC_ClearInterruptStatus (ASRC_Type *base, uint32_t status)
 clear the ASRC interrupt status flag state. More...
 
static uint32_t ASRC_GetFifoStatus (ASRC_Type *base, asrc_context_t context)
 Gets the ASRC fifo status flag. More...
 

fifo Operations

static void ASRC_WriteContextFifo (ASRC_Type *base, asrc_context_t context, uint32_t data)
 write the ASRC context fifo. More...
 
static uint32_t ASRC_ReadContextFifo (ASRC_Type *base, asrc_context_t context)
 read the ASRC context fifo. More...
 
static uint32_t ASRC_GetWriteContextFifoAddr (ASRC_Type *base, asrc_context_t context)
 Get ASRC write fifo address. More...
 
static uint32_t ASRC_GetReadContextFifoAddr (ASRC_Type *base, asrc_context_t context)
 Get the ASRC read context fifo address. More...
 
uint32_t ASRC_ReadFIFORemainedSample (ASRC_Type *base, asrc_context_t context, uint32_t *outAddr, uint32_t outWidth, uint32_t sampleCount)
 Get the ASRC read fifo remained samples. More...
 

Transactional

status_t ASRC_TransferBlocking (ASRC_Type *base, asrc_context_t context, asrc_transfer_t *xfer)
 ASRC blocking convert audio sample rate. More...
 

Data Structure Documentation

struct _asrc_data_format

Data Fields

uint8_t dataPosition
 context input data sample position
 
asrc_data_endianness_t dataEndianness
 context input data endianness
 
asrc_data_width_t dataWidth
 context input data width
 
asrc_data_type_t dataType
 context input data type
 
asrc_data_sign_t dataSign
 context input data signed or unsigned
 
struct _asrc_access_ctrl

The interleave patter is controlled using 3 register fields: GROUP_LENGTH, ACCESS_LENGTH, ITERATIONIS. This is intended to support hardware configurations which distribute a single context across samples from multiple audio sources. Take a example as below: accessGroupLen = 6, the sample group length is 6 samples accessIterations = 2, the 2 sequential ACCESS_LENGTH read from single source accessLen = 2, the 2 samples fetch from one source.

Data Fields

uint8_t accessIterations
 number of sequential fetches per source
 
uint8_t accessGroupLen
 number of channels in a context
 
uint8_t accessLen
 number of channels per source1
 
struct _asrc_context_input_config

Data Fields

uint32_t sampleRate
 input audio data sample rate
 
uint8_t watermark
 input water mark per samples
 
asrc_access_ctrl_t accessCtrl
 input access control
 
asrc_data_format_t dataFormat
 input data format
 
struct _asrc_context_output_config

Data Fields

uint32_t sampleRate
 output audio data sample rate
 
uint8_t watermark
 output water mark per samples
 
asrc_access_ctrl_t accessCtrl
 output access control
 
asrc_data_format_t dataFormat
 output data format
 
bool enableDither
 output path contains a TPDF dither function. More...
 
bool enableIEC60958
 output IEC60958 bit field insertion enable
 

Field Documentation

bool _asrc_context_output_config::enableDither

The dither function support all fixed output modes(16, 20, 24, 32bits) dither is not supported in 32bit floating point output mode

struct _asrc_context_prefilter_config

Data Fields

asrc_sampleBuffer_init_mode_t initMode
 prefilter initial mode
 
asrc_sampleBuffer_stop_mode_t stopMode
 prefilter stop mode
 
asrc_prefilter_stage1_result_t stage1Result
 stage1 data store format
 
uint32_t filterSt1Taps
 prefilter stage1 taps
 
uint32_t filterSt2Taps
 prefilter stage2 taps
 
uint32_t filterSt1Exp
 prefilter stage1 expansion factor
 
const uint32_t * filterCoeffAddress
 prefilter coeff address
 
struct _asrc_context_resampler_config

Data Fields

asrc_sampleBuffer_init_mode_t initMode
 initial mode
 
asrc_sampleBuffer_stop_mode_t stopMode
 resampler stop mode
 
asrc_resampler_taps_t tap
 resampleer taps
 
uint32_t filterPhases
 interpolation phases
 
uint64_t filterCenterTap
 interpolation center tap
 
const uint32_t * filterCoeffAddress
 interpolation coeff address
 
struct _asrc_context_config

Data Fields

uint8_t contextChannelNums
 context channel numbers
 
asrc_context_input_config_t contextInput
 context input configuration
 
asrc_context_output_config_t contextOutput
 context output configuration
 
asrc_context_prefilter_config_t contextPrefilter
 context pre filter configuration
 
asrc_context_resampler_config_t contextResampler
 context resampler configuration
 
struct _asrc_transfer

Data Fields

uint32_t * inDataAddr
 address of audio data to be converted
 
uint32_t inDataSize
 size of the audio data
 
uint32_t * outDataAddr
 address of audio data that is been converted
 
uint32_t outDataSize
 size of the audio data
 

Typedef Documentation

The interleave patter is controlled using 3 register fields: GROUP_LENGTH, ACCESS_LENGTH, ITERATIONIS. This is intended to support hardware configurations which distribute a single context across samples from multiple audio sources. Take a example as below: accessGroupLen = 6, the sample group length is 6 samples accessIterations = 2, the 2 sequential ACCESS_LENGTH read from single source accessLen = 2, the 2 samples fetch from one source.

Enumeration Type Documentation

anonymous enum
Enumerator
kStatus_ASRCIdle 

ASRC is idle.

kStatus_ASRCBusy 

ASRC is busy.

kStatus_ASRCInvalidArgument 

ASRC invalid argument.

kStatus_ASRCConfigureFailed 

ASRC configure failed.

kStatus_ASRCConvertError 

ASRC convert error failed.

kStatus_ASRCNotSupport 

ASRC not support.

kStatus_ASRCQueueFull 

ASRC queue full.

kStatus_ASRCQueueIdle 

ASRC quue idle.

kStatus_ASRCLoadFirmwareFailed 

ASRC load firmware failed.

kStatus_ASRCResamplerConfigureFailed 

ASRC resampler configured failed.

kStatus_ASRCPrefilterConfigureFailed 

ASRC prefilter configured failed.

Enumerator
kASRC_Context0 

Context 0 value.

kASRC_Context1 

Context 1 value.

kASRC_Context2 

Context 2 value.

kASRC_Context3 

Context 3 value.

anonymous enum
Enumerator
kASRC_Context0InputFifoOverflow 

context 0 input fifo overflow

kASRC_Context1InputFifoOverflow 

context 1 input fifo overflow

kASRC_Context2InputFifoOverflow 

context 2 input fifo overflow

kASRC_Context3InputFifoOverflow 

context 3 input fifo overflow

kASRC_Context0OutFifoReadEmpty 

context 0 out fifo read empty

kASRC_Context1OutFifoReadEmpty 

context 1 out fifo read empty

kASRC_Context2OutFifoReadEmpty 

context 2 out fifo read empty

kASRC_Context3OutFifoReadEmpty 

context 3 out fifo read empty

kASRC_Context0RunStopDone 

context 0 run stop done interrupt

kASRC_Context1RunStopDone 

context 1 run stop done interrupt

kASRC_Context2RunStopDone 

context 2 run stop done interrupt

kASRC_Context3RunStopDone 

context 3 run stop done interrupt

kASRC_ContextAllInterruptStatus 

all the context interrupt status

anonymous enum
Enumerator
kASRC_FifoStatusInputFifoWatermarkFlag 

input water mark flag raised

kASRC_FifoStatusOutputFifoWatermarkFlag 

output water mark flag raised

Enumerator
kASRC_DataEndianLittle 

context data little endian

kASRC_DataEndianBig 

context data big endian

Enumerator
kASRC_DataWidth32Bit 

data width 32bit

kASRC_DataWidth24Bit 

data width 24bit

kASRC_DataWidth20Bit 

data width 20bit

kASRC_DataWidth16Bit 

data width 16bit

Enumerator
kASRC_DataTypeInteger 

data type int

kASRC_DataTypeFloat 

data type float, single precision floating point format

Enumerator
kASRC_DataSigned 

input data is signed

kASRC_DataUnsigned 

input data is unsinged

Enumerator
kASRC_SampleBufferNoPreFillOnInit 

do not pre-fill

kASRC_SampleBufferFillFirstSampleOnInit 

replicate the first sample to fill the right half of the sample buffer

kASRC_SampleBufferFillZeroOnInit 

zero fill the right half og the sample buffer

Enumerator
kASRC_SampleBufferFillLastSampleOnStop 

replicate the last sample to fill the left half of the sample buffer

kASRC_SampleBufferFillZeroOnStop 

zero fill the left half of the sample buffer

Enumerator
kASRC_PrefilterStage1ResultInt 

prefilter stage1 results are stored in 32 bit int format

kASRC_PrefilterStage1ResultFloat 

prefilter stage1 results are stored in 32 bit float format

Enumerator
kASRC_ResamplerTaps_32 

resampler taps 32

kASRC_ResamplerTaps_64 

resampler taps 64

kASRC_ResamplerTaps_128 

resampler taps 128

anonymous enum
Enumerator
kASRC_SampleRate_8000 

8K sample rate

kASRC_SampleRate_11025 

11025 sample rate

kASRC_SampleRate_12000 

12K sample rate

kASRC_SampleRate_16000 

16K sample rate

kASRC_SampleRate_22050 

22.05K sample rate

kASRC_SampleRate_24000 

24K sample rate

kASRC_SampleRate_32000 

32K sample rate

kASRC_SampleRate_44100 

44.1K sample rate

kASRC_SampleRate_48000 

48K sample rate

kASRC_SampleRate_64000 

64K sample rate

kASRC_SampleRate_88200 

88.2K sample rate

kASRC_SampleRate_96000 

96K sample rate

kASRC_SampleRate_128000 

128K sample rate

kASRC_SampleRate_176400 

176K sample rate

kASRC_SampleRate_192000 

256K sample rate

kASRC_SampleRate_256000 

256K sample rate

kASRC_SampleRate_352800 

352.8K sample rate

kASRC_SampleRate_384000 

384K sample rate

kASRC_SampleRate_768000 

768K sample rate

Function Documentation

uint32_t ASRC_GetInstance ( ASRC_Type *  base)
Parameters
baseASRC base pointer.
void ASRC_Init ( ASRC_Type *  base)

This API gates the asrc clock. The asrc module can't operate unless ASRC_Init is called to enable the clock.

param base asrc base pointer.

void ASRC_Deinit ( ASRC_Type *  base)

This API gates the ASRC clock and disable ASRC module. The ASRC module can't operate unless ASRC_Init

Parameters
baseASRC base pointer.
void ASRC_GetContextDefaultConfig ( asrc_context_config_t *  config,
uint32_t  channels,
uint32_t  inSampleRate,
uint32_t  outSampleRate 
)
Parameters
configASRC context configuration pointer.
channelsinput audio data channel numbers.
inSampleRateinput sample rate.
outSampleRateoutput sample rate.
status_t ASRC_SetContextConfig ( ASRC_Type *  base,
asrc_context_t  context,
asrc_context_config_t *  config 
)
Parameters
baseASRC base pointer.
contextindex of asrc context, reference asrc_context_t.
configASRC context configuration pointer.
Return values
kStatus_InvalidArgumentinvalid parameters. kStatus_ASRCConfigureFailed context configure failed. kStatus_Success context configure success.
status_t ASRC_SetContextOutputConfig ( ASRC_Type *  base,
asrc_context_t  context,
asrc_context_output_config_t *  config 
)
Parameters
baseASRC base pointer.
contextindex of asrc context, reference asrc_context_t.
configASRC context output configuration pointer.
status_t ASRC_SetContextInputConfig ( ASRC_Type *  base,
asrc_context_t  context,
asrc_context_input_config_t *  config 
)
Parameters
baseASRC base pointer.
contextindex of asrc context, reference asrc_context_t.
configASRC context input configuration pointer.
static void ASRC_EnableContextRun ( ASRC_Type *  base,
asrc_context_t  context,
bool  enable 
)
inlinestatic

All control fileds associated with a context must be stable prior to setting context run enable.

Parameters
baseASRC base pointer.
contextASRC context index.
enabletrue is enable, inform the datapath begin processing sample data for the context. false is disable, data processing will halt immediately.
static void ASRC_EnableContextRunStop ( ASRC_Type *  base,
asrc_context_t  context,
bool  enable 
)
inlinestatic

This function used to flush the ASRC pipeline and completely end processing for a context.

Parameters
baseASRC base pointer.
contextASRC context index.
enabletrue is enable, false is disable.
static void ASRC_EnableContextInDMA ( ASRC_Type *  base,
asrc_context_t  context,
bool  enable 
)
inlinestatic
Parameters
baseASRC base pointer.
contextASRC context index.
enabletrue is enable, false is disable.
static void ASRC_EnableContextOutDMA ( ASRC_Type *  base,
asrc_context_t  context,
bool  enable 
)
inlinestatic
Parameters
baseASRC base pointer.
contextASRC context index.
enabletrue is enable, false is disable.
static void ASRC_EnablePreFilterBypass ( ASRC_Type *  base,
asrc_context_t  context,
bool  bypass 
)
inlinestatic
Parameters
baseASRC peripheral base address.
contextcontext processor number.
bypasstrue is bypass, false is normal mode.
static void ASRC_EnableResamplerBypass ( ASRC_Type *  base,
asrc_context_t  context,
bool  bypass 
)
inlinestatic
Parameters
baseASRC peripheral base address.
contextcontext processor number.
bypasstrue is bypass, false is normal mode.
static void ASRC_SetContextChannelNumber ( ASRC_Type *  base,
asrc_context_t  context,
uint32_t  channels 
)
inlinestatic

Note: The maximum channel number in one context can not exceed 32.

Parameters
baseASRC peripheral base address.
contextcontext number.
channelschannel number, should <= 32.
uint32_t ASRC_GetContextOutSampleSize ( uint32_t  inSampleRate,
uint32_t  inSamplesSize,
uint32_t  inWidth,
uint32_t  outSampleRate,
uint32_t  outWidth 
)
Parameters
inSampleRateoutput sample rate.
inSamplesSizeinput sample rate.
inWidthinput samples buffer size, the size of buffer should be converted to align with 4 byte .
outSampleRateinput sample width.
outWidthOutput width.
Return values
outputsamples size.
static void ASRC_EnableInterrupt ( ASRC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseASRC peripheral base address.
maskThe interrupts to enable. Logical OR of _asrc_interrupt_mask.
static void ASRC_DisableInterrupt ( ASRC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseASRC peripheral base address.
maskThe interrupts to disable. Logical OR of _asrc_interrupt_mask.
static uint32_t ASRC_GetInterruptStatus ( ASRC_Type *  base)
inlinestatic
Parameters
baseASRC base pointer
Returns
ASRC Tx status flag value. Use the Status Mask to get the status value needed.
static void ASRC_ClearInterruptStatus ( ASRC_Type *  base,
uint32_t  status 
)
inlinestatic
Parameters
baseASRC base pointer
statusstatus flag to be cleared.
static uint32_t ASRC_GetFifoStatus ( ASRC_Type *  base,
asrc_context_t  context 
)
inlinestatic
Parameters
baseASRC base pointer
contextcontext id
static void ASRC_WriteContextFifo ( ASRC_Type *  base,
asrc_context_t  context,
uint32_t  data 
)
inlinestatic
Parameters
baseASRC base pointer.
contextcontext id.
datadata to write.
static uint32_t ASRC_ReadContextFifo ( ASRC_Type *  base,
asrc_context_t  context 
)
inlinestatic
Parameters
baseASRC base pointer.
contextcontext id.
Return values
readdata.
static uint32_t ASRC_GetWriteContextFifoAddr ( ASRC_Type *  base,
asrc_context_t  context 
)
inlinestatic
Parameters
baseASRC base pointer.
contextcontext id.
Return values
writefifo address.
static uint32_t ASRC_GetReadContextFifoAddr ( ASRC_Type *  base,
asrc_context_t  context 
)
inlinestatic
Parameters
baseASRC base pointer.
contextcontext id.
Return values
readfifo address.
uint32_t ASRC_ReadFIFORemainedSample ( ASRC_Type *  base,
asrc_context_t  context,
uint32_t *  outAddr,
uint32_t  outWidth,
uint32_t  sampleCount 
)

Since the DMA request will be triggered only when the sample group in read fifo is bigger then the watermark, so when the data size cannot be divisible by the (watermark + 1), then part of sample will left in read fifo, application should call this api to get the left samples.

Parameters
baseASRC base pointer.
contextcontext id.
outAddraddress to receive remained sample in read fifo.
outWidthoutput data width.
sampleCountspecify the read sample count.
Return values
samplecounts actual read from output fifo.
status_t ASRC_TransferBlocking ( ASRC_Type *  base,
asrc_context_t  context,
asrc_transfer_t *  xfer 
)

This function depends on the configuration of input and output, so it should be called after the ASRC_SetContextConfig. The data format it supports: 1.16bit 16bit per sample in input buffer, input buffer size should be calculate as: samples 2U output buffer size can be calculated by call function ASRC_GetContextOutSampleSize, the parameter outWidth should be 2 2.20bit 24bit per sample in input buffer, input buffer size should be calculate as: samples 3U output buffer size can be calculated by call function ASRC_GetContextOutSampleSize, the outWidth should be 3. 3.24bit 24bit per sample in input buffer, input buffer size should be calculate as: samples * 3U output buffer size can be calculated by call function ASRC_GetContextOutSampleSize, the outWidth should be 3. 4.32bit 32bit per sample in input buffer, input buffer size should be calculate as: samples * 4U output buffer size can be calculated by call function ASRC_GetContextOutSampleSize, the outWidth should be 4.

Parameters
baseASRC base pointer.
contextcontext id.
xfer.xfer configuration.
Return values
kStatus_Success.