![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
Modules | |
| FGPIO Driver | |
| GPIO Driver | |
Data Structures | |
| struct | _gpio_pin_config |
| The GPIO pin configuration structure. More... | |
Typedefs | |
| typedef enum _gpio_port_num | gpio_port_num_t |
| PORT definition. | |
| typedef enum _gpio_pin_direction | gpio_pin_direction_t |
| GPIO direction definition. | |
| typedef struct _gpio_pin_config | gpio_pin_config_t |
| The GPIO pin configuration structure. More... | |
Enumerations | |
| enum | _gpio_port_num |
| PORT definition. | |
| enum | _gpio_pin_direction { kGPIO_DigitalInput = 0U, kGPIO_DigitalOutput = 1U } |
| GPIO direction definition. More... | |
Driver version | |
| #define | FSL_GPIO_DRIVER_VERSION (MAKE_VERSION(2, 1, 1)) |
| GPIO driver version. More... | |
| struct _gpio_pin_config |
Each pin can only be configured as either an output pin or an input pin at a time. If configured as an input pin, leave the outputConfig unused. Note that in some use cases, the corresponding port property should be configured in advance with the PORT_SetPinConfig().
Data Fields | |
| gpio_pin_direction_t | pinDirection |
| GPIO direction, input or output. | |
| uint8_t | outputLogic |
| Set a default output logic, which has no use in input. | |
| #define FSL_GPIO_DRIVER_VERSION (MAKE_VERSION(2, 1, 1)) |
| typedef struct _gpio_pin_config gpio_pin_config_t |
Each pin can only be configured as either an output pin or an input pin at a time. If configured as an input pin, leave the outputConfig unused. Note that in some use cases, the corresponding port property should be configured in advance with the PORT_SetPinConfig().
| enum _gpio_pin_direction |