MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Audio_Adapter

Overview

Data Structures

struct  _hal_audio_dma_mux_config_t
 HAL Audio DMA mux user configuration. More...
 
struct  _hal_audio_dma_channel_mux_config_t
 HAL Audio DMA channel mux user configuration. More...
 
struct  _hal_audio_dma_extra_config_t
 HAL Audio DMA extra user configuration. More...
 
struct  _hal_audio_dma_config
 HAL Audio DMA user configuration. More...
 
struct  _hal_audio_ip_config
 HAL Audio IP specific feature configuration. More...
 
struct  _hal_audio_config
 HAL Audio configuration structure. More...
 
struct  _hal_audio_transfer
 HAL Audio transfer structure. More...
 

Macros

#define HAL_AUDIO_HANDLE_SIZE   (HAL_AUDIO_HANDLE_SIZE_TEMP)
 Definition of audio adapter handle size. More...
 
#define HAL_AUDIO_HANDLE_DEFINE(name)   uint32_t name[(HAL_AUDIO_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t)]
 Defines the Audio handle. More...
 

Typedefs

typedef enum _hal_AUDIO_status hal_audio_status_t
 HAL Audio status. More...
 
typedef enum _hal_audio_channel hal_audio_channel_t
 HAL Audio channel number.
 
typedef enum _hal_audio_sample_rate hal_audio_sample_rate_t
 HAL Audio sample rate.
 
typedef enum _hal_audio_bit_width hal_audio_bit_width_t
 HAL Audio bit width.
 
typedef enum
_hal_audio_bclk_polarity 
hal_audio_bclk_polarity_t
 HAL Audio bit clock polarity.
 
typedef enum
_hal_audio_frame_sync_width 
hal_audio_frame_sync_width_t
 HAL Audio frame sync width.
 
typedef enum
_hal_audio_frame_sync_polarity 
hal_audio_frame_sync_polarity_t
 HAL Audio frame sync polarity.
 
typedef enum
_hal_audio_master_slave 
hal_audio_master_slave_t
 HAL Audio master or slave mode.
 
typedef enum
_hal_audio_sai_sync_mode 
hal_audio_sai_sync_mode_t
 Synchronous or asynchronous mode, only for SAI configuration.
 
typedef enum _hal_audio_data_format hal_audio_data_format_t
 HAL Audio data format.
 
typedef enum
_hal_audio_dma_channel_priority 
hal_audio_dma_channel_priority_t
 HAL Audio DMA channel priority.
 
typedef struct
_hal_audio_dma_mux_config_t 
hal_audio_dma_mux_config_t
 HAL Audio DMA mux user configuration.
 
typedef struct
_hal_audio_dma_channel_mux_config_t 
hal_audio_dma_channel_mux_config_t
 HAL Audio DMA channel mux user configuration.
 
typedef struct
_hal_audio_dma_extra_config_t 
hal_audio_dma_extra_config_t
 HAL Audio DMA extra user configuration.
 
typedef struct
_hal_audio_dma_config 
hal_audio_dma_config_t
 HAL Audio DMA user configuration.
 
typedef struct _hal_audio_ip_config hal_audio_ip_config_t
 HAL Audio IP specific feature configuration.
 
typedef struct _hal_audio_config hal_audio_config_t
 HAL Audio configuration structure. More...
 
typedef struct _hal_audio_transfer hal_audio_transfer_t
 HAL Audio transfer structure. More...
 
typedef void * hal_audio_handle_t
 HAL Audio transfer handle. More...
 
typedef void(* hal_audio_transfer_callback_t )(hal_audio_handle_t handle, hal_audio_status_t completionStatus, void *callbackParam)
 HAL Audio completion callback function pointer type. More...
 

Enumerations

enum  _hal_AUDIO_status {
  kStatus_HAL_AudioSuccess = kStatus_Success,
  kStatus_HAL_AudioError = MAKE_STATUS(kStatusGroup_HAL_I2S, 1),
  kStatus_HAL_AudioBusy = MAKE_STATUS(kStatusGroup_HAL_I2S, 2),
  kStatus_HAL_AudioIdle = MAKE_STATUS(kStatusGroup_HAL_I2S, 3),
  kStatus_HAL_AudioQueueFull = MAKE_STATUS(kStatusGroup_HAL_I2S, 4)
}
 HAL Audio status. More...
 
enum  _hal_audio_channel {
  kHAL_AudioMono = 0x7FU,
  kHAL_AudioMonoRight = 0x0U,
  kHAL_AudioMonoLeft,
  kHAL_AudioStereo,
  kHAL_AudioStereo3Channel,
  kHAL_AudioStereo4Channel,
  kHAL_AudioStereo5Channel,
  kHAL_AudioStereo6Channel,
  kHAL_AudioStereo7Channel,
  kHAL_AudioStereo8Channel,
  kHAL_AudioStereo9Channel,
  kHAL_AudioStereo10Channel,
  kHAL_AudioStereo11Channel,
  kHAL_AudioStereo12Channel,
  kHAL_AudioStereo13Channel,
  kHAL_AudioStereo14Channel,
  kHAL_AudioStereo15Channel,
  kHAL_AudioStereo16Channel
}
 HAL Audio channel number. More...
 
enum  _hal_audio_sample_rate {
  kHAL_AudioSampleRate8KHz = 8000U,
  kHAL_AudioSampleRate11025Hz = 11025U,
  kHAL_AudioSampleRate12KHz = 12000U,
  kHAL_AudioSampleRate16KHz = 16000U,
  kHAL_AudioSampleRate22050Hz = 22050U,
  kHAL_AudioSampleRate24KHz = 24000U,
  kHAL_AudioSampleRate32KHz = 32000U,
  kHAL_AudioSampleRate44100Hz = 44100U,
  kHAL_AudioSampleRate48KHz = 48000U,
  kHAL_AudioSampleRate96KHz = 96000U,
  kHAL_AudioSampleRate192KHz = 192000U,
  kHAL_AudioSampleRate384KHz = 384000U
}
 HAL Audio sample rate. More...
 
enum  _hal_audio_bit_width {
  kHAL_AudioWordWidth8bits = 8U,
  kHAL_AudioWordWidth16bits = 16U,
  kHAL_AudioWordWidth24bits = 24U,
  kHAL_AudioWordWidth32bits = 32U
}
 HAL Audio bit width. More...
 
enum  _hal_audio_bclk_polarity {
  kHAL_AudioSampleOnFallingEdge = 0x00U,
  kHAL_AudioSampleOnRisingEdge
}
 HAL Audio bit clock polarity. More...
 
enum  _hal_audio_frame_sync_width {
  kHAL_AudioFrameSyncWidthOneBitClk = 0x00U,
  kHAL_AudioFrameSyncWidthPerWordWidth,
  kHAL_AudioFrameSyncWidthHalfFrame
}
 HAL Audio frame sync width. More...
 
enum  _hal_audio_frame_sync_polarity {
  kHAL_AudioBeginAtRisingEdge = 0x00U,
  kHAL_AudioBeginAtFallingEdge
}
 HAL Audio frame sync polarity. More...
 
enum  _hal_audio_master_slave {
  kHAL_AudioMaster = 0x0U,
  kHAL_AudioSlave,
  kHAL_AudioBclkMasterFrameSyncSlave,
  kHAL_AudioBclkSlaveFrameSyncMaster
}
 HAL Audio master or slave mode. More...
 
enum  _hal_audio_sai_sync_mode {
  kHAL_AudioSaiModeAsync = 0x0U,
  kHAL_AudioSaiModeSync
}
 Synchronous or asynchronous mode, only for SAI configuration. More...
 
enum  _hal_audio_data_format {
  kHAL_AudioDataFormatI2sClassic = 0x0U,
  kHAL_AudioDataFormatLeftJustified,
  kHAL_AudioDataFormatRightJustified,
  kHAL_AudioDataFormatDspModeA,
  kHAL_AudioDataFormatDspModeB
}
 HAL Audio data format. More...
 
enum  _hal_audio_dma_channel_priority { , kHAL_AudioDmaChannelPriorityDefault = 0xFFU }
 HAL Audio DMA channel priority. More...
 

Initialization and de-initialization

hal_audio_status_t HAL_AudioTxInit (hal_audio_handle_t handle, const hal_audio_config_t *config)
 Initializes the HAL Audio peripheral. More...
 
hal_audio_status_t HAL_AudioRxInit (hal_audio_handle_t handle, const hal_audio_config_t *config)
 Initializes the HAL Audio peripheral. More...
 
hal_audio_status_t HAL_AudioTxDeinit (hal_audio_handle_t handle)
 De-initializes the HAL Audio peripheral. More...
 
hal_audio_status_t HAL_AudioRxDeinit (hal_audio_handle_t handle)
 De-initializes the HAL Audio peripheral. More...
 

Transactional

hal_audio_status_t HAL_AudioTxInstallCallback (hal_audio_handle_t handle, hal_audio_transfer_callback_t callback, void *callbackParam)
 Installs a callback and callback parameter. More...
 
hal_audio_status_t HAL_AudioRxInstallCallback (hal_audio_handle_t handle, hal_audio_transfer_callback_t callback, void *callbackParam)
 Installs a callback and callback parameter. More...
 
hal_audio_status_t HAL_AudioTransferSendNonBlocking (hal_audio_handle_t handle, hal_audio_transfer_t *xfer)
 Performs a DMA non-blocking send on the data bus. More...
 
hal_audio_status_t HAL_AudioTransferReceiveNonBlocking (hal_audio_handle_t handle, hal_audio_transfer_t *xfer)
 Performs a DMA non-blocking receive on the HAL Audio bus. More...
 
hal_audio_status_t HAL_AudioTransferAbortSend (hal_audio_handle_t handle)
 Aborts a DMA non-blocking transfer early. More...
 
hal_audio_status_t HAL_AudioTransferAbortReceive (hal_audio_handle_t handle)
 Aborts a DMA non-blocking transfer early. More...
 
hal_audio_status_t HAL_AudioTransferGetSendCount (hal_audio_handle_t handle, size_t *count)
 Gets the tx transfer status during a DMA non-blocking transfer. More...
 
hal_audio_status_t HAL_AudioTransferGetReceiveCount (hal_audio_handle_t handle, size_t *count)
 Gets the rx transfer status during a DMA non-blocking transfer. More...
 

Data Structure Documentation

struct _hal_audio_dma_mux_config_t
struct _hal_audio_dma_channel_mux_config_t
struct _hal_audio_dma_extra_config_t
struct _hal_audio_dma_config

Data Fields

uint8_t instance
 DMA instance.
 
uint8_t channel
 DMA channel.
 
hal_audio_dma_channel_priority_t priority
 DMA channel priority.
 
bool enablePreemption
 If true, a channel can be suspended by other channel with higher priority. More...
 
bool enablePreemptAbility
 If true, a channel can suspend other channel with low priority Not all SOCs support this feature. More...
 
void * dmaMuxConfig
 The pointer points to an entity defined by hal_audio_dma_mux_config_t. More...
 
void * dmaChannelMuxConfig
 The pointer points to an entity defined by hal_audio_dma_channel_mux_config_t. More...
 
void * dmaChannelConfig
 The pointer points to an entity defined by channel configuration structure that is defined in dma driver, such as edma_channel_config_t. More...
 
void * dmaExtraConfig
 The pointer points to an entity defined by hal_audio_dma_extra_config_t. More...
 

Field Documentation

bool _hal_audio_dma_config::enablePreemption

Not all SOCs support this feature. For example, EDMA, DMA4 supports this feature. For detailed information please refer to the SOC corresponding RM. If not supported, the value should be set to false.

bool _hal_audio_dma_config::enablePreemptAbility

For example, EDMA, DMA4 supports this feature. For detailed information please refer to the SOC corresponding RM. If not supported, the value should be set to false.

void* _hal_audio_dma_config::dmaMuxConfig

Not all SOCs support this feature. In general, when the macro FSL_FEATURE_SOC_DMAMUX_COUNT is defined as non-zero, the SOC supports this feature. For detailed information please refer to the SOC corresponding RM. If not supported, the pointer should be set to NULL.

void* _hal_audio_dma_config::dmaChannelMuxConfig

Not all SOCs support this feature. In general, when the macro FSL_FEATURE_EDMA_HAS_CHANNEL_MUX is defined as non-zero, the SOC supports this feature. For detailed information please refer to the SOC corresponding RM. If not supported, the pointer should be set to NULL.

void* _hal_audio_dma_config::dmaChannelConfig

Not all SOCs support this feature. In general, when the macro FSL_FEATURE_EDMA_HAS_CHANNEL_CONFIG is defined as non-zero, the SOC supports this feature. For detailed information please refer to the SOC corresponding RM. If not supported, the pointer should be set to NULL.

void* _hal_audio_dma_config::dmaExtraConfig

Some DMA IPs have extra configurations, such as EDMA, DMA4. The structure is used for these extra configurations. Not all SOCs support this feature. For detailed information please refer to the SOC corresponding RM. If not supported, the pointer should be set to NULL.

struct _hal_audio_ip_config

Field Documentation

uint32_t _hal_audio_ip_config::lineMask

lineMask = 0x1U, represents RX0/TX0 data line is enabled. lineMask = 0xFU, represents RX0-3/TX0-3 data line are enabled.

struct _hal_audio_config

Data Fields

hal_audio_dma_config_t * dmaConfig
 DMA configuration.
 
void * ipConfig
 IP specific feature configuration. More...
 
uint32_t srcClock_Hz
 Source clock.
 
uint32_t sampleRate_Hz
 Sample rate.
 
uint16_t frameLength
 Only flexcomm_i2s uses this field. More...
 
uint16_t fifoWatermark
 FIFO watermark value. More...
 
hal_audio_master_slave_t masterSlave
 master or slave, configure where the bclk and frame sync come from. More...
 
hal_audio_bclk_polarity_t bclkPolarity
 bclk polarity, data sample on rising edge or falling edge. More...
 
hal_audio_frame_sync_width_t frameSyncWidth
 Only DSP mode uses this field. More...
 
hal_audio_frame_sync_polarity_t frameSyncPolarity
 frame sync polarity, frame sync begin at rising or falling edge. More...
 
hal_audio_channel_t lineChannels
 Configure the number of channel on the data line. More...
 
hal_audio_data_format_t dataFormat
 data format on bus
 
uint8_t bitWidth
 Bit Width.
 
uint8_t instance
 Instance (0 - I2S0/SAI0, 1 - I2S1/SAI1, ...), for detailed information please refer to the SOC corresponding RM. More...
 

Field Documentation

void* _hal_audio_config::ipConfig

The pointer points to an entity defined by hal_audio_ip_config_t. If there is no specific feature configuration, it should be set to NULL.

uint16_t _hal_audio_config::frameLength

In most cases, frameLength is equal to bitWidth times lineChannels. In some cases, frameLength needs to be set to other value. For example, when the number of bit clock on the bus between two neighboring WS value is greater than bitWidth times lineChannels, frameLength needs to be set to the value that is equal to the number of bit clock between two neighboring WS signal. SAI does not use this field because frameLength can be determined internally by bitWidth and lineChannels.

uint16_t _hal_audio_config::fifoWatermark

Generally, the value is set to half the number of FIFO(F). Note that the receive(R) or transmit length(T) is related to fifoWatermark(W) and bitWidth(B). The relationship between them is: R = N * W * B, T = N * (F - W) * B (N is integer). On some SOCs, the W and (F - W) is constant 1 and setting the W does not take effect. In that case the fifoWatermark does not need to be set. If the value set by application is greater than the number of FIFO, a maximum value will be used. For example, if the number of FIFO is 32 on a SOC but the watermark is set to 64 by application, the real value that is written to register will be 31.

hal_audio_master_slave_t _hal_audio_config::masterSlave
hal_audio_bclk_polarity_t _hal_audio_config::bclkPolarity
hal_audio_frame_sync_width_t _hal_audio_config::frameSyncWidth

For other data format, this field does not need to be set and the frameSyncWidth is determined internally that depends on different mode. For example, for I2S classic mode, frameSyncWidth is equal to bitWidth.

hal_audio_frame_sync_polarity_t _hal_audio_config::frameSyncPolarity

This field is not used now and reserved for future use. The frameSyncPolarity is set internally that depends on different mode. For example, for I2S classic mode, frameSyncWidth is equal to kHAL_AudioBeginAtFallingEdge.

hal_audio_channel_t _hal_audio_config::lineChannels
uint8_t _hal_audio_config::instance

Invalid instance value will cause initialization failure.

struct _hal_audio_transfer

Data Fields

uint8_t * data
 A transfer buffer. More...
 
size_t dataSize
 A transfer size. More...
 

Field Documentation

uint8_t* _hal_audio_transfer::data
size_t _hal_audio_transfer::dataSize

Macro Definition Documentation

#define HAL_AUDIO_HANDLE_SIZE   (HAL_AUDIO_HANDLE_SIZE_TEMP)
#define HAL_AUDIO_HANDLE_DEFINE (   name)    uint32_t name[(HAL_AUDIO_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t)]

This macro is used to define a 4 byte aligned Audio handle. Then use "(hal_audio_handle_t)name" to get the Audio handle.

The macro should be global and could be optional. You could also define Audio handle by yourself.

This is an example,

* HAL_AUDIO_HANDLE_DEFINE(audioTxHandle);
*
Parameters
nameThe name string of the Audio transfer handle.

Typedef Documentation

typedef void* hal_audio_handle_t
typedef void(* hal_audio_transfer_callback_t)(hal_audio_handle_t handle, hal_audio_status_t completionStatus, void *callbackParam)

This callback is used only for the non-blocking Audio transfer API. Specify the callback you wish to use in the call to HAL_AudioTxInstallCallback() or HAL_AudioRxInstallCallback().

Parameters
handleaudio transfer handle pointer, this should be a static variable.
completionStatusEither kStatus_HAL_AudioIdle or an error code describing how the transfer completed.
callbackParamArbitrary pointer-sized value passed from the application.

Enumeration Type Documentation

Enumerator
kStatus_HAL_AudioSuccess 

Successfully.

kStatus_HAL_AudioError 

Error occurs on HAL Audio.

kStatus_HAL_AudioBusy 

HAL Audio is busy with current transfer.

kStatus_HAL_AudioIdle 

HAL Audio transmitter is idle.

kStatus_HAL_AudioQueueFull 

Transfer queue is full.

Enumerator
kHAL_AudioMono 

Only one channel on bus.

kHAL_AudioMonoRight 

Only Right channel have sound.

kHAL_AudioMonoLeft 

Only left channel have sound.

kHAL_AudioStereo 

Stereo sound.

kHAL_AudioStereo3Channel 

Stereo 3 channel sound.

kHAL_AudioStereo4Channel 

Stereo 4 channel sound.

kHAL_AudioStereo5Channel 

Stereo 5 channel sound.

kHAL_AudioStereo6Channel 

Stereo 6 channel sound.

kHAL_AudioStereo7Channel 

Stereo 7 channel sound.

kHAL_AudioStereo8Channel 

Stereo 8 channel sound.

kHAL_AudioStereo9Channel 

Stereo 9 channel sound.

kHAL_AudioStereo10Channel 

Stereo 10 channel sound.

kHAL_AudioStereo11Channel 

Stereo 11 channel sound.

kHAL_AudioStereo12Channel 

Stereo 12 channel sound.

kHAL_AudioStereo13Channel 

Stereo 13 channel sound.

kHAL_AudioStereo14Channel 

Stereo 14 channel sound.

kHAL_AudioStereo15Channel 

Stereo 15 channel sound.

kHAL_AudioStereo16Channel 

Stereo 16 channel sound.

Enumerator
kHAL_AudioSampleRate8KHz 

Sample rate 8000 Hz.

kHAL_AudioSampleRate11025Hz 

Sample rate 11025 Hz.

kHAL_AudioSampleRate12KHz 

Sample rate 12000 Hz.

kHAL_AudioSampleRate16KHz 

Sample rate 16000 Hz.

kHAL_AudioSampleRate22050Hz 

Sample rate 22050 Hz.

kHAL_AudioSampleRate24KHz 

Sample rate 24000 Hz.

kHAL_AudioSampleRate32KHz 

Sample rate 32000 Hz.

kHAL_AudioSampleRate44100Hz 

Sample rate 44100 Hz.

kHAL_AudioSampleRate48KHz 

Sample rate 48000 Hz.

kHAL_AudioSampleRate96KHz 

Sample rate 96000 Hz.

kHAL_AudioSampleRate192KHz 

Sample rate 192000 Hz.

kHAL_AudioSampleRate384KHz 

Sample rate 384000 Hz.

Enumerator
kHAL_AudioWordWidth8bits 

Audio data width 8 bits.

kHAL_AudioWordWidth16bits 

Audio data width 16 bits.

kHAL_AudioWordWidth24bits 

Audio data width 24 bits.

kHAL_AudioWordWidth32bits 

Audio data width 32 bits.

Enumerator
kHAL_AudioSampleOnFallingEdge 

Data samples at the falling edge.

kHAL_AudioSampleOnRisingEdge 

Data samples at the rising edge.

Enumerator
kHAL_AudioFrameSyncWidthOneBitClk 

1 bit clock frame sync len for DSP mode

kHAL_AudioFrameSyncWidthPerWordWidth 

Frame sync length decided by word width.

kHAL_AudioFrameSyncWidthHalfFrame 

Frame sync length is half of frame length.

Enumerator
kHAL_AudioBeginAtRisingEdge 

Frame sync begins at the rising edge.

kHAL_AudioBeginAtFallingEdge 

Frame sync begins at the falling edge.

Enumerator
kHAL_AudioMaster 

Master mode include bclk and frame sync.

kHAL_AudioSlave 

Slave mode include bclk and frame sync.

kHAL_AudioBclkMasterFrameSyncSlave 

BCLK in master mode, frame sync in slave mode.

kHAL_AudioBclkSlaveFrameSyncMaster 

BCLK in slave mode, frame sync in master mode.

Enumerator
kHAL_AudioSaiModeAsync 

Asynchronous mode.

kHAL_AudioSaiModeSync 

Synchronous mode (with receiver or transmit)

Enumerator
kHAL_AudioDataFormatI2sClassic 

I2S classic mode.

kHAL_AudioDataFormatLeftJustified 

Left-Justified mode.

kHAL_AudioDataFormatRightJustified 

Right-Justified mode.

kHAL_AudioDataFormatDspModeA 

DSP mode A, channel is available on 2nd rising edge of BCLK following a rising edge of frame sync.

kHAL_AudioDataFormatDspModeB 

DSP mode B, channel is available on 1st rising edge of BCLK following a rising edge of frame sync.

Enumerator
kHAL_AudioDmaChannelPriorityDefault 

Use default value, not to configure priority.

Function Documentation

hal_audio_status_t HAL_AudioTxInit ( hal_audio_handle_t  handle,
const hal_audio_config_t *  config 
)
Note
This API should be called at the beginning of the application. Otherwise, any operation to the HAL Audio module can cause a hard fault because the clock is not enabled. This function configures the audio with user-defined settings. The user can configure the configuration structure. The parameter handle is a pointer to point to a memory space of size HAL_AUDIO_HANDLE_SIZE allocated by the caller.
DMA will be initialized and enabled by default in this function and calling HAL_AudioTransferSendNonBlocking or HAL_AudioTransferReceiveNonBlocking will use DMA to transfer data. Thus application should avoid initializing DMA repeatedly and dmaConfig should be configured.

Example below shows how to use this API to configure the audio peripheral. For SAI,

* HAL_AUDIO_HANDLE_DEFINE(audioTxHandle);
* hal_audio_config_t audioConfig;
* dmaMuxConfig.dmaMuxConfig.dmaMuxInstance = 0;
* dmaMuxConfig.dmaMuxConfig.dmaRequestSource = (uint32_t)kDmaRequestMuxSai1Tx;
* dmaConfig.instance = 0;
* dmaConfig.channel = 0;
* dmaConfig.enablePreemption = false;
* dmaConfig.enablePreemptAbility = false;
* dmaConfig.dmaMuxConfig = &dmaMuxConfig;
* dmaConfig.dmaChannelMuxConfig = NULL;
* ipConfig.sai.lineMask = 1U << 0U;
* ipConfig.sai.syncMode = kHAL_AudioSaiModeAsync;
* audioConfig.dmaConfig = &dmaConfig;
* audioConfig.ipConfig = &ipConfig;
* audioConfig.srcClock_Hz = 24576000;
* audioConfig.sampleRate_Hz = (uint32_t)kHAL_AudioSampleRate48KHz;
* audioConfig.fifoWatermark = 16;
* audioConfig.masterSlave = kHAL_AudioMaster;
* audioConfig.bitWidth = (uint8_t)kHAL_AudioWordWidth16bits;
* audioConfig.instance = 0U;
* HAL_AudioTxInit((hal_audio_handle_t)audioTxHandle, &audioConfig);
*

For I2S,

* HAL_AUDIO_HANDLE_DEFINE(audioTxHandle);
* hal_audio_config_t audioConfig;
* dmaConfig.instance = 0;
* dmaConfig.channel = 0;
* dmaConfig.enablePreemption = false;
* dmaConfig.enablePreemptAbility = false;
* dmaConfig.dmaMuxConfig = NULL;
* dmaConfig.dmaChannelMuxConfig = NULL;
* audioConfig.dmaConfig = &dmaConfig;
* audioConfig.ipConfig = NULL;
* audioConfig.srcClock_Hz = 24576000;
* audioConfig.sampleRate_Hz = (uint32_t)kHAL_AudioSampleRate48KHz;
* audioConfig.fifoWatermark = 0;
* audioConfig.masterSlave = kHAL_AudioMaster;
* audioConfig.bitWidth = (uint8_t)kHAL_AudioWordWidth16bits;
* audioConfig.instance = 0U;
* HAL_AudioTxInit((hal_audio_handle_t)audioTxHandle, &audioConfig);
*
Parameters
handlePointer to point to a memory space of size HAL_AUDIO_HANDLE_SIZE allocated by the caller. The handle should be 4 byte aligned, because unaligned access doesn't be supported on some devices. You can define the handle in the following two ways: HAL_AUDIO_HANDLE_DEFINE(handle); or uint32_t handle[((HAL_AUDIO_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))];
configA pointer to the audio configuration structure
Return values
kStatus_HAL_AudioSuccessaudio initialization succeed
hal_audio_status_t HAL_AudioRxInit ( hal_audio_handle_t  handle,
const hal_audio_config_t *  config 
)
Note
This API should be called at the beginning of the application. Otherwise, any operation to the HAL Audio module can cause a hard fault because the clock is not enabled. This function configures the audio with user-defined settings. The user can configure the configuration structure. The parameter handle is a pointer to point to a memory space of size HAL_AUDIO_HANDLE_SIZE allocated by the caller.
DMA will be initialized and enabled by default in this function and calling HAL_AudioTransferSendNonBlocking or HAL_AudioTransferReceiveNonBlocking will use DMA to transfer data. Thus application should avoid initializing DMA repeatedly and dmaConfig should be configured.

Example below shows how to use this API to configure the audio peripheral. For SAI,

* HAL_AUDIO_HANDLE_DEFINE(audioRxHandle);
* hal_audio_config_t audioConfig;
* dmaMuxConfig.dmaMuxConfig.dmaMuxInstance = 0;
* dmaMuxConfig.dmaMuxConfig.dmaRequestSource = (uint32_t)kDmaRequestMuxSai1Rx;
* dmaConfig.instance = 0;
* dmaConfig.channel = 0;
* dmaConfig.enablePreemption = false;
* dmaConfig.enablePreemptAbility = false;
* dmaConfig.dmaMuxConfig = &dmaMuxConfig;
* dmaConfig.dmaChannelMuxConfig = NULL;
* ipConfig.sai.lineMask = 1U << 0U;
* ipConfig.sai.syncMode = kHAL_AudioSaiModeAsync;
* audioConfig.dmaConfig = &dmaConfig;
* audioConfig.ipConfig = &ipConfig;
* audioConfig.srcClock_Hz = 24576000;
* audioConfig.sampleRate_Hz = (uint32_t)kHAL_AudioSampleRate48KHz;
* audioConfig.fifoWatermark = 16;
* audioConfig.masterSlave = kHAL_AudioMaster;
* audioConfig.bitWidth = (uint8_t)kHAL_AudioWordWidth16bits;
* audioConfig.instance = 0U;
* HAL_AudioRxInit((hal_audio_handle_t)audioRxHandle, &audioConfig);
*

For I2S,

* HAL_AUDIO_HANDLE_DEFINE(audioRxHandle);
* hal_audio_config_t audioConfig;
* dmaConfig.instance = 0;
* dmaConfig.channel = 0;
* dmaConfig.enablePreemption = false;
* dmaConfig.enablePreemptAbility = false;
* dmaConfig.dmaMuxConfig = NULL;
* dmaConfig.dmaChannelMuxConfig = NULL;
* audioConfig.dmaConfig = &dmaConfig;
* audioConfig.ipConfig = NULL;
* audioConfig.srcClock_Hz = 24576000;
* audioConfig.sampleRate_Hz = (uint32_t)kHAL_AudioSampleRate48KHz;
* audioConfig.fifoWatermark = 0;
* audioConfig.masterSlave = kHAL_AudioMaster;
* audioConfig.bitWidth = (uint8_t)kHAL_AudioWordWidth16bits;
* audioConfig.instance = 0U;
* HAL_AudioRxInit((hal_audio_handle_t)audioRxHandle, &audioConfig);
*
Parameters
handlePointer to point to a memory space of size HAL_AUDIO_HANDLE_SIZE allocated by the caller. The handle should be 4 byte aligned, because unaligned access doesn't be supported on some devices. You can define the handle in the following two ways: HAL_AUDIO_HANDLE_DEFINE(handle); or uint32_t handle[((HAL_AUDIO_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))];
configA pointer to the audio configuration structure
Return values
kStatus_HAL_AudioSuccessaudio initialization succeed
hal_audio_status_t HAL_AudioTxDeinit ( hal_audio_handle_t  handle)

Call this API to gate the HAL Audio clock. The HAL Audio module can't work unless the HAL_AudioTxInit is called.

Parameters
handleaudio handle pointer, this should be a static variable.
Return values
kStatus_HAL_AudioSuccessaudio de-initialization succeed
hal_audio_status_t HAL_AudioRxDeinit ( hal_audio_handle_t  handle)

Call this API to gate the HAL Audio clock. The HAL Audio module can't work unless the HAL_AudioRxInit is called.

Parameters
handleaudio handle pointer, this should be a static variable.
Return values
kStatus_HAL_AudioSuccessaudio de-initialization succeed
hal_audio_status_t HAL_AudioTxInstallCallback ( hal_audio_handle_t  handle,
hal_audio_transfer_callback_t  callback,
void *  callbackParam 
)

This function is used to install the callback and callback parameter for audio module. When any status of the audio changed, the driver will notify the upper layer by the installed callback function. And the status is also passed as status parameter when the callback is called.

Parameters
handleaudio handle pointer, this should be a static variable.
callbackpointer to user callback function.
callbackParamuser parameter passed to the callback function.
Return values
kStatus_HAL_AudioSuccessaudio tx transfer handle created
hal_audio_status_t HAL_AudioRxInstallCallback ( hal_audio_handle_t  handle,
hal_audio_transfer_callback_t  callback,
void *  callbackParam 
)

This function is used to install the callback and callback parameter for audio module. When any status of the audio changed, the driver will notify the upper layer by the installed callback function. And the status is also passed as status parameter when the callback is called.

Parameters
handleaudio handle pointer, this should be a static variable.
callbackpointer to user callback function.
callbackParamuser parameter passed to the callback function.
Return values
kStatus_HAL_AudioSuccessaudio rx transfer handle created
hal_audio_status_t HAL_AudioTransferSendNonBlocking ( hal_audio_handle_t  handle,
hal_audio_transfer_t *  xfer 
)
Note
Calling the API returns immediately after transfer initiates. The user can call HAL_AudioTransferGetSendCount to poll the transfer status to check whether the transfer is finished. If the return status is kStatus_HAL_AudioIdle, the transfer is finished.
Parameters
handleaudio handle pointer, this should be a static variable.
xferpointer to hal_audio_transfer_t structure.
Note
The transmit length(T) is related to fifoWatermark(W), bitWidth(B) and the number of FIFO(F). The relationship between them is: T = N * (F - W) * B (N is integer).
Return values
kStatus_HAL_AudioSuccessSuccessfully start the data transmission.
kStatus_HAL_AudioBusyPrevious transmission still not finished.
kStatus_HAL_AudioErrorAn error occurred.
hal_audio_status_t HAL_AudioTransferReceiveNonBlocking ( hal_audio_handle_t  handle,
hal_audio_transfer_t *  xfer 
)
Note
Calling the API returns immediately after transfer initiates. The user can call HAL_AudioTransferGetReceiveCount to poll the transfer status to check whether the transfer is finished. If the return status is kStatus_HAL_AudioIdle, the transfer is finished.
Parameters
handleaudio handle pointer, this should be a static variable.
xferpointer to hal_audio_transfer_t structure.
Note
The receive length(R) is related to fifoWatermark(W), bitWidth(B) and the number of FIFO(F). The relationship between them is: R = N * W * B (N is integer).
Return values
kStatus_HAL_AudioSuccessSuccessfully start the data transmission.
kStatus_HAL_AudioBusyPrevious transmission still not finished.
kStatus_HAL_AudioErrorAn error occurred.
hal_audio_status_t HAL_AudioTransferAbortSend ( hal_audio_handle_t  handle)
Note
This API can be called at any time when a DMA non-blocking transfer initiates to abort the transfer early.
Parameters
handleaudio handle pointer, this should be a static variable.
Return values
kStatus_HAL_AudioSuccessSuccessfully abort the transfer.
hal_audio_status_t HAL_AudioTransferAbortReceive ( hal_audio_handle_t  handle)
Note
This API can be called at any time when a DMA non-blocking transfer initiates to abort the transfer early.
Parameters
handleaudio handle pointer, this should be a static variable.
Return values
kStatus_HAL_AudioSuccessSuccessfully abort the transfer.
hal_audio_status_t HAL_AudioTransferGetSendCount ( hal_audio_handle_t  handle,
size_t *  count 
)
Parameters
handleaudio handle pointer, this should be a static variable.
countNumber of bytes sent so far by the non-blocking transaction.
Return values
kStatus_HAL_AudioSuccessSuccessfully return the count.
kStatus_HAL_AudioIdlePrevious transmission has been finished.
kStatus_HAL_AudioErrorAn error occurred.
hal_audio_status_t HAL_AudioTransferGetReceiveCount ( hal_audio_handle_t  handle,
size_t *  count 
)
Parameters
handleaudio handle pointer, this should be a static variable.
countNumber of bytes received so far by the non-blocking transaction.
Return values
kStatus_HAL_AudioSuccessSuccessfully return the count.
kStatus_HAL_AudioIdlePrevious transmission has been finished.
kStatus_HAL_AudioErrorAn error occurred.