MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
CACHE: CACHE Memory Controller

Overview

The MCUXpresso SDK provides a peripheral driver for the CACHE Controller of MCUXpresso SDK devices.

The CACHE driver is created to help the user more easily operate the cache memory. The APIs for basic operations are including the following three levels: 1L. The local cache driver API. This level provides the caches controller drivers.

2L. The unified cache driver API. This level provides many APIs for unified cache driver APIs for combined L1 and L2 cache maintain operations. This is provided for SDK drivers (DMA, ENET, USDHC, etc) which should do the cache maintenance in their transactional APIs. Because in this arch, there is no L2 cache so the unified cache driver API directly calls local driver APIs.

Function groups

CACHE Operation

There are Enable/Disable APIs for cache control and cache maintenance operations as Invalidate/Clean/CleanInvalidate by all and by address range.

Data Structures

struct  _cache64_config
 CACHE64 configuration structure. More...
 

Macros

#define CACHE64_LINESIZE_BYTE   (FSL_FEATURE_CACHE64_CTRL_LINESIZE_BYTE)
 cache line size. More...
 
#define CACHE64_REGION_NUM   (3U)
 cache region number. More...
 
#define CACHE64_REGION_ALIGNMENT   (0x400U)
 cache region alignment. More...
 

Typedefs

typedef enum _cache64_policy cache64_policy_t
 Level 2 cache controller way size. More...
 
typedef struct _cache64_config cache64_config_t
 CACHE64 configuration structure. More...
 

Enumerations

enum  _cache64_policy {
  kCACHE64_PolicyNonCacheable = 0,
  kCACHE64_PolicyWriteThrough = 1,
  kCACHE64_PolicyWriteBack = 2
}
 Level 2 cache controller way size. More...
 

Driver version

#define FSL_CACHE_DRIVER_VERSION   (MAKE_VERSION(2, 0, 7))
 cache driver version. More...
 

cache control for cache64

uint32_t CACHE64_GetInstance (CACHE64_POLSEL_Type *base)
 Returns an instance number given periphearl base address. More...
 
uint32_t CACHE64_GetInstanceByAddr (uint32_t address)
 brief Returns an instance number given physical memory address. More...
 
status_t CACHE64_Init (CACHE64_POLSEL_Type *base, const cache64_config_t *config)
 Initializes an CACHE64 instance with the user configuration structure. More...
 
void CACHE64_GetDefaultConfig (cache64_config_t *config)
 Gets the default configuration structure. More...
 
void CACHE64_EnableCache (CACHE64_CTRL_Type *base)
 Enables the cache. More...
 
void CACHE64_DisableCache (CACHE64_CTRL_Type *base)
 Disables the cache. More...
 
void CACHE64_InvalidateCache (CACHE64_CTRL_Type *base)
 Invalidates the cache. More...
 
void CACHE64_InvalidateCacheByRange (uint32_t address, uint32_t size_byte)
 Invalidates cache by range. More...
 
void CACHE64_CleanCache (CACHE64_CTRL_Type *base)
 Cleans the cache. More...
 
void CACHE64_CleanCacheByRange (uint32_t address, uint32_t size_byte)
 Cleans cache by range. More...
 
void CACHE64_CleanInvalidateCache (CACHE64_CTRL_Type *base)
 Cleans and invalidates the cache. More...
 
void CACHE64_CleanInvalidateCacheByRange (uint32_t address, uint32_t size_byte)
 Cleans and invalidate cache by range. More...
 
void CACHE64_EnableWriteBuffer (CACHE64_CTRL_Type *base, bool enable)
 Enables/disables the write buffer. More...
 

Unified Cache Control for all caches

static void ICACHE_InvalidateByRange (uint32_t address, uint32_t size_byte)
 Invalidates instruction cache by range. More...
 
static void DCACHE_InvalidateByRange (uint32_t address, uint32_t size_byte)
 Invalidates data cache by range. More...
 
static void DCACHE_CleanByRange (uint32_t address, uint32_t size_byte)
 Clean data cache by range. More...
 
static void DCACHE_CleanInvalidateByRange (uint32_t address, uint32_t size_byte)
 Cleans and Invalidates data cache by range. More...
 

Data Structure Documentation

struct _cache64_config

Data Fields

uint32_t boundaryAddr [CACHE64_REGION_NUM-1]
 < The cache controller can divide whole memory into 3 regions. More...
 

Field Documentation

uint32_t _cache64_config::boundaryAddr[CACHE64_REGION_NUM-1]

Boundary address is the FlexSPI internal address (start from 0) instead of system address (start from FlexSPI AMBA base) to split adjacent regions and must be 1KB aligned. The boundary address itself locates in upper region. Cacheable policy for each region.

Macro Definition Documentation

#define FSL_CACHE_DRIVER_VERSION   (MAKE_VERSION(2, 0, 7))
#define CACHE64_LINESIZE_BYTE   (FSL_FEATURE_CACHE64_CTRL_LINESIZE_BYTE)
#define CACHE64_REGION_NUM   (3U)
#define CACHE64_REGION_ALIGNMENT   (0x400U)

Typedef Documentation

Enumeration Type Documentation

Enumerator
kCACHE64_PolicyNonCacheable 

Non-cacheable.

kCACHE64_PolicyWriteThrough 

Write through.

kCACHE64_PolicyWriteBack 

Write back.

Function Documentation

uint32_t CACHE64_GetInstance ( CACHE64_POLSEL_Type *  base)
Parameters
baseThe peripheral base address.
Returns
CACHE64_POLSEL instance number starting from 0.
uint32_t CACHE64_GetInstanceByAddr ( uint32_t  address)

param address The physical memory address.

Returns
CACHE64_CTRL instance number starting from 0.
status_t CACHE64_Init ( CACHE64_POLSEL_Type *  base,
const cache64_config_t config 
)

This function configures the CACHE64 module with user-defined settings. Call the CACHE64_GetDefaultConfig() function to configure the configuration structure and get the default configuration.

Parameters
baseCACHE64_POLSEL peripheral base address.
configPointer to a user-defined configuration structure.
Return values
kStatus_SuccessCACHE64 initialize succeed
void CACHE64_GetDefaultConfig ( cache64_config_t config)

This function initializes the CACHE64 configuration structure to a default value. The default values are first region covers whole cacheable area, and policy set to write back.

Parameters
configPointer to a configuration structure.
void CACHE64_EnableCache ( CACHE64_CTRL_Type *  base)
Parameters
baseCACHE64_CTRL peripheral base address.
void CACHE64_DisableCache ( CACHE64_CTRL_Type *  base)
Parameters
baseCACHE64_CTRL peripheral base address.
void CACHE64_InvalidateCache ( CACHE64_CTRL_Type *  base)
Parameters
baseCACHE64_CTRL peripheral base address.
void CACHE64_InvalidateCacheByRange ( uint32_t  address,
uint32_t  size_byte 
)
Parameters
addressThe physical address of cache.
size_bytesize of the memory to be invalidated, should be larger than 0.
Note
Address and size should be aligned to "CACHE64_LINESIZE_BYTE". The startAddr here will be forced to align to CACHE64_LINESIZE_BYTE if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
void CACHE64_CleanCache ( CACHE64_CTRL_Type *  base)
Parameters
baseCACHE64_CTRL peripheral base address.
void CACHE64_CleanCacheByRange ( uint32_t  address,
uint32_t  size_byte 
)
Parameters
addressThe physical address of cache.
size_bytesize of the memory to be cleaned, should be larger than 0.
Note
Address and size should be aligned to "CACHE64_LINESIZE_BYTE". The startAddr here will be forced to align to CACHE64_LINESIZE_BYTE if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
void CACHE64_CleanInvalidateCache ( CACHE64_CTRL_Type *  base)
Parameters
baseCACHE64_CTRL peripheral base address.
void CACHE64_CleanInvalidateCacheByRange ( uint32_t  address,
uint32_t  size_byte 
)
Parameters
addressThe physical address of cache.
size_bytesize of the memory to be Cleaned and Invalidated, should be larger than 0.
Note
Address and size should be aligned to "CACHE64_LINESIZE_BYTE". The startAddr here will be forced to align to CACHE64_LINESIZE_BYTE if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
void CACHE64_EnableWriteBuffer ( CACHE64_CTRL_Type *  base,
bool  enable 
)
Parameters
baseCACHE64_CTRL peripheral base address.
enableThe enable or disable flag. true - enable the write buffer. false - disable the write buffer.
static void ICACHE_InvalidateByRange ( uint32_t  address,
uint32_t  size_byte 
)
inlinestatic
Parameters
addressThe physical address.
size_bytesize of the memory to be invalidated, should be larger than 0.
Note
Address and size should be aligned to CACHE64_LINESIZE_BYTE due to the cache operation unit FSL_FEATURE_CACHE64_CTRL_LINESIZE_BYTE. The startAddr here will be forced to align to the cache line size if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
static void DCACHE_InvalidateByRange ( uint32_t  address,
uint32_t  size_byte 
)
inlinestatic
Parameters
addressThe physical address.
size_bytesize of the memory to be invalidated, should be larger than 0.
Note
Address and size should be aligned to CACHE64_LINESIZE_BYTE due to the cache operation unit FSL_FEATURE_CACHE64_CTRL_LINESIZE_BYTE. The startAddr here will be forced to align to the cache line size if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
static void DCACHE_CleanByRange ( uint32_t  address,
uint32_t  size_byte 
)
inlinestatic
Parameters
addressThe physical address.
size_bytesize of the memory to be cleaned, should be larger than 0.
Note
Address and size should be aligned to CACHE64_LINESIZE_BYTE due to the cache operation unit FSL_FEATURE_CACHE64_CTRL_LINESIZE_BYTE. The startAddr here will be forced to align to the cache line size if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
static void DCACHE_CleanInvalidateByRange ( uint32_t  address,
uint32_t  size_byte 
)
inlinestatic
Parameters
addressThe physical address.
size_bytesize of the memory to be Cleaned and Invalidated, should be larger than 0.
Note
Address and size should be aligned to CACHE64_LINESIZE_BYTE due to the cache operation unit FSL_FEATURE_CACHE64_CTRL_LINESIZE_BYTE. The startAddr here will be forced to align to the cache line size if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.